arm: omap4: Fix SDRAM AUTO DETECTION
Commit "8602114 omap: emif: configure emif only when required"
breaks SDRAM_AUTO_DETECTION.
The issue is dmm_init() depends on emif_sizes[](SDRAM Auto detection)
done in do_sdram_init(). The above commit moves dmm_init() above
do_sdram_init() because of which dmm_init() uses uninitialized
emif_sizes[].
So instead of using global emif_sizes[], get sdram details locally
and calculate emif sizes.
Reported-by: Michael Cashwell <mboards@prograde.net>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Commit "8602114 omap: emif: configure emif only when required"
breaks SDRAM_AUTO_DETECTION.
The issue is dmm_init() depends on emif_sizes[](SDRAM Auto detection)
done in do_sdram_init(). The above commit moves dmm_init() above
do_sdram_init() because of which dmm_init() uses uninitialized
emif_sizes[].
So instead of using global emif_sizes[], get sdram details locally
and calculate emif sizes.
Reported-by: Michael Cashwell <mboards@prograde.net>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
OMAP: Fix copy-paste bug that did not enable UART4 clock
V2 fixes line wrap issue of the patch itself.
UART3 was enabled twice instead of UART4.
One more cosmetic change in a comment on EMIF clock.
Signed-off-by: Lubomir Popov <lpopov@mm-sol.com>
Reviewed-by: R Sricharan <r.sricharan@ti.com>
V2 fixes line wrap issue of the patch itself.
UART3 was enabled twice instead of UART4.
One more cosmetic change in a comment on EMIF clock.
Signed-off-by: Lubomir Popov <lpopov@mm-sol.com>
Reviewed-by: R Sricharan <r.sricharan@ti.com>
doc/feature-removal-schedule.txt: Add CONFIG_SYS_(CLOCKS|PADS)_ENABLE_ALL
We shall remove these OMAP4/5-specific options in v2013.07, barring
insufficient progress on the kernel side.
Cc: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
We shall remove these OMAP4/5-specific options in v2013.07, barring
insufficient progress on the kernel side.
Cc: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
ARM: OMAP4/5: Make bootz as the default boot command
So with OMAP added to multi platform kernel,
the uImage no more contains a valid load address.
With the uboot already supporting zImage,
change the default boot command to bootz
instead.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
So with OMAP added to multi platform kernel,
the uImage no more contains a valid load address.
With the uboot already supporting zImage,
change the default boot command to bootz
instead.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
ARM: OMAP4/5: Change the default boot command to work with device tree
Now with kernel moving to all device tree, the default
boot command is changed to pass the device tree blob.
Also, adding the findfdt command to get the dt-blob
based on the board.
Thanks to Tom Rini <trini@ti.com> for suggesting this.
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Now with kernel moving to all device tree, the default
boot command is changed to pass the device tree blob.
Also, adding the findfdt command to get the dt-blob
based on the board.
Thanks to Tom Rini <trini@ti.com> for suggesting this.
Signed-off-by: Sricharan R <r.sricharan@ti.com>
omap5: Allow use of a plain text env file
For production systems it is better to use script images since
they are protected by checksums and carry valuable information
like name and timestamp. Also, you can't validate the content
passed to env import.
But for development, it is easier to use the env import command and
plain text files instead of script-images.
Since both OMAP5evm/uevm boards are used primarily for development,
we allow U-Boot to load env var from a text file in case that an
boot.scr script-image is not present.
The variable uenvcmd (if existent) will be executed (using run) after
uEnv.txt was loaded. If uenvcmd doesn't exist the default boot sequence
will be started.
Inspired by commit: d70f54808dfa83b574e1239c3eccbcf3317343e1
(omap4: allow the use of a plain text env file instead boot scripts)
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
Tested-by: Sricharan R <r.sricharan@ti.com>
For production systems it is better to use script images since
they are protected by checksums and carry valuable information
like name and timestamp. Also, you can't validate the content
passed to env import.
But for development, it is easier to use the env import command and
plain text files instead of script-images.
Since both OMAP5evm/uevm boards are used primarily for development,
we allow U-Boot to load env var from a text file in case that an
boot.scr script-image is not present.
The variable uenvcmd (if existent) will be executed (using run) after
uEnv.txt was loaded. If uenvcmd doesn't exist the default boot sequence
will be started.
Inspired by commit: d70f54808dfa83b574e1239c3eccbcf3317343e1
(omap4: allow the use of a plain text env file instead boot scripts)
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
Tested-by: Sricharan R <r.sricharan@ti.com>
ARM: OMAP5: Set fdt_high to enable booting with Device tree
While booting with dt blob, if fdt_high is not set to
0xffffffff, the dt blob gets relocated to a high ram address,
which the kernel is not able to use without HIGHMEM.
So set it to 0xffffffff to avoid the issue.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
While booting with dt blob, if fdt_high is not set to
0xffffffff, the dt blob gets relocated to a high ram address,
which the kernel is not able to use without HIGHMEM.
So set it to 0xffffffff to avoid the issue.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
ARM: OMAP5: Rename omap5_evm to omap5_uevm
The omap5-uevm is the reference board name for OMAP5 soc
based platform. So rename it accordingly.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
The omap5-uevm is the reference board name for OMAP5 soc
based platform. So rename it accordingly.
Acked-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Sricharan R <r.sricharan@ti.com>
Tested-by: Nishanth Menon <nm@ti.com>
omap2420-h4: Fix get_timer() and CONFIG_SYS_HZ
The function get_timer() should return time in ms and CONFIG_SYS_HZ
should be set to 1000 by default. Fix both of these items.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The function get_timer() should return time in ms and CONFIG_SYS_HZ
should be set to 1000 by default. Fix both of these items.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap2420-h4: Add device tree support
Enable device-tree support for the omap2420-h4 board.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
Enable device-tree support for the omap2420-h4 board.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap2420-h4: Fix booting from NOR flash
The omap2420-h4 board is using a RAM based address as the linker
location for code. This is causing several problems when attempting
to run the latest u-boot code base on this board from flash. Update
the default linker location for code to be in NOR flash. Please note
that OMAP maps the NOR flash to address 0x08000000 by default and so
use this as the default address for the NOR flash.
Also remove legacy code that attempts to calculate where in flash the
sdata structure, that holds the memory interface configuration data,
is located. By changing the default linker location for code to flash
this is no longer necessary.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The omap2420-h4 board is using a RAM based address as the linker
location for code. This is causing several problems when attempting
to run the latest u-boot code base on this board from flash. Update
the default linker location for code to be in NOR flash. Please note
that OMAP maps the NOR flash to address 0x08000000 by default and so
use this as the default address for the NOR flash.
Also remove legacy code that attempts to calculate where in flash the
sdata structure, that holds the memory interface configuration data,
is located. By changing the default linker location for code to flash
this is no longer necessary.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
omap2420-h4: Fix DRAM initialisation
The size of the DRAM for the omap2420-h4 board is getting setup in the
dram_init() function. However, for the current u-boot release this is
too late and needs to be done in dram_init_banksize(). Therefore, add
a dram_init_banksize() function for the omap2420-h4 board and setup the
DRAM size there.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
The size of the DRAM for the omap2420-h4 board is getting setup in the
dram_init() function. However, for the current u-boot release this is
too late and needs to be done in dram_init_banksize(). Therefore, add
a dram_init_banksize() function for the omap2420-h4 board and setup the
DRAM size there.
Signed-off-by: Jon Hunter <jon-hunter@ti.com>
tricorder: enable hw assisted BCH8 in SPL and u-boot
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Thomas Weber <weber@corscience.de>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Thomas Weber <weber@corscience.de>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
omap_gpmc: add support for hw assisted BCH8
The kernel states:
---8<---
The OMAP3 GPMC hardware BCH engine computes remainder polynomials, it does not
provide automatic error location and correction: this step is implemented using
the BCH library.
--->8---
And we do so in u-boot.
This implementation uses the same layout for BCH8 but it is fix. The current
provided layout does only work with 64 Byte OOB.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Cc: Mansoor Ahamed <mansoor.ahamed@ti.com>
Cc: Thomas Weber <thomas.weber.linux@googlemail.com>
The kernel states:
---8<---
The OMAP3 GPMC hardware BCH engine computes remainder polynomials, it does not
provide automatic error location and correction: this step is implemented using
the BCH library.
--->8---
And we do so in u-boot.
This implementation uses the same layout for BCH8 but it is fix. The current
provided layout does only work with 64 Byte OOB.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Cc: Mansoor Ahamed <mansoor.ahamed@ti.com>
Cc: Thomas Weber <thomas.weber.linux@googlemail.com>
omap_gpmc: change nandecc command
With uppcoming BCH support on OMAP devices we need to decide between differnt
algorithms when switching the ECC engine. Currently we support 1-bit hammign
and 8-bit BCH on HW backend.
In order to switch between differnet ECC algorithms we need to change the
interface of omap_nand_switch_ecc() also.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Thomas Weber <thomas.weber.linux@googlemail.com>
With uppcoming BCH support on OMAP devices we need to decide between differnt
algorithms when switching the ECC engine. Currently we support 1-bit hammign
and 8-bit BCH on HW backend.
In order to switch between differnet ECC algorithms we need to change the
interface of omap_nand_switch_ecc() also.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Thomas Weber <thomas.weber.linux@googlemail.com>
omap3/omap_gpmc.h: add ooblayout for BCH8 as in kernel
This patch adds BCH8 ooblayout for NAND as provided by
0e618ef0a6a33cf7ef96c2c824402088dd8ef48c in linux kernel. This Layout is
currently only provided for 64 byte OOB.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Reviewed-by: Tom Rini <trini@ti.com>
This patch adds BCH8 ooblayout for NAND as provided by
0e618ef0a6a33cf7ef96c2c824402088dd8ef48c in linux kernel. This Layout is
currently only provided for 64 byte OOB.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Reviewed-by: Tom Rini <trini@ti.com>
asm/omap_gpmc.h: consolidate common defines
arch/arm/include/asm/arch-am33xx/omap_gpmc.h and
arch/arm/include/asm/arch-omap3/omap_gpmc.h are almost the same, consolidate
the common parts into a new header.
Introduce a new asm/omap_gpmc.h which defines the command part and pulls in
the architecture specific one.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Reviewed-by: Tom Rini <trini@ti.com>
arch/arm/include/asm/arch-am33xx/omap_gpmc.h and
arch/arm/include/asm/arch-omap3/omap_gpmc.h are almost the same, consolidate
the common parts into a new header.
Introduce a new asm/omap_gpmc.h which defines the command part and pulls in
the architecture specific one.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Reviewed-by: Tom Rini <trini@ti.com>
omap3/cpu.h: add BCH support
This patch adds the BCH result registers to register mapping for OMAP3 gpmc.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Reviewed-by: Tom Rini <trini@ti.com>
This patch adds the BCH result registers to register mapping for OMAP3 gpmc.
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Cc: Tom Rini <trini@ti.com>
Cc: Ilya Yanok <ilya.yanok@cogentembedded.com>
Cc: Scott Wood <scottwood@freescale.com>
Reviewed-by: Tom Rini <trini@ti.com>
omap3_beagle: Flush UART3 xmit on enable if TEMT is broken
Flush UART3 xmit on enable if TEMT is broken
On some OMAP3 devices when UART3 is configured for boot mode before SPL starts
only THRE bit is set. We have to empty the transmitter before initialization
starts. This patch avoids the use of CONFIG_SYS_NS16550_BROKEN_TEMT.
Signed-off-by: Manfred Huber <man.huber@arcor.de>
Tested-by: Javier Martinez Canillas <javier@dowhile0.org>
Tested-by: Andreas Bießmann <andreas.devel@googlemail.com>
Flush UART3 xmit on enable if TEMT is broken
On some OMAP3 devices when UART3 is configured for boot mode before SPL starts
only THRE bit is set. We have to empty the transmitter before initialization
starts. This patch avoids the use of CONFIG_SYS_NS16550_BROKEN_TEMT.
Signed-off-by: Manfred Huber <man.huber@arcor.de>
Tested-by: Javier Martinez Canillas <javier@dowhile0.org>
Tested-by: Andreas Bießmann <andreas.devel@googlemail.com>
am335x: Enable MMC1 clock
We must not assume ROM has enabled the clock for MMC1.
Reported-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Peter Korsgaard <jacmet@sunsite.dk>
We must not assume ROM has enabled the clock for MMC1.
Reported-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Peter Korsgaard <jacmet@sunsite.dk>
pcm051: Enable DDR PHY dynamic power down bit
This is done already for am335x in
59dcf970d11ebff5d9f4bbbde79fda584e9e7ad4 and also applies for pcm051.
It powers down the IO receiver when not performing read which helps
reducing the overall power consuption in low power states
(suspend/standby).
Signed-off-by: Lars Poeschel <poeschel@lemonage.de>
This is done already for am335x in
59dcf970d11ebff5d9f4bbbde79fda584e9e7ad4 and also applies for pcm051.
It powers down the IO receiver when not performing read which helps
reducing the overall power consuption in low power states
(suspend/standby).
Signed-off-by: Lars Poeschel <poeschel@lemonage.de>
musb: set MUSB speed based on CONFIG
Do not config MUSB to highspeed mode if CONFIG_USB_GADGET_DUALSPEED
is not set, in which case Ether gadget only operates in fullspeed.
Reviewed-by: Tom Rini <trini@ti.com>
Signed-off-by: Bin Liu <b-liu@ti.com>
Do not config MUSB to highspeed mode if CONFIG_USB_GADGET_DUALSPEED
is not set, in which case Ether gadget only operates in fullspeed.
Reviewed-by: Tom Rini <trini@ti.com>
Signed-off-by: Bin Liu <b-liu@ti.com>
musb: am335x: disable bulk split-combine feature
On TI AM335x devices, MUSB has bulk split/combine feature enabled
in the ConfigData register, but the current MUSB driver does not
support it yet. Therefore, disable the feature for now, until the
driver adds the support.
One usecase which is broken because of this feature is that Ether
gadget stops working in Fullspeed mode (by un-defining
CONFIG_USB_GADGET_DUALSPEED)
After desabled this feature, MUSB driver send packets in proper size
(no more than 64 bytes) in Fullspeed mode.
This has been validated with Ether gadget in Fullspeed mode on AM335x
EVM.
Signed-off-by: Bin Liu <b-liu@ti.com>
On TI AM335x devices, MUSB has bulk split/combine feature enabled
in the ConfigData register, but the current MUSB driver does not
support it yet. Therefore, disable the feature for now, until the
driver adds the support.
One usecase which is broken because of this feature is that Ether
gadget stops working in Fullspeed mode (by un-defining
CONFIG_USB_GADGET_DUALSPEED)
After desabled this feature, MUSB driver send packets in proper size
(no more than 64 bytes) in Fullspeed mode.
This has been validated with Ether gadget in Fullspeed mode on AM335x
EVM.
Signed-off-by: Bin Liu <b-liu@ti.com>
logo: update to the new logo for ATMEL
Atmel change to new logo since 2012. This patch update the logo to new one.
Signed-off-by: Josh Wu <josh.wu@atmel.com>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Atmel change to new logo since 2012. This patch update the logo to new one.
Signed-off-by: Josh Wu <josh.wu@atmel.com>
Signed-off-by: Andreas Bießmann <andreas.devel@googlemail.com>
Merge branch 'u-boot-samsung/master' into 'u-boot-arm/master'
exynos: change indentation of defines in cpu.h
Fix the indentation of some defines by tab.
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Fix the indentation of some defines by tab.
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Merge branch 'u-boot-imx/master' into 'u-boot-arm/master'
spi: mxc_spi: Fix ECSPI reset handling
Reviewing the ECSPI reset handling shows two issues:
1. For the enable/reset bit (MXC_CSPICTRL_EN) in the control reg
(ECSPIx_CONGREG) the i.MX6 technical reference manual states:
-- cut --
ECSPIx_CONREG[0]: EN: Writing zero to this bit disables the block
and resets the internal logic with the exception of the ECSPI_CONREG.
-- cut --
Note the exception mentioned: The CONREG itself isn't reset.
Fix this by manually writing the reset value 0 to the whole register.
This sets the EN bit to zero, too (i.e. includes the old
~MXC_CSPICTRL_EN).
2. We want to reset the whole SPI block here. So it makes no sense
to first read the old value of the CONREG and write it back, later.
This will give us the old (historic/random) value of the CONREG back.
And doesn't reset the CONREG.
To get a clean CONREG after the reset of the block, too, don't use
the old (historic/random) value of the CONREG while doing the reset.
And read the clean CONREG after the reset.
This was found while working on a SPI boot device where the i.MX6 boot
ROM has already initialized the SPI block. The initialization by the
boot ROM might be different to what the U-Boot driver wants to configure.
I.e. we need a clean reset of SPI block, including the CONREG.
Signed-off-by: Dirk Behme <dirk.behme@de.bosch.com>
CC: Stefano Babic <sbabic@denx.de>
CC: Fabio Estevam <fabio.estevam@freescale.com>
Reviewing the ECSPI reset handling shows two issues:
1. For the enable/reset bit (MXC_CSPICTRL_EN) in the control reg
(ECSPIx_CONGREG) the i.MX6 technical reference manual states:
-- cut --
ECSPIx_CONREG[0]: EN: Writing zero to this bit disables the block
and resets the internal logic with the exception of the ECSPI_CONREG.
-- cut --
Note the exception mentioned: The CONREG itself isn't reset.
Fix this by manually writing the reset value 0 to the whole register.
This sets the EN bit to zero, too (i.e. includes the old
~MXC_CSPICTRL_EN).
2. We want to reset the whole SPI block here. So it makes no sense
to first read the old value of the CONREG and write it back, later.
This will give us the old (historic/random) value of the CONREG back.
And doesn't reset the CONREG.
To get a clean CONREG after the reset of the block, too, don't use
the old (historic/random) value of the CONREG while doing the reset.
And read the clean CONREG after the reset.
This was found while working on a SPI boot device where the i.MX6 boot
ROM has already initialized the SPI block. The initialization by the
boot ROM might be different to what the U-Boot driver wants to configure.
I.e. we need a clean reset of SPI block, including the CONREG.
Signed-off-by: Dirk Behme <dirk.behme@de.bosch.com>
CC: Stefano Babic <sbabic@denx.de>
CC: Fabio Estevam <fabio.estevam@freescale.com>
ARM: bcm2835: fix get_timer() to return ms
Apparently, CONFIG_SYS_HZ must be 1000. Change this, and fix the timer
driver to conform to this.
Have the timer implementation export a custom API get_timer_us() for use
by the BCM2835 MMC API, which needs us resolution for a HW workaround.
Signed-off-by: Stephen Warren <swarren@wwwdotorg.org>
Apparently, CONFIG_SYS_HZ must be 1000. Change this, and fix the timer
driver to conform to this.
Have the timer implementation export a custom API get_timer_us() for use
by the BCM2835 MMC API, which needs us resolution for a HW workaround.
Signed-off-by: Stephen Warren <swarren@wwwdotorg.org>
i.MX6: mx6qsabrelite: README: don't pass chip-select to sf probe command
board/freescale/mx6qsabrelite/README explain a procedure to
update the SPI-NOR on the SabreLite board without Freescale
manufacturing tool but following this procedure leads to both
"sf erase" and "sf write" failing on a mx6qsabrelite board:
MX6QSABRELITE U-Boot > sf probe 1
MX6QSABRELITE U-Boot > sf erase 0 0x40000
SPI flash erase failed
MX6QSABRELITE U-Boot > sf write 0x10800000 0 0x40000
SPI flash write failed
This is because the chip-select 1 is wrong and the correct
value is 0x7300.
Since commit c1173bd0 ("sf command: allow default bus and chip selects")
the chip-select and bus arguments for the sf probe command are optional
so let's just remove it and use "sf probe" instead.
Signed-off-by: Javier Martinez Canillas <javier.martinez@collabora.co.uk>
board/freescale/mx6qsabrelite/README explain a procedure to
update the SPI-NOR on the SabreLite board without Freescale
manufacturing tool but following this procedure leads to both
"sf erase" and "sf write" failing on a mx6qsabrelite board:
MX6QSABRELITE U-Boot > sf probe 1
MX6QSABRELITE U-Boot > sf erase 0 0x40000
SPI flash erase failed
MX6QSABRELITE U-Boot > sf write 0x10800000 0 0x40000
SPI flash write failed
This is because the chip-select 1 is wrong and the correct
value is 0x7300.
Since commit c1173bd0 ("sf command: allow default bus and chip selects")
the chip-select and bus arguments for the sf probe command are optional
so let's just remove it and use "sf probe" instead.
Signed-off-by: Javier Martinez Canillas <javier.martinez@collabora.co.uk>
wandboard: Remove CONFIG_SYS_FSL_USDHC_NUM
CONFIG_SYS_FSL_USDHC_NUM is not used for wandboard.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Otavio Salvador <otavio@ossystems.com.br>
CONFIG_SYS_FSL_USDHC_NUM is not used for wandboard.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Otavio Salvador <otavio@ossystems.com.br>
mx6qsabrelite: Remove duplicate 'mmc dev'
No need to call 'mmc dev' twice.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Otavio Salvador <otavio@ossystems.com.br>
No need to call 'mmc dev' twice.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Otavio Salvador <otavio@ossystems.com.br>
wandboard: Remove duplicate 'mmc dev'
No need to call 'mmc dev' twice.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Otavio Salvador <otavio@ossystems.com.br>
No need to call 'mmc dev' twice.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Otavio Salvador <otavio@ossystems.com.br>
mx6: Fix get_board_rev() for the mx6 solo case
When booting a Freescale kernel 3.0.35 on a Wandboard solo, the get_board_rev()
returns 0x62xxx, which is not a value understood by the VPU
(Video Processing Unit) library in the kernel and causes the video playback to
fail.
The expected values for get_board_rev are:
0x63xxx: For mx6quad/dual
0x61xxx: For mx6dual-lite/solo
So adjust get_board_rev() accordingly and make it as weak function, so that we
do not need to define it in every mx6 board file.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Dirk Behme <dirk.behme@de.bosch.com>
Acked-by: Eric Nelson <eric.nelson@boundarydevices.com>
When booting a Freescale kernel 3.0.35 on a Wandboard solo, the get_board_rev()
returns 0x62xxx, which is not a value understood by the VPU
(Video Processing Unit) library in the kernel and causes the video playback to
fail.
The expected values for get_board_rev are:
0x63xxx: For mx6quad/dual
0x61xxx: For mx6dual-lite/solo
So adjust get_board_rev() accordingly and make it as weak function, so that we
do not need to define it in every mx6 board file.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Acked-by: Dirk Behme <dirk.behme@de.bosch.com>
Acked-by: Eric Nelson <eric.nelson@boundarydevices.com>
mx23_olinuxino: Fix netboot console
The netargs variable was referencing the non-existing variable
console_mainline. Change that to console variable instead.
Signed-off-by: Alexandre Pereira da Silva <aletes.xgr@gmail.com>
Acked-by: Otavio Salvador <otavio@ossystems.com.br>
The netargs variable was referencing the non-existing variable
console_mainline. Change that to console variable instead.
Signed-off-by: Alexandre Pereira da Silva <aletes.xgr@gmail.com>
Acked-by: Otavio Salvador <otavio@ossystems.com.br>
mmc: i.MX6: fsl_esdhc: Define maximum bus width supported by a board
Maximum bus width supported by some i.MX6 boards is not 8bit like
others. In case where both host controller and card support 8bit transfers,
they agree to communicate on 8bit interface while some boards support only 4bit interface.
Due to this reason the mmc 8bit default mode fails on these boards. To rectify this,
define maximum bus width supported by these boards (4bit). If max_bus_width is not
defined, it is 0 by default and 8bit width support will be enabled in host
capabilities otherwise host capabilities are modified accordingly.
It is tested with a MMCplus card.
Signed-off-by: Abbas Raza <Abbas_Raza@mentor.com>
cc: stefano Babic <sbabic@denx.de>
cc: Andy Fleming <afleming@gmail.com>
Acked-by: Dirk Behme <dirk.behme@de.bosch.com>
Acked-by: Andrew Gabbasov <andrew_gabbasov@mentor.com>
Maximum bus width supported by some i.MX6 boards is not 8bit like
others. In case where both host controller and card support 8bit transfers,
they agree to communicate on 8bit interface while some boards support only 4bit interface.
Due to this reason the mmc 8bit default mode fails on these boards. To rectify this,
define maximum bus width supported by these boards (4bit). If max_bus_width is not
defined, it is 0 by default and 8bit width support will be enabled in host
capabilities otherwise host capabilities are modified accordingly.
It is tested with a MMCplus card.
Signed-off-by: Abbas Raza <Abbas_Raza@mentor.com>
cc: stefano Babic <sbabic@denx.de>
cc: Andy Fleming <afleming@gmail.com>
Acked-by: Dirk Behme <dirk.behme@de.bosch.com>
Acked-by: Andrew Gabbasov <andrew_gabbasov@mentor.com>
mx23_olinuxino: Change definitions to use spaces instead of tabs
Change all "#define/ifdef<TAB>" sequences into "#define/ifdef<SPACE>".
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Change all "#define/ifdef<TAB>" sequences into "#define/ifdef<SPACE>".
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
mx25pdk: Enable imxdi RTC
The mx25pdk board supports the i.MX25 DryIce RTC (imxdi), so enable it. This
allows to compile-test the imxdi driver in the mainline tree.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Fabio Estevam <fabio.estevam@freescale.com>
The mx25pdk board supports the i.MX25 DryIce RTC (imxdi), so enable it. This
allows to compile-test the imxdi driver in the mainline tree.
Signed-off-by: Benoît Thébaudeau <benoit.thebaudeau@advansee.com>
Acked-by: Fabio Estevam <fabio.estevam@freescale.com>
mx6qsabrelite: README: No need to pass 'u-boot.imx'
The u-boot.imx binary is generated by default, so no need to pass it in the
'make' line.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
The u-boot.imx binary is generated by default, so no need to pass it in the
'make' line.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
mx28evk: Introduce a new target for saving env vars to NAND
Introduce 'mx28evk_nand' target for saving environment variables into NAND.
The mx28evk board does not come with a NAND flash populated from the
factory. It comes with an empty slot (U23), which allows the insertion of a
48-pin TSOP flash device.
Tested with a K9LBG08U0D.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Reviewed-by: Otavio Salvador <otavio@ossystems.com.br>
Introduce 'mx28evk_nand' target for saving environment variables into NAND.
The mx28evk board does not come with a NAND flash populated from the
factory. It comes with an empty slot (U23), which allows the insertion of a
48-pin TSOP flash device.
Tested with a K9LBG08U0D.
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Reviewed-by: Otavio Salvador <otavio@ossystems.com.br>
mx6qsabre{sd,auto}: Add boot mode select
Adds support for 'bmode' command which let user to choose where to
boot from; this allows U-Boot to load system from another storage
without messing with jumpers.
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Adds support for 'bmode' command which let user to choose where to
boot from; this allows U-Boot to load system from another storage
without messing with jumpers.
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
mx6qsabresd: Fix card detection for invalid card id case
This changes the code so in case an unkown value is passed it will
return as invalid.
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
This changes the code so in case an unkown value is passed it will
return as invalid.
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
mx6qsabresd: Document the mapping of USDHC[2-4]
This documents the SD card identifier so it is easier for user to spot
which card number will be used, if need.
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
This documents the SD card identifier so it is easier for user to spot
which card number will be used, if need.
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
Exynos: pwm: Remove dead code of function exynos5_get_pwm_clk
As we shall now be using clock_get_periph_rate function.
We find no reason for keeping code in function exynos5_get_pwm_clk.
Hence, removing it.
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
As we shall now be using clock_get_periph_rate function.
We find no reason for keeping code in function exynos5_get_pwm_clk.
Hence, removing it.
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: pwm: Use generic api to get pwm clk freq
Use generic api to get the pwm clock frequency
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Padmavathi Venna <padma.v@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Use generic api to get the pwm clock frequency
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Padmavathi Venna <padma.v@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: clock: Correct pwm source clk selection
MPLL is selected as the source clk of pwm by default
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Padmavathi Venna <padma.v@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
MPLL is selected as the source clk of pwm by default
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Padmavathi Venna <padma.v@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: clock: Add generic api to get the clk freq
Add generic api to get the frequency of the required peripherial. This
API gets the source clock frequency and returns the required frequency
by dividing with first and second dividers based on the requirement.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Padmavathi Venna <padma.v@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add generic api to get the frequency of the required peripherial. This
API gets the source clock frequency and returns the required frequency
by dividing with first and second dividers based on the requirement.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Padmavathi Venna <padma.v@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: Add peripherial id for pwm
Add peripherial id for pwm inorder to support
generic api to get the clk frequency
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Padmavathi Venna <padma.v@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add peripherial id for pwm inorder to support
generic api to get the clk frequency
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Padmavathi Venna <padma.v@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: Tidy up the pwm_config function in the exynos pwm driver
Some small fixes in the exynos pwm driver:
1. NS_IN_HZ is non-sensical since these are not compatible units. This
constant actually describes the number of nanoseconds in a second. Renamed it
to NS_IN_SEC. Also dropped the unnecessary parenthesis.
2. The variable "period" is not used to hold a period, it's used to hold a
frequency. Renamed it to "frequency".
3. tcmp is an unsigned value, so (tcmp < 0) will never be true and the if
which checks that condition will never execute. Also, there should be no
problem if the pwm never switches, so there's no reason to subtract one from
tcmp and therefore no reason to compare it against zero. Removed both ifs. If
they weren't removed, tcmp should be a signed value.
4. Add a check for a 0 period.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Gabe Black <gabeblack@google.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Some small fixes in the exynos pwm driver:
1. NS_IN_HZ is non-sensical since these are not compatible units. This
constant actually describes the number of nanoseconds in a second. Renamed it
to NS_IN_SEC. Also dropped the unnecessary parenthesis.
2. The variable "period" is not used to hold a period, it's used to hold a
frequency. Renamed it to "frequency".
3. tcmp is an unsigned value, so (tcmp < 0) will never be true and the if
which checks that condition will never execute. Also, there should be no
problem if the pwm never switches, so there's no reason to subtract one from
tcmp and therefore no reason to compare it against zero. Removed both ifs. If
they weren't removed, tcmp should be a signed value.
4. Add a check for a 0 period.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Gabe Black <gabeblack@google.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: Avoid a divide by zero by specifying a non-zero period for pwm 4
The pwm_config function in the exynos pwm driver divides by its period
period parameter. A function was calling pwm_config with a 0ns period and a
0ns duty cycle. That doesn't actually make any sense physically, and results
in a divide by zero in the driver. This change changes the parameters to be a
100000ns period and duty cycle.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Gabe Black <gabeblack@google.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
The pwm_config function in the exynos pwm driver divides by its period
period parameter. A function was calling pwm_config with a 0ns period and a
0ns duty cycle. That doesn't actually make any sense physically, and results
in a divide by zero in the driver. This change changes the parameters to be a
100000ns period and duty cycle.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Gabe Black <gabeblack@google.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: pwm: Fix two bugs in the exynos pwm configuration code
First, the "div" value was being used incorrectly to compute the frequency of
the PWM timer. The value passed in is a constant which reflects the value
that would be found in a configuration register, 0 to 4. That should
correspond to a scaling factor of 1, 2, 4, 8, or 16, 1 << div, but div + 1 was
being used instead.
Second, the reset value of the timers were being calculated to give an overall
frequency, thrown out, and set to a maximum value. This was done so that PWM 4
could be used as the system clock by counting down from a high value, but it
was applied indiscriminantly. It should at most be applied only to PWM 4.
This change also takes the opportunity to tidy up the pwm_init function.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Gabe Black <gabeblack@google.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
First, the "div" value was being used incorrectly to compute the frequency of
the PWM timer. The value passed in is a constant which reflects the value
that would be found in a configuration register, 0 to 4. That should
correspond to a scaling factor of 1, 2, 4, 8, or 16, 1 << div, but div + 1 was
being used instead.
Second, the reset value of the timers were being calculated to give an overall
frequency, thrown out, and set to a maximum value. This was done so that PWM 4
could be used as the system clock by counting down from a high value, but it
was applied indiscriminantly. It should at most be applied only to PWM 4.
This change also takes the opportunity to tidy up the pwm_init function.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Build and boot U-boot with this patch, backlight works properly.
Signed-off-by: Gabe Black <gabeblack@google.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: Add timer_get_us function
timer_get_us returns the time in microseconds since a certain reference
point of history. However, it does not guarantee to return an accurate
time after a long period; instead, it wraps around (that is, the
reference point is reset to some other point of history) after some
periods. The frequency of wrapping around is about an hour (or 2^32
microseconds).
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Signed-off-by: Che-Liang Chiou <clchiou@chromium.org>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
timer_get_us returns the time in microseconds since a certain reference
point of history. However, it does not guarantee to return an accurate
time after a long period; instead, it wraps around (that is, the
reference point is reset to some other point of history) after some
periods. The frequency of wrapping around is about an hour (or 2^32
microseconds).
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Signed-off-by: Che-Liang Chiou <clchiou@chromium.org>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: Change get_timer() to work correctly
At present get_timer() does not return sane values. It should count up
smoothly in milliscond intervals.
We can change the PWM to count down at 1MHz, providing a resolution
of 1us and a range of about an hour between required get_timer() calls.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Signed-off-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
At present get_timer() does not return sane values. It should count up
smoothly in milliscond intervals.
We can change the PWM to count down at 1MHz, providing a resolution
of 1us and a range of about an hour between required get_timer() calls.
Test with command "sf probe 1:0; time sf read 40008000 0 1000".
Try with different numbers of bytes and see that sane values are obtained
Signed-off-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos5: config: enable time command
This patch enables time command.
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
This patch enables time command.
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos5: clock: Fix a typo bug in exynos clock init
We intended to clear the bits of CLK_SRC_TOP2 register, instead we were
writing on the reserved bits of src_core1 register. Since the default
value of clk_src_top2 register were itself zero, this typo was not
creating any big issue. But it is better to fix this error for better
readability of the code.
Signed-off-by: Hatim Ali <hatim.rv@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
We intended to clear the bits of CLK_SRC_TOP2 register, instead we were
writing on the reserved bits of src_core1 register. Since the default
value of clk_src_top2 register were itself zero, this typo was not
creating any big issue. But it is better to fix this error for better
readability of the code.
Signed-off-by: Hatim Ali <hatim.rv@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Exynos: config: Enable hash command
This enables hash command.
Tested with command "hash sha256 0x40008000 0x2B 0x40009000".
Used mm and md to write a standard string to memory location
0x40008000 and ran the above command to verify the output.
Signed-off-by: ARUN MANKUZHI <arun.m@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
This enables hash command.
Tested with command "hash sha256 0x40008000 0x2B 0x40009000".
Used mm and md to write a standard string to memory location
0x40008000 and ran the above command to verify the output.
Signed-off-by: ARUN MANKUZHI <arun.m@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
gen: Add sha h/w acceleration to hash
Adding H/W acceleration support to hash which can be used
to test SHA 256 hash algorithm.
Signed-off-by: ARUN MANKUZHI <arun.m@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Adding H/W acceleration support to hash which can be used
to test SHA 256 hash algorithm.
Signed-off-by: ARUN MANKUZHI <arun.m@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Exynos: config: Enable ACE HW for SHA 256 for Exynos
This enables SHA 256 for exynos.
Signed-off-by: ARUN MANKUZHI <arun.m@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
This enables SHA 256 for exynos.
Signed-off-by: ARUN MANKUZHI <arun.m@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Exynos: Add hardware accelerated SHA256 and SHA1
SHA-256 and SHA-1 accelerated using ACE hardware.
Signed-off-by: ARUN MANKUZHI <arun.m@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
SHA-256 and SHA-1 accelerated using ACE hardware.
Signed-off-by: ARUN MANKUZHI <arun.m@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Exynos: clock: Fix a bug in PLL lock check condition
The condition for testing of PLL getting locked was incorrect. Rectify
this error in this patch.
Reported-by: Alexei Fedorov <alexie.fedorov@arm.com>
Signed-off-by: Hatim Ali <hatim.rv@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
The condition for testing of PLL getting locked was incorrect. Rectify
this error in this patch.
Reported-by: Alexei Fedorov <alexie.fedorov@arm.com>
Signed-off-by: Hatim Ali <hatim.rv@samsung.com>
Signed-off-by: Akshay Saraswat <akshay.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
spl:falcon:trats: Fix SPL image size computing.
"spl_imgsize" was set as decimal variable by "setexpr"
and this causes wrong image size written by "ext4write".
Preset this val with "0x" prefix allow to fix this issue.
Signed-off-by: Przemyslaw Marczak <p.marczak@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Cc: Minkyu Kang <mk7.kang@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
"spl_imgsize" was set as decimal variable by "setexpr"
and this causes wrong image size written by "ext4write".
Preset this val with "0x" prefix allow to fix this issue.
Signed-off-by: Przemyslaw Marczak <p.marczak@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Cc: Minkyu Kang <mk7.kang@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
spi: exynos: Fix compiler warnings for non-dt systems
Enclosing process_nodes() and spi_get_config() inside
CONFIG_OF_CONTROL, since they are compiled only for DT systems.
This fixes following warning:
exynos_spi.c:391:12: warning: 'process_nodes' defined but not used [-Wunused-function]
Signed-off-by: Vivek Gautam <gautam.vivek@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Enclosing process_nodes() and spi_get_config() inside
CONFIG_OF_CONTROL, since they are compiled only for DT systems.
This fixes following warning:
exynos_spi.c:391:12: warning: 'process_nodes' defined but not used [-Wunused-function]
Signed-off-by: Vivek Gautam <gautam.vivek@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
SMDK5250: Fix compiler warning for non-dt systems
Compiling for non-dt systems gives folowing warning:
smdk5250.c: In function 'board_eth_init':
smdk5250.c:152:6: warning: unused variable 'node' [-Wunused-variable]
Declare variable 'node' only for dt enabled systems to remove this
warning.
Signed-off-by: Vivek Gautam <gautam.vivek@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Compiling for non-dt systems gives folowing warning:
smdk5250.c: In function 'board_eth_init':
smdk5250.c:152:6: warning: unused variable 'node' [-Wunused-variable]
Declare variable 'node' only for dt enabled systems to remove this
warning.
Signed-off-by: Vivek Gautam <gautam.vivek@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Merge branch 'u-boot/master' into 'u-boot-arm/master'
Conflicts:
drivers/spi/tegra20_sflash.c
include/fdtdec.h
lib/fdtdec.c
Conflicts:
drivers/spi/tegra20_sflash.c
include/fdtdec.h
lib/fdtdec.c
armv7: do not relocate _start twice
The _start symbol is already relocated, so do not add the relocation the second
time in c_runtime_cpu_setup.
This fixes e.g. the abort exception handling path, which ended in double fault
due to bad address in VBAR.
Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
Reported-by: Lubomir Popov <lpopov@mm-sol.com>
The _start symbol is already relocated, so do not add the relocation the second
time in c_runtime_cpu_setup.
This fixes e.g. the abort exception handling path, which ended in double fault
due to bad address in VBAR.
Signed-off-by: Vincent Stehlé <v-stehle@ti.com>
Reported-by: Lubomir Popov <lpopov@mm-sol.com>
ARM: mmu: Set domain permissions to client access
The 'XN' execute never bit is set in the pagetables. This will
prevent speculative prefetches to non executable regions. But the
domain permissions are set as master in the DACR register.
So the pagetable attribute for 'XN' is not effective. Change the
permissions to client.
This fixes lot of speculative prefetch aborts seen on OMAP5
secure devices.
Signed-off-by: R Sricharan <r.sricharan@ti.com>
Tested-by: Vincent Stehle <v-stehle@ti.com>
Cc: Vincent Stehle <v-stehle@ti.com>
Cc: Tom Rini <trini@ti.com>
Cc: Albert ARIBAUD <albert.u.boot@aribaud.net>
The 'XN' execute never bit is set in the pagetables. This will
prevent speculative prefetches to non executable regions. But the
domain permissions are set as master in the DACR register.
So the pagetable attribute for 'XN' is not effective. Change the
permissions to client.
This fixes lot of speculative prefetch aborts seen on OMAP5
secure devices.
Signed-off-by: R Sricharan <r.sricharan@ti.com>
Tested-by: Vincent Stehle <v-stehle@ti.com>
Cc: Vincent Stehle <v-stehle@ti.com>
Cc: Tom Rini <trini@ti.com>
Cc: Albert ARIBAUD <albert.u.boot@aribaud.net>
ARM: mmu: Introduce weak dram_bank_setup function
Introduce a weak version of dram_bank_setup function
to allow a platform specific function.
This is used in the subsequent patch to setup dram region
without 'XN' attribute in order to enable the region
under client permissions.
Signed-off-by: R Sricharan <r.sricharan@ti.com>
Cc: Vincent Stehle <v-stehle@ti.com>
Cc: Tom Rini <trini@ti.com>
Cc: Albert ARIBAUD <albert.u.boot@aribaud.net>
Introduce a weak version of dram_bank_setup function
to allow a platform specific function.
This is used in the subsequent patch to setup dram region
without 'XN' attribute in order to enable the region
under client permissions.
Signed-off-by: R Sricharan <r.sricharan@ti.com>
Cc: Vincent Stehle <v-stehle@ti.com>
Cc: Tom Rini <trini@ti.com>
Cc: Albert ARIBAUD <albert.u.boot@aribaud.net>
ARM: cache: declare set_section_dcache
We declare the set_section_dcache function globally in the cache header, for
later use by e.g. machine specific code.
Signed-off-by: Vincent Stehlé <v-stehle <at> ti.com>
Cc: Tom Rini <trini <at> ti.com>
Cc: Albert ARIBAUD <albert.u.boot@aribaud.net>
We declare the set_section_dcache function globally in the cache header, for
later use by e.g. machine specific code.
Signed-off-by: Vincent Stehlé <v-stehle <at> ti.com>
Cc: Tom Rini <trini <at> ti.com>
Cc: Albert ARIBAUD <albert.u.boot@aribaud.net>
apx4devkit: change maintainer
As I am no longer working for Bluegiga I will pass apx4devkit maintenance
to Lauri.
Signed-off-by: Veli-Pekka Peltola <veli-pekka.peltola@iki.fi>
Acked-by: Lauri Hintsala <lauri.hintsala@bluegiga.com>
As I am no longer working for Bluegiga I will pass apx4devkit maintenance
to Lauri.
Signed-off-by: Veli-Pekka Peltola <veli-pekka.peltola@iki.fi>
Acked-by: Lauri Hintsala <lauri.hintsala@bluegiga.com>
image: Add support for Plan 9
Signed-off-by: Steven Stallion <sstallion@gmail.com>
Cc: Tom Rini <trini@ti.com>
Reviewed-by: Tom Rini <trini@ti.com>
Signed-off-by: Steven Stallion <sstallion@gmail.com>
Cc: Tom Rini <trini@ti.com>
Reviewed-by: Tom Rini <trini@ti.com>
cmd_ext4: BREAK and correct ext4write parameter order
The ext4write command was taking the in-memory address and filename path
in reverse order from the rest of the filesystem read and write
commands. This corrects the order to be the same as fatload, etc.
Signed-off-by: Tom Rini <trini@ti.com>
The ext4write command was taking the in-memory address and filename path
in reverse order from the rest of the filesystem read and write
commands. This corrects the order to be the same as fatload, etc.
Signed-off-by: Tom Rini <trini@ti.com>
.checkpatch.conf: ignore udelay->usleep_range warnings
usleep_range() is a Linux facility, ignore it when udelay()
is encountered.
Signed-off-by: Matt Porter <mporter@ti.com>
usleep_range() is a Linux facility, ignore it when udelay()
is encountered.
Signed-off-by: Matt Porter <mporter@ti.com>
checkpatch.pl: Add 'debug' to the list of logFunctions
While the kernel mainly uses pr_debug(...), etc, for debug messages, we
use debug(...). Add this to the list of logFunctions so that they are
correctly checked (and not warned against) for long string literals.
Signed-off-by: Tom Rini <trini@ti.com>
While the kernel mainly uses pr_debug(...), etc, for debug messages, we
use debug(...). Add this to the list of logFunctions so that they are
correctly checked (and not warned against) for long string literals.
Signed-off-by: Tom Rini <trini@ti.com>
env_callback: Mark find_env_callback as static
This is not called outside of env_callback.c so mark static, remove from
<env_callback.h>
Cc: Joe Hershberger <joe.hershberger@ni.com>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Joe Hershberger <joe.hershberger@ni.com>
This is not called outside of env_callback.c so mark static, remove from
<env_callback.h>
Cc: Joe Hershberger <joe.hershberger@ni.com>
Signed-off-by: Tom Rini <trini@ti.com>
Acked-by: Joe Hershberger <joe.hershberger@ni.com>
MAKEALL: allow regex matches for -s option
This allows:
MAKEALL -s tegra
to replace:
MAKEALL -s tegra20 -s tegra30 -s tegra114
The following also works:
MAKEALL -s tegra -s omap
Signed-off-by: Stephen Warren <swarren@nvidia.com>
This allows:
MAKEALL -s tegra
to replace:
MAKEALL -s tegra20 -s tegra30 -s tegra114
The following also works:
MAKEALL -s tegra -s omap
Signed-off-by: Stephen Warren <swarren@nvidia.com>
SMDK5250: Use statically defined structures only in non DT case
Since we have DT support in exynos_fb and exynos_dp drivers now,
we need not define any static structure or platform data related to
display in the board file smdk5250.c.
So, we place the already existing structures inside #ifndef CONFIG_OF_CONTROL block.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Since we have DT support in exynos_fb and exynos_dp drivers now,
we need not define any static structure or platform data related to
display in the board file smdk5250.c.
So, we place the already existing structures inside #ifndef CONFIG_OF_CONTROL block.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
SMDK5250: Add device node for DP
Add DT bindings for DP supporting an eDP panel of size 2560x1600.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add DT bindings for DP supporting an eDP panel of size 2560x1600.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
EXYNOS5: Add device node for DP
Add DT node and bindings documentaion for DP.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add DT node and bindings documentaion for DP.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
video: exynos_dp: Add function to parse DP DT node
Add function to parse the required platform data fron DP DT node
and fill the edp_info structure.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add function to parse the required platform data fron DP DT node
and fill the edp_info structure.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
EXYNOS5: FDT: Add compatible strings for FIMD
Add required compatible information for FIMD.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add required compatible information for FIMD.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
video: exynos_dp: Make dp_regs global
dp_regs variable was redundantly defined across all the functions in
the driver even though it contains just the same address. We make it
global and initialize it once using exynos_dp_set_base_addr().
>From then on, other funtions can use the address stored in the global variable.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
dp_regs variable was redundantly defined across all the functions in
the driver even though it contains just the same address. We make it
global and initialize it once using exynos_dp_set_base_addr().
>From then on, other funtions can use the address stored in the global variable.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
SMDK5250: Add device node for FIMD
Add DT bindings for FIMD supporting an eDP panel of size 2560x1600.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add DT bindings for FIMD supporting an eDP panel of size 2560x1600.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
EXYNOS5: Add device node for FIMD
Add DT node and bindings documentation for FIMD.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add DT node and bindings documentation for FIMD.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
video: exynos_fb: add DT support for FIMD driver
Add function to parse FIMD data from device tree.
The driver still supports non-DT case.
Define panel_info statically in some file if you are not using DT.
If you have defined DT node for FIMD, panel_info will be filled
using the bindings of FIMD DT node.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add function to parse FIMD data from device tree.
The driver still supports non-DT case.
Define panel_info statically in some file if you are not using DT.
If you have defined DT node for FIMD, panel_info will be filled
using the bindings of FIMD DT node.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
EXYNOS: FDT: Add compatible strings for FIMD
Add required compatible information for FIMD.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Add required compatible information for FIMD.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
video: exynos_fb: Make fimd_ctrl global
fimd_ctrl variable was redundantly defined across all the functions in
the driver even though it contains just the same address. We make it
global and initialize it in exynos_fimd_lcd_init. From then on, other
funtions can use the data in the global variable.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
fimd_ctrl variable was redundantly defined across all the functions in
the driver even though it contains just the same address. We make it
global and initialize it in exynos_fimd_lcd_init. From then on, other
funtions can use the data in the global variable.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
video: exynos_dp: Remove callbacks from the driver
Replaced the functionality of callbacks by using a standard set of functions.
Instead of implementing and hooking up a callback, put the same code in one of
the standard set of functions by overriding it.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Replaced the functionality of callbacks by using a standard set of functions.
Instead of implementing and hooking up a callback, put the same code in one of
the standard set of functions by overriding it.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
video: exynos_fb: Remove callbacks from the driver
Replaced the functionality of callbacks by using a standard set of functions.
Instead of implementing and hooking up a callback, put the same code in one of
the standard set of functions by overriding it.
This patch is tested only on SMDK5250.
For Trats and universal_c210 board, it is only compile tested.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Replaced the functionality of callbacks by using a standard set of functions.
Instead of implementing and hooking up a callback, put the same code in one of
the standard set of functions by overriding it.
This patch is tested only on SMDK5250.
For Trats and universal_c210 board, it is only compile tested.
Signed-off-by: Ajay Kumar <ajaykumar.rs@samsung.com>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
EXYNOS5: Add L2 Cache Support.
This patch set adds L2 Cache Support to EXYNOS.
Signed-off-by: Arun Mankuzhi <arun.m@samsung.com>
Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
This patch set adds L2 Cache Support to EXYNOS.
Signed-off-by: Arun Mankuzhi <arun.m@samsung.com>
Signed-off-by: Rajeshwari Shinde <rajeshwari.s@samsung.com>
Acked-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Minkyu Kang <mk7.kang@samsung.com>
Merge branch 'u-boot-tegra/master' into 'u-boot-arm/master'
Merge branch 'u-boot-samsung/master' into 'u-boot-arm/master'
Tegra114: MMC: Enable DT MMC driver support for Tegra114 Dalmore boards
Tested on my Dalmore E1611 board, eMMC and SD-Card work fine, can load
a kernel off of an SD card OK, card detect works, and the env is now
stored in eMMC (end of the 2nd 'boot' sector, same as Tegra20/30).
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Tested on my Dalmore E1611 board, eMMC and SD-Card work fine, can load
a kernel off of an SD card OK, card detect works, and the env is now
stored in eMMC (end of the 2nd 'boot' sector, same as Tegra20/30).
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Tegra114: MMC: Add SD bus power-rail init routine
T114 requires SD bus power-rail bringup for the SDIO card on SDMMC3.
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
T114 requires SD bus power-rail bringup for the SDIO card on SDMMC3.
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Tegra114: Dalmore: Add SDIO3 pad config to pinctrl_config table
SDIO1 (the SD-card slot on Dalmore) needs to have its pads setup
before the MMC driver is added.
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
SDIO1 (the SD-card slot on Dalmore) needs to have its pads setup
before the MMC driver is added.
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Tegra114: fdt: Add SDMMC (sdhci) nodes for T114 boards (Dalmore for now)
Took these values directly from the kernel dts files.
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Took these values directly from the kernel dts files.
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
tegra114: dalmore: config: enable SPI
Turn on SPI in dalmore config file
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Turn on SPI in dalmore config file
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
tegra114: add SPI driver
Add driver for tegra114 SPI controller. This controller is not
compatible with either the tegra20 or tegra30 controllers, so it
requires a new driver.
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Add driver for tegra114 SPI controller. This controller is not
compatible with either the tegra20 or tegra30 controllers, so it
requires a new driver.
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
tegra114: dalmore: fdt: enable dalmore SPI controller
Dalmore has a SPI flash part attached to controller 4, so enable
controller 4 and set to 25MHz.
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Dalmore has a SPI flash part attached to controller 4, so enable
controller 4 and set to 25MHz.
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
tegra114: fdt: add SPI blocks
Add nodes for t114 SPI controller hardware
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Add nodes for t114 SPI controller hardware
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
tegra114: fdt: add apbdma block
Add node for apbdma controller hardware.
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>
Add node for apbdma controller hardware.
Signed-off-by: Allen Martin <amartin@nvidia.com>
Signed-off-by: Tom Warren <twarren@nvidia.com>
Reviewed-by: Stephen Warren <swarren@nvidia.com>