]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/shortlog
glsdk/glsdk-u-boot.git
2012-12-11 Piotr Wilczekdrivers:i2c: Modify I2C driver for Exynos4
2012-12-11 Piotr Wilczekexynos:pinmux: Add pinmux support for i2c
2012-12-11 Piotr Wilczekexynos:cpu: Add Exynos4 I2C spacing
2012-12-11 Piotr Wilczekexynos:clock: Add i2c clock
2012-12-11 Vincent Stehléomap24xx_i2c: Handle OMAP5 like OMAP2,3,4
2012-12-11 Marek Vasutmxs: i2c: Implement algorithm to set up arbitrary i2c...
2012-12-11 Marek Vasutmxs: i2c: Restore speed setting after block reset
2012-12-11 Marek Vasuti2c: mxs: Fix TIMING2 register value
2012-12-11 Marek Vasuti2c: mxs: Use i2c_set_bus_speed() in i2c_init()
2012-12-11 Marek Vasuti2c: mxs: Implement i2c_get/set_bus_speed()
2012-12-11 Marek Vasuti2c: mxs: Abstract out the MXS I2C speed setup
2012-12-11 Marek Vasuti2c: kerneldoc: Add kerneldoc annotations to cmd_i2c.c
2012-12-11 Marek Vasuti2c: Staticize local functions in mxc i2c driver
2012-12-11 Marek Vasuti2c: Use __weak instead of __attribute__((weak, alias))
2012-12-11 Andreas Bießmannsoft_i2c: add necessary includes for AVR32
2012-12-11 Fabio Estevamwoodburn: Set gpio value in gpio_direction_output()
2012-12-11 Fabio Estevammx25pdk: Adapt it for the new PMIC framework
2012-12-11 Lars RasmussonCorrect comment to show the parameters as defined in...
2012-12-11 Minkyu Kanguniversal_c210: check the NULL pointer when get the...
2012-12-11 Rajeshwari... SMDK5250: Enable pmic MAX77686
2012-12-11 Rajeshwari... POWER: MAX77686: Modified as per the latest Implementation
2012-12-10 Nikita Kiryanovcm-t35: enable zero bootdelay check
2012-12-10 Vincent Stehlépower: twl6035: complain on LDO9 error
2012-12-10 Vincent Stehléomap24xx_i2c: Handle wait_for_bb error
2012-12-10 Nikita Kiryanovgpio: add gpio_is_valid() to omap_gpio API
2012-12-10 Thomas WeberOMAP3: Remove unused PHYS_SDRAM_1_SIZE
2012-12-10 Yegor Yefremovam335x: cpsw: make phy address configurable
2012-12-10 Yegor Yefremovam335x: disable internal delay for RGMII mode
2012-12-10 Stefano BabicOMAP3: TAM3517: add macros for reading eeprom
2012-12-10 Stefano BabicOMAP3: fix panel timing on the mt_ventoux board
2012-12-10 Davide Bonfantidavinci: fixed cpu reset
2012-12-10 ajoyOMAP3 SPI : Fixed bugs related to SPI transfer
2012-12-10 Lokesh Vutlaomap: emif: configure emif only when required
2012-12-10 Robert P. J... OMAP: Tweak omap-common/Makefile since reset.S -> reset.c
2012-12-10 Robert P. J... omap4: Add comments on some "#endif"s for readability.
2012-12-10 Robert P. J... omap3: Add a few comments to "#endif"s for readability.
2012-12-10 Peter BaradaPass sdrc timing values through board_sdrc_timings...
2012-12-10 Robert P. J... omap3_beagle.h: Fix comment for true/false return value.
2012-12-10 Ilya Yanokam335x_evm: enable SPL NAND support
2012-12-10 Ilya Yanokam33xx_spl_bch: simple SPL nand loader for AM33XX
2012-12-10 Mansoor Ahamedomap_gpmc: BCH8 support (ELM based)
2012-12-10 Mansoor Ahamedam33xx: add ELM support
2012-12-10 Ilya Yanokam335x_evm: enable NAND support
2012-12-10 Ilya Yanokam33xx: NAND support
2012-12-10 Ilya Yanokam335x_evm: add nand pinmux definition
2012-12-10 Ilya YanokOMAP: include sys_proto.h from boot-common
2012-12-10 Andreas Bießmannomap3/mem.c: remove unused defines
2012-12-10 Minkyu Kanguniversal_c210: fix compiler error and compiler warning
2012-12-10 Minkyu KangMerge branch 'master' of git://git.denx.de/u-boot into...
2012-12-08 Daniel SchwierzeckMIPS: constify address pointer in test_bit()
2012-12-08 Zhi-zhou ZhangMIPS: fix a latent bug on initialize $gp
2012-12-08 Stefano BabicMerge branch 'master' of git://git.denx.de/u-boot into...
2012-12-07 Tom RiniMerge branch 'master' of git://git.denx.de/u-boot-x86
2012-12-07 Łukasz Majewskifs:ext4:write: Initialize cache aligned filename buffer
2012-12-07 Łukasz Majewskifs:ext4:fix: Code refactoring to suppress compiler...
2012-12-07 Łukasz Majewskifs:ext4:write: Store block device descriptor in file...
2012-12-07 Łukasz Majewskifs:ext4:write: Add lldiv and do_div to perform 64-32...
2012-12-07 Luka PerkovChange e-mail address of Luka Perkov
2012-12-07 Joshua Houshserial_pl011: Set RTS during initialization
2012-12-07 Robert P. J... MAINTAINERS: Add a pointer to the custodians page.
2012-12-07 Otavio Salvadormxs: SPL: Generalize memory initialization
2012-12-06 Simon Glassx86: Fix coreboot config to boot on Chromebook
2012-12-06 Gabe Blackx86: Turn on support for EFI's GPT in the coreboot...
2012-12-06 Simon Glassx86: coreboot: Enable video display
2012-12-06 Simon Glassx86: Build vga video code only if CONFIG_VIDEO_VGA...
2012-12-06 Simon Glassx86: Remove video_init() prototype from u-boot-x86.h
2012-12-06 Duncan Laurievideo: Check for valid FB pointer before clearing
2012-12-06 Stefan Reinauerx86: drop unused code in coreboot.c
2012-12-06 Stefan Reinauerx86: Remove coreboot_ from file name
2012-12-06 Vadim Bendeburyx86: Provide a way to throttle port80 accesses
2012-12-06 Vadim Bendeburyx86: Provide tick counter and frequency reference for...
2012-12-06 Duncan Lauriex86: Issue SMI to finalize Coreboot in final stage
2012-12-06 Duncan Lauriex86: Fix MTRR clear to detect which MTRR to use
2012-12-06 Stefan Reinauerx86: Emit port 80 post codes in show_boot_progress()
2012-12-06 Simon Glassx86: fdt: Create basic .dtsi file for coreboot
2012-12-06 Gabe Blackx86: coreboot: Set CONFIG_ARCH_DEVICE_TREE correctly
2012-12-06 Gabe Blackx86: Add support for CONFIG_OF_CONTROL
2012-12-06 Stefan Reinauerx86: Add CONFIG_DELAY_ENVIRONMENT to delay environment...
2012-12-06 Gabe Blackx86: Add back cold- and warm-boot flags
2012-12-06 Gabe Blackx86: Override calculate_relocation_address to use the...
2012-12-06 Gabe Blackx86: Make calculate_relocation_address an overridable...
2012-12-06 Gabe Blackx86: Make the upper bound on relocated symbols closed...
2012-12-06 Gabe Blackx86: Reorder x86's post relocation memory layout
2012-12-06 Gabe Blackx86: Initialise SPI if enabled
2012-12-06 Gabe Blackx86: Implement arch_phys_memset so that it can wipe...
2012-12-06 Gabe BlackIntroduce arch_phys_memset which works like memset...
2012-12-06 Gabe Blackx86: Increase the size of the phys_size_t and phys_addr...
2012-12-06 Duncan Lauriex86: Fix off-by-one error in do_elf_reloc_fixups()
2012-12-06 Duncan Lauriex86: Ignore memory >4GB when parsing Coreboot tables
2012-12-06 Simon Glassx86: Enable CONFIG_CMD_ZBOOT for coreboot
2012-12-06 Simon Glassx86: Fix indirect jmp warning in zimage.c
2012-12-06 Stefan Reinauerx86: Clean up MTRR 7 right before jumping to the kernel
2012-12-06 Graeme Russx86: Import MSR/MTRR code from Linux
2012-12-06 Stefan Reinauerx86: Provide a function to clean up just before booting...
2012-12-06 Stefan Reinauerx86: Add basic cache operations
2012-12-06 Gabe Blackx86: Fill in the dram info using the e820 map on corebo...
2012-12-06 Vadim Bendeburyx86: Add a CBMEM timestamp generated right before the...
2012-12-06 Vadim Bendeburyx86: Enable coreboot timestamp facility support in...
2012-12-06 Vadim Bendeburyx86: Add function to read time stamp counter
2012-12-06 Bill Richardsonx86: gpio: Add additional GPIO banks to the ICH6 driver
next