glsdk/glsdk-u-boot.git
2013-04-08 Lokesh Vutlaarm: omap4: Fix SDRAM AUTO DETECTION
2013-04-08 Lubomir PopovOMAP: Fix copy-paste bug that did not enable UART4...
2013-04-08 Tom Rinidoc/feature-removal-schedule.txt: Add CONFIG_SYS_(CLOCK...
2013-04-08 SRICHARAN RARM: OMAP4/5: Make bootz as the default boot command
2013-04-08 SRICHARAN RARM: OMAP4/5: Change the default boot command to work...
2013-04-08 Nishanth Menonomap5: Allow use of a plain text env file
2013-04-08 SRICHARAN RARM: OMAP5: Set fdt_high to enable booting with Device...
2013-04-08 SRICHARAN RARM: OMAP5: Rename omap5_evm to omap5_uevm
2013-04-08 Hunter, Jonomap2420-h4: Fix get_timer() and CONFIG_SYS_HZ
2013-04-08 Hunter, Jonomap2420-h4: Add device tree support
2013-04-08 Hunter, Jonomap2420-h4: Fix booting from NOR flash
2013-04-08 Hunter, Jonomap2420-h4: Fix DRAM initialisation
2013-04-08 Andreas Bießmanntricorder: enable hw assisted BCH8 in SPL and u-boot
2013-04-08 Andreas Bießmannomap_gpmc: add support for hw assisted BCH8
2013-04-08 Andreas Bießmannomap_gpmc: change nandecc command
2013-04-08 Andreas Bießmannomap3/omap_gpmc.h: add ooblayout for BCH8 as in kernel
2013-04-08 Andreas Bießmannasm/omap_gpmc.h: consolidate common defines
2013-04-08 Andreas Bießmannomap3/cpu.h: add BCH support
2013-04-08 Manfred Huberomap3_beagle: Flush UART3 xmit on enable if TEMT is...
2013-04-08 Tom Riniam335x: Enable MMC1 clock
2013-04-08 Lars Poeschelpcm051: Enable DDR PHY dynamic power down bit
2013-04-08 Bin Liumusb: set MUSB speed based on CONFIG
2013-04-08 Bin Liumusb: am335x: disable bulk split-combine feature
2013-04-05 Josh Wulogo: update to the new logo for ATMEL
2013-04-04 Albert ARIBAUDMerge branch 'u-boot-samsung/master' into 'u-boot-arm...
2013-04-04 Minkyu Kangexynos: change indentation of defines in cpu.h
2013-04-04 Albert ARIBAUDMerge branch 'u-boot-imx/master' into 'u-boot-arm/master'
2013-04-04 Dirk Behmespi: mxc_spi: Fix ECSPI reset handling
2013-04-04 Stephen WarrenARM: bcm2835: fix get_timer() to return ms
2013-04-03 Javier Martinez... i.MX6: mx6qsabrelite: README: don't pass chip-select...
2013-04-03 Fabio Estevamwandboard: Remove CONFIG_SYS_FSL_USDHC_NUM
2013-04-03 Fabio Estevammx6qsabrelite: Remove duplicate 'mmc dev'
2013-04-03 Fabio Estevamwandboard: Remove duplicate 'mmc dev'
2013-04-03 Fabio Estevammx6: Fix get_board_rev() for the mx6 solo case
2013-04-03 Alexandre Pereira... mx23_olinuxino: Fix netboot console
2013-04-03 Abbas Razammc: i.MX6: fsl_esdhc: Define maximum bus width support...
2013-04-03 Otavio Salvadormx23_olinuxino: Change definitions to use spaces instea...
2013-04-03 Benoît Thébaudeaumx25pdk: Enable imxdi RTC
2013-04-03 Fabio Estevammx6qsabrelite: README: No need to pass 'u-boot.imx'
2013-04-03 Fabio Estevammx28evk: Introduce a new target for saving env vars...
2013-04-03 Otavio Salvadormx6qsabre{sd,auto}: Add boot mode select
2013-04-03 Otavio Salvadormx6qsabresd: Fix card detection for invalid card id...
2013-04-03 Otavio Salvadormx6qsabresd: Document the mapping of USDHC[2-4]
2013-04-01 Akshay SaraswatExynos: pwm: Remove dead code of function exynos5_get_p...
2013-04-01 Padmavathi... Exynos: pwm: Use generic api to get pwm clk freq
2013-04-01 Padmavathi... Exynos: clock: Correct pwm source clk selection
2013-04-01 Padmavathi... Exynos: clock: Add generic api to get the clk freq
2013-04-01 Padmavathi... Exynos: Add peripherial id for pwm
2013-04-01 Gabe BlackExynos: Tidy up the pwm_config function in the exynos...
2013-04-01 Gabe BlackExynos: Avoid a divide by zero by specifying a non...
2013-04-01 Gabe BlackExynos: pwm: Fix two bugs in the exynos pwm configurati...
2013-04-01 Che-Liang ChiouExynos: Add timer_get_us function
2013-04-01 Simon GlassExynos: Change get_timer() to work correctly
2013-04-01 Akshay SaraswatExynos5: config: enable time command
2013-03-29 Akshay SaraswatExynos5: clock: Fix a typo bug in exynos clock init
2013-03-29 Akshay SaraswatExynos: config: Enable hash command
2013-03-29 Akshay Saraswatgen: Add sha h/w acceleration to hash
2013-03-29 Akshay SaraswatExynos: config: Enable ACE HW for SHA 256 for Exynos
2013-03-29 Akshay SaraswatExynos: Add hardware accelerated SHA256 and SHA1
2013-03-29 Akshay SaraswatExynos: clock: Fix a bug in PLL lock check condition
2013-03-29 Przemyslaw... spl:falcon:trats: Fix SPL image size computing.
2013-03-29 Vivek Gautamspi: exynos: Fix compiler warnings for non-dt systems
2013-03-29 Vivek GautamSMDK5250: Fix compiler warning for non-dt systems
2013-03-28 Albert ARIBAUDMerge branch 'u-boot/master' into 'u-boot-arm/master'
2013-03-28 Vincent Stehléarmv7: do not relocate _start twice
2013-03-28 R SricharanARM: mmu: Set domain permissions to client access
2013-03-28 R SricharanARM: mmu: Introduce weak dram_bank_setup function
2013-03-28 Vincent StehléARM: cache: declare set_section_dcache
2013-03-27 Veli-Pekka... apx4devkit: change maintainer
2013-03-27 Steven Stallionimage: Add support for Plan 9
2013-03-27 Tom Rinicmd_ext4: BREAK and correct ext4write parameter order
2013-03-27 Matt Porter.checkpatch.conf: ignore udelay->usleep_range warnings
2013-03-27 Tom Rinicheckpatch.pl: Add 'debug' to the list of logFunctions
2013-03-27 Tom Rinienv_callback: Mark find_env_callback as static
2013-03-27 Stephen WarrenMAKEALL: allow regex matches for -s option
2013-03-27 Ajay KumarSMDK5250: Use statically defined structures only in...
2013-03-27 Ajay KumarSMDK5250: Add device node for DP
2013-03-27 Ajay KumarEXYNOS5: Add device node for DP
2013-03-27 Ajay Kumarvideo: exynos_dp: Add function to parse DP DT node
2013-03-27 Ajay KumarEXYNOS5: FDT: Add compatible strings for FIMD
2013-03-27 Ajay Kumarvideo: exynos_dp: Make dp_regs global
2013-03-27 Ajay KumarSMDK5250: Add device node for FIMD
2013-03-27 Ajay KumarEXYNOS5: Add device node for FIMD
2013-03-27 Ajay Kumarvideo: exynos_fb: add DT support for FIMD driver
2013-03-27 Ajay KumarEXYNOS: FDT: Add compatible strings for FIMD
2013-03-27 Ajay Kumarvideo: exynos_fb: Make fimd_ctrl global
2013-03-27 Ajay Kumarvideo: exynos_dp: Remove callbacks from the driver
2013-03-27 Ajay Kumarvideo: exynos_fb: Remove callbacks from the driver
2013-03-27 Rajeshwari... EXYNOS5: Add L2 Cache Support.
2013-03-26 Albert ARIBAUDMerge branch 'u-boot-tegra/master' into 'u-boot-arm...
2013-03-26 Albert ARIBAUDMerge branch 'u-boot-samsung/master' into 'u-boot-arm...
2013-03-25 Tom WarrenTegra114: MMC: Enable DT MMC driver support for Tegra11...
2013-03-25 Tom WarrenTegra114: MMC: Add SD bus power-rail init routine
2013-03-25 Tom WarrenTegra114: Dalmore: Add SDIO3 pad config to pinctrl_conf...
2013-03-25 Tom WarrenTegra114: fdt: Add SDMMC (sdhci) nodes for T114 boards...
2013-03-25 Allen Martintegra114: dalmore: config: enable SPI
2013-03-25 Allen Martintegra114: add SPI driver
2013-03-25 Allen Martintegra114: dalmore: fdt: enable dalmore SPI controller
2013-03-25 Allen Martintegra114: fdt: add SPI blocks
2013-03-25 Allen Martintegra114: fdt: add apbdma block
next