02d8f775c1700d49da8356a1268e28e6a70a6db5
[glsdk/gst-plugin-ducati.git] / src / gstducati.c
1 /*
2  * GStreamer
3  * Copyright (c) 2010, Texas Instruments Incorporated
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Lesser General Public
7  * License as published by the Free Software Foundation
8  * version 2.1 of the License.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13  * Lesser General Public License for more details.
14  *
15  * You should have received a copy of the GNU Lesser General Public
16  * License along with this library; if not, write to the Free Software
17  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
18  */
20 #ifdef HAVE_CONFIG_H
21 #  include <config.h>
22 #endif
24 #include "gstducati.h"
25 #include "gstducatih264dec.h"
26 #include "gstducatimpeg4dec.h"
27 #include "gstducatimpeg2dec.h"
28 #include "gstducativc1dec.h"
29 #include "gstducativp6dec.h"
30 #include "gstducativp7dec.h"
31 #include "gstducatirvdec.h"
32 #include "gstducatih264enc.h"
33 #include "gstducatimpeg4enc.h"
35 GST_DEBUG_CATEGORY (gst_ducati_debug);
37 #ifndef GST_DISABLE_GST_DEBUG
38 void
39 gst_ducati_log_extended_error_info (int error)
40 {
41   GST_ERROR ("Error %s%s%s%s%s%s%s%x",
42       XDM_ISFATALERROR (error) ? "[fatal] " : "",
43       XDM_ISUNSUPPORTEDPARAM (error) ? "[unsupported param] " : "",
44       XDM_ISUNSUPPORTEDINPUT (error) ? "[unsupported input] " : "",
45       XDM_ISCORRUPTEDHEADER (error) ? "[corrupted header] " : "",
46       XDM_ISCORRUPTEDDATA (error) ? "[corrupted data] " : "",
47       XDM_ISINSUFFICIENTDATA (error) ? "[insufficient data] " : "",
48       XDM_ISAPPLIEDCONCEALMENT (error) ? "[applied concealment] " : "", error);
49 }
50 #endif
52 static gboolean
53 plugin_init (GstPlugin * plugin)
54 {
55   GST_DEBUG_CATEGORY_INIT (gst_ducati_debug, "ducati", 0, "ducati");
57   /* TODO .. find some way to reasonably detect if the corresponding
58    * codecs are actually available..
59    */
60   return gst_element_register (plugin, "ducatih264dec", GST_RANK_PRIMARY,
61       GST_TYPE_DUCATIH264DEC) &&
62       gst_element_register (plugin, "ducatimpeg4dec", GST_RANK_PRIMARY,
63       GST_TYPE_DUCATIMPEG4DEC) &&
64       gst_element_register (plugin, "ducatimpeg2dec", GST_RANK_PRIMARY,
65       GST_TYPE_DUCATIMPEG2DEC) &&
66       gst_element_register (plugin, "ducativc1dec", GST_RANK_PRIMARY,
67       GST_TYPE_DUCATIVC1DEC) &&
68       gst_element_register (plugin, "ducativp6dec", GST_RANK_PRIMARY,
69       GST_TYPE_DUCATIVP6DEC) &&
70       gst_element_register (plugin, "ducativp7dec", GST_RANK_PRIMARY,
71       GST_TYPE_DUCATIVP7DEC) &&
72       gst_element_register (plugin, "ducatirvdec", GST_RANK_PRIMARY,
73       GST_TYPE_DUCATIRVDEC) &&
74       gst_element_register (plugin, "ducatih264enc", GST_RANK_PRIMARY + 1,
75       GST_TYPE_DUCATIH264ENC) &&
76       gst_element_register (plugin, "ducatimpeg4enc", GST_RANK_PRIMARY + 1,
77       GST_TYPE_DUCATIMPEG4ENC);
78 }
80 /* PACKAGE: this is usually set by autotools depending on some _INIT macro
81  * in configure.ac and then written into and defined in config.h, but we can
82  * just set it ourselves here in case someone doesn't use autotools to
83  * compile this code. GST_PLUGIN_DEFINE needs PACKAGE to be defined.
84  */
85 #ifndef PACKAGE
86 #  define PACKAGE "ducati"
87 #endif
89 GST_PLUGIN_DEFINE (GST_VERSION_MAJOR, GST_VERSION_MINOR, "ducati",
90     "Hardware accellerated codecs for OMAP4",
91     plugin_init, VERSION, "LGPL", "GStreamer", "http://gstreamer.net/")