5cb800b5c9c3ef98cad4e1af95ceef7c6a84fc51
[glsdk/gst-plugin-ducati.git] / src / gstducati.c
1 /*
2  * GStreamer
3  * Copyright (c) 2010, Texas Instruments Incorporated
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Lesser General Public
7  * License as published by the Free Software Foundation
8  * version 2.1 of the License.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13  * Lesser General Public License for more details.
14  *
15  * You should have received a copy of the GNU Lesser General Public
16  * License along with this library; if not, write to the Free Software
17  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
18  */
20 #ifdef HAVE_CONFIG_H
21 #  include <config.h>
22 #endif
24 #include <gst/gst.h>
26 #include "gstducatih264dec.h"
27 #include "gstducatimpeg4dec.h"
28 #include "gstducativc1dec.h"
29 #include "gstducativp6dec.h"
31 GST_DEBUG_CATEGORY (gst_ducati_debug);
33 static gboolean
34 plugin_init (GstPlugin * plugin)
35 {
36   GST_DEBUG_CATEGORY_INIT (gst_ducati_debug, "ducati", 0, "ducati");
38   /* TODO .. find some way to reasonably detect if the corresponding
39    * codecs are actually available..
40    */
41   return gst_element_register (plugin, "ducatih264dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIH264DEC) &&
42       gst_element_register (plugin, "ducatimpeg4dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIMPEG4DEC) &&
43       gst_element_register (plugin, "ducativc1dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIVC1DEC) &&
44       gst_element_register (plugin, "ducativp6dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIVP6DEC);
45 }
47 void *
48 gst_ducati_alloc_1d (gint sz)
49 {
50   MemAllocBlock block = {
51     .pixelFormat = PIXEL_FMT_PAGE,
52     .dim.len = sz,
53   };
54   return MemMgr_Alloc (&block, 1);
55 }
57 void *
58 gst_ducati_alloc_2d (gint width, gint height)
59 {
60   MemAllocBlock block[] = { {
61           .pixelFormat = PIXEL_FMT_8BIT,
62           .dim = {.area = {
63                       .width = width,
64                       .height = height,
65                   }}
66       }, {
67         .pixelFormat = PIXEL_FMT_16BIT,
68         .dim = {.area = {
69                     .width = width,
70                     .height = height / 2,
71                 }}
72       }
73   };
74   return MemMgr_Alloc (block, 2);
75 }
77 XDAS_Int16
78 gst_ducati_get_mem_type (SSPtr paddr)
79 {
80   if ((0x60000000 <= paddr) && (paddr < 0x68000000))
81     return XDM_MEMTYPE_TILED8;
82   if ((0x68000000 <= paddr) && (paddr < 0x70000000))
83     return XDM_MEMTYPE_TILED16;
84   if ((0x70000000 <= paddr) && (paddr < 0x78000000))
85     return XDM_MEMTYPE_TILED32;
86   if ((0x78000000 <= paddr) && (paddr < 0x80000000))
87     return XDM_MEMTYPE_RAW;
88   return -1;
89 }
91 /* PACKAGE: this is usually set by autotools depending on some _INIT macro
92  * in configure.ac and then written into and defined in config.h, but we can
93  * just set it ourselves here in case someone doesn't use autotools to
94  * compile this code. GST_PLUGIN_DEFINE needs PACKAGE to be defined.
95  */
96 #ifndef PACKAGE
97 #  define PACKAGE "ducati"
98 #endif
100 GST_PLUGIN_DEFINE (
101     GST_VERSION_MAJOR,
102     GST_VERSION_MINOR,
103     "ducati",
104     "Hardware accellerated codecs for OMAP4",
105     plugin_init,
106     VERSION,
107     "LGPL",
108     "GStreamer",
109     "http://gstreamer.net/"