rvdec: add RealVideo support
[glsdk/gst-plugin-ducati.git] / src / gstducati.c
1 /*
2  * GStreamer
3  * Copyright (c) 2010, Texas Instruments Incorporated
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Lesser General Public
7  * License as published by the Free Software Foundation
8  * version 2.1 of the License.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13  * Lesser General Public License for more details.
14  *
15  * You should have received a copy of the GNU Lesser General Public
16  * License along with this library; if not, write to the Free Software
17  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
18  */
20 #ifdef HAVE_CONFIG_H
21 #  include <config.h>
22 #endif
24 #include <gst/gst.h>
26 #include "gstducati.h"
27 #include "gstducatih264dec.h"
28 #include "gstducatimpeg4dec.h"
29 #include "gstducatimpeg2dec.h"
30 #include "gstducativc1dec.h"
31 #include "gstducativp6dec.h"
32 #include "gstducativp7dec.h"
33 #include "gstducatirvdec.h"
35 GST_DEBUG_CATEGORY (gst_ducati_debug);
37 static gboolean
38 plugin_init (GstPlugin * plugin)
39 {
40   GST_DEBUG_CATEGORY_INIT (gst_ducati_debug, "ducati", 0, "ducati");
42   /* TODO .. find some way to reasonably detect if the corresponding
43    * codecs are actually available..
44    */
45   return gst_element_register (plugin, "ducatih264dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIH264DEC) &&
46       gst_element_register (plugin, "ducatimpeg4dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIMPEG4DEC) &&
47       gst_element_register (plugin, "ducatimpeg2dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIMPEG2DEC) &&
48       gst_element_register (plugin, "ducativc1dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIVC1DEC) &&
49       gst_element_register (plugin, "ducativp6dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIVP6DEC) &&
50       gst_element_register (plugin, "ducativp7dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIVP7DEC) &&
51       gst_element_register (plugin, "ducatirvdec", GST_RANK_PRIMARY, GST_TYPE_DUCATIRVDEC);
52 }
54 void *
55 gst_ducati_alloc_1d (gint sz)
56 {
57   MemAllocBlock block = {
58     .pixelFormat = PIXEL_FMT_PAGE,
59     .dim.len = sz,
60   };
61   return MemMgr_Alloc (&block, 1);
62 }
64 void *
65 gst_ducati_alloc_2d (gint width, gint height, guint * sz)
66 {
67   MemAllocBlock block[] = { {
68           .pixelFormat = PIXEL_FMT_8BIT,
69           .dim = {.area = {
70                       .width = width,
71                       .height = ALIGN2 (height, 1),
72                   }},
73           .stride = 4096
74       }, {
75         .pixelFormat = PIXEL_FMT_16BIT,
76         .dim = {.area = {
77                     .width = width,
78                     .height = ALIGN2 (height, 1) / 2,
79                 }},
80         .stride = 4096
81       }
82   };
83   if (sz) {
84     *sz = (4096 * ALIGN2 (height, 1) * 3) / 2;
85   }
86   return MemMgr_Alloc (block, 2);
87 }
89 XDAS_Int16
90 gst_ducati_get_mem_type (SSPtr paddr)
91 {
92   if ((0x60000000 <= paddr) && (paddr < 0x68000000))
93     return XDM_MEMTYPE_TILED8;
94   if ((0x68000000 <= paddr) && (paddr < 0x70000000))
95     return XDM_MEMTYPE_TILED16;
96   if ((0x70000000 <= paddr) && (paddr < 0x78000000))
97     return XDM_MEMTYPE_TILED32;
98   if ((0x78000000 <= paddr) && (paddr < 0x80000000))
99     return XDM_MEMTYPE_RAW;
100   return -1;
103 /* PACKAGE: this is usually set by autotools depending on some _INIT macro
104  * in configure.ac and then written into and defined in config.h, but we can
105  * just set it ourselves here in case someone doesn't use autotools to
106  * compile this code. GST_PLUGIN_DEFINE needs PACKAGE to be defined.
107  */
108 #ifndef PACKAGE
109 #  define PACKAGE "ducati"
110 #endif
112 GST_PLUGIN_DEFINE (
113     GST_VERSION_MAJOR,
114     GST_VERSION_MINOR,
115     "ducati",
116     "Hardware accellerated codecs for OMAP4",
117     plugin_init,
118     VERSION,
119     "LGPL",
120     "GStreamer",
121     "http://gstreamer.net/"