mpeg2dec: Fix negotiation issue with playbin
[glsdk/gst-plugin-ducati.git] / src / gstducati.h
1 /*
2  * GStreamer
3  * Copyright (c) 2010, Texas Instruments Incorporated
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Lesser General Public
7  * License as published by the Free Software Foundation
8  * version 2.1 of the License.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13  * Lesser General Public License for more details.
14  *
15  * You should have received a copy of the GNU Lesser General Public
16  * License along with this library; if not, write to the Free Software
17  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
18  */
20 #ifndef __GST_DUCATI_H__
21 #define __GST_DUCATI_H__
23 #include <stdint.h>
24 #include <string.h>
26 #include <libdce.h>
27 #include <xdc/std.h>
28 #include <ti/sdo/ce/Engine.h>
29 #include <ti/sdo/ce/video3/viddec3.h>
31 #include <gst/gst.h>
33 G_BEGIN_DECLS
35 GST_DEBUG_CATEGORY_EXTERN (gst_ducati_debug);
36 #define GST_CAT_DEFAULT gst_ducati_debug
38 /* align x to next highest multiple of 2^n */
39 #define ALIGN2(x,n)   (((x) + ((1 << (n)) - 1)) & ~((1 << (n)) - 1))
41 G_END_DECLS
43 #ifndef GST_DISABLE_GST_DEBUG
44 extern void gst_ducati_set_generic_error_strings (const char * strings[]);
45 extern void gst_ducati_log_extended_error_info (uint32_t error, const char *strings[]);
46 #else
47 #define gst_ducati_log_extended_error_info(f) ((void)0)
48 #endif
50 #endif /* __GST_DUCATI_H__ */