mpeg2dec: Fix negotiation issue with playbin
[glsdk/gst-plugin-ducati.git] / src / gstducatibufferpriv.h
1 /*
2  * GStreamer
3  *
4  * Copyright (C) 2012 Texas Instruments
5  * Copyright (C) 2012 Collabora Ltd
6  *
7  * Authors:
8  *  Alessandro Decina <alessandro.decina@collabora.co.uk>
9  *  Rob Clark <rob.clark@linaro.org>
10  *
11  * This library is free software; you can redistribute it and/or
12  * modify it under the terms of the GNU Lesser General Public
13  * License as published by the Free Software Foundation
14  * version 2.1 of the License.
15  *
16  * This library is distributed in the hope that it will be useful,
17  * but WITHOUT ANY WARRANTY; without even the implied warranty of
18  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
19  * Lesser General Public License for more details.
20  *
21  * You should have received a copy of the GNU Lesser General Public
22  * License along with this library; if not, write to the Free Software
23  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
24  */
26 #ifndef __GSTDUCATIBUFFERPRIV_H__
27 #define __GSTDUCATIBUFFERPRIV_H__
29 #include <stdint.h>
30 #include <gst/gst.h>
32 G_BEGIN_DECLS
34 /**
35  * GstMetaDucatiBufferPriv:
36  *
37  * A structure that enables setting required metadata on a buffer.
38  *
39  * Since: 1.2.?
40  */
41 typedef struct
42 {
43   GstMeta meta;
45   struct omap_bo *bo;
46   gint uv_offset, size;
48 } GstMetaDucatiBufferPriv;
51 /* add the GstMetaDucatiBufferPriv metadata */
52 GstMetaDucatiBufferPriv * gst_ducati_buffer_priv_set (GstBuffer * buf,  struct omap_bo *bo, gint uv_offset, gint size);
53 /* retrieve the GstMetaDucatiBufferPriv metadata */
54 GstMetaDucatiBufferPriv * gst_ducati_buffer_priv_get (GstBuffer * buf);
57 G_END_DECLS
60 #endif /* __GSTDUCATIBUFFERPRIV_H__ */