ducatividdec: detect unsupported codecs when switching from NULL to READY
[glsdk/gst-plugin-ducati.git] / src / gstducatividdec.c
1 /*
2  * GStreamer
3  * Copyright (c) 2010, Texas Instruments Incorporated
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Lesser General Public
7  * License as published by the Free Software Foundation
8  * version 2.1 of the License.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13  * Lesser General Public License for more details.
14  *
15  * You should have received a copy of the GNU Lesser General Public
16  * License along with this library; if not, write to the Free Software
17  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
18  */
20 #ifdef HAVE_CONFIG_H
21 #  include <config.h>
22 #endif
24 #include "gstducatividdec.h"
25 #include "gstducatibufferpriv.h"
27 GST_BOILERPLATE (GstDucatiVidDec, gst_ducati_viddec, GstElement,
28     GST_TYPE_ELEMENT);
30 static GstStaticPadTemplate src_factory = GST_STATIC_PAD_TEMPLATE ("src",
31     GST_PAD_SRC,
32     GST_PAD_ALWAYS,
33     GST_STATIC_CAPS (GST_VIDEO_CAPS_YUV_STRIDED ("NV12", "[ 0, max ]"))
34     );
36 enum
37 {
38   PROP_0,
39   PROP_VERSION,
40 };
42 /* helper functions */
44 static void
45 engine_close (GstDucatiVidDec * self)
46 {
47   if (self->engine) {
48     Engine_close (self->engine);
49     self->engine = NULL;
50   }
52   if (self->params) {
53     dce_free (self->params);
54     self->params = NULL;
55   }
57   if (self->dynParams) {
58     dce_free (self->dynParams);
59     self->dynParams = NULL;
60   }
62   if (self->status) {
63     dce_free (self->status);
64     self->status = NULL;
65   }
67   if (self->inBufs) {
68     dce_free (self->inBufs);
69     self->inBufs = NULL;
70   }
72   if (self->outBufs) {
73     dce_free (self->outBufs);
74     self->outBufs = NULL;
75   }
77   if (self->inArgs) {
78     dce_free (self->inArgs);
79     self->inArgs = NULL;
80   }
82   if (self->outArgs) {
83     dce_free (self->outArgs);
84     self->outArgs = NULL;
85   }
87   if (self->device) {
88     dce_deinit (self->device);
89     self->device = NULL;
90   }
91 }
93 static gboolean
94 engine_open (GstDucatiVidDec * self)
95 {
96   gboolean ret;
97   int ec;
99   if (G_UNLIKELY (self->engine)) {
100     return TRUE;
101   }
103   if (self->device == NULL) {
104     self->device = dce_init ();
105     if (self->device == NULL) {
106       GST_ERROR_OBJECT (self, "dce_init() failed");
107       return FALSE;
108     }
109   }
111   GST_DEBUG_OBJECT (self, "opening engine");
113   self->engine = Engine_open ((String) "ivahd_vidsvr", NULL, &ec);
114   if (G_UNLIKELY (!self->engine)) {
115     GST_ERROR_OBJECT (self, "could not create engine");
116     return FALSE;
117   }
119   ret = GST_DUCATIVIDDEC_GET_CLASS (self)->allocate_params (self,
120       sizeof (IVIDDEC3_Params), sizeof (IVIDDEC3_DynamicParams),
121       sizeof (IVIDDEC3_Status), sizeof (IVIDDEC3_InArgs),
122       sizeof (IVIDDEC3_OutArgs));
124   return ret;
127 static void
128 codec_delete (GstDucatiVidDec * self)
130   if (self->pool) {
131     gst_drm_buffer_pool_destroy (self->pool);
132     self->pool = NULL;
133   }
135   if (self->codec) {
136     VIDDEC3_delete (self->codec);
137     self->codec = NULL;
138   }
140   if (self->input_bo) {
141     omap_bo_del (self->input_bo);
142     self->input_bo = NULL;
143   }
146 static gboolean
147 codec_create (GstDucatiVidDec * self)
149   gint err;
150   const gchar *codec_name;
152   codec_delete (self);
154   if (G_UNLIKELY (!self->engine)) {
155     GST_ERROR_OBJECT (self, "no engine");
156     return FALSE;
157   }
159   /* these need to be set before VIDDEC3_create */
160   self->params->maxWidth = self->width;
161   self->params->maxHeight = self->height;
163   codec_name = GST_DUCATIVIDDEC_GET_CLASS (self)->codec_name;
165   /* create codec: */
166   GST_DEBUG_OBJECT (self, "creating codec: %s", codec_name);
167   self->codec =
168       VIDDEC3_create (self->engine, (String) codec_name, self->params);
170   if (!self->codec) {
171     return FALSE;
172   }
174   err =
175       VIDDEC3_control (self->codec, XDM_SETPARAMS, self->dynParams,
176       self->status);
177   if (err) {
178     GST_ERROR_OBJECT (self, "failed XDM_SETPARAMS");
179     return FALSE;
180   }
182   self->first_in_buffer = TRUE;
183   self->first_out_buffer = TRUE;
185   /* allocate input buffer and initialize inBufs: */
186   self->input_bo = omap_bo_new (self->device,
187       self->width * self->height, OMAP_BO_WC);
188   self->input = omap_bo_map (self->input_bo);
189   self->inBufs->numBufs = 1;
190   self->inBufs->descs[0].buf = (XDAS_Int8 *) omap_bo_handle (self->input_bo);
192   return TRUE;
195 static inline GstBuffer *
196 codec_buffer_pool_get (GstDucatiVidDec * self, GstBuffer * buf)
198   if (G_UNLIKELY (!self->pool)) {
199     guint size = gst_video_format_get_size (GST_VIDEO_FORMAT_NV12,
200         self->padded_width, self->padded_height);
202     GST_DEBUG_OBJECT (self, "creating bufferpool");
203     self->pool = gst_drm_buffer_pool_new (GST_ELEMENT (self),
204         dce_get_fd (), GST_PAD_CAPS (self->srcpad), size);
205   }
206   return GST_BUFFER (gst_drm_buffer_pool_get (self->pool, FALSE));
209 static GstDucatiBufferPriv *
210 get_buffer_priv (GstDucatiVidDec * self, GstBuffer * buf)
212   GstDucatiBufferPriv *priv = gst_ducati_buffer_priv_get (buf);
213   if (!priv) {
214     GstVideoFormat format = GST_VIDEO_FORMAT_NV12;
215     GstDmaBuf *dmabuf = gst_buffer_get_dma_buf (buf);
217     /* if it isn't a dmabuf buffer that we can import, then there
218      * is nothing we can do with it:
219      */
220     if (!dmabuf) {
221       GST_DEBUG_OBJECT (self, "not importing non dmabuf buffer");
222       return NULL;
223     }
225     priv = gst_ducati_buffer_priv_new ();
227     priv->bo = omap_bo_from_dmabuf (self->device,
228         gst_dma_buf_get_fd (dmabuf));
230     priv->uv_offset = gst_video_format_get_component_offset (format,
231         1, self->stride, self->padded_height);
232     priv->size = gst_video_format_get_size (format,
233         self->stride, self->padded_height);
235     gst_ducati_buffer_priv_set (buf, priv);
236   }
237   return priv;
240 static XDAS_Int32
241 codec_prepare_outbuf (GstDucatiVidDec * self, GstBuffer ** buf,
242     gboolean force_internal)
244   GstDucatiBufferPriv *priv = NULL;
246   if (!force_internal)
247     priv = get_buffer_priv (self, *buf);
249   if (!priv) {
250     GstBuffer *orig = *buf;
252     GST_DEBUG_OBJECT (self, "internal bufferpool forced");
253     *buf = codec_buffer_pool_get (self, NULL);
254     GST_BUFFER_TIMESTAMP (*buf) = GST_BUFFER_TIMESTAMP (orig);
255     GST_BUFFER_DURATION (*buf) = GST_BUFFER_DURATION (orig);
256     gst_buffer_unref (orig);
257     return codec_prepare_outbuf (self, buf, FALSE);
258   }
260   self->outBufs->numBufs = 2;
261   self->outBufs->descs[0].memType = XDM_MEMTYPE_BO;
262   self->outBufs->descs[0].buf = (XDAS_Int8 *) omap_bo_handle (priv->bo);
263   self->outBufs->descs[0].bufSize.bytes = priv->uv_offset;
264   self->outBufs->descs[1].memType = XDM_MEMTYPE_BO_OFFSET;
265   self->outBufs->descs[1].buf = (XDAS_Int8 *) priv->uv_offset;
266   self->outBufs->descs[1].bufSize.bytes = priv->size - priv->uv_offset;
268   return (XDAS_Int32) * buf;    // XXX use lookup table
271 static GstBuffer *
272 codec_get_outbuf (GstDucatiVidDec * self, XDAS_Int32 id)
274   GstBuffer *buf = (GstBuffer *) id;    // XXX use lookup table
275   if (buf) {
276     gst_buffer_ref (buf);
277   }
278   return buf;
281 static void
282 codec_unlock_outbuf (GstDucatiVidDec * self, XDAS_Int32 id)
284   GstBuffer *buf = (GstBuffer *) id;    // XXX use lookup table
285   if (buf) {
286     GST_DEBUG_OBJECT (self, "free buffer: %d %p", id, buf);
287     gst_buffer_unref (buf);
288   }
291 static gint
292 codec_process (GstDucatiVidDec * self, gboolean send, gboolean flush,
293     GstFlowReturn * flow_ret)
295   gint err;
296   GstClockTime t;
297   GstBuffer *outbuf = NULL;
298   gint i;
299   GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
300   GstFlowReturn ret = GST_FLOW_OK;
301   if (flow_ret)
302     /* never leave flow_ret uninitialized */
303     *flow_ret = GST_FLOW_OK;
305   memset (&self->outArgs->outputID, 0, sizeof (self->outArgs->outputID));
306   memset (&self->outArgs->freeBufID, 0, sizeof (self->outArgs->freeBufID));
308   t = gst_util_get_timestamp ();
309   err = VIDDEC3_process (self->codec,
310       self->inBufs, self->outBufs, self->inArgs, self->outArgs);
311   GST_DEBUG_OBJECT (self, "%10dns", (gint) (gst_util_get_timestamp () - t));
313   if (err) {
314     GST_WARNING_OBJECT (self, "err=%d, extendedError=%08x",
315         err, self->outArgs->extendedError);
317     err = VIDDEC3_control (self->codec, XDM_GETSTATUS,
318         self->dynParams, self->status);
319     if (!err) {
320       GST_WARNING_OBJECT (self, "XDM_GETSTATUS: err=%d, extendedError=%08x",
321           err, self->status->extendedError);
322     }
324     if (flush)
325       err = XDM_EFAIL;
326     else
327       err = klass->handle_error (self, err,
328           self->outArgs->extendedError, self->status->extendedError);
329   }
331   for (i = 0; self->outArgs->outputID[i]; i++) {
332     gboolean interlaced;
334     outbuf = codec_get_outbuf (self, self->outArgs->outputID[i]);
336     interlaced =
337         self->outArgs->decodedBufs.contentType ==
338         IVIDEO_PROGRESSIVE ? FALSE : TRUE;
340     /* if send is FALSE, don't try to renegotiate as we could be flushing during
341      * a PAUSED->READY state change
342      */
343     if (send && interlaced != self->interlaced) {
344       GstCaps *caps;
346       GST_WARNING_OBJECT (self, "upstream set interlaced=%d but codec "
347           "thinks interlaced=%d... trusting codec", self->interlaced,
348           interlaced);
350       self->interlaced = interlaced;
352       caps =
353           gst_caps_make_writable (gst_pad_get_negotiated_caps (self->srcpad));
354       GST_INFO_OBJECT (self, "changing interlace field in caps");
355       gst_caps_set_simple (caps, "interlaced", G_TYPE_BOOLEAN, interlaced,
356           NULL);
357       gst_drm_buffer_pool_set_caps (self->pool, caps);
358       if (!gst_pad_set_caps (self->srcpad, caps)) {
359         GST_ERROR_OBJECT (self,
360             "downstream didn't want to change interlace mode");
361         err = XDM_EFAIL;
362       }
363       gst_caps_unref (caps);
365       /* this buffer still has the old caps so we skip it */
366       send = FALSE;
367     }
369     if (G_UNLIKELY (self->send_crop_event) && send) {
370       gint crop_width, crop_height;
371       GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
373       /* send region of interest to sink on first buffer: */
374       XDM_Rect *r = &(self->outArgs->displayBufs.bufDesc[0].activeFrameRegion);
376       crop_width = r->bottomRight.x - r->topLeft.x;
377       crop_height = r->bottomRight.y - r->topLeft.y;
379       if (crop_width > self->input_width)
380         crop_width = self->input_width;
381       if (crop_height > self->input_height)
382         crop_height = self->input_height;
384       if (self->interlaced && !strcmp (klass->codec_name, "ivahd_mpeg2vdec"))
385         crop_height = crop_height / 2;
387       GST_INFO_OBJECT (self, "active frame region %d, %d, %d, %d, crop %dx%d",
388           r->topLeft.x, r->topLeft.y, r->bottomRight.x, r->bottomRight.y,
389           crop_width, crop_height);
391       gst_pad_push_event (self->srcpad,
392           gst_event_new_crop (r->topLeft.y, r->topLeft.x,
393               crop_width, crop_height));
395       if (self->crop)
396         gst_video_crop_unref (self->crop);
398       self->crop = gst_video_crop_new (r->topLeft.y, r->topLeft.x,
399           crop_width, crop_height);
401       self->send_crop_event = FALSE;
402     }
404     if (G_UNLIKELY (self->first_out_buffer) && send) {
405       GstDRMBufferPool *pool;
406       self->first_out_buffer = FALSE;
408       /* Destroy the pool so the buffers we used so far are eventually released.
409        * The pool will be recreated if needed.
410        */
411       pool = self->pool;
412       self->pool = NULL;
413       gst_drm_buffer_pool_destroy (pool);
414     }
416     if (send) {
417       GstClockTime ts;
419       ts = GST_BUFFER_TIMESTAMP (outbuf);
421       GST_DEBUG_OBJECT (self, "got buffer: %d %p (%" GST_TIME_FORMAT ")",
422           i, outbuf, GST_TIME_ARGS (ts));
424       if (self->ts_may_be_pts) {
425         if ((self->last_pts != GST_CLOCK_TIME_NONE) && (self->last_pts > ts)) {
426           GST_DEBUG_OBJECT (self, "detected PTS going backwards, "
427               "enabling ts_is_pts");
428           self->ts_is_pts = TRUE;
429         }
430       }
432       self->last_pts = ts;
434       if (self->dts_ridx != self->dts_widx) {
435         ts = self->dts_queue[self->dts_ridx++ % NDTS];
436       }
438       if (self->ts_is_pts) {
439         /* if we have a queued DTS from demuxer, use that instead: */
440         GST_BUFFER_TIMESTAMP (outbuf) = ts;
441         GST_DEBUG_OBJECT (self, "fixed ts: %d %p (%" GST_TIME_FORMAT ")",
442             i, outbuf, GST_TIME_ARGS (ts));
443       }
445       if (GST_BUFFER_CAPS (outbuf) &&
446           !gst_caps_is_equal (GST_BUFFER_CAPS (outbuf),
447               GST_PAD_CAPS (self->srcpad))) {
448         /* this looks a bit scary but it's really just to change the interlace=
449          * field in caps when we start as !interlaced and the codec detects
450          * otherwise */
451         GST_WARNING_OBJECT (self, "overriding buffer caps to fix "
452             "interlace mismatch");
453         outbuf = gst_buffer_make_metadata_writable (outbuf);
454         gst_buffer_set_caps (outbuf, GST_PAD_CAPS (self->srcpad));
455       }
457       if (self->crop)
458         gst_buffer_set_video_crop (outbuf, self->crop);
460       ret = gst_pad_push (self->srcpad, outbuf);
461       if (flow_ret)
462         *flow_ret = ret;
463       if (ret != GST_FLOW_OK) {
464         GST_WARNING_OBJECT (self, "push failed %s", gst_flow_get_name (ret));
465         /* just unref the remaining buffers (if any) */
466         send = FALSE;
467       }
468     } else {
469       GST_DEBUG_OBJECT (self, "free buffer: %d %p", i, outbuf);
470       gst_buffer_unref (outbuf);
471     }
472   }
474   for (i = 0; self->outArgs->freeBufID[i]; i++) {
475     codec_unlock_outbuf (self, self->outArgs->freeBufID[i]);
476   }
478   return err;
481 /** call control(FLUSH), and then process() to pop out all buffers */
482 gboolean
483 gst_ducati_viddec_codec_flush (GstDucatiVidDec * self, gboolean eos)
485   gint err;
487   GST_DEBUG_OBJECT (self, "flush: eos=%d", eos);
489   /* note: flush is synchronized against _chain() to avoid calling
490    * the codec from multiple threads
491    */
492   GST_PAD_STREAM_LOCK (self->sinkpad);
494   self->dts_ridx = self->dts_widx = 0;
495   self->last_dts = self->last_pts = GST_CLOCK_TIME_NONE;
496   self->ts_may_be_pts = TRUE;
497   self->ts_is_pts = FALSE;
498   self->wait_keyframe = TRUE;
500   if (G_UNLIKELY (self->first_in_buffer)) {
501     return TRUE;
502   }
504   if (G_UNLIKELY (!self->codec)) {
505     GST_WARNING_OBJECT (self, "no codec");
506     return TRUE;
507   }
509   err = VIDDEC3_control (self->codec, XDM_FLUSH, self->dynParams, self->status);
510   if (err) {
511     GST_ERROR_OBJECT (self, "failed XDM_FLUSH");
512     goto out;
513   }
515   self->inBufs->descs[0].bufSize.bytes = 0;
516   self->inArgs->numBytes = 0;
517   self->inArgs->inputID = 0;
519   do {
520     err = codec_process (self, eos, TRUE, NULL);
521   } while (err != XDM_EFAIL);
523   /* reset outArgs in case we're flushing in codec_process trying to do error
524    * recovery */
525   memset (&self->outArgs->outputID, 0, sizeof (self->outArgs->outputID));
526   memset (&self->outArgs->freeBufID, 0, sizeof (self->outArgs->freeBufID));
528   /* on a flush, it is normal (and not an error) for the last _process() call
529    * to return an error..
530    */
531   err = XDM_EOK;
533 out:
534   GST_PAD_STREAM_UNLOCK (self->sinkpad);
535   GST_DEBUG_OBJECT (self, "done");
537   return !err;
540 /* GstDucatiVidDec vmethod default implementations */
542 static gboolean
543 gst_ducati_viddec_parse_caps (GstDucatiVidDec * self, GstStructure * s)
545   const GValue *codec_data;
546   gint w, h;
548   if (gst_structure_get_int (s, "width", &self->input_width) &&
549       gst_structure_get_int (s, "height", &self->input_height)) {
551     h = ALIGN2 (self->input_height, 4); /* round up to MB */
552     w = ALIGN2 (self->input_width, 4);  /* round up to MB */
554     /* if we've already created codec, but the resolution has changed, we
555      * need to re-create the codec:
556      */
557     if (G_UNLIKELY (self->codec)) {
558       if ((h != self->height) || (w != self->width)) {
559         codec_delete (self);
560       }
561     }
563     self->width = w;
564     self->height = h;
566     codec_data = gst_structure_get_value (s, "codec_data");
568     if (codec_data) {
569       GstBuffer *buffer = gst_value_get_buffer (codec_data);
570       GST_DEBUG_OBJECT (self, "codec_data: %" GST_PTR_FORMAT, buffer);
571       self->codec_data = gst_buffer_ref (buffer);
572     }
574     return TRUE;
575   }
577   return FALSE;
580 static gboolean
581 gst_ducati_viddec_allocate_params (GstDucatiVidDec * self, gint params_sz,
582     gint dynparams_sz, gint status_sz, gint inargs_sz, gint outargs_sz)
585   /* allocate params: */
586   self->params = dce_alloc (params_sz);
587   if (G_UNLIKELY (!self->params)) {
588     return FALSE;
589   }
590   self->params->size = params_sz;
591   self->params->maxFrameRate = 30000;
592   self->params->maxBitRate = 10000000;
594   self->params->dataEndianness = XDM_BYTE;
595   self->params->forceChromaFormat = XDM_YUV_420SP;
596   self->params->operatingMode = IVIDEO_DECODE_ONLY;
598   self->params->displayBufsMode = IVIDDEC3_DISPLAYBUFS_EMBEDDED;
599   self->params->inputDataMode = IVIDEO_ENTIREFRAME;
600   self->params->outputDataMode = IVIDEO_ENTIREFRAME;
601   self->params->numInputDataUnits = 0;
602   self->params->numOutputDataUnits = 0;
604   self->params->metadataType[0] = IVIDEO_METADATAPLANE_NONE;
605   self->params->metadataType[1] = IVIDEO_METADATAPLANE_NONE;
606   self->params->metadataType[2] = IVIDEO_METADATAPLANE_NONE;
607   self->params->errorInfoMode = IVIDEO_ERRORINFO_OFF;
609   /* allocate dynParams: */
610   self->dynParams = dce_alloc (dynparams_sz);
611   if (G_UNLIKELY (!self->dynParams)) {
612     return FALSE;
613   }
614   self->dynParams->size = dynparams_sz;
615   self->dynParams->decodeHeader = XDM_DECODE_AU;
616   self->dynParams->displayWidth = 0;
617   self->dynParams->frameSkipMode = IVIDEO_NO_SKIP;
618   self->dynParams->newFrameFlag = XDAS_TRUE;
620   /* allocate status: */
621   self->status = dce_alloc (status_sz);
622   if (G_UNLIKELY (!self->status)) {
623     return FALSE;
624   }
625   self->status->size = status_sz;
627   /* allocate inBufs/outBufs: */
628   self->inBufs = dce_alloc (sizeof (XDM2_BufDesc));
629   self->outBufs = dce_alloc (sizeof (XDM2_BufDesc));
630   if (G_UNLIKELY (!self->inBufs) || G_UNLIKELY (!self->outBufs)) {
631     return FALSE;
632   }
634   /* allocate inArgs/outArgs: */
635   self->inArgs = dce_alloc (inargs_sz);
636   self->outArgs = dce_alloc (outargs_sz);
637   if (G_UNLIKELY (!self->inArgs) || G_UNLIKELY (!self->outArgs)) {
638     return FALSE;
639   }
640   self->inArgs->size = inargs_sz;
641   self->outArgs->size = outargs_sz;
643   return TRUE;
646 static GstBuffer *
647 gst_ducati_viddec_push_input (GstDucatiVidDec * self, GstBuffer * buf)
649   if (G_UNLIKELY (self->first_in_buffer) && self->codec_data) {
650     push_input (self, GST_BUFFER_DATA (self->codec_data),
651         GST_BUFFER_SIZE (self->codec_data));
652   }
654   /* just copy entire buffer */
655   push_input (self, GST_BUFFER_DATA (buf), GST_BUFFER_SIZE (buf));
656   gst_buffer_unref (buf);
658   return NULL;
661 static gint
662 gst_ducati_viddec_handle_error (GstDucatiVidDec * self, gint ret,
663     gint extended_error, gint status_extended_error)
665   if (XDM_ISFATALERROR (extended_error))
666     ret = XDM_EFAIL;
667   else
668     ret = XDM_EOK;
670   return ret;
673 /* GstElement vmethod implementations */
675 static gboolean
676 gst_ducati_viddec_sink_setcaps (GstPad * pad, GstCaps * caps)
678   gboolean ret = TRUE;
679   GstDucatiVidDec *self = GST_DUCATIVIDDEC (gst_pad_get_parent (pad));
680   GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
681   GstStructure *s;
682   GstCaps *outcaps = NULL;
683   GstStructure *out_s;
684   gint par_width, par_height;
685   gboolean par_present;
687   GST_INFO_OBJECT (self, "setcaps (sink): %" GST_PTR_FORMAT, caps);
689   s = gst_caps_get_structure (caps, 0);
690   if (!klass->parse_caps (self, s)) {
691     GST_WARNING_OBJECT (self, "missing required fields");
692     ret = FALSE;
693     goto out;
694   }
696   /* update output/padded sizes */
697   klass->update_buffer_size (self);
699   if (!gst_structure_get_fraction (s, "framerate", &self->fps_n, &self->fps_d)) {
700     self->fps_n = 0;
701     self->fps_d = 1;
702   }
703   gst_structure_get_boolean (s, "interlaced", &self->interlaced);
704   par_present = gst_structure_get_fraction (s, "pixel-aspect-ratio",
705       &par_width, &par_height);
707   outcaps = gst_pad_get_allowed_caps (self->srcpad);
708   if (outcaps) {
709     outcaps = gst_caps_make_writable (outcaps);
710     gst_caps_truncate (outcaps);
711     if (gst_caps_is_empty (outcaps)) {
712       gst_caps_unref (outcaps);
713       outcaps = NULL;
714     }
715   }
717   if (!outcaps) {
718     /* note: default to non-strided for better compatibility with
719      * other gst elements that don't understand stride:
720      */
721     outcaps = gst_caps_new_simple ("video/x-raw-yuv",
722         "format", GST_TYPE_FOURCC, GST_MAKE_FOURCC ('N', 'V', '1', '2'), NULL);
723   }
725   out_s = gst_caps_get_structure (outcaps, 0);
726   gst_structure_set (out_s,
727       "width", G_TYPE_INT, self->padded_width,
728       "height", G_TYPE_INT, self->padded_height,
729       "framerate", GST_TYPE_FRACTION, self->fps_n, self->fps_d, NULL);
730   if (par_present)
731     gst_structure_set (out_s, "pixel-aspect-ratio", GST_TYPE_FRACTION,
732         par_width, par_height, NULL);
734   if (self->interlaced)
735     gst_structure_set (out_s, "interlaced", G_TYPE_BOOLEAN, TRUE, NULL);
737   if (!strcmp (gst_structure_get_name (out_s), "video/x-raw-yuv-strided")) {
738     if (!gst_structure_get_int (out_s, "rowstride", &self->stride)) {
739       self->stride = 4096;
740       gst_structure_set (out_s, "rowstride", G_TYPE_INT, self->stride, NULL);
741     }
742   } else {
743     self->stride = gst_video_format_get_row_stride (GST_VIDEO_FORMAT_NV12,
744         0, self->padded_width);
745   }
747   self->outsize = gst_video_format_get_size (GST_VIDEO_FORMAT_NV12,
748       self->stride, self->padded_height);
750   GST_INFO_OBJECT (self, "outsize %d stride %d outcaps: %" GST_PTR_FORMAT,
751       self->outsize, self->stride, outcaps);
753   if (!self->first_in_buffer) {
754     /* Caps changed mid stream. We flush the codec to unlock all the potentially
755      * locked buffers. This is needed for downstream sinks that provide a
756      * buffer pool and need to destroy all the outstanding buffers before they
757      * can negotiate new caps (hello v4l2sink).
758      */
759     gst_ducati_viddec_codec_flush (self, FALSE);
760   }
762   /* (re)send a crop event when caps change */
763   self->send_crop_event = TRUE;
765   ret = gst_pad_set_caps (self->srcpad, outcaps);
767   GST_INFO_OBJECT (self, "set caps done %d, %" GST_PTR_FORMAT, ret, outcaps);
769 out:
770   if (outcaps)
771     gst_caps_unref (outcaps);
772   gst_object_unref (self);
774   return ret;
777 static GstCaps *
778 gst_ducati_viddec_src_getcaps (GstPad * pad)
780   GstCaps *caps = NULL;
781   GstCaps *outcaps = NULL;
782   int i;
784   caps = GST_PAD_CAPS (pad);
785   if (caps == NULL) {
786     outcaps = gst_caps_copy (gst_pad_get_pad_template_caps (pad));
787     return outcaps;
788   }
790   outcaps = gst_caps_new_empty ();
792   /* allow -rowstrided and regular yuv */
793   for (i = 0; i < gst_caps_get_size (caps); i++) {
794     GstStructure *structure;
795     GstStructure *modified_structure;
796     GValue value = { 0 };
798     structure = gst_caps_get_structure (caps, i);
799     gst_caps_append_structure (outcaps, gst_structure_copy (structure));
800     modified_structure = gst_structure_copy (structure);
802     if (gst_structure_has_name (structure, "video/x-raw-yuv")) {
803       gst_structure_set_name (modified_structure, "video/x-raw-yuv-strided");
804       g_value_init (&value, GST_TYPE_INT_RANGE);
805       gst_value_set_int_range (&value, 0, G_MAXINT);
806       gst_structure_set_value (modified_structure, "rowstride", &value);
807       gst_caps_append_structure (outcaps, modified_structure);
808       g_value_unset (&value);
809     } else {
810       gst_structure_set_name (modified_structure, "video/x-raw-yuv");
811       gst_structure_remove_field (modified_structure, "rowstride");
812       gst_caps_append_structure (outcaps, modified_structure);
813     }
814   }
815   return outcaps;
818 static gboolean
819 gst_ducati_viddec_query (GstDucatiVidDec * self, GstPad * pad,
820     GstQuery * query, gboolean * forward)
822   gboolean res = TRUE;
824   switch (GST_QUERY_TYPE (query)) {
825     case GST_QUERY_BUFFERS:
826       GST_DEBUG_OBJECT (self, "min buffers: %d", self->min_buffers);
827       gst_query_set_buffers_count (query, self->min_buffers);
829       GST_DEBUG_OBJECT (self, "min dimensions: %dx%d",
830           self->padded_width, self->padded_height);
831       gst_query_set_buffers_dimensions (query,
832           self->padded_width, self->padded_height);
833       *forward = FALSE;
834       break;
835     default:
836       break;
837   }
840   return res;
843 static gboolean
844 gst_ducati_viddec_src_query (GstPad * pad, GstQuery * query)
846   gboolean res = TRUE, forward = TRUE;
847   GstDucatiVidDec *self = GST_DUCATIVIDDEC (GST_OBJECT_PARENT (pad));
848   GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
850   GST_DEBUG_OBJECT (self, "query: %" GST_PTR_FORMAT, query);
851   res = klass->query (self, pad, query, &forward);
852   if (res && forward)
853     res = gst_pad_query_default (pad, query);
855   return res;
858 static gboolean
859 gst_ducati_viddec_do_qos (GstDucatiVidDec * self, GstBuffer * buf)
861   GstClockTime timestamp, qostime;
862   GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
863   gint64 diff;
865   if (self->wait_keyframe) {
866     if (GST_BUFFER_FLAG_IS_SET (buf, GST_BUFFER_FLAG_DELTA_UNIT)) {
867       GST_INFO_OBJECT (self, "skipping until the next keyframe");
868       return FALSE;
869     }
871     self->wait_keyframe = FALSE;
872   }
874   timestamp = GST_BUFFER_TIMESTAMP (buf);
875   if (self->segment.format != GST_FORMAT_TIME ||
876       self->qos_earliest_time == GST_CLOCK_TIME_NONE)
877     goto no_qos;
879   if (G_UNLIKELY (!GST_CLOCK_TIME_IS_VALID (timestamp)))
880     goto no_qos;
882   qostime = gst_segment_to_running_time (&self->segment,
883       GST_FORMAT_TIME, timestamp);
884   if (G_UNLIKELY (!GST_CLOCK_TIME_IS_VALID (qostime)))
885     /* out of segment */
886     goto no_qos;
888   /* see how our next timestamp relates to the latest qos timestamp. negative
889    * values mean we are early, positive values mean we are too late. */
890   diff = GST_CLOCK_DIFF (qostime, self->qos_earliest_time);
892   GST_DEBUG_OBJECT (self, "QOS: qostime %" GST_TIME_FORMAT
893       ", earliest %" GST_TIME_FORMAT " diff %" G_GINT64_FORMAT " proportion %f",
894       GST_TIME_ARGS (qostime), GST_TIME_ARGS (self->qos_earliest_time), diff,
895       self->qos_proportion);
897   if (klass->drop_frame (self, buf, diff)) {
898     GST_INFO_OBJECT (self, "dropping frame");
899     return FALSE;
900   }
902 no_qos:
903   return TRUE;
906 static gboolean
907 gst_ducati_viddec_drop_frame (GstDucatiVidDec * self, GstBuffer * buf,
908     gint64 diff)
910   gboolean is_keyframe = !GST_BUFFER_FLAG_IS_SET (buf,
911       GST_BUFFER_FLAG_DELTA_UNIT);
913   if (diff >= 0 && !is_keyframe)
914     return TRUE;
916   return FALSE;
919 static GstFlowReturn
920 gst_ducati_viddec_chain (GstPad * pad, GstBuffer * buf)
922   GstDucatiVidDec *self = GST_DUCATIVIDDEC (GST_OBJECT_PARENT (pad));
923   GstClockTime ts = GST_BUFFER_TIMESTAMP (buf);
924   GstFlowReturn ret = GST_FLOW_OK;
925   Int32 err;
926   GstBuffer *outbuf = NULL;
927   GstCaps *outcaps = NULL;
928   gboolean decode;
930   if (G_UNLIKELY (!self->engine)) {
931     GST_ERROR_OBJECT (self, "no engine");
932     return GST_FLOW_ERROR;
933   }
935   GST_DEBUG_OBJECT (self, "chain: %" GST_TIME_FORMAT " (%d bytes, flags %d)",
936       GST_TIME_ARGS (ts), GST_BUFFER_SIZE (buf), GST_BUFFER_FLAGS (buf));
938   decode = gst_ducati_viddec_do_qos (self, buf);
939   if (!decode) {
940     gst_buffer_unref (buf);
941     return GST_FLOW_OK;
942   }
944   if (!self->need_out_buf)
945     goto have_out_buf;
947   /* do this before creating codec to ensure reverse caps negotiation
948    * happens first:
949    */
950 allocate_buffer:
951   ret = gst_pad_alloc_buffer (self->srcpad, 0, self->outsize,
952       GST_PAD_CAPS (self->srcpad), &outbuf);
953   if (ret != GST_FLOW_OK) {
954     GST_WARNING_OBJECT (self, "alloc_buffer failed %s",
955         gst_flow_get_name (ret));
956     return ret;
957   }
959   outcaps = GST_BUFFER_CAPS (outbuf);
960   if (outcaps && !gst_caps_is_equal (outcaps, GST_PAD_CAPS (self->srcpad))) {
961     GstStructure *s;
963     GST_INFO_OBJECT (self, "doing upstream negotiation bufsize %d",
964         GST_BUFFER_SIZE (outbuf));
966     s = gst_caps_get_structure (outcaps, 0);
967     gst_structure_get_int (s, "rowstride", &self->stride);
968     self->outsize = gst_video_format_get_size (GST_VIDEO_FORMAT_NV12,
969         self->stride, self->padded_height);
971     GST_INFO_OBJECT (self, "outsize %d stride %d outcaps: %" GST_PTR_FORMAT,
972         self->outsize, self->stride, outcaps);
974     gst_pad_set_caps (self->srcpad, outcaps);
976     if (GST_BUFFER_SIZE (outbuf) != self->outsize) {
977       GST_INFO_OBJECT (self, "dropping buffer (bufsize %d != outsize %d)",
978           GST_BUFFER_SIZE (outbuf), self->outsize);
979       gst_buffer_unref (outbuf);
980       goto allocate_buffer;
981     }
982   }
984   if (G_UNLIKELY (!self->codec)) {
985     if (!codec_create (self)) {
986       GST_ERROR_OBJECT (self, "could not create codec");
987       return GST_FLOW_ERROR;
988     }
989   }
991   GST_BUFFER_TIMESTAMP (outbuf) = GST_BUFFER_TIMESTAMP (buf);
992   GST_BUFFER_DURATION (outbuf) = GST_BUFFER_DURATION (buf);
994   /* Pass new output buffer to the decoder to decode into. Use buffers from the
995    * internal pool while self->first_out_buffer == TRUE in order to simplify
996    * things in case we need to renegotiate */
997   self->inArgs->inputID =
998       codec_prepare_outbuf (self, &outbuf, self->first_out_buffer);
999   if (!self->inArgs->inputID) {
1000     GST_ERROR_OBJECT (self, "could not prepare output buffer");
1001     return GST_FLOW_ERROR;
1002   }
1004 have_out_buf:
1005   self->in_size = 0;
1006   buf = GST_DUCATIVIDDEC_GET_CLASS (self)->push_input (self, buf);
1008   if (ts != GST_CLOCK_TIME_NONE) {
1009     self->dts_queue[self->dts_widx++ % NDTS] = ts;
1010     /* if next buffer has earlier ts than previous, then the ts
1011      * we are getting are definitely decode order (DTS):
1012      */
1013     if ((self->last_dts != GST_CLOCK_TIME_NONE) && (self->last_dts > ts)) {
1014       GST_DEBUG_OBJECT (self, "input timestamp definitely DTS");
1015       self->ts_may_be_pts = FALSE;
1016     }
1017     self->last_dts = ts;
1018   }
1020   if (self->in_size == 0 && outbuf) {
1021     GST_DEBUG_OBJECT (self, "no input, skipping process");
1022     gst_buffer_unref (outbuf);
1023     return GST_FLOW_OK;
1024   }
1026   self->inArgs->numBytes = self->in_size;
1027   self->inBufs->descs[0].bufSize.bytes = self->in_size;
1028   self->inBufs->descs[0].memType = XDM_MEMTYPE_BO;
1030   err = codec_process (self, TRUE, FALSE, &ret);
1031   if (err) {
1032     GST_ELEMENT_ERROR (self, STREAM, DECODE, (NULL),
1033         ("process returned error: %d %08x", err, self->outArgs->extendedError));
1034     return GST_FLOW_ERROR;
1035   }
1036   if (ret != GST_FLOW_OK) {
1037     GST_WARNING_OBJECT (self, "push from codec_process failed %s",
1038         gst_flow_get_name (ret));
1039     return ret;
1040   }
1042   self->first_in_buffer = FALSE;
1044   if (self->outArgs->outBufsInUseFlag) {
1045     GST_DEBUG_OBJECT (self, "outBufsInUseFlag set");
1046     self->need_out_buf = FALSE;
1047   } else {
1048     self->need_out_buf = TRUE;
1049   }
1051   if (buf) {
1052     GST_DEBUG_OBJECT (self, "found remaining data: %d bytes",
1053         GST_BUFFER_SIZE (buf));
1054     ts = GST_BUFFER_TIMESTAMP (buf);
1055     goto allocate_buffer;
1056   }
1058   return GST_FLOW_OK;
1061 static gboolean
1062 gst_ducati_viddec_event (GstPad * pad, GstEvent * event)
1064   GstDucatiVidDec *self = GST_DUCATIVIDDEC (GST_OBJECT_PARENT (pad));
1065   gboolean ret = TRUE;
1067   GST_DEBUG_OBJECT (self, "begin: event=%s", GST_EVENT_TYPE_NAME (event));
1069   switch (GST_EVENT_TYPE (event)) {
1070     case GST_EVENT_NEWSEGMENT:
1071     {
1072       gboolean update;
1073       GstFormat fmt;
1074       gint64 start, stop, time;
1075       gdouble rate, arate;
1077       gst_event_parse_new_segment_full (event, &update, &rate, &arate, &fmt,
1078           &start, &stop, &time);
1079       gst_segment_set_newsegment_full (&self->segment, update,
1080           rate, arate, fmt, start, stop, time);
1081       break;
1082     }
1083     case GST_EVENT_EOS:
1084       if (!gst_ducati_viddec_codec_flush (self, TRUE)) {
1085         GST_ERROR_OBJECT (self, "could not flush on eos");
1086         ret = FALSE;
1087       }
1088       break;
1089     case GST_EVENT_FLUSH_STOP:
1090       if (!gst_ducati_viddec_codec_flush (self, FALSE)) {
1091         GST_ERROR_OBJECT (self, "could not flush");
1092         ret = FALSE;
1093       }
1094       gst_segment_init (&self->segment, GST_FORMAT_UNDEFINED);
1095       self->qos_earliest_time = GST_CLOCK_TIME_NONE;
1096       self->qos_proportion = 1;
1097       self->need_out_buf = TRUE;
1098       break;
1099     default:
1100       break;
1101   }
1103   if (ret)
1104     ret = gst_pad_push_event (self->srcpad, event);
1105   GST_LOG_OBJECT (self, "end");
1107   return ret;
1110 static gboolean
1111 gst_ducati_viddec_src_event (GstPad * pad, GstEvent * event)
1113   GstDucatiVidDec *self = GST_DUCATIVIDDEC (GST_OBJECT_PARENT (pad));
1114   gboolean ret = TRUE;
1116   GST_LOG_OBJECT (self, "begin: event=%s", GST_EVENT_TYPE_NAME (event));
1118   switch (GST_EVENT_TYPE (event)) {
1119     case GST_EVENT_QOS:
1120     {
1121       gdouble proportion;
1122       GstClockTimeDiff diff;
1123       GstClockTime timestamp;
1125       gst_event_parse_qos (event, &proportion, &diff, &timestamp);
1127       GST_OBJECT_LOCK (self);
1128       self->qos_proportion = proportion;
1129       self->qos_earliest_time = timestamp + 2 * diff;
1130       GST_OBJECT_UNLOCK (self);
1132       GST_DEBUG_OBJECT (self,
1133           "got QoS proportion %f %" GST_TIME_FORMAT ", %" G_GINT64_FORMAT,
1134           proportion, GST_TIME_ARGS (timestamp), diff);
1136       ret = gst_pad_push_event (self->sinkpad, event);
1137       break;
1138     }
1139     default:
1140       ret = gst_pad_push_event (self->sinkpad, event);
1141       break;
1142   }
1144   GST_LOG_OBJECT (self, "end");
1146   return ret;
1149 static GstStateChangeReturn
1150 gst_ducati_viddec_change_state (GstElement * element, GstStateChange transition)
1152   GstStateChangeReturn ret = GST_STATE_CHANGE_SUCCESS;
1153   GstDucatiVidDec *self = GST_DUCATIVIDDEC (element);
1154   gboolean supported;
1156   GST_DEBUG_OBJECT (self, "begin: changing state %s -> %s",
1157       gst_element_state_get_name (GST_STATE_TRANSITION_CURRENT (transition)),
1158       gst_element_state_get_name (GST_STATE_TRANSITION_NEXT (transition)));
1160   switch (transition) {
1161     case GST_STATE_CHANGE_NULL_TO_READY:
1162       if (!engine_open (self)) {
1163         GST_ERROR_OBJECT (self, "could not open");
1164         return GST_STATE_CHANGE_FAILURE;
1165       }
1166       /* try to create/destroy the codec here, it may not be supported */
1167       supported = codec_create (self);
1168       codec_delete (self);
1169       self->codec = NULL;
1170       if (!supported) {
1171         GST_ERROR_OBJECT (element, "Failed to create codec %s, not supported",
1172             GST_DUCATIVIDDEC_GET_CLASS (self)->codec_name);
1173         engine_close (self);
1174         return GST_STATE_CHANGE_FAILURE;
1175       }
1176       break;
1177     default:
1178       break;
1179   }
1181   ret = GST_ELEMENT_CLASS (parent_class)->change_state (element, transition);
1183   if (ret == GST_STATE_CHANGE_FAILURE)
1184     goto leave;
1186   switch (transition) {
1187     case GST_STATE_CHANGE_PAUSED_TO_READY:
1188       self->interlaced = FALSE;
1189       self->send_crop_event = TRUE;
1190       gst_ducati_viddec_codec_flush (self, FALSE);
1191       break;
1192     case GST_STATE_CHANGE_READY_TO_NULL:
1193       codec_delete (self);
1194       engine_close (self);
1195       break;
1196     default:
1197       break;
1198   }
1200 leave:
1201   GST_LOG_OBJECT (self, "end");
1203   return ret;
1206 /* GObject vmethod implementations */
1208 #define VERSION_LENGTH 256
1210 static void
1211 gst_ducati_viddec_get_property (GObject * obj,
1212     guint prop_id, GValue * value, GParamSpec * pspec)
1214   GstDucatiVidDec *self = GST_DUCATIVIDDEC (obj);
1217   switch (prop_id) {
1218     case PROP_VERSION:{
1219       int err;
1220       char *version = NULL;
1222       if (!self->engine)
1223         engine_open (self);
1225       if (!self->codec)
1226         codec_create (self);
1228       if (self->codec) {
1229         version = dce_alloc (VERSION_LENGTH);
1230         self->status->data.buf = (XDAS_Int8 *) version;
1231         self->status->data.bufSize = VERSION_LENGTH;
1233         err = VIDDEC3_control (self->codec, XDM_GETVERSION,
1234             self->dynParams, self->status);
1235         if (err) {
1236           GST_ERROR_OBJECT (self, "failed XDM_GETVERSION");
1237         }
1239         self->status->data.buf = NULL;
1240         self->status->data.bufSize = 0;
1241       }
1243       g_value_set_string (value, version);
1244       if (version)
1245         dce_free (version);
1247       break;
1248     }
1249     default:{
1250       G_OBJECT_WARN_INVALID_PROPERTY_ID (obj, prop_id, pspec);
1251       break;
1252     }
1253   }
1256 static void
1257 gst_ducati_viddec_finalize (GObject * obj)
1259   GstDucatiVidDec *self = GST_DUCATIVIDDEC (obj);
1261   codec_delete (self);
1262   engine_close (self);
1264   if (self->codec_data) {
1265     gst_buffer_unref (self->codec_data);
1266     self->codec_data = NULL;
1267   }
1269   G_OBJECT_CLASS (parent_class)->finalize (obj);
1272 static void
1273 gst_ducati_viddec_base_init (gpointer gclass)
1275   GstElementClass *element_class = GST_ELEMENT_CLASS (gclass);
1277   gst_element_class_add_pad_template (element_class,
1278       gst_static_pad_template_get (&src_factory));
1281 static void
1282 gst_ducati_viddec_class_init (GstDucatiVidDecClass * klass)
1284   GObjectClass *gobject_class = G_OBJECT_CLASS (klass);
1285   GstElementClass *gstelement_class = GST_ELEMENT_CLASS (klass);
1287   gobject_class->get_property =
1288       GST_DEBUG_FUNCPTR (gst_ducati_viddec_get_property);
1289   gobject_class->finalize = GST_DEBUG_FUNCPTR (gst_ducati_viddec_finalize);
1290   gstelement_class->change_state =
1291       GST_DEBUG_FUNCPTR (gst_ducati_viddec_change_state);
1293   klass->parse_caps = GST_DEBUG_FUNCPTR (gst_ducati_viddec_parse_caps);
1294   klass->allocate_params =
1295       GST_DEBUG_FUNCPTR (gst_ducati_viddec_allocate_params);
1296   klass->push_input = GST_DEBUG_FUNCPTR (gst_ducati_viddec_push_input);
1297   klass->handle_error = GST_DEBUG_FUNCPTR (gst_ducati_viddec_handle_error);
1298   klass->drop_frame = GST_DEBUG_FUNCPTR (gst_ducati_viddec_drop_frame);
1299   klass->query = GST_DEBUG_FUNCPTR (gst_ducati_viddec_query);
1301   g_object_class_install_property (gobject_class, PROP_VERSION,
1302       g_param_spec_string ("version", "Version",
1303           "The codec version string", "",
1304           G_PARAM_READABLE | G_PARAM_STATIC_STRINGS));
1307 static void
1308 gst_ducati_viddec_init (GstDucatiVidDec * self, GstDucatiVidDecClass * klass)
1310   GstElementClass *gstelement_class = GST_ELEMENT_CLASS (klass);
1312   self->sinkpad =
1313       gst_pad_new_from_template (gst_element_class_get_pad_template
1314       (gstelement_class, "sink"), "sink");
1315   gst_pad_set_setcaps_function (self->sinkpad,
1316       GST_DEBUG_FUNCPTR (gst_ducati_viddec_sink_setcaps));
1317   gst_pad_set_chain_function (self->sinkpad,
1318       GST_DEBUG_FUNCPTR (gst_ducati_viddec_chain));
1319   gst_pad_set_event_function (self->sinkpad,
1320       GST_DEBUG_FUNCPTR (gst_ducati_viddec_event));
1322   self->srcpad = gst_pad_new_from_static_template (&src_factory, "src");
1323   gst_pad_set_event_function (self->srcpad,
1324       GST_DEBUG_FUNCPTR (gst_ducati_viddec_src_event));
1325   gst_pad_set_query_function (self->srcpad,
1326       GST_DEBUG_FUNCPTR (gst_ducati_viddec_src_query));
1327   gst_pad_set_getcaps_function (self->srcpad,
1328       GST_DEBUG_FUNCPTR (gst_ducati_viddec_src_getcaps));
1330   gst_element_add_pad (GST_ELEMENT (self), self->sinkpad);
1331   gst_element_add_pad (GST_ELEMENT (self), self->srcpad);
1333   self->input_width = 0;
1334   self->input_height = 0;
1335   /* sane defaults in case we need to create codec without caps negotiation
1336    * (for example, to get 'version' property)
1337    */
1338   self->width = 128;
1339   self->height = 128;
1340   self->fps_n = -1;
1341   self->fps_d = -1;
1343   self->first_in_buffer = TRUE;
1344   self->first_out_buffer = TRUE;
1345   self->interlaced = FALSE;
1346   self->send_crop_event = TRUE;
1348   self->dts_ridx = self->dts_widx = 0;
1349   self->last_dts = self->last_pts = GST_CLOCK_TIME_NONE;
1350   self->ts_may_be_pts = TRUE;
1351   self->ts_is_pts = FALSE;
1353   self->pageMemType = XDM_MEMTYPE_TILEDPAGE;
1355   gst_segment_init (&self->segment, GST_FORMAT_UNDEFINED);
1357   self->qos_proportion = 1;
1358   self->qos_earliest_time = GST_CLOCK_TIME_NONE;
1359   self->wait_keyframe = TRUE;
1361   self->need_out_buf = TRUE;
1362   self->device = NULL;
1363   self->input_bo = NULL;