ducati: add some more detailed logging about video decoder extended errors
[glsdk/gst-plugin-ducati.git] / src / gstducatividdec.c
1 /*
2  * GStreamer
3  * Copyright (c) 2010, Texas Instruments Incorporated
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Lesser General Public
7  * License as published by the Free Software Foundation
8  * version 2.1 of the License.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13  * Lesser General Public License for more details.
14  *
15  * You should have received a copy of the GNU Lesser General Public
16  * License along with this library; if not, write to the Free Software
17  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
18  */
20 #ifdef HAVE_CONFIG_H
21 #  include <config.h>
22 #endif
24 #include "gstducatividdec.h"
25 #include "gstducatibufferpriv.h"
27 GST_BOILERPLATE (GstDucatiVidDec, gst_ducati_viddec, GstElement,
28     GST_TYPE_ELEMENT);
30 static GstStaticPadTemplate src_factory = GST_STATIC_PAD_TEMPLATE ("src",
31     GST_PAD_SRC,
32     GST_PAD_ALWAYS,
33     GST_STATIC_CAPS (GST_VIDEO_CAPS_YUV_STRIDED ("NV12", "[ 0, max ]"))
34     );
36 enum
37 {
38   PROP_0,
39   PROP_VERSION,
40 };
42 /* helper functions */
44 static void
45 engine_close (GstDucatiVidDec * self)
46 {
47   if (self->engine) {
48     Engine_close (self->engine);
49     self->engine = NULL;
50   }
52   if (self->params) {
53     dce_free (self->params);
54     self->params = NULL;
55   }
57   if (self->dynParams) {
58     dce_free (self->dynParams);
59     self->dynParams = NULL;
60   }
62   if (self->status) {
63     dce_free (self->status);
64     self->status = NULL;
65   }
67   if (self->inBufs) {
68     dce_free (self->inBufs);
69     self->inBufs = NULL;
70   }
72   if (self->outBufs) {
73     dce_free (self->outBufs);
74     self->outBufs = NULL;
75   }
77   if (self->inArgs) {
78     dce_free (self->inArgs);
79     self->inArgs = NULL;
80   }
82   if (self->outArgs) {
83     dce_free (self->outArgs);
84     self->outArgs = NULL;
85   }
87   if (self->device) {
88     dce_deinit (self->device);
89     self->device = NULL;
90   }
91 }
93 static gboolean
94 engine_open (GstDucatiVidDec * self)
95 {
96   gboolean ret;
97   int ec;
99   if (G_UNLIKELY (self->engine)) {
100     return TRUE;
101   }
103   if (self->device == NULL) {
104     self->device = dce_init ();
105     if (self->device == NULL) {
106       GST_ERROR_OBJECT (self, "dce_init() failed");
107       return FALSE;
108     }
109   }
111   GST_DEBUG_OBJECT (self, "opening engine");
113   self->engine = Engine_open ((String) "ivahd_vidsvr", NULL, &ec);
114   if (G_UNLIKELY (!self->engine)) {
115     GST_ERROR_OBJECT (self, "could not create engine");
116     return FALSE;
117   }
119   ret = GST_DUCATIVIDDEC_GET_CLASS (self)->allocate_params (self,
120       sizeof (IVIDDEC3_Params), sizeof (IVIDDEC3_DynamicParams),
121       sizeof (IVIDDEC3_Status), sizeof (IVIDDEC3_InArgs),
122       sizeof (IVIDDEC3_OutArgs));
124   return ret;
127 static void
128 codec_delete (GstDucatiVidDec * self)
130   if (self->pool) {
131     gst_drm_buffer_pool_destroy (self->pool);
132     self->pool = NULL;
133   }
135   if (self->codec) {
136     VIDDEC3_delete (self->codec);
137     self->codec = NULL;
138   }
140   if (self->input_bo) {
141     omap_bo_del (self->input_bo);
142     self->input_bo = NULL;
143   }
146 static gboolean
147 codec_create (GstDucatiVidDec * self)
149   gint err;
150   const gchar *codec_name;
152   codec_delete (self);
154   if (G_UNLIKELY (!self->engine)) {
155     GST_ERROR_OBJECT (self, "no engine");
156     return FALSE;
157   }
159   /* these need to be set before VIDDEC3_create */
160   self->params->maxWidth = self->width;
161   self->params->maxHeight = self->height;
163   codec_name = GST_DUCATIVIDDEC_GET_CLASS (self)->codec_name;
165   /* create codec: */
166   GST_DEBUG_OBJECT (self, "creating codec: %s", codec_name);
167   self->codec =
168       VIDDEC3_create (self->engine, (String) codec_name, self->params);
170   if (!self->codec) {
171     return FALSE;
172   }
174   err =
175       VIDDEC3_control (self->codec, XDM_SETPARAMS, self->dynParams,
176       self->status);
177   if (err) {
178     GST_ERROR_OBJECT (self, "failed XDM_SETPARAMS");
179     return FALSE;
180   }
182   self->first_in_buffer = TRUE;
183   self->first_out_buffer = TRUE;
185   /* allocate input buffer and initialize inBufs: */
186   self->input_bo = omap_bo_new (self->device,
187       self->width * self->height, OMAP_BO_WC);
188   self->input = omap_bo_map (self->input_bo);
189   self->inBufs->numBufs = 1;
190   self->inBufs->descs[0].buf = (XDAS_Int8 *) omap_bo_handle (self->input_bo);
192   return TRUE;
195 static inline GstBuffer *
196 codec_buffer_pool_get (GstDucatiVidDec * self, GstBuffer * buf)
198   if (G_UNLIKELY (!self->pool)) {
199     guint size = gst_video_format_get_size (GST_VIDEO_FORMAT_NV12,
200         self->padded_width, self->padded_height);
202     GST_DEBUG_OBJECT (self, "creating bufferpool");
203     self->pool = gst_drm_buffer_pool_new (GST_ELEMENT (self),
204         dce_get_fd (), GST_PAD_CAPS (self->srcpad), size);
205   }
206   return GST_BUFFER (gst_drm_buffer_pool_get (self->pool, FALSE));
209 static GstDucatiBufferPriv *
210 get_buffer_priv (GstDucatiVidDec * self, GstBuffer * buf)
212   GstDucatiBufferPriv *priv = gst_ducati_buffer_priv_get (buf);
213   if (!priv) {
214     GstVideoFormat format = GST_VIDEO_FORMAT_NV12;
215     GstDmaBuf *dmabuf = gst_buffer_get_dma_buf (buf);
217     /* if it isn't a dmabuf buffer that we can import, then there
218      * is nothing we can do with it:
219      */
220     if (!dmabuf) {
221       GST_DEBUG_OBJECT (self, "not importing non dmabuf buffer");
222       return NULL;
223     }
225     priv = gst_ducati_buffer_priv_new ();
227     priv->bo = omap_bo_from_dmabuf (self->device, gst_dma_buf_get_fd (dmabuf));
229     priv->uv_offset = gst_video_format_get_component_offset (format,
230         1, self->stride, self->padded_height);
231     priv->size = gst_video_format_get_size (format,
232         self->stride, self->padded_height);
234     gst_ducati_buffer_priv_set (buf, priv);
235   }
236   return priv;
239 static XDAS_Int32
240 codec_prepare_outbuf (GstDucatiVidDec * self, GstBuffer ** buf,
241     gboolean force_internal)
243   GstDucatiBufferPriv *priv = NULL;
245   if (!force_internal)
246     priv = get_buffer_priv (self, *buf);
248   if (!priv) {
249     GstBuffer *orig = *buf;
251     GST_DEBUG_OBJECT (self, "internal bufferpool forced");
252     *buf = codec_buffer_pool_get (self, NULL);
253     GST_BUFFER_TIMESTAMP (*buf) = GST_BUFFER_TIMESTAMP (orig);
254     GST_BUFFER_DURATION (*buf) = GST_BUFFER_DURATION (orig);
255     gst_buffer_unref (orig);
256     return codec_prepare_outbuf (self, buf, FALSE);
257   }
259   self->outBufs->numBufs = 2;
260   self->outBufs->descs[0].memType = XDM_MEMTYPE_BO;
261   self->outBufs->descs[0].buf = (XDAS_Int8 *) omap_bo_handle (priv->bo);
262   self->outBufs->descs[0].bufSize.bytes = priv->uv_offset;
263   self->outBufs->descs[1].memType = XDM_MEMTYPE_BO_OFFSET;
264   self->outBufs->descs[1].buf = (XDAS_Int8 *) priv->uv_offset;
265   self->outBufs->descs[1].bufSize.bytes = priv->size - priv->uv_offset;
267   return (XDAS_Int32) * buf;    // XXX use lookup table
270 static GstBuffer *
271 codec_get_outbuf (GstDucatiVidDec * self, XDAS_Int32 id)
273   GstBuffer *buf = (GstBuffer *) id;    // XXX use lookup table
274   if (buf) {
275     gst_buffer_ref (buf);
276   }
277   return buf;
280 static void
281 codec_unlock_outbuf (GstDucatiVidDec * self, XDAS_Int32 id)
283   GstBuffer *buf = (GstBuffer *) id;    // XXX use lookup table
284   if (buf) {
285     GST_DEBUG_OBJECT (self, "free buffer: %d %p", id, buf);
286     gst_buffer_unref (buf);
287   }
290 static gint
291 codec_process (GstDucatiVidDec * self, gboolean send, gboolean flush,
292     GstFlowReturn * flow_ret)
294   gint err;
295   GstClockTime t;
296   GstBuffer *outbuf = NULL;
297   gint i;
298   GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
299   GstFlowReturn ret = GST_FLOW_OK;
300   if (flow_ret)
301     /* never leave flow_ret uninitialized */
302     *flow_ret = GST_FLOW_OK;
304   memset (&self->outArgs->outputID, 0, sizeof (self->outArgs->outputID));
305   memset (&self->outArgs->freeBufID, 0, sizeof (self->outArgs->freeBufID));
307   t = gst_util_get_timestamp ();
308   err = VIDDEC3_process (self->codec,
309       self->inBufs, self->outBufs, self->inArgs, self->outArgs);
310   GST_DEBUG_OBJECT (self, "%10dns", (gint) (gst_util_get_timestamp () - t));
312   if (err) {
313     GST_WARNING_OBJECT (self, "err=%d, extendedError=%08x",
314         err, self->outArgs->extendedError);
315     gst_ducati_log_extended_error_info (self->outArgs->extendedError);
317     err = VIDDEC3_control (self->codec, XDM_GETSTATUS,
318         self->dynParams, self->status);
319     if (!err) {
320       GST_WARNING_OBJECT (self, "XDM_GETSTATUS: err=%d, extendedError=%08x",
321           err, self->status->extendedError);
322       gst_ducati_log_extended_error_info (self->outArgs->extendedError);
323     }
325     if (flush)
326       err = XDM_EFAIL;
327     else
328       err = klass->handle_error (self, err,
329           self->outArgs->extendedError, self->status->extendedError);
330   }
332   for (i = 0; i < IVIDEO2_MAX_IO_BUFFERS && self->outArgs->outputID[i]; i++) {
333     gboolean interlaced;
335     outbuf = codec_get_outbuf (self, self->outArgs->outputID[i]);
337     interlaced =
338         self->outArgs->decodedBufs.contentType ==
339         IVIDEO_PROGRESSIVE ? FALSE : TRUE;
341     /* if send is FALSE, don't try to renegotiate as we could be flushing during
342      * a PAUSED->READY state change
343      */
344     if (send && interlaced != self->interlaced) {
345       GstCaps *caps;
347       GST_WARNING_OBJECT (self, "upstream set interlaced=%d but codec "
348           "thinks interlaced=%d... trusting codec", self->interlaced,
349           interlaced);
351       self->interlaced = interlaced;
353       caps =
354           gst_caps_make_writable (gst_pad_get_negotiated_caps (self->srcpad));
355       GST_INFO_OBJECT (self, "changing interlace field in caps");
356       gst_caps_set_simple (caps, "interlaced", G_TYPE_BOOLEAN, interlaced,
357           NULL);
358       gst_drm_buffer_pool_set_caps (self->pool, caps);
359       if (!gst_pad_set_caps (self->srcpad, caps)) {
360         GST_ERROR_OBJECT (self,
361             "downstream didn't want to change interlace mode");
362         err = XDM_EFAIL;
363       }
364       gst_caps_unref (caps);
366       /* this buffer still has the old caps so we skip it */
367       send = FALSE;
368     }
370     if (G_UNLIKELY (self->send_crop_event) && send) {
371       gint crop_width, crop_height;
372       GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
374       /* send region of interest to sink on first buffer: */
375       XDM_Rect *r = &(self->outArgs->displayBufs.bufDesc[0].activeFrameRegion);
377       crop_width = r->bottomRight.x - r->topLeft.x;
378       crop_height = r->bottomRight.y - r->topLeft.y;
380       if (crop_width > self->input_width)
381         crop_width = self->input_width;
382       if (crop_height > self->input_height)
383         crop_height = self->input_height;
385       if (self->interlaced && !strcmp (klass->codec_name, "ivahd_mpeg2vdec"))
386         crop_height = crop_height / 2;
388       GST_INFO_OBJECT (self, "active frame region %d, %d, %d, %d, crop %dx%d",
389           r->topLeft.x, r->topLeft.y, r->bottomRight.x, r->bottomRight.y,
390           crop_width, crop_height);
392       gst_pad_push_event (self->srcpad,
393           gst_event_new_crop (r->topLeft.y, r->topLeft.x,
394               crop_width, crop_height));
396       if (self->crop)
397         gst_video_crop_unref (self->crop);
399       self->crop = gst_video_crop_new (r->topLeft.y, r->topLeft.x,
400           crop_width, crop_height);
402       self->send_crop_event = FALSE;
403     }
405     if (G_UNLIKELY (self->first_out_buffer) && send) {
406       GstDRMBufferPool *pool;
407       self->first_out_buffer = FALSE;
409       /* Destroy the pool so the buffers we used so far are eventually released.
410        * The pool will be recreated if needed.
411        */
412       pool = self->pool;
413       self->pool = NULL;
414       gst_drm_buffer_pool_destroy (pool);
415     }
417     if (send) {
418       GstClockTime ts;
420       ts = GST_BUFFER_TIMESTAMP (outbuf);
422       GST_DEBUG_OBJECT (self, "got buffer: %d %p (%" GST_TIME_FORMAT ")",
423           i, outbuf, GST_TIME_ARGS (ts));
425       if (self->ts_may_be_pts) {
426         if ((self->last_pts != GST_CLOCK_TIME_NONE) && (self->last_pts > ts)) {
427           GST_DEBUG_OBJECT (self, "detected PTS going backwards, "
428               "enabling ts_is_pts");
429           self->ts_is_pts = TRUE;
430         }
431       }
433       self->last_pts = ts;
435       if (self->dts_ridx != self->dts_widx) {
436         ts = self->dts_queue[self->dts_ridx++ % NDTS];
437       }
439       if (self->ts_is_pts) {
440         /* if we have a queued DTS from demuxer, use that instead: */
441         GST_BUFFER_TIMESTAMP (outbuf) = ts;
442         GST_DEBUG_OBJECT (self, "fixed ts: %d %p (%" GST_TIME_FORMAT ")",
443             i, outbuf, GST_TIME_ARGS (ts));
444       }
446       if (GST_BUFFER_CAPS (outbuf) &&
447           !gst_caps_is_equal (GST_BUFFER_CAPS (outbuf),
448               GST_PAD_CAPS (self->srcpad))) {
449         /* this looks a bit scary but it's really just to change the interlace=
450          * field in caps when we start as !interlaced and the codec detects
451          * otherwise */
452         GST_WARNING_OBJECT (self, "overriding buffer caps to fix "
453             "interlace mismatch");
454         outbuf = gst_buffer_make_metadata_writable (outbuf);
455         gst_buffer_set_caps (outbuf, GST_PAD_CAPS (self->srcpad));
456       }
458       if (self->crop)
459         gst_buffer_set_video_crop (outbuf, self->crop);
461       ret = gst_pad_push (self->srcpad, outbuf);
462       if (flow_ret)
463         *flow_ret = ret;
464       if (ret != GST_FLOW_OK) {
465         GST_WARNING_OBJECT (self, "push failed %s", gst_flow_get_name (ret));
466         /* just unref the remaining buffers (if any) */
467         send = FALSE;
468       }
469     } else {
470       GST_DEBUG_OBJECT (self, "free buffer: %d %p", i, outbuf);
471       gst_buffer_unref (outbuf);
472     }
473   }
475   for (i = 0; i < IVIDEO2_MAX_IO_BUFFERS && self->outArgs->freeBufID[i]; i++) {
476     codec_unlock_outbuf (self, self->outArgs->freeBufID[i]);
477   }
479   return err;
482 /** call control(FLUSH), and then process() to pop out all buffers */
483 gboolean
484 gst_ducati_viddec_codec_flush (GstDucatiVidDec * self, gboolean eos)
486   gint err = FALSE;
488   GST_DEBUG_OBJECT (self, "flush: eos=%d", eos);
490   /* note: flush is synchronized against _chain() to avoid calling
491    * the codec from multiple threads
492    */
493   GST_PAD_STREAM_LOCK (self->sinkpad);
495   self->dts_ridx = self->dts_widx = 0;
496   self->last_dts = self->last_pts = GST_CLOCK_TIME_NONE;
497   self->ts_may_be_pts = TRUE;
498   self->ts_is_pts = FALSE;
499   self->wait_keyframe = TRUE;
501   if (G_UNLIKELY (self->first_in_buffer)) {
502     goto out;
503   }
505   if (G_UNLIKELY (!self->codec)) {
506     GST_WARNING_OBJECT (self, "no codec");
507     goto out;
508   }
510   err = VIDDEC3_control (self->codec, XDM_FLUSH, self->dynParams, self->status);
511   if (err) {
512     GST_ERROR_OBJECT (self, "failed XDM_FLUSH");
513     goto out;
514   }
516   self->inBufs->descs[0].bufSize.bytes = 0;
517   self->inArgs->numBytes = 0;
518   self->inArgs->inputID = 0;
520   do {
521     err = codec_process (self, eos, TRUE, NULL);
522   } while (err != XDM_EFAIL);
524   /* reset outArgs in case we're flushing in codec_process trying to do error
525    * recovery */
526   memset (&self->outArgs->outputID, 0, sizeof (self->outArgs->outputID));
527   memset (&self->outArgs->freeBufID, 0, sizeof (self->outArgs->freeBufID));
529   /* on a flush, it is normal (and not an error) for the last _process() call
530    * to return an error..
531    */
532   err = XDM_EOK;
534 out:
535   GST_PAD_STREAM_UNLOCK (self->sinkpad);
536   GST_DEBUG_OBJECT (self, "done");
538   return !err;
541 /* GstDucatiVidDec vmethod default implementations */
543 static gboolean
544 gst_ducati_viddec_parse_caps (GstDucatiVidDec * self, GstStructure * s)
546   const GValue *codec_data;
547   gint w, h;
549   if (gst_structure_get_int (s, "width", &self->input_width) &&
550       gst_structure_get_int (s, "height", &self->input_height)) {
552     h = ALIGN2 (self->input_height, 4); /* round up to MB */
553     w = ALIGN2 (self->input_width, 4);  /* round up to MB */
555     /* if we've already created codec, but the resolution has changed, we
556      * need to re-create the codec:
557      */
558     if (G_UNLIKELY (self->codec)) {
559       if ((h != self->height) || (w != self->width)) {
560         codec_delete (self);
561       }
562     }
564     self->width = w;
565     self->height = h;
567     codec_data = gst_structure_get_value (s, "codec_data");
569     if (codec_data) {
570       GstBuffer *buffer = gst_value_get_buffer (codec_data);
571       GST_DEBUG_OBJECT (self, "codec_data: %" GST_PTR_FORMAT, buffer);
572       self->codec_data = gst_buffer_ref (buffer);
573     }
575     return TRUE;
576   }
578   return FALSE;
581 static gboolean
582 gst_ducati_viddec_allocate_params (GstDucatiVidDec * self, gint params_sz,
583     gint dynparams_sz, gint status_sz, gint inargs_sz, gint outargs_sz)
586   /* allocate params: */
587   self->params = dce_alloc (params_sz);
588   if (G_UNLIKELY (!self->params)) {
589     return FALSE;
590   }
591   self->params->size = params_sz;
592   self->params->maxFrameRate = 30000;
593   self->params->maxBitRate = 10000000;
595   self->params->dataEndianness = XDM_BYTE;
596   self->params->forceChromaFormat = XDM_YUV_420SP;
597   self->params->operatingMode = IVIDEO_DECODE_ONLY;
599   self->params->displayBufsMode = IVIDDEC3_DISPLAYBUFS_EMBEDDED;
600   self->params->inputDataMode = IVIDEO_ENTIREFRAME;
601   self->params->outputDataMode = IVIDEO_ENTIREFRAME;
602   self->params->numInputDataUnits = 0;
603   self->params->numOutputDataUnits = 0;
605   self->params->metadataType[0] = IVIDEO_METADATAPLANE_NONE;
606   self->params->metadataType[1] = IVIDEO_METADATAPLANE_NONE;
607   self->params->metadataType[2] = IVIDEO_METADATAPLANE_NONE;
608   self->params->errorInfoMode = IVIDEO_ERRORINFO_OFF;
610   /* allocate dynParams: */
611   self->dynParams = dce_alloc (dynparams_sz);
612   if (G_UNLIKELY (!self->dynParams)) {
613     return FALSE;
614   }
615   self->dynParams->size = dynparams_sz;
616   self->dynParams->decodeHeader = XDM_DECODE_AU;
617   self->dynParams->displayWidth = 0;
618   self->dynParams->frameSkipMode = IVIDEO_NO_SKIP;
619   self->dynParams->newFrameFlag = XDAS_TRUE;
621   /* allocate status: */
622   self->status = dce_alloc (status_sz);
623   if (G_UNLIKELY (!self->status)) {
624     return FALSE;
625   }
626   self->status->size = status_sz;
628   /* allocate inBufs/outBufs: */
629   self->inBufs = dce_alloc (sizeof (XDM2_BufDesc));
630   self->outBufs = dce_alloc (sizeof (XDM2_BufDesc));
631   if (G_UNLIKELY (!self->inBufs) || G_UNLIKELY (!self->outBufs)) {
632     return FALSE;
633   }
635   /* allocate inArgs/outArgs: */
636   self->inArgs = dce_alloc (inargs_sz);
637   self->outArgs = dce_alloc (outargs_sz);
638   if (G_UNLIKELY (!self->inArgs) || G_UNLIKELY (!self->outArgs)) {
639     return FALSE;
640   }
641   self->inArgs->size = inargs_sz;
642   self->outArgs->size = outargs_sz;
644   return TRUE;
647 static GstBuffer *
648 gst_ducati_viddec_push_input (GstDucatiVidDec * self, GstBuffer * buf)
650   if (G_UNLIKELY (self->first_in_buffer) && self->codec_data) {
651     push_input (self, GST_BUFFER_DATA (self->codec_data),
652         GST_BUFFER_SIZE (self->codec_data));
653   }
655   /* just copy entire buffer */
656   push_input (self, GST_BUFFER_DATA (buf), GST_BUFFER_SIZE (buf));
657   gst_buffer_unref (buf);
659   return NULL;
662 static gint
663 gst_ducati_viddec_handle_error (GstDucatiVidDec * self, gint ret,
664     gint extended_error, gint status_extended_error)
666   if (XDM_ISFATALERROR (extended_error))
667     ret = XDM_EFAIL;
668   else
669     ret = XDM_EOK;
671   return ret;
674 /* GstElement vmethod implementations */
676 static gboolean
677 gst_ducati_viddec_sink_setcaps (GstPad * pad, GstCaps * caps)
679   gboolean ret = TRUE;
680   GstDucatiVidDec *self = GST_DUCATIVIDDEC (gst_pad_get_parent (pad));
681   GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
682   GstStructure *s;
683   GstCaps *outcaps = NULL;
684   GstStructure *out_s;
685   gint par_width, par_height;
686   gboolean par_present;
688   GST_INFO_OBJECT (self, "setcaps (sink): %" GST_PTR_FORMAT, caps);
690   s = gst_caps_get_structure (caps, 0);
691   if (!klass->parse_caps (self, s)) {
692     GST_WARNING_OBJECT (self, "missing required fields");
693     ret = FALSE;
694     goto out;
695   }
697   /* update output/padded sizes */
698   klass->update_buffer_size (self);
700   if (!gst_structure_get_fraction (s, "framerate", &self->fps_n, &self->fps_d)) {
701     self->fps_n = 0;
702     self->fps_d = 1;
703   }
704   gst_structure_get_boolean (s, "interlaced", &self->interlaced);
705   par_present = gst_structure_get_fraction (s, "pixel-aspect-ratio",
706       &par_width, &par_height);
708   outcaps = gst_pad_get_allowed_caps (self->srcpad);
709   if (outcaps) {
710     outcaps = gst_caps_make_writable (outcaps);
711     gst_caps_truncate (outcaps);
712     if (gst_caps_is_empty (outcaps)) {
713       gst_caps_unref (outcaps);
714       outcaps = NULL;
715     }
716   }
718   if (!outcaps) {
719     /* note: default to non-strided for better compatibility with
720      * other gst elements that don't understand stride:
721      */
722     outcaps = gst_caps_new_simple ("video/x-raw-yuv",
723         "format", GST_TYPE_FOURCC, GST_MAKE_FOURCC ('N', 'V', '1', '2'), NULL);
724   }
726   out_s = gst_caps_get_structure (outcaps, 0);
727   gst_structure_set (out_s,
728       "width", G_TYPE_INT, self->padded_width,
729       "height", G_TYPE_INT, self->padded_height,
730       "framerate", GST_TYPE_FRACTION, self->fps_n, self->fps_d, NULL);
731   if (par_present)
732     gst_structure_set (out_s, "pixel-aspect-ratio", GST_TYPE_FRACTION,
733         par_width, par_height, NULL);
735   if (self->interlaced)
736     gst_structure_set (out_s, "interlaced", G_TYPE_BOOLEAN, TRUE, NULL);
738   if (!strcmp (gst_structure_get_name (out_s), "video/x-raw-yuv-strided")) {
739     if (!gst_structure_get_int (out_s, "rowstride", &self->stride)) {
740       self->stride = 4096;
741       gst_structure_set (out_s, "rowstride", G_TYPE_INT, self->stride, NULL);
742     }
743   } else {
744     self->stride = gst_video_format_get_row_stride (GST_VIDEO_FORMAT_NV12,
745         0, self->padded_width);
746   }
748   self->outsize = gst_video_format_get_size (GST_VIDEO_FORMAT_NV12,
749       self->stride, self->padded_height);
751   GST_INFO_OBJECT (self, "outsize %d stride %d outcaps: %" GST_PTR_FORMAT,
752       self->outsize, self->stride, outcaps);
754   if (!self->first_in_buffer) {
755     /* Caps changed mid stream. We flush the codec to unlock all the potentially
756      * locked buffers. This is needed for downstream sinks that provide a
757      * buffer pool and need to destroy all the outstanding buffers before they
758      * can negotiate new caps (hello v4l2sink).
759      */
760     gst_ducati_viddec_codec_flush (self, FALSE);
761   }
763   /* (re)send a crop event when caps change */
764   self->send_crop_event = TRUE;
766   ret = gst_pad_set_caps (self->srcpad, outcaps);
768   GST_INFO_OBJECT (self, "set caps done %d, %" GST_PTR_FORMAT, ret, outcaps);
770 out:
771   if (outcaps)
772     gst_caps_unref (outcaps);
773   gst_object_unref (self);
775   return ret;
778 static GstCaps *
779 gst_ducati_viddec_src_getcaps (GstPad * pad)
781   GstCaps *caps = NULL;
782   GstCaps *outcaps = NULL;
783   int i;
785   caps = GST_PAD_CAPS (pad);
786   if (caps == NULL) {
787     outcaps = gst_caps_copy (gst_pad_get_pad_template_caps (pad));
788     return outcaps;
789   }
791   outcaps = gst_caps_new_empty ();
793   /* allow -rowstrided and regular yuv */
794   for (i = 0; i < gst_caps_get_size (caps); i++) {
795     GstStructure *structure;
796     GstStructure *modified_structure;
797     GValue value = { 0 };
799     structure = gst_caps_get_structure (caps, i);
800     gst_caps_append_structure (outcaps, gst_structure_copy (structure));
801     modified_structure = gst_structure_copy (structure);
803     if (gst_structure_has_name (structure, "video/x-raw-yuv")) {
804       gst_structure_set_name (modified_structure, "video/x-raw-yuv-strided");
805       g_value_init (&value, GST_TYPE_INT_RANGE);
806       gst_value_set_int_range (&value, 0, G_MAXINT);
807       gst_structure_set_value (modified_structure, "rowstride", &value);
808       gst_caps_append_structure (outcaps, modified_structure);
809       g_value_unset (&value);
810     } else {
811       gst_structure_set_name (modified_structure, "video/x-raw-yuv");
812       gst_structure_remove_field (modified_structure, "rowstride");
813       gst_caps_append_structure (outcaps, modified_structure);
814     }
815   }
816   return outcaps;
819 static gboolean
820 gst_ducati_viddec_query (GstDucatiVidDec * self, GstPad * pad,
821     GstQuery * query, gboolean * forward)
823   gboolean res = TRUE;
825   switch (GST_QUERY_TYPE (query)) {
826     case GST_QUERY_BUFFERS:
827       GST_DEBUG_OBJECT (self, "min buffers: %d", self->min_buffers);
828       gst_query_set_buffers_count (query, self->min_buffers);
830       GST_DEBUG_OBJECT (self, "min dimensions: %dx%d",
831           self->padded_width, self->padded_height);
832       gst_query_set_buffers_dimensions (query,
833           self->padded_width, self->padded_height);
834       *forward = FALSE;
835       break;
836     default:
837       break;
838   }
841   return res;
844 static gboolean
845 gst_ducati_viddec_src_query (GstPad * pad, GstQuery * query)
847   gboolean res = TRUE, forward = TRUE;
848   GstDucatiVidDec *self = GST_DUCATIVIDDEC (GST_OBJECT_PARENT (pad));
849   GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
851   GST_DEBUG_OBJECT (self, "query: %" GST_PTR_FORMAT, query);
852   res = klass->query (self, pad, query, &forward);
853   if (res && forward)
854     res = gst_pad_query_default (pad, query);
856   return res;
859 static gboolean
860 gst_ducati_viddec_do_qos (GstDucatiVidDec * self, GstBuffer * buf)
862   GstClockTime timestamp, qostime;
863   GstDucatiVidDecClass *klass = GST_DUCATIVIDDEC_GET_CLASS (self);
864   gint64 diff;
866   if (self->wait_keyframe) {
867     if (GST_BUFFER_FLAG_IS_SET (buf, GST_BUFFER_FLAG_DELTA_UNIT)) {
868       GST_INFO_OBJECT (self, "skipping until the next keyframe");
869       return FALSE;
870     }
872     self->wait_keyframe = FALSE;
873   }
875   timestamp = GST_BUFFER_TIMESTAMP (buf);
876   if (self->segment.format != GST_FORMAT_TIME ||
877       self->qos_earliest_time == GST_CLOCK_TIME_NONE)
878     goto no_qos;
880   if (G_UNLIKELY (!GST_CLOCK_TIME_IS_VALID (timestamp)))
881     goto no_qos;
883   qostime = gst_segment_to_running_time (&self->segment,
884       GST_FORMAT_TIME, timestamp);
885   if (G_UNLIKELY (!GST_CLOCK_TIME_IS_VALID (qostime)))
886     /* out of segment */
887     goto no_qos;
889   /* see how our next timestamp relates to the latest qos timestamp. negative
890    * values mean we are early, positive values mean we are too late. */
891   diff = GST_CLOCK_DIFF (qostime, self->qos_earliest_time);
893   GST_DEBUG_OBJECT (self, "QOS: qostime %" GST_TIME_FORMAT
894       ", earliest %" GST_TIME_FORMAT " diff %" G_GINT64_FORMAT " proportion %f",
895       GST_TIME_ARGS (qostime), GST_TIME_ARGS (self->qos_earliest_time), diff,
896       self->qos_proportion);
898   if (klass->drop_frame (self, buf, diff)) {
899     GST_INFO_OBJECT (self, "dropping frame");
900     return FALSE;
901   }
903 no_qos:
904   return TRUE;
907 static gboolean
908 gst_ducati_viddec_drop_frame (GstDucatiVidDec * self, GstBuffer * buf,
909     gint64 diff)
911   gboolean is_keyframe = !GST_BUFFER_FLAG_IS_SET (buf,
912       GST_BUFFER_FLAG_DELTA_UNIT);
914   if (diff >= 0 && !is_keyframe)
915     return TRUE;
917   return FALSE;
920 static GstFlowReturn
921 gst_ducati_viddec_chain (GstPad * pad, GstBuffer * buf)
923   GstDucatiVidDec *self = GST_DUCATIVIDDEC (GST_OBJECT_PARENT (pad));
924   GstClockTime ts = GST_BUFFER_TIMESTAMP (buf);
925   GstFlowReturn ret = GST_FLOW_OK;
926   Int32 err;
927   GstBuffer *outbuf = NULL;
928   GstCaps *outcaps = NULL;
929   gboolean decode;
931   if (G_UNLIKELY (!self->engine)) {
932     GST_ERROR_OBJECT (self, "no engine");
933     gst_buffer_unref (buf);
934     return GST_FLOW_ERROR;
935   }
937   GST_DEBUG_OBJECT (self, "chain: %" GST_TIME_FORMAT " (%d bytes, flags %d)",
938       GST_TIME_ARGS (ts), GST_BUFFER_SIZE (buf), GST_BUFFER_FLAGS (buf));
940   decode = gst_ducati_viddec_do_qos (self, buf);
941   if (!decode) {
942     gst_buffer_unref (buf);
943     return GST_FLOW_OK;
944   }
946   if (!self->need_out_buf)
947     goto have_out_buf;
949   /* do this before creating codec to ensure reverse caps negotiation
950    * happens first:
951    */
952 allocate_buffer:
953   ret = gst_pad_alloc_buffer (self->srcpad, 0, self->outsize,
954       GST_PAD_CAPS (self->srcpad), &outbuf);
955   if (ret != GST_FLOW_OK) {
956     GST_WARNING_OBJECT (self, "alloc_buffer failed %s",
957         gst_flow_get_name (ret));
958     gst_buffer_unref (buf);
959     return ret;
960   }
962   outcaps = GST_BUFFER_CAPS (outbuf);
963   if (outcaps && !gst_caps_is_equal (outcaps, GST_PAD_CAPS (self->srcpad))) {
964     GstStructure *s;
966     GST_INFO_OBJECT (self, "doing upstream negotiation bufsize %d",
967         GST_BUFFER_SIZE (outbuf));
969     s = gst_caps_get_structure (outcaps, 0);
970     gst_structure_get_int (s, "rowstride", &self->stride);
971     self->outsize = gst_video_format_get_size (GST_VIDEO_FORMAT_NV12,
972         self->stride, self->padded_height);
974     GST_INFO_OBJECT (self, "outsize %d stride %d outcaps: %" GST_PTR_FORMAT,
975         self->outsize, self->stride, outcaps);
977     gst_pad_set_caps (self->srcpad, outcaps);
979     if (GST_BUFFER_SIZE (outbuf) != self->outsize) {
980       GST_INFO_OBJECT (self, "dropping buffer (bufsize %d != outsize %d)",
981           GST_BUFFER_SIZE (outbuf), self->outsize);
982       gst_buffer_unref (outbuf);
983       goto allocate_buffer;
984     }
985   }
987   if (G_UNLIKELY (!self->codec)) {
988     if (!codec_create (self)) {
989       GST_ERROR_OBJECT (self, "could not create codec");
990       gst_buffer_unref (buf);
991       gst_buffer_unref (outbuf);
992       return GST_FLOW_ERROR;
993     }
994   }
996   GST_BUFFER_TIMESTAMP (outbuf) = GST_BUFFER_TIMESTAMP (buf);
997   GST_BUFFER_DURATION (outbuf) = GST_BUFFER_DURATION (buf);
999   /* Pass new output buffer to the decoder to decode into. Use buffers from the
1000    * internal pool while self->first_out_buffer == TRUE in order to simplify
1001    * things in case we need to renegotiate */
1002   self->inArgs->inputID =
1003       codec_prepare_outbuf (self, &outbuf, self->first_out_buffer);
1004   if (!self->inArgs->inputID) {
1005     GST_ERROR_OBJECT (self, "could not prepare output buffer");
1006     gst_buffer_unref (buf);
1007     return GST_FLOW_ERROR;
1008   }
1010 have_out_buf:
1011   self->in_size = 0;
1012   buf = GST_DUCATIVIDDEC_GET_CLASS (self)->push_input (self, buf);
1014   if (ts != GST_CLOCK_TIME_NONE) {
1015     self->dts_queue[self->dts_widx++ % NDTS] = ts;
1016     /* if next buffer has earlier ts than previous, then the ts
1017      * we are getting are definitely decode order (DTS):
1018      */
1019     if ((self->last_dts != GST_CLOCK_TIME_NONE) && (self->last_dts > ts)) {
1020       GST_DEBUG_OBJECT (self, "input timestamp definitely DTS");
1021       self->ts_may_be_pts = FALSE;
1022     }
1023     self->last_dts = ts;
1024   }
1026   if (self->in_size == 0 && outbuf) {
1027     GST_DEBUG_OBJECT (self, "no input, skipping process");
1028     gst_buffer_unref (outbuf);
1029     return GST_FLOW_OK;
1030   }
1032   self->inArgs->numBytes = self->in_size;
1033   self->inBufs->descs[0].bufSize.bytes = self->in_size;
1034   self->inBufs->descs[0].memType = XDM_MEMTYPE_BO;
1036   err = codec_process (self, TRUE, FALSE, &ret);
1037   if (err) {
1038     GST_ELEMENT_ERROR (self, STREAM, DECODE, (NULL),
1039         ("process returned error: %d %08x", err, self->outArgs->extendedError));
1040     gst_ducati_log_extended_error_info (self->outArgs->extendedError);
1041     return GST_FLOW_ERROR;
1042   }
1043   if (ret != GST_FLOW_OK) {
1044     GST_WARNING_OBJECT (self, "push from codec_process failed %s",
1045         gst_flow_get_name (ret));
1046     return ret;
1047   }
1049   self->first_in_buffer = FALSE;
1051   if (self->outArgs->outBufsInUseFlag) {
1052     GST_DEBUG_OBJECT (self, "outBufsInUseFlag set");
1053     self->need_out_buf = FALSE;
1054   } else {
1055     self->need_out_buf = TRUE;
1056   }
1058   if (buf) {
1059     GST_DEBUG_OBJECT (self, "found remaining data: %d bytes",
1060         GST_BUFFER_SIZE (buf));
1061     ts = GST_BUFFER_TIMESTAMP (buf);
1062     goto allocate_buffer;
1063   }
1065   return GST_FLOW_OK;
1068 static gboolean
1069 gst_ducati_viddec_event (GstPad * pad, GstEvent * event)
1071   GstDucatiVidDec *self = GST_DUCATIVIDDEC (GST_OBJECT_PARENT (pad));
1072   gboolean ret = TRUE;
1074   GST_DEBUG_OBJECT (self, "begin: event=%s", GST_EVENT_TYPE_NAME (event));
1076   switch (GST_EVENT_TYPE (event)) {
1077     case GST_EVENT_NEWSEGMENT:
1078     {
1079       gboolean update;
1080       GstFormat fmt;
1081       gint64 start, stop, time;
1082       gdouble rate, arate;
1084       gst_event_parse_new_segment_full (event, &update, &rate, &arate, &fmt,
1085           &start, &stop, &time);
1086       gst_segment_set_newsegment_full (&self->segment, update,
1087           rate, arate, fmt, start, stop, time);
1088       break;
1089     }
1090     case GST_EVENT_EOS:
1091       if (!gst_ducati_viddec_codec_flush (self, TRUE)) {
1092         GST_ERROR_OBJECT (self, "could not flush on eos");
1093         ret = FALSE;
1094       }
1095       break;
1096     case GST_EVENT_FLUSH_STOP:
1097       if (!gst_ducati_viddec_codec_flush (self, FALSE)) {
1098         GST_ERROR_OBJECT (self, "could not flush");
1099         gst_event_unref (event);
1100         ret = FALSE;
1101       }
1102       gst_segment_init (&self->segment, GST_FORMAT_UNDEFINED);
1103       self->qos_earliest_time = GST_CLOCK_TIME_NONE;
1104       self->qos_proportion = 1;
1105       self->need_out_buf = TRUE;
1106       break;
1107     default:
1108       break;
1109   }
1111   if (ret)
1112     ret = gst_pad_push_event (self->srcpad, event);
1113   GST_LOG_OBJECT (self, "end");
1115   return ret;
1118 static gboolean
1119 gst_ducati_viddec_src_event (GstPad * pad, GstEvent * event)
1121   GstDucatiVidDec *self = GST_DUCATIVIDDEC (GST_OBJECT_PARENT (pad));
1122   gboolean ret = TRUE;
1124   GST_LOG_OBJECT (self, "begin: event=%s", GST_EVENT_TYPE_NAME (event));
1126   switch (GST_EVENT_TYPE (event)) {
1127     case GST_EVENT_QOS:
1128     {
1129       gdouble proportion;
1130       GstClockTimeDiff diff;
1131       GstClockTime timestamp;
1133       gst_event_parse_qos (event, &proportion, &diff, &timestamp);
1135       GST_OBJECT_LOCK (self);
1136       self->qos_proportion = proportion;
1137       self->qos_earliest_time = timestamp + 2 * diff;
1138       GST_OBJECT_UNLOCK (self);
1140       GST_DEBUG_OBJECT (self,
1141           "got QoS proportion %f %" GST_TIME_FORMAT ", %" G_GINT64_FORMAT,
1142           proportion, GST_TIME_ARGS (timestamp), diff);
1144       ret = gst_pad_push_event (self->sinkpad, event);
1145       break;
1146     }
1147     default:
1148       ret = gst_pad_push_event (self->sinkpad, event);
1149       break;
1150   }
1152   GST_LOG_OBJECT (self, "end");
1154   return ret;
1157 static GstStateChangeReturn
1158 gst_ducati_viddec_change_state (GstElement * element, GstStateChange transition)
1160   GstStateChangeReturn ret = GST_STATE_CHANGE_SUCCESS;
1161   GstDucatiVidDec *self = GST_DUCATIVIDDEC (element);
1162   gboolean supported;
1164   GST_DEBUG_OBJECT (self, "begin: changing state %s -> %s",
1165       gst_element_state_get_name (GST_STATE_TRANSITION_CURRENT (transition)),
1166       gst_element_state_get_name (GST_STATE_TRANSITION_NEXT (transition)));
1168   switch (transition) {
1169     case GST_STATE_CHANGE_NULL_TO_READY:
1170       if (!engine_open (self)) {
1171         GST_ERROR_OBJECT (self, "could not open");
1172         return GST_STATE_CHANGE_FAILURE;
1173       }
1174       /* try to create/destroy the codec here, it may not be supported */
1175       supported = codec_create (self);
1176       codec_delete (self);
1177       self->codec = NULL;
1178       if (!supported) {
1179         GST_ERROR_OBJECT (element, "Failed to create codec %s, not supported",
1180             GST_DUCATIVIDDEC_GET_CLASS (self)->codec_name);
1181         engine_close (self);
1182         return GST_STATE_CHANGE_FAILURE;
1183       }
1184       break;
1185     default:
1186       break;
1187   }
1189   ret = GST_ELEMENT_CLASS (parent_class)->change_state (element, transition);
1191   if (ret == GST_STATE_CHANGE_FAILURE)
1192     goto leave;
1194   switch (transition) {
1195     case GST_STATE_CHANGE_PAUSED_TO_READY:
1196       self->interlaced = FALSE;
1197       self->send_crop_event = TRUE;
1198       gst_ducati_viddec_codec_flush (self, FALSE);
1199       break;
1200     case GST_STATE_CHANGE_READY_TO_NULL:
1201       codec_delete (self);
1202       engine_close (self);
1203       break;
1204     default:
1205       break;
1206   }
1208 leave:
1209   GST_LOG_OBJECT (self, "end");
1211   return ret;
1214 /* GObject vmethod implementations */
1216 #define VERSION_LENGTH 256
1218 static void
1219 gst_ducati_viddec_get_property (GObject * obj,
1220     guint prop_id, GValue * value, GParamSpec * pspec)
1222   GstDucatiVidDec *self = GST_DUCATIVIDDEC (obj);
1225   switch (prop_id) {
1226     case PROP_VERSION:{
1227       int err;
1228       char *version = NULL;
1230       if (!self->engine)
1231         engine_open (self);
1233       if (!self->codec)
1234         codec_create (self);
1236       if (self->codec) {
1237         version = dce_alloc (VERSION_LENGTH);
1238         self->status->data.buf = (XDAS_Int8 *) version;
1239         self->status->data.bufSize = VERSION_LENGTH;
1241         err = VIDDEC3_control (self->codec, XDM_GETVERSION,
1242             self->dynParams, self->status);
1243         if (err) {
1244           GST_ERROR_OBJECT (self, "failed XDM_GETVERSION");
1245         }
1247         self->status->data.buf = NULL;
1248         self->status->data.bufSize = 0;
1249       }
1251       g_value_set_string (value, version);
1252       if (version)
1253         dce_free (version);
1255       break;
1256     }
1257     default:{
1258       G_OBJECT_WARN_INVALID_PROPERTY_ID (obj, prop_id, pspec);
1259       break;
1260     }
1261   }
1264 static void
1265 gst_ducati_viddec_finalize (GObject * obj)
1267   GstDucatiVidDec *self = GST_DUCATIVIDDEC (obj);
1269   codec_delete (self);
1270   engine_close (self);
1272   if (self->codec_data) {
1273     gst_buffer_unref (self->codec_data);
1274     self->codec_data = NULL;
1275   }
1277   G_OBJECT_CLASS (parent_class)->finalize (obj);
1280 static void
1281 gst_ducati_viddec_base_init (gpointer gclass)
1283   GstElementClass *element_class = GST_ELEMENT_CLASS (gclass);
1285   gst_element_class_add_pad_template (element_class,
1286       gst_static_pad_template_get (&src_factory));
1289 static void
1290 gst_ducati_viddec_class_init (GstDucatiVidDecClass * klass)
1292   GObjectClass *gobject_class = G_OBJECT_CLASS (klass);
1293   GstElementClass *gstelement_class = GST_ELEMENT_CLASS (klass);
1295   gobject_class->get_property =
1296       GST_DEBUG_FUNCPTR (gst_ducati_viddec_get_property);
1297   gobject_class->finalize = GST_DEBUG_FUNCPTR (gst_ducati_viddec_finalize);
1298   gstelement_class->change_state =
1299       GST_DEBUG_FUNCPTR (gst_ducati_viddec_change_state);
1301   klass->parse_caps = GST_DEBUG_FUNCPTR (gst_ducati_viddec_parse_caps);
1302   klass->allocate_params =
1303       GST_DEBUG_FUNCPTR (gst_ducati_viddec_allocate_params);
1304   klass->push_input = GST_DEBUG_FUNCPTR (gst_ducati_viddec_push_input);
1305   klass->handle_error = GST_DEBUG_FUNCPTR (gst_ducati_viddec_handle_error);
1306   klass->drop_frame = GST_DEBUG_FUNCPTR (gst_ducati_viddec_drop_frame);
1307   klass->query = GST_DEBUG_FUNCPTR (gst_ducati_viddec_query);
1309   g_object_class_install_property (gobject_class, PROP_VERSION,
1310       g_param_spec_string ("version", "Version",
1311           "The codec version string", "",
1312           G_PARAM_READABLE | G_PARAM_STATIC_STRINGS));
1315 static void
1316 gst_ducati_viddec_init (GstDucatiVidDec * self, GstDucatiVidDecClass * klass)
1318   GstElementClass *gstelement_class = GST_ELEMENT_CLASS (klass);
1320   self->sinkpad =
1321       gst_pad_new_from_template (gst_element_class_get_pad_template
1322       (gstelement_class, "sink"), "sink");
1323   gst_pad_set_setcaps_function (self->sinkpad,
1324       GST_DEBUG_FUNCPTR (gst_ducati_viddec_sink_setcaps));
1325   gst_pad_set_chain_function (self->sinkpad,
1326       GST_DEBUG_FUNCPTR (gst_ducati_viddec_chain));
1327   gst_pad_set_event_function (self->sinkpad,
1328       GST_DEBUG_FUNCPTR (gst_ducati_viddec_event));
1330   self->srcpad = gst_pad_new_from_static_template (&src_factory, "src");
1331   gst_pad_set_event_function (self->srcpad,
1332       GST_DEBUG_FUNCPTR (gst_ducati_viddec_src_event));
1333   gst_pad_set_query_function (self->srcpad,
1334       GST_DEBUG_FUNCPTR (gst_ducati_viddec_src_query));
1335   gst_pad_set_getcaps_function (self->srcpad,
1336       GST_DEBUG_FUNCPTR (gst_ducati_viddec_src_getcaps));
1338   gst_element_add_pad (GST_ELEMENT (self), self->sinkpad);
1339   gst_element_add_pad (GST_ELEMENT (self), self->srcpad);
1341   self->input_width = 0;
1342   self->input_height = 0;
1343   /* sane defaults in case we need to create codec without caps negotiation
1344    * (for example, to get 'version' property)
1345    */
1346   self->width = 128;
1347   self->height = 128;
1348   self->fps_n = -1;
1349   self->fps_d = -1;
1351   self->first_in_buffer = TRUE;
1352   self->first_out_buffer = TRUE;
1353   self->interlaced = FALSE;
1354   self->send_crop_event = TRUE;
1356   self->dts_ridx = self->dts_widx = 0;
1357   self->last_dts = self->last_pts = GST_CLOCK_TIME_NONE;
1358   self->ts_may_be_pts = TRUE;
1359   self->ts_is_pts = FALSE;
1361   self->pageMemType = XDM_MEMTYPE_TILEDPAGE;
1363   gst_segment_init (&self->segment, GST_FORMAT_UNDEFINED);
1365   self->qos_proportion = 1;
1366   self->qos_earliest_time = GST_CLOCK_TIME_NONE;
1367   self->wait_keyframe = TRUE;
1369   self->need_out_buf = TRUE;
1370   self->device = NULL;
1371   self->input_bo = NULL;