ducatividdec: remove another leftover -strided caps remnant
[glsdk/gst-plugin-ducati.git] / src / gstducatividdec.h
1 /*
2  * GStreamer
3  * Copyright (c) 2010, Texas Instruments Incorporated
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Lesser General Public
7  * License as published by the Free Software Foundation
8  * version 2.1 of the License.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13  * Lesser General Public License for more details.
14  *
15  * You should have received a copy of the GNU Lesser General Public
16  * License along with this library; if not, write to the Free Software
17  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
18  */
20 #ifndef __GST_DUCATIVIDDEC_H__
21 #define __GST_DUCATIVIDDEC_H__
23 #include <stdint.h>
24 #include <stddef.h>
25 #include <omap_drm.h>
26 #include <omap_drmif.h>
28 #include "gstducati.h"
29 #include "gstducatibufferpriv.h"
31 #include <gst/drm/gstdrmbufferpool.h>
32 #include <gst/video/video.h>
33 #include <gst/video/video-crop.h>
35 G_BEGIN_DECLS
37 #define GST_TYPE_DUCATIVIDDEC               (gst_ducati_viddec_get_type())
38 #define GST_DUCATIVIDDEC(obj)               (G_TYPE_CHECK_INSTANCE_CAST((obj), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDec))
39 #define GST_DUCATIVIDDEC_CLASS(klass)       (G_TYPE_CHECK_CLASS_CAST((klass), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDecClass))
40 #define GST_IS_DUCATIVIDDEC(obj)            (G_TYPE_CHECK_INSTANCE_TYPE((obj), GST_TYPE_DUCATIVIDDEC))
41 #define GST_IS_DUCATIVIDDEC_CLASS(klass)    (G_TYPE_CHECK_CLASS_TYPE((klass), GST_TYPE_DUCATIVIDDEC))
42 #define GST_DUCATIVIDDEC_GET_CLASS(obj)     (G_TYPE_INSTANCE_GET_CLASS((obj), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDecClass))
44 typedef struct _GstDucatiVidDec      GstDucatiVidDec;
45 typedef struct _GstDucatiVidDecClass GstDucatiVidDecClass;
47 #define MAX_BACKLOG_FRAMES 16
49 struct _GstDucatiVidDec
50 {
51   GstElement parent;
53   GstPad *sinkpad, *srcpad;
55   GstDRMBufferPool *pool;
57   /* minimum output size required by the codec: */
58   gint outsize;
60   /* minimum number of buffers required by the codec: */
61   gint min_buffers;
63   /* input (unpadded, unaligned) size of video: */
64   gint input_width, input_height;
66   /* input (unpadded, aligned to MB) size of video: */
67   gint width, height;
69   gint fps_n, fps_d;
71   /* output (padded) size including any codec padding: */
72   gint padded_width, padded_height;
74   /* output stride (>= padded_width) */
75   gint stride;
77   gboolean interlaced;
79   struct omap_bo *input_bo;
80   /* input buffer, allocated when codec is created: */
81   guint8 *input;
83   /* number of bytes pushed to input on current frame: */
84   gint in_size;
86   /* the crop to attach to output buffers: */
87   GstVideoCrop *crop;
89   /* on first output buffer, we need to send crop info to sink.. and some
90    * operations like flushing should be avoided if we haven't sent any
91    * input buffers:
92    */
93   gboolean first_out_buffer, first_in_buffer;
94   gboolean send_crop_event;
96   GstSegment segment;
97   gdouble qos_proportion;
98   GstClockTime qos_earliest_time;
100   gboolean need_out_buf;
102   /* by default, codec_data from sinkpad is prepended to first buffer: */
103   GstBuffer *codec_data;
105   /* workaround enabled to indicate that timestamp from demuxer is PTS,
106    * not DTS (cough, cough.. avi):
107    */
108   gboolean ts_is_pts;
110   /* auto-detection for ts_is_pts workaround.. if we detect out of order
111    * timestamps from demuxer/parser, then the ts is definitely DTS,
112    * otherwise it may be PTS and out of order timestamps out of decoder
113    * will trigger the ts_is_pts workaround.
114    */
115   gboolean ts_may_be_pts;
117   gboolean wait_keyframe;
119   gboolean needs_flushing;
121   GHashTable *passed_in_bufs;
123 #define NDTS 32
124   GstClockTime dts_queue[NDTS];
125   gint dts_ridx, dts_widx;
126   GstClockTime last_dts, last_pts;
128   Engine_Handle           engine;
129   VIDDEC3_Handle          codec;
130   VIDDEC3_Params         *params;
131   VIDDEC3_DynamicParams  *dynParams;
132   VIDDEC3_Status         *status;
133   XDM2_BufDesc           *inBufs;
134   XDM2_BufDesc           *outBufs;
135   VIDDEC3_InArgs         *inArgs;
136   VIDDEC3_OutArgs        *outArgs;
138   XDAS_Int16 pageMemType;
139   struct omap_device *device;
141   /* Frames waiting to be reordered */
142   GstBuffer *backlog_frames[MAX_BACKLOG_FRAMES + 1];
143   gint backlog_maxframes;
144   gint backlog_nframes;
145   gint backlog_max_maxframes;
146 };
148 struct _GstDucatiVidDecClass
150   GstElementClass parent_class;
152   const gchar *codec_name;
154   /**
155    * Parse codec specific fields the given caps structure.  The base-
156    * class implementation of this method handles standard stuff like
157    * width/height/framerate/codec_data.
158    */
159   gboolean (*parse_caps) (GstDucatiVidDec * self, GstStructure * s);
161   /**
162    * Called when the input buffer size changes, to recalculate codec required
163    * output buffer size and minimum count
164    */
165   void (*update_buffer_size) (GstDucatiVidDec * self);
167   /**
168    * Called to allocate/initialize  params/dynParams/status/inArgs/outArgs
169    */
170   gboolean (*allocate_params) (GstDucatiVidDec * self, gint params_sz,
171       gint dynparams_sz, gint status_sz, gint inargs_sz, gint outargs_sz);
173   /**
174    * Push input data into codec's input buffer, returning a sub-buffer of
175    * any remaining data, or NULL if none.  Consumes reference to 'buf'
176    */
177   GstBuffer * (*push_input) (GstDucatiVidDec * self, GstBuffer * buf);
179   /**
180    * Called to handle errors returned by VIDDEC3_process.
181    */
182   gint (*handle_error) (GstDucatiVidDec * self, gint ret, gint extended_error,
183       gint status_extended_error);
185   /**
186    * Called to check whether it's a good idea to drop buf or not.
187    */
188   gboolean (*can_drop_frame) (GstDucatiVidDec * self, GstBuffer * buf, gint64 diff);
190   gboolean (*query) (GstDucatiVidDec * self, GstPad * pad, GstQuery * query,
191       gboolean * forward);
193   /**
194    * Called to push a decoder buffer. Consumes reference to 'buf'.
195    */
196   GstFlowReturn (*push_output) (GstDucatiVidDec * self, GstBuffer * buf);
198   /**
199    * Called before a flush happens.
200    */
201   void (*on_flush) (GstDucatiVidDec * self, gboolean eos);
203   /**
204    * Called to set new caps on the sink pad.
205    */
206   gboolean (*set_sink_caps) (GstDucatiVidDec * self, GstCaps *caps);
207 };
209 GType gst_ducati_viddec_get_type (void);
211 /* helper methods for derived classes: */
213 static inline void
214 push_input (GstDucatiVidDec * self, const guint8 *in, gint sz)
216   GST_DEBUG_OBJECT (self, "push: %d bytes)", sz);
217   memcpy (self->input + self->in_size, in, sz);
218   self->in_size += sz;
221 static inline int
222 check_start_code (const guint8 *sc, gint scsize,
223     const guint8 *inbuf, gint insize)
225   if (insize < scsize)
226     return FALSE;
228   while (scsize) {
229     if (*sc != *inbuf)
230       return FALSE;
231     scsize--;
232     sc++;
233     inbuf++;
234   }
236   return TRUE;
239 static inline int
240 find_start_code (const guint8 *sc, gint scsize,
241     const guint8 *inbuf, gint insize)
243   gint size = 0;
244   while (insize) {
245     if (check_start_code (sc, scsize, inbuf, insize))
246       break;
247     insize--;
248     size++;
249     inbuf++;
250   }
251   return size;
254 gboolean
255 gst_ducati_viddec_codec_flush (GstDucatiVidDec * self, gboolean eos);
257 G_END_DECLS
259 #endif /* __GST_DUCATIVIDDEC_H__ */