ducatividdec: move frame reordering to the base class
[glsdk/gst-plugin-ducati.git] / src / gstducatividdec.h
1 /*
2  * GStreamer
3  * Copyright (c) 2010, Texas Instruments Incorporated
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Lesser General Public
7  * License as published by the Free Software Foundation
8  * version 2.1 of the License.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
13  * Lesser General Public License for more details.
14  *
15  * You should have received a copy of the GNU Lesser General Public
16  * License along with this library; if not, write to the Free Software
17  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301  USA
18  */
20 #ifndef __GST_DUCATIVIDDEC_H__
21 #define __GST_DUCATIVIDDEC_H__
23 #include <stdint.h>
24 #include <stddef.h>
25 #include <omap_drm.h>
26 #include <omap_drmif.h>
28 #include "gstducati.h"
29 #include "gstducatibufferpriv.h"
31 #include <gst/drm/gstdrmbufferpool.h>
32 #include <gst/video/video.h>
33 #include <gst/video/video-crop.h>
35 G_BEGIN_DECLS
37 #define GST_TYPE_DUCATIVIDDEC               (gst_ducati_viddec_get_type())
38 #define GST_DUCATIVIDDEC(obj)               (G_TYPE_CHECK_INSTANCE_CAST((obj), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDec))
39 #define GST_DUCATIVIDDEC_CLASS(klass)       (G_TYPE_CHECK_CLASS_CAST((klass), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDecClass))
40 #define GST_IS_DUCATIVIDDEC(obj)            (G_TYPE_CHECK_INSTANCE_TYPE((obj), GST_TYPE_DUCATIVIDDEC))
41 #define GST_IS_DUCATIVIDDEC_CLASS(klass)    (G_TYPE_CHECK_CLASS_TYPE((klass), GST_TYPE_DUCATIVIDDEC))
42 #define GST_DUCATIVIDDEC_GET_CLASS(obj)     (G_TYPE_INSTANCE_GET_CLASS((obj), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDecClass))
44 typedef struct _GstDucatiVidDec      GstDucatiVidDec;
45 typedef struct _GstDucatiVidDecClass GstDucatiVidDecClass;
47 #define MAX_BACKLOG_FRAMES 16
49 struct _GstDucatiVidDec
50 {
51   GstElement parent;
53   GstPad *sinkpad, *srcpad;
55   GstDRMBufferPool *pool;
57   /* minimum output size required by the codec: */
58   gint outsize;
60   /* minimum number of buffers required by the codec: */
61   gint min_buffers;
63   /* input (unpadded, unaligned) size of video: */
64   gint input_width, input_height;
66   /* input (unpadded, aligned to MB) size of video: */
67   gint width, height;
69   gint fps_n, fps_d;
71   /* output (padded) size including any codec padding: */
72   gint padded_width, padded_height;
74   /* output stride (>= padded_width) */
75   gint stride;
77   gboolean interlaced;
79   struct omap_bo *input_bo;
80   /* input buffer, allocated when codec is created: */
81   guint8 *input;
83   /* number of bytes pushed to input on current frame: */
84   gint in_size;
86   /* the crop to attach to output buffers: */
87   GstVideoCrop *crop;
89   /* on first output buffer, we need to send crop info to sink.. and some
90    * operations like flushing should be avoided if we haven't sent any
91    * input buffers:
92    */
93   gboolean first_out_buffer, first_in_buffer;
94   gboolean send_crop_event;
96   GstSegment segment;
97   gdouble qos_proportion;
98   GstClockTime qos_earliest_time;
100   gboolean need_out_buf;
102   /* by default, codec_data from sinkpad is prepended to first buffer: */
103   GstBuffer *codec_data;
105   /* workaround enabled to indicate that timestamp from demuxer is PTS,
106    * not DTS (cough, cough.. avi):
107    */
108   gboolean ts_is_pts;
110   /* auto-detection for ts_is_pts workaround.. if we detect out of order
111    * timestamps from demuxer/parser, then the ts is definitely DTS,
112    * otherwise it may be PTS and out of order timestamps out of decoder
113    * will trigger the ts_is_pts workaround.
114    */
115   gboolean ts_may_be_pts;
117   gboolean wait_keyframe;
119   gboolean needs_flushing;
121   GHashTable *passed_in_bufs;
123 #define NDTS 32
124   GstClockTime dts_queue[NDTS];
125   gint dts_ridx, dts_widx;
126   GstClockTime last_dts, last_pts;
128   Engine_Handle           engine;
129   VIDDEC3_Handle          codec;
130   VIDDEC3_Params         *params;
131   VIDDEC3_DynamicParams  *dynParams;
132   VIDDEC3_Status         *status;
133   XDM2_BufDesc           *inBufs;
134   XDM2_BufDesc           *outBufs;
135   VIDDEC3_InArgs         *inArgs;
136   VIDDEC3_OutArgs        *outArgs;
138   XDAS_Int16 pageMemType;
139   struct omap_device *device;
141   /* Frames waiting to be reordered */
142   GstBuffer *backlog_frames[MAX_BACKLOG_FRAMES + 1];
143   gint backlog_maxframes;
144   gint backlog_nframes;
145 };
147 struct _GstDucatiVidDecClass
149   GstElementClass parent_class;
151   const gchar *codec_name;
153   /**
154    * Parse codec specific fields the given caps structure.  The base-
155    * class implementation of this method handles standard stuff like
156    * width/height/framerate/codec_data.
157    */
158   gboolean (*parse_caps) (GstDucatiVidDec * self, GstStructure * s);
160   /**
161    * Called when the input buffer size changes, to recalculate codec required
162    * output buffer size and minimum count
163    */
164   void (*update_buffer_size) (GstDucatiVidDec * self);
166   /**
167    * Called to allocate/initialize  params/dynParams/status/inArgs/outArgs
168    */
169   gboolean (*allocate_params) (GstDucatiVidDec * self, gint params_sz,
170       gint dynparams_sz, gint status_sz, gint inargs_sz, gint outargs_sz);
172   /**
173    * Push input data into codec's input buffer, returning a sub-buffer of
174    * any remaining data, or NULL if none.  Consumes reference to 'buf'
175    */
176   GstBuffer * (*push_input) (GstDucatiVidDec * self, GstBuffer * buf);
178   /**
179    * Called to handle errors returned by VIDDEC3_process.
180    */
181   gint (*handle_error) (GstDucatiVidDec * self, gint ret, gint extended_error,
182       gint status_extended_error);
184   /**
185    * Called to check whether it's a good idea to drop buf or not.
186    */
187   gboolean (*can_drop_frame) (GstDucatiVidDec * self, GstBuffer * buf, gint64 diff);
189   gboolean (*query) (GstDucatiVidDec * self, GstPad * pad, GstQuery * query,
190       gboolean * forward);
192   /**
193    * Called to push a decoder buffer. Consumes reference to 'buf'.
194    */
195   GstFlowReturn (*push_output) (GstDucatiVidDec * self, GstBuffer * buf);
197   /**
198    * Called before a flush happens.
199    */
200   void (*on_flush) (GstDucatiVidDec * self, gboolean eos);
202   /**
203    * Called to set new caps on the sink pad.
204    */
205   gboolean (*set_sink_caps) (GstDucatiVidDec * self, GstCaps *caps);
206 };
208 GType gst_ducati_viddec_get_type (void);
210 /* helper methods for derived classes: */
212 static inline void
213 push_input (GstDucatiVidDec * self, const guint8 *in, gint sz)
215   GST_DEBUG_OBJECT (self, "push: %d bytes)", sz);
216   memcpy (self->input + self->in_size, in, sz);
217   self->in_size += sz;
220 static inline int
221 check_start_code (const guint8 *sc, gint scsize,
222     const guint8 *inbuf, gint insize)
224   if (insize < scsize)
225     return FALSE;
227   while (scsize) {
228     if (*sc != *inbuf)
229       return FALSE;
230     scsize--;
231     sc++;
232     inbuf++;
233   }
235   return TRUE;
238 static inline int
239 find_start_code (const guint8 *sc, gint scsize,
240     const guint8 *inbuf, gint insize)
242   gint size = 0;
243   while (insize) {
244     if (check_start_code (sc, scsize, inbuf, insize))
245       break;
246     insize--;
247     size++;
248     inbuf++;
249   }
250   return size;
253 gboolean
254 gst_ducati_viddec_codec_flush (GstDucatiVidDec * self, gboolean eos);
256 G_END_DECLS
258 #endif /* __GST_DUCATIVIDDEC_H__ */