/* * GStreamer * Copyright (c) 2010, Texas Instruments Incorporated * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Lesser General Public * License as published by the Free Software Foundation * version 2.1 of the License. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Lesser General Public License for more details. * * You should have received a copy of the GNU Lesser General Public * License along with this library; if not, write to the Free Software * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA */ #ifdef HAVE_CONFIG_H # include #endif #include #include "gstducatih264dec.h" #include "gstducatimpeg4dec.h" #include "gstducativc1dec.h" #include "gstducativp6dec.h" GST_DEBUG_CATEGORY (gst_ducati_debug); static gboolean plugin_init (GstPlugin * plugin) { GST_DEBUG_CATEGORY_INIT (gst_ducati_debug, "ducati", 0, "ducati"); /* TODO .. find some way to reasonably detect if the corresponding * codecs are actually available.. */ return gst_element_register (plugin, "ducatih264dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIH264DEC) && gst_element_register (plugin, "ducatimpeg4dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIMPEG4DEC) && gst_element_register (plugin, "ducativc1dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIVC1DEC) && gst_element_register (plugin, "ducativp6dec", GST_RANK_PRIMARY, GST_TYPE_DUCATIVP6DEC); } void * gst_ducati_alloc_1d (gint sz) { MemAllocBlock block = { .pixelFormat = PIXEL_FMT_PAGE, .dim.len = sz, }; return MemMgr_Alloc (&block, 1); } void * gst_ducati_alloc_2d (gint width, gint height) { MemAllocBlock block[] = { { .pixelFormat = PIXEL_FMT_8BIT, .dim = {.area = { .width = width, .height = height, }} }, { .pixelFormat = PIXEL_FMT_16BIT, .dim = {.area = { .width = width, .height = height / 2, }} } }; return MemMgr_Alloc (block, 2); } XDAS_Int16 gst_ducati_get_mem_type (SSPtr paddr) { if ((0x60000000 <= paddr) && (paddr < 0x68000000)) return XDM_MEMTYPE_TILED8; if ((0x68000000 <= paddr) && (paddr < 0x70000000)) return XDM_MEMTYPE_TILED16; if ((0x70000000 <= paddr) && (paddr < 0x78000000)) return XDM_MEMTYPE_TILED32; if ((0x78000000 <= paddr) && (paddr < 0x80000000)) return XDM_MEMTYPE_RAW; return -1; } /* PACKAGE: this is usually set by autotools depending on some _INIT macro * in configure.ac and then written into and defined in config.h, but we can * just set it ourselves here in case someone doesn't use autotools to * compile this code. GST_PLUGIN_DEFINE needs PACKAGE to be defined. */ #ifndef PACKAGE # define PACKAGE "ducati" #endif GST_PLUGIN_DEFINE ( GST_VERSION_MAJOR, GST_VERSION_MINOR, "ducati", "Hardware accellerated codecs for OMAP4", plugin_init, VERSION, "LGPL", "GStreamer", "http://gstreamer.net/" )