/*
* GStreamer
* Copyright (c) 2010, Texas Instruments Incorporated
*
* This library is free software; you can redistribute it and/or
* modify it under the terms of the GNU Lesser General Public
* License as published by the Free Software Foundation
* version 2.1 of the License.
*
* This library is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
* Lesser General Public License for more details.
*
* You should have received a copy of the GNU Lesser General Public
* License along with this library; if not, write to the Free Software
* Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA
*/
/**
* SECTION:element-ducatijpegdec
*
* FIXME:Describe ducatijpegdec here.
*
*
* Example launch line
* |[
* gst-launch -v -m fakesrc ! ducatijpegdec ! fakesink silent=TRUE
* ]|
*
*/
#ifdef HAVE_CONFIG_H
# include
#endif
#include "gstducatijpegdec.h"
GST_BOILERPLATE (GstDucatiJpegDec, gst_ducati_jpegdec, GstDucatiVidDec,
GST_TYPE_DUCATIVIDDEC);
static GstStaticPadTemplate sink_factory = GST_STATIC_PAD_TEMPLATE ("sink",
GST_PAD_SINK,
GST_PAD_ALWAYS,
GST_STATIC_CAPS ("image/jpeg, "
"parsed = (boolean)true, "
"width = (int)[ 32, 4096 ], "
"height = (int)[ 32, 4096 ], " "framerate = (fraction)[ 0, max ];")
);
/* GstDucatiVidDec vmethod implementations */
static void
gst_ducati_jpegdec_update_buffer_size (GstDucatiVidDec * self)
{
gint w = self->width;
gint h = self->height;
/* calculate output buffer parameters: */
self->padded_width = w;
self->padded_height = h;
self->min_buffers = 1;
}
static gboolean
gst_ducati_jpegdec_allocate_params (GstDucatiVidDec * self, gint params_sz,
gint dynparams_sz, gint status_sz, gint inargs_sz, gint outargs_sz)
{
IJPEGVDEC_DynamicParams *dynParams;
gboolean ret = parent_class->allocate_params (self,
sizeof (IJPEGVDEC_Params), sizeof (IJPEGVDEC_DynamicParams),
sizeof (IJPEGVDEC_Status), sizeof (IJPEGVDEC_InArgs),
sizeof (IJPEGVDEC_OutArgs));
if (!ret)
return ret;
/* We're doing ENTIREFRAME decoding so in theory 0 should be a valid value
* for this. The codec seems to check that it's non-zero though...
*/
self->params->numOutputDataUnits = 1;
dynParams = (IJPEGVDEC_DynamicParams *) self->dynParams;
dynParams->decodeThumbnail = 0;
dynParams->thumbnailMode = 3;
dynParams->downsamplingFactor = 1;
dynParams->streamingCompliant = 0;
return ret;
}
/* GObject vmethod implementations */
static void
gst_ducati_jpegdec_base_init (gpointer gclass)
{
GstElementClass *element_class = GST_ELEMENT_CLASS (gclass);
gst_element_class_set_details_simple (element_class,
"DucatiJpegDec",
"Codec/Decoder/Video",
"Decodes video in MJPEG format with ducati",
"Alessandro Decina ");
gst_element_class_add_pad_template (element_class,
gst_static_pad_template_get (&sink_factory));
}
static void
gst_ducati_jpegdec_class_init (GstDucatiJpegDecClass * klass)
{
GstDucatiVidDecClass *bclass = GST_DUCATIVIDDEC_CLASS (klass);
bclass->codec_name = "ivahd_jpegvdec";
bclass->update_buffer_size =
GST_DEBUG_FUNCPTR (gst_ducati_jpegdec_update_buffer_size);
bclass->allocate_params =
GST_DEBUG_FUNCPTR (gst_ducati_jpegdec_allocate_params);
}
static void
gst_ducati_jpegdec_init (GstDucatiJpegDec * self,
GstDucatiJpegDecClass * gclass)
{
GstDucatiVidDec *vdec = GST_DUCATIVIDDEC (self);
vdec->pageMemType = XDM_MEMTYPE_RAW;
#ifndef GST_DISABLE_GST_DEBUG
vdec->error_strings[0] = "unsupported VIDDEC3 parameters";
vdec->error_strings[1] = "unsupported VIDDEC3 dynamic parameters";
vdec->error_strings[2] = "unsupported JPEGDEC dynamic parameters";
vdec->error_strings[3] = "no slice";
vdec->error_strings[4] = "MB data error";
vdec->error_strings[5] = "standby";
vdec->error_strings[6] = "invalid mbox message";
vdec->error_strings[7] = "HDVICP reset";
vdec->error_strings[16] = "HDVICP wait not clean exit";
vdec->error_strings[17] = "Frame header error";
vdec->error_strings[18] = "Scan header error";
vdec->error_strings[19] = "Huffman table header error";
vdec->error_strings[20] = "Quantization table header error";
vdec->error_strings[21] = "Bad chroma format";
vdec->error_strings[22] = "Unsupported marker";
vdec->error_strings[23] = "Thumbnail error";
vdec->error_strings[24] = "IRES handle error";
vdec->error_strings[25] = "Dynamic params handle error";
vdec->error_strings[26] = "Data sync error";
vdec->error_strings[27] = "Downsample input format error";
vdec->error_strings[28] = "Unsupported feature";
vdec->error_strings[29] = "Unsupported resolution";
#endif
}