/* * GStreamer * Copyright (c) 2010, Texas Instruments Incorporated * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Lesser General Public * License as published by the Free Software Foundation * version 2.1 of the License. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Lesser General Public License for more details. * * You should have received a copy of the GNU Lesser General Public * License along with this library; if not, write to the Free Software * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA */ #ifndef __GST_DUCATIVIDDEC_H__ #define __GST_DUCATIVIDDEC_H__ #include "gstducati.h" #include "gstducatibufferpool.h" #include G_BEGIN_DECLS #define GST_TYPE_DUCATIVIDDEC (gst_ducati_viddec_get_type()) #define GST_DUCATIVIDDEC(obj) (G_TYPE_CHECK_INSTANCE_CAST((obj), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDec)) #define GST_DUCATIVIDDEC_CLASS(klass) (G_TYPE_CHECK_CLASS_CAST((klass), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDecClass)) #define GST_IS_DUCATIVIDDEC(obj) (G_TYPE_CHECK_INSTANCE_TYPE((obj), GST_TYPE_DUCATIVIDDEC)) #define GST_IS_DUCATIVIDDEC_CLASS(klass) (G_TYPE_CHECK_CLASS_TYPE((klass), GST_TYPE_DUCATIVIDDEC)) #define GST_DUCATIVIDDEC_GET_CLASS(obj) (G_TYPE_INSTANCE_GET_CLASS((obj), GST_TYPE_DUCATIVIDDEC, GstDucatiVidDecClass)) typedef struct _GstDucatiVidDec GstDucatiVidDec; typedef struct _GstDucatiVidDecClass GstDucatiVidDecClass; struct _GstDucatiVidDec { GstElement parent; GstPad *sinkpad, *srcpad; GstDucatiBufferPool *pool; /* minimum output size required by the codec: */ gint outsize; /* minimum number of buffers required by the codec: */ gint min_buffers; /* input (unpadded, unaligned) size of video: */ gint input_width, input_height; /* input (unpadded, aligned to MB) size of video: */ gint width, height; /* output (padded) size including any codec padding: */ gint padded_width, padded_height; /* output stride (>= padded_width) */ gint stride; gboolean interlaced; /* input buffer, allocated when codec is created: */ guint8 *input; /* number of bytes pushed to input on current frame: */ gint in_size; /* on first output buffer, we need to send crop info to sink.. and some * operations like flushing should be avoided if we haven't sent any * input buffers: */ gboolean first_out_buffer, first_in_buffer; GstSegment segment; gdouble qos_proportion; GstClockTime qos_earliest_time; gboolean need_out_buf; /* by default, codec_data from sinkpad is prepended to first buffer: */ GstBuffer *codec_data; /* workaround enabled to indicate that timestamp from demuxer is PTS, * not DTS (cough, cough.. avi): */ gboolean ts_is_pts; /* auto-detection for ts_is_pts workaround.. if we detect out of order * timestamps from demuxer/parser, then the ts is definitely DTS, * otherwise it may be PTS and out of order timestamps out of decoder * will trigger the ts_is_pts workaround. */ gboolean ts_may_be_pts; #define NDTS 32 GstClockTime dts_queue[NDTS]; gint dts_ridx, dts_widx; GstClockTime last_dts, last_pts; Engine_Handle engine; VIDDEC3_Handle codec; VIDDEC3_Params *params; VIDDEC3_DynamicParams *dynParams; VIDDEC3_Status *status; XDM2_BufDesc *inBufs; XDM2_BufDesc *outBufs; VIDDEC3_InArgs *inArgs; VIDDEC3_OutArgs *outArgs; XDAS_Int16 pageMemType; }; struct _GstDucatiVidDecClass { GstElementClass parent_class; const gchar *codec_name; /** * Parse codec specific fields the given caps structure. The base- * class implementation of this method handles standard stuff like * width/height/framerate/codec_data. */ gboolean (*parse_caps) (GstDucatiVidDec * self, GstStructure * s); /** * Called when the input buffer size changes, to recalculate codec required * output buffer size and minimum count */ void (*update_buffer_size) (GstDucatiVidDec * self); /** * Called to allocate/initialize params/dynParams/status/inArgs/outArgs */ gboolean (*allocate_params) (GstDucatiVidDec * self, gint params_sz, gint dynparams_sz, gint status_sz, gint inargs_sz, gint outargs_sz); /** * Push input data into codec's input buffer, returning a sub-buffer of * any remaining data, or NULL if none. Consumes reference to 'buf' */ GstBuffer * (*push_input) (GstDucatiVidDec * self, GstBuffer * buf); /** * Called to handle errors returned by VIDDEC3_process. */ gint (*handle_error) (GstDucatiVidDec * self, gint ret, gint extended_error, gint status_extended_error); }; GType gst_ducati_viddec_get_type (void); /* helper methods for derived classes: */ static inline void push_input (GstDucatiVidDec * self, const guint8 *in, gint sz) { GST_DEBUG_OBJECT (self, "push: %d bytes)", sz); memcpy (self->input + self->in_size, in, sz); self->in_size += sz; } static inline int check_start_code (const guint8 *sc, gint scsize, const guint8 *inbuf, gint insize) { if (insize < scsize) return FALSE; while (scsize) { if (*sc != *inbuf) return FALSE; scsize--; sc++; inbuf++; } return TRUE; } static inline int find_start_code (const guint8 *sc, gint scsize, const guint8 *inbuf, gint insize) { gint size = 0; while (insize) { if (check_start_code (sc, scsize, inbuf, insize)) break; insize--; size++; inbuf++; } return size; } G_END_DECLS #endif /* __GST_DUCATIVIDDEC_H__ */