]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gst-plugin-ducati.git/history - src/gstducatividdec.c
ducativideodec: add a max-reorder-frames decoder property
[glsdk/gst-plugin-ducati.git] / src / gstducatividdec.c
2012-10-19 Vincent Penquerc'hducativideodec: add a max-reorder-frames decoder property
2012-10-15 Vincent Penquerc'hducatividdec: move frame reordering to the base class
2012-10-09 Vincent Penquerc'hducatih264dec: reorder buffers by picture order count
2012-10-02 Vincent Penquerc'hducatividdec: set number of out buffers to 0 when we...
2012-09-07 Vincent Penquerc'hducatividdec: do not tell ducati we pass input when...
2012-09-06 Thibault Saunierviddec: Add a lookup table between decoder arrays and...
2012-09-05 Thibault Saunierviddec: Do not rely on the decoder setting freeBufID...
2012-09-05 Thibault Saunierviddec: Pass through gst-indent
2012-08-03 Vincent Penquerc'hducatividdec: remove the interlaced MPEG2 half height...
2012-07-27 Vincent Penquerc'hducatividdec: ensure status is zeroed at start
2012-07-24 Vincent Penquerc'hducatividdec: only heed bytesConsumed when not in entir...
2012-07-20 Vincent Penquerc'hducatividdec: remove memory dump debug trace
2012-07-18 Vincent Penquerc'hgst-ducati: reorder H.264 frames ourselves
2012-07-17 Vincent Penquerc'hducatividdec: do not skip outputID processing when...
2012-07-17 Vincent Penquerc'hducatividdec: rename drop_frame to can_drop_frame
2012-07-17 Vincent Penquerc'hRevert "ducatividdec: perform QoS after feeding the...
2012-07-17 Vincent Penquerc'hducatividdec: perform QoS after feeding the data to...
2012-07-17 Vincent Penquerc'hducatividdec: add a comment about a fishy, but OK,...
2012-07-17 Vincent Penquerc'hducatividdec: do not discard unused input data
2012-07-17 Vincent Penquerc'hducatividdec: only send buffers when the decoder is...
2012-07-17 Vincent Penquerc'hducatividdec: delay flushing till the end of the codec...
2012-07-17 Vincent Penquerc'hducatividdec: print error when there actually is one
2012-06-29 Vincent Penquerc'hducatividdec: fix a miniobject and bo leak
2012-06-28 Vincent Penquerc'hducati: add some more detailed logging about video...
2012-06-27 Vincent Penquerc'hducatividdec: fix event leak
2012-06-27 Vincent Penquerc'hducatividdec: fix buffer leaks on error paths
2012-06-27 Vincent Penquerc'hducatividdec: fix deadlocks on early out paths
2012-06-27 Vincent Penquerc'hducatividdec: prevent overread when all buffer slots...
2012-06-26 Vincent Penquerc'hducatividdec: detect unsupported codecs when switching...
2012-06-14 Rob Clarkducatividdec: support crop qdata
2012-06-14 Rob Clarkuse GstDRMBufferPool and dmabuf for sharing buffers
2012-06-11 Rob ClarkRevert "ducatividdec: share the drm fd with other eleme...
2012-05-24 Alessandro Decinaducatividdec: share the drm fd with other elements...
2012-05-09 Alessandro DecinaInitial port to omapdce
2012-05-08 Alessandro Decinaducatividdec: never leave the flow_ret outarg uninitial...
2012-04-11 Alessandro Decinaducatividdec: propagate downstream flow errors
2012-04-11 Alessandro Decinaducatividdec: reset outArgs in flush()
2012-04-01 Luciana Fujii Pontelloducatividdec: fix getcaps method adding rowstride
2012-03-29 Luciana Fujii Pontelloducatividdec: Implement src pad getcaps function
2012-03-29 Luciana Fujii Pontelloducatividdec: Fix indentation
2012-03-22 Alessandro Decinaducatih264dec: implement LATENCY query
2012-03-22 Alessandro Decinaducatividdec: store upstream framerate
2012-02-28 Alessandro Decinaducatividdec: flush the codec on caps changes
2012-02-28 Alessandro Decinaducatividdec: send a crop event every time caps change
2012-02-16 Alessandro Decinaducatividdec: make codec_flush non-static so it can...
2012-02-16 Alessandro Decinaducatividdec: add var to skip buffers until the next...
2012-02-14 Alessandro Decinaducatividdec: don't discard input timestamps at stream...
2011-11-29 Alessandro Decinaducatividdec: workaround for the mpeg2 decoder giving...
2011-11-29 Alessandro Decinaducatividdec: don't renegotiate while flushing
2012-02-02 Alessandro Decinaducatividdec: flush the codec going to READY
2012-01-31 Alessandro Decinaducatividdec: make it possible for subclasses to partic...
2012-01-20 Alessandro Decinaducatividdec: destroy the internal pool once we have...
2012-01-20 Alessandro Decinaducatividdec: update the internal pool caps when switch...
2012-01-19 Alessandro Decinaducatividdec: workaround for interlaced clips that...
2012-01-11 Alessandro Decinaducatividdec: fix regression with clips having outBufsI...
2012-01-05 Rob Clarkducatividdec: auto-detect when input ts are PTS
2012-01-05 Rob Clarkducatividdec: some minor trace cleanups
2011-12-23 Alessandro Decinaducatividdec: make it possible for decoders to implemen...
2011-12-12 Rob Clarkducatividdec: fix memory leak with bufferpool buffers
2011-12-11 Rob Clarkducatividdec: fix seek issue with xvid (ts_is_pts)...
2011-12-11 Rob Clarkducatimpeg4dec/ducatividdec: implement DTS queue
2011-12-11 Rob Clarkducatimpeg4dec: xvid support
2011-12-11 Rob Clarkducatividdec: fix NPE if outcaps are EMPTY
2011-12-11 Rob Clarkducatividdec: reduce debug verbosity
2011-12-09 Alessandro Decinaducatividdec: add support for outBufsInUseFlag
2011-12-06 Alessandro Decinaducatividdec: emit a STREAM DECODE error when codec_pro...
2011-12-04 Alessandro Decinaducatividdec: implement QoS handling
2011-11-29 Alessandro Decinaducatividdec: set unaligned width and height in the...
2011-11-17 Luciana Fujii Pontelloducatividdec: propagate pixel-aspect-ratio in caps
2011-11-16 Alessandro Decinagst-indent gstducatividdec.c
2011-11-16 Alessandro Decinaducatividdec: don't log an ERROR when pad_alloc returns...
2011-11-15 Alessandro Decinaducatividdec: don't error out on non fatal errors
2011-11-14 Alessandro Decinaducatividdec: add support for video/x-raw-yuv-strided
2011-09-29 Alessandro Decinaviddec: workaround for the vc1 codec
2011-09-29 Alessandro DecinaUndo a change in gst_ducati_get_mem_type.
2011-09-29 Alessandro Decinaviddec: set the size in bytes OR pixels for outbufs...
2011-09-29 Alessandro Decinaviddec: more fixes to support 1d buffers
2011-09-29 Alessandro Decinaviddec: use 1d buffers
2011-08-31 Alessandro Decinaviddec: forward queries that we don't handle directly
2011-01-26 Rob ClarkImproved compiler warning flags strictness
2011-01-12 Rob Clarkviddec: fix typo
2011-01-01 Rob Clarkviddec: add "version" property
2011-01-01 Rob Clarkfix compile error with latest gst headers
2010-12-16 Rob Clarkviddec: fix for width/height that is not a multiple...
2010-12-16 Rob Clarkviddec: some cleanups
2010-12-12 Rob Clarkrvdec: add RealVideo support
2010-12-11 Rob Clarkviddec: fixes for seek
2010-12-05 Rob Clarkviddec: add fallback support for non-TILER buffers
2010-12-05 Rob Clarkviddec: add interlaced support
2010-12-05 Rob Clarkmpeg2dec: add MPEG-2 support
2010-12-04 Rob Clarkviddec: error handling
2010-11-29 Rob ClarkVIDDEC3_delete crash is fixed as of libdce bbbc0dd
2010-11-27 Rob Clarkvp6dec: add On2 VP6 support
2010-11-26 Rob Clarkvc1dec: add VC-1 Advanced, Main, and Simple profile...
2010-11-25 Rob Clarkmpeg4dec: add MPEG-4 support
2010-11-25 Rob Clarkviddec: implement flush (seek/eos)
2010-11-25 Rob Clarkviddec: add profiling traces for process call
2010-11-25 Rob Clarkviddec: add support for cropping
2010-11-25 Rob Clarkinitial commit