glsdk/gst-plugins-bad0-10.git
2014-12-18 Karthik Ramananwaylandsink: Remove dependency with dri2 master
2014-08-20 Harinarayan... waylandsink: Enable moving wayland video sink window
2014-04-08 Harinarayan... jpegparse: change caps/prio to be picked by decodebin2
2014-04-08 Harinarayan... kmssink: Increase num of held buffers to fix video...
2013-12-12 Olivier Naudanwaylandsink: added missing dependencies
2013-12-11 Chandramohanwayland: workaround for UV offset issue
2013-12-11 Chandramohanwayland:drm interface changes according to wayland1...
2013-12-11 Rob ClarkWIP: wayland: update to support drm/dri
2013-12-11 Tim-Philipp... configure: fix wayland check
2013-12-11 Rob Bradfordwaylandsink: Port to 1.0 protocol
2013-12-11 Tim-Philipp... waylandsink: fail gracefully with an error message...
2013-12-11 ChandramohanRevert "WIP: wayland: update to support drm/dri"
2013-12-11 ChandramohanRevert "waylandsink: added missing dependencies"
2013-10-03 Chandramohankmssink: header file alignment with latest libdce release
2013-05-22 Nikhil DevshatwarDEBIAN: Removed delivery of gstwaylandsink.so glsdk-6_00_00_07
2013-05-22 Nikhil DevshatwarDEBIAN: removed wayland compilation
2013-05-22 Nikhil DevshatwarDEBIAN: debianization
2013-05-15 Vincent Penquerc'hvp8dec: set rank to NONE, ffdec_vp8 is preferred
2013-05-15 Vincent Penquerc'hdri2videosink: fix performance issue with software...
2013-05-15 Olivier Naudanwaylandsink: added missing dependencies
2013-05-15 Olivier Naudanpvrvideosink: link explicitly with DRI2 library
2013-05-15 Vincent Penquerc'hpvrvideosink: fix rendering of sources with a non-nulti...
2013-05-15 Vincent Penquerc'hh264parse: disable passthrough when we might see B...
2013-05-15 Vincent Penquerc'homxcamerabinsrc: use the modes we know are working
2013-05-15 Vincent Penquerc'hkmssink: fix bo leak
2013-05-15 Olivier Naudandri2videosink: Added GST_PERFORMANCE traces, in order...
2013-05-15 Vincent Penquerc'hh264parse: fix AU chunking for interlaced streams
2013-05-15 Vincent Penquerc'hh264parse: simulate passthrough mode when it is scheduled
2013-05-15 Vincent Penquerc'hh264parse: use num-reorder-frames from caps if not...
2013-05-15 Vincent Penquerc'hkmssink: mark connector-name property as non-construct
2013-05-15 Vincent Penquerc'hkmssink: allow specifying a connector with a type based...
2013-05-15 Vincent Penquerc'hpvrvideosink: remove -strided caps remnants, and allow...
2013-05-15 Vincent Penquerc'hh264parser: make poc ordering cross IDR boundaries
2013-05-15 Vincent Penquerc'hpvrvideosink: lock writes to render_rect
2013-05-15 Vincent Penquerc'hkmssink: make automatic connector selection the default
2013-05-15 Vincent Penquerc'hkmssink: allow automatic selection of connector
2013-05-15 Vincent Penquerc'hkmssink: do not unref a NULL buffer on error
2013-05-15 Vincent Penquerc'hpvrvideosink: call _got_window_handle after creating...
2013-05-15 Vincent Penquerc'hdri2videosink: call _got_window_handle when creating...
2013-05-15 Vincent Penquerc'hh264parser: fix poc value resetting on IDR pictures
2013-05-15 Vincent Penquerc'hcodecparsers: use the new start code scanner where...
2013-05-15 Vincent Penquerc'hmpeg4parser: speed up scan for start codes
2013-05-15 Thibault Saunierkmssink: remove GstVideoContext implementation
2013-05-15 Thibault Saunierkms: Use dce to get device instead of doing it ourself
2013-05-15 Vincent Penquerc'hkmssink: wind down the drm machinery on reset
2013-05-15 Vincent Penquerc'hkmssink: fix leak
2013-05-15 Vincent Penquerc'hkmssink: make fb_id the right type the DRM API expects
2013-05-15 Vincent Penquerc'hkmssink: do not free mode, we do not own it
2013-05-15 Vincent Penquerc'hdri2videosink: pipe through gst-indent
2013-05-15 Vincent Penquerc'hdri2videosink: heed to map/unmap events
2013-05-15 Vincent Penquerc'hh264parse: add num-reorder-frames to the caps, if present
2013-05-15 Vincent Penquerc'hh264parser: fix poc memory of past reference frame
2013-05-15 Vincent Penquerc'hh264parser: rename variables from spec naming to gst...
2013-05-15 Vincent Penquerc'hdri2videosink: fix locking bug
2013-05-15 Rob ClarkWIP: wayland: update to support drm/dri
2013-05-15 Wim Taymanswayland: compile against older wayland
2013-05-15 Sreerenj Balachandranwaylandsink: Fix warnings, proper structuring, dead...
2013-05-15 Sreerenj Balachandranwaylandsink: Fix in shell_surface_set_fullscreen
2013-05-15 Sreerenj Balachandranwaylandsink: More fixes -- update to Wayland 0.85 proto...
2013-05-15 Sreerenj BalachandranUpdate with new APIs in wayland-client.
2013-05-15 Sreerenj BalachandranMore Fixes: * Adding buffer_alloc * perform buffer_dama...
2013-05-15 Sreerenj BalachandranInitial Commit: Adding Wayland Video Sink
2013-05-15 Vincent Penquerc'hdri2videosink: fix caps leak
2013-05-15 Vincent Penquerc'hh264parse: attach picture order count to buffers
2013-05-15 Vincent Penquerc'hh264parser: add poc calculation
2013-05-15 Vincent Penquerc'hdri2videosink: fix cropping with software decoders
2013-05-15 Vincent Penquerc'hh264parse: do not send PPS and SPS alone in byte-stream...
2013-05-15 Thibault Saunierdri2videosink, pvrvideosink: Accept height up to 2048...
2013-05-15 Thibault Saunierpvrvideosink: Limit size to 1080p as it is a hardware...
2013-05-15 Thibault Saunierdri2videosink: Limit size to 2k as it is the maximum...
2013-05-15 Thibault Saunierdri2videosink: Limit size to 1080p as it is a hardware...
2013-05-15 Vincent Penquerc'hh264parse: do not use VUI values if they were not found...
2013-05-15 Vincent Penquerc'hdrm: do not dereference a NULL pointer
2013-05-15 Vincent Penquerc'hdrm: do not dereference a NULL pointer
2013-05-15 Vincent Penquerc'hdrm: add a signal for notifying when a buffer is return...
2013-05-15 Vincent Penquerc'hAdd a pkg-config file for the drm lib
2013-05-15 Thibault Saunierdrm and dri: Enhance debug messages
2013-05-15 Thibault Saunierdri2 and drm: Pass through gst-indent
2013-05-15 Vincent Penquerc'hdrmbufferpool: fix dmabuf leak
2013-05-15 Mark Nauwelaertscodecparsers: mpeg4: do not expect a marker bit where...
2013-05-15 Vincent Penquerc'hdri2videosink: fix a crash on resizing the window
2013-05-15 Vincent Penquerc'hdri2videosink: deinterlaced interlaced input
2013-05-15 Vincent Penquerc'hdri2videosink: DRI2 stride has a pixel constraint,...
2013-05-15 Vincent Penquerc'hdri2videosink: fix window/video width confusion
2013-05-15 Vincent Penquerc'hdri2videosink: copy correct number of bytes for interla...
2013-05-15 Vincent Penquerc'hdri2videosink: copy buffers which do not match strides...
2013-05-15 Vincent Penquerc'hdri2videosink: bump rank to PRIMARY + 1
2013-05-15 Vincent Penquerc'hkmssink: bump rank to PRIMARY + 1
2013-05-15 Vincent Penquerc'hdri2videosink: destroy context only whe window is destroyed
2013-05-15 Vincent Penquerc'hh264parse: add num-ref-frames in caps
2013-05-15 Vincent Penquerc'hh264parse: delay setting passthrough mode when waiting...
2013-05-15 Vincent Penquerc'hdri2: link libgstdrm in-tree
2013-05-15 Vincent Penquerc'hkms: add missing backslash in lib list
2013-05-15 Vincent Penquerc'hkmssink: link to our in-tree libgstbasevideo
2013-05-15 Vincent Penquerc'hh264parse: do not use a buffer after it was unreffed
2013-05-15 Vincent Penquerc'hh264parse: split interlaced fields in separate packets
2013-05-15 Vincent Penquerc'hRevert "h264parse: disable some optimizations with...
2013-05-15 Vincent Penquerc'hpvrvideosink: fix unwanted scaling on cropped videos
2013-05-15 Vincent Penquerc'hh264parse: wait to get resolution before pushing buffers
2013-05-15 Vincent Penquerc'hdrmbufferpool: give this code a separate debug category
next