1c35817f8bd2b2dcf39f0b3b3afe3b715b85b033
1 2005-09-30 Michael Smith <msmith@fluendo.com>
3 * gst/realmedia/rmdemux.c: (gst_rmdemux_src_event),
4 (gst_rmdemux_perform_seek), (gst_rmdemux_src_query),
5 (gst_rmdemux_change_state), (gst_rmdemux_loop),
6 (gst_rmdemux_fourcc_isplausible), (gst_rmdemux_chain),
7 (gst_rmdemux_send_event), (gst_rmdemux_add_stream),
8 (gst_rmdemux_parse_packet):
9 * gst/realmedia/rmdemux.h:
10 Sanity checking, and fix some minor memory leaks
12 2005-09-29 Michael Smith <msmith@fluendo.com>
14 * gst/realmedia/rmdemux.c: (gst_rmdemux_src_event),
15 (gst_rmdemux_perform_seek), (gst_rmdemux_loop),
16 (gst_rmdemux_send_event), (gst_rmdemux_add_stream),
17 (gst_rmdemux_parse_mdpr), (gst_rmdemux_parse_packet):
18 Real demuxer fixes. Make it more bulletproof against bad data,
19 identify a few more stream types.
20 Fix seeking so that it works (at least with the seek example program;
21 it still fails with totem).
23 2005-09-26 Wim Taymans <wim@fluendo.com>
25 * gst/mpegaudioparse/gstmpegaudioparse.c:
26 (gst_mp3parse_sink_event), (gst_mp3parse_chain):
27 Set correct caps on buffers too.
29 2005-09-26 Wim Taymans <wim@fluendo.com>
31 * gst/mpegaudioparse/gstmpegaudioparse.c: (gst_mp3parse_init),
32 (gst_mp3parse_sink_event), (gst_mp3parse_chain):
33 * gst/mpegaudioparse/gstmpegaudioparse.h:
34 Put timestamps on buffers.
36 2005-09-21 Flavio Oliveira <flavio.oliveira@indt.org.br>
38 * ext/amrnb/amrnbenc.c: (gst_amrnbenc_base_init):
39 Changed amrnbenc description, it is an encoder, not decoder.
41 2005-09-21 Michael Smith <msmith@fluendo.com>
43 * gst/ac3parse/gstac3parse.c: (gst_ac3parse_class_init),
44 (gst_ac3parse_init), (gst_ac3parse_chain):
45 * gst/iec958/ac3_padder.c: (ac3_crc_init), (ac3_crc_update),
46 (ac3_crc_validate), (ac3p_init), (ac3p_parse):
47 * gst/iec958/ac3_padder.h:
48 * gst/iec958/ac3iec.c:
49 Various changes to AC3->IEC958 framer. Mostly to make our IEC958
50 headers more accurate, and to check AC3 checksums (both of them in
51 each frame), and dump the frame (as a probable sync failure) if they
52 don't match. General code cleanup, improved comments. Changed to not
53 construct the header backwards, and not byteswap everything else.
54 If we end up needing to do little-endian output, we should swap in
55 the element doing the output (AC3 is big-endian).
57 2005-09-20 Thomas Vander Stichele <thomas at apestaart dot org>
59 * docs/plugins/gst-plugins-ugly-plugins.args:
60 * docs/plugins/gst-plugins-ugly-plugins.hierarchy:
61 * docs/plugins/gst-plugins-ugly-plugins.interfaces:
62 * docs/plugins/gst-plugins-ugly-plugins.prerequisites:
63 commit missing files
64 * docs/plugins/inspect/plugin-lame.xml:
65 update
67 2005-09-19 Wim Taymans <wim@fluendo.com>
69 * ext/lame/gstlame.c: (gst_lame_chain):
70 Set caps on outgoing buffers.
72 2005-09-16 Thomas Vander Stichele <thomas at apestaart dot org>
74 * ext/lame/gstlame.c:
75 * ext/lame/gstlame.h:
76 clean up further so we don't try to set up five times for
77 a simple pipeline
79 2005-09-16 Michael Smith <msmith@fluendo.com>
81 * gst/iec958/ac3iec.c: (ac3iec_init):
82 Set setcaps function on sink pad, not source pad. Produce correct
83 caps on output buffers.
85 2005-09-07 Stefan Kost <ensonic@users.sf.net>
87 * ext/mad/gstid3tag.c:
88 gsttaginterface.h -> gsttagsetter.h
90 === release 0.9.1 ===
92 2005-09-06 Thomas Vander Stichele <thomas at apestaart dot org>
94 * README:
95 * NEWS:
96 * autogen.sh:
97 * configure.ac:
98 releasing 0.9.1, "The Rat"
100 2005-09-06 Wim Taymans <wim@fluendo.com>
102 * ext/amrnb/amrnbdec.c: (gst_amrnbdec_state_change):
103 * ext/amrnb/amrnbenc.c: (gst_amrnbenc_state_change):
104 * ext/amrnb/amrnbparse.c: (gst_amrnbparse_state_change):
105 State change function updates.
107 2005-09-05 Jan Schmidt <thaytan@mad.scientist.com>
109 * ext/mpeg2dec/gstmpeg2dec.c:
110 GST_CAT_SEEK disappeared from the public API at some point
112 2005-09-02 Michael Smith <msmith@fluendo.com>
114 * gst/iec958/ac3iec.c:
115 Use the right mime-type for AC3 input, audio/x-private1-ac3, as
116 output by demux
118 2005-09-02 Michael Smith <msmith@fluendo.com>
120 * gst/dvdlpcmdec/gstdvdlpcmdec.c: (gst_dvdlpcmdec_chain_dvd):
121 * gst/iec958/ac3iec.c: (ac3iec_get_type), (ac3iec_base_init),
122 (ac3iec_class_init), (ac3iec_init), (ac3iec_finalize),
123 (ac3iec_setcaps), (ac3iec_set_property), (ac3iec_get_property),
124 (ac3iec_chain_dvd), (ac3iec_chain_raw), (ac3iec_change_state),
125 (plugin_init):
126 Changes to use the first_access parameter correctly in ac3 and lpcm
127 plugins. General cleanups in iec958 framer.
129 2005-09-01 Michael Smith <msmith@fluendo.com>
131 * configure.ac:
132 * gst/iec958/Makefile.am:
133 * gst/iec958/ac3_padder.c: (ac3p_init), (ac3p_push_data),
134 (ac3p_parse):
135 * gst/iec958/ac3_padder.h:
136 * gst/iec958/ac3iec.c: (ac3iec_get_type), (ac3iec_base_init),
137 (ac3iec_class_init), (ac3iec_init), (ac3iec_finalize),
138 (ac3iec_set_property), (ac3iec_get_property), (ac3iec_chain),
139 (ac3iec_change_state), (plugin_init):
140 * gst/iec958/ac3iec.h:
141 AC3 -> IEC958 (S/PDIF) framer, port of Martin Soto's 0.8 plugin.
143 2005-09-01 Wim Taymans <wim@fluendo.com>
145 * gst/dvdlpcmdec/gstdvdlpcmdec.c: (gst_dvdlpcmdec_setcaps),
146 (gst_dvdlpcmdec_chain_dvd), (gst_dvdlpcmdec_chain_raw),
147 (gst_dvdlpcmdec_change_state):
148 Cleanups, fixed header parsing and stripping.
150 2005-09-01 Michael Smith <msmith@fluendo.com>
152 * gst/dvdlpcmdec/gstdvdlpcmdec.c: (gst_dvdlpcm_reset),
153 (gst_dvdlpcmdec_init), (gst_dvdlpcmdec_setcaps),
154 (update_timestamps), (parse_header), (gst_dvdlpcmdec_chain_dvd),
155 (gst_dvdlpcmdec_chain_raw):
156 Use the right bytes to parse the LPCM dvd header
158 2005-09-01 Michael Smith <msmith@fluendo.com>
160 * gst/dvdlpcmdec/gstdvdlpcmdec.c: (gst_dvdlpcm_reset),
161 (gst_dvdlpcmdec_init), (gst_dvdlpcmdec_setcaps),
162 (update_timestamps), (parse_header), (gst_dvdlpcmdec_chain_dvd),
163 (gst_dvdlpcmdec_chain_raw):
164 Return the correct values from chain function.
166 2005-08-31 Michael Smith <msmith@fluendo.com>
168 * gst/dvdlpcmdec/gstdvdlpcmdec.c: (gst_dvdlpcm_reset),
169 (gst_dvdlpcmdec_init), (gst_dvdlpcmdec_setcaps),
170 (update_timestamps), (parse_header), (gst_dvdlpcmdec_chain_dvd),
171 (gst_dvdlpcmdec_chain_raw):
172 * gst/dvdlpcmdec/gstdvdlpcmdec.h:
173 Restructure LPCM decoder to not expect the demuxer to parse the LPCM
174 header; instead do this internally. Also support the old way, using
175 a different mime-type.
177 2005-08-31 Thomas Vander Stichele <thomas at apestaart dot org>
179 * Makefile.am:
180 * configure.ac:
181 * docs/plugins/Makefile.am:
182 * docs/plugins/gst-plugins-ugly-plugins-docs.sgml:
183 * docs/plugins/gst-plugins-ugly-plugins-sections.txt:
184 * docs/plugins/gst-plugins-ugly-plugins.types:
185 * ext/dvdnav/dvdnavsrc.c: (dvdnavsrc_tca_seek):
186 * ext/dvdread/dvdreadsrc.c: (_open), (_seek_title),
187 (_seek_chapter), (_read):
188 * gst/mpegaudioparse/gstmpegaudioparse.c:
189 add plugin documentation