]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gst-plugins-ugly0-10.git/blob - LICENSE_readme
LICENSE_readme: Mention that synaesthesia is derived from GPL code.
[glsdk/gst-plugins-ugly0-10.git] / LICENSE_readme
1 GStreamer is developed under the terms of the LGPL (see LICENSE file for details). Some of our plugins however rely on libraries which are available under i other licenses. This means that if you are using an application which has a non-GPL compatible license, for instance a closed-source application with GStreamer you have to make sure not to use GPL linked or derived plugins.
2 When using GPL linked plugins GStreamer is for all practical reasons under the GPL itself. 
4 The plugins which use a GPL library are as follows:
5 cdparanoia      libcdparanoia   (http://www.xiph.org/paranoia/)
6 aasink          aalib           (http://aa-project.sourceforge.net/aalib/)
7 xmms            libxmms         (http://www.xmms.org)
8 decdvd          ac3dec,mpeg2dec (http://linuxvideo.org/mpeg2dec/,http://linuxvideo.org/ac3dec/)
10 Plugins derived from GPL code are as follows:
11 synaesthesia    synaesthesia    (http://yoyo.cc.monash.edu.au/~pfh/synaesthesia.html)
13 Plugins which use library a LGPL are as follows:
14 Colorspace      Hermes          (http://www.clanlib.org/hermes/)
15 httpsrc         libghttp        (ftp.gnome.org/pub/GNOME/stable/sources/libghttp/)
16 alsasink        alsa            (http://alsa-project.org)
17 aRts            aRts            (http://arts-project.org)
18 sdlsink         libsdl          (http://www.libsdl.org)
19 gnomevfssource  gnome-vfs       (ftp.gnome.org//pub/GNOME/stable/sources/gnome-vfs)
20 gnomevfssink    gnome-vfs
21 esdsink         libesd          (ftp.gnome.org/pub/GNOME/stable/sources/esound)
22 icastsend       libshout        (http://www.icecast.org)
23 lame            libmp3lame      (http://www.mp3dev.org/mp3/)
24 gst1394         libraw1394      (http://linux1394.sourceforge.net)
25 flac            libFLAC         (http://flac.sourceforge.net)
26 RTP             ortp            (http://www.linphone.org/ortp/)
28 Plugins which use a BSD covered library are as follows:
29 vorbisenc       libogg/libvorbis        (http://www.xiph.org/ogg/vorbis)
30 vorbisdec       libogg/libvorbis
32 Plugins based on libraries with other free licenses:
33 xsink           libXv           (MIT X11 / X Consortium license)
34 gsm             libgsm          (MIT license http://kbs.cs.tu-berlin.de/~jutta/toast.html)
36 Plugins using non-free libraries:
37 xamp3 decoder   libxaudio       (http://www.xaudio.com/)
38 wincodec        win32ddl        (http://divx.euro.ru/)