lame: fix printf format in debug statements
[glsdk/gst-plugins-ugly0-10.git] / README
1 WHAT IT IS
2 ----------
4 This is GStreamer, a framework for streaming media.
6 WHERE TO START
7 --------------
9 We have a website at
10 http://gstreamer.freedesktop.org/
12 You should start by going through our FAQ at
13 http://gstreamer.freedesktop.org/data/doc/gstreamer/head/faq/html/
15 There is more documentation; go to
16 http://gstreamer.freedesktop.org/documentation
18 You can subscribe to our mailing lists; see the website for details.
20 We track bugs in GNOME's bugzilla; see the website for details.
22 You can join us on IRC - #gstreamer on irc.freenode.org
24 GStreamer 0.10 series
25 ---------------------
27 Starring
29   GSTREAMER
31 The core around which all other modules revolve.  Base functionality and
32 libraries, some essential elements, documentation, and testing.
34   BASE
36 A well-groomed and well-maintained collection of GStreamer plug-ins and
37 elements, spanning the range of possible types of elements one would want
38 to write for GStreamer.  
40 And introducing, for the first time ever, on the development screen ...
42   THE GOOD
44  --- "Such ingratitude.  After all the times I've saved your life."
46 A collection of plug-ins you'd want to have right next to you on the
47 battlefield.  Shooting sharp and making no mistakes, these plug-ins have it
48 all: good looks, good code, and good licensing.  Documented and dressed up
49 in tests.  If you're looking for a role model to base your own plug-in on,
50 here it is.
52 If you find a plot hole or a badly lip-synced line of code in them,
53 let us know - it is a matter of honour for us to ensure Blondie doesn't look
54 like he's been walking 100 miles through the desert without water.
56   THE UGLY
58   --- "When you have to shoot, shoot.  Don't talk."
60 There are times when the world needs a color between black and white.
61 Quality code to match the good's, but two-timing, backstabbing and ready to
62 sell your freedom down the river.  These plug-ins might have a patent noose
63 around their neck, or a lock-up license, or any other problem that makes you
64 think twice about shipping them.
66 We don't call them ugly because we like them less.  Does a mother love her
67 son less because he's not as pretty as the other ones ? No  - she commends
68 him on his great personality.  These plug-ins are the life of the party.
69 And we'll still step in and set them straight if you report any unacceptable
70 behaviour - because there are two kinds of people in the world, my friend:
71 those with a rope around their neck and the people who do the cutting.
73   THE BAD
75   --- "That an accusation?"
77 No perfectly groomed moustache or any amount of fine clothing is going to
78 cover up the truth - these plug-ins are Bad with a capital B. 
79 They look fine on the outside, and might even appear to get the job done, but
80 at the end of the day they're a black sheep. Without a golden-haired angel
81 to watch over them, they'll probably land in an unmarked grave at the final
82 showdown.
84 Don't bug us about their quality - exercise your Free Software rights,
85 patch up the offender and send us the patch on the fastest steed you can
86 steal from the Confederates. Because you see, in this world, there's two
87 kinds of people, my friend: those with loaded guns and those who dig.
88 You dig.
90 The Lowdown
91 -----------
93   --- "I've never seen so many plug-ins wasted so badly."
95 GStreamer Plug-ins has grown so big that it's hard to separate the wheat from
96 the chaff.  Also, distributors have brought up issues about the legal status
97 of some of the plug-ins we ship.  To remedy this, we've divided the previous
98 set of available plug-ins into four modules:
100 - gst-plugins-base: a small and fixed set of plug-ins, covering a wide range
101   of possible types of elements; these are continuously kept up-to-date
102   with any core changes during the development series.
104   - We believe distributors can safely ship these plug-ins.
105   - People writing elements should base their code on these elements.
106   - These elements come with examples, documentation, and regression tests.
108 - gst-plugins-good: a set of plug-ins that we consider to have good quality
109   code, correct functionality, our preferred license (LGPL for the plug-in
110   code, LGPL or LGPL-compatible for the supporting library).
112   - We believe distributors can safely ship these plug-ins.
113   - People writing elements should base their code on these elements.
114  
115 - gst-plugins-ugly: a set of plug-ins that have good quality and correct
116   functionality, but distributing them might pose problems.  The license
117   on either the plug-ins or the supporting libraries might not be how we'd
118   like. The code might be widely known to present patent problems.
120   - Distributors should check if they want/can ship these plug-ins.
121   - People writing elements should base their code on these elements.
123 - gst-plugins-bad: a set of plug-ins that aren't up to par compared to the
124   rest.  They might be close to being good quality, but they're missing
125   something - be it a good code review, some documentation, a set of tests,
126   a real live maintainer, or some actual wide use.
127   If the blanks are filled in they might be upgraded to become part of
128   either gst-plugins-good or gst-plugins-ugly, depending on the other factors.
130   - If the plug-ins break, you can't complain - instead, you can fix the
131     problem and send us a patch, or bribe someone into fixing them for you.
132   - New contributors can start here for things to work on.
134 PLATFORMS
135 ---------
137 - Linux is of course fully supported
138 - FreeBSD is reported to work; other BSD's should work too
139 - Solaris is reported to work; a specific sunaudiosink plugin has been written
140 - MacOSX is reported to work; specific audio and video sinks have been written
141 - Windows support is experimental but improving.  Output sinks have been
142   written but are not yet included in the code. We support
143   - MSys/MingW builds
144   - Microsoft Visual Studio 6 builds (see win32/README.txt)
146 INSTALLING FROM PACKAGES
147 ------------------------
149 You should always prefer installing from packages first.  GStreamer is
150 well-maintained for a number of distributions, including Fedora, Debian,
151 Ubuntu, Mandrake, Gentoo, ...
153 Only in cases where you:
154 - want to hack on GStreamer
155 - want to verify that a bug has been fixed
156 - do not have a sane distribution
157 should you choose to build from source tarballs or CVS.
159 Find more information about the various packages at
160 http://gstreamer.freedesktop.org/download/
162 COMPILING FROM SOURCE TARBALLS
163 ------------------------------
165 - again, make sure that you really need to install from source !
166   If GStreamer is one of your first projects ever that you build from source,
167   consider taking on an easier project.
169 - check output of ./configure --help to see if any options apply to you
170 - run
171   ./configure
172   make
174   to build GStreamer.
175 - if you want to install it (not required, but what you usually want to do), run
176   make install
178 - try out a simple test:
179   gst-launch -v fakesrc num_buffers=5 ! fakesink
180   (If you didn't install GStreamer, prefix gst-launch with tools/)
182   If it outputs a bunch of messages from fakesrc and fakesink, everything is
183   ok.
185   If it did not work, keep in mind that you might need to adjust the
186   PATH and/or LD_LIBRARY_PATH environment variables to make the system
187   find GStreamer in the prefix where you installed (by default that is /usr/local).
189 - After this, you're ready to install gst-plugins, which will provide the
190   functionality you're probably looking for by now, so go on and read
191   that README.
193 COMPILING FROM CVS
194 ------------------
196 When building from CVS sources, you will need to run autogen.sh to generate 
197 the build system files.
199 You will need a set of additional tools typical for building from CVS,
200 including:
201 - autoconf
202 - automake
203 - libtool
205 autogen.sh will check for recent enough versions and complain if you don't have
206 them.  You can also specify specific versions of automake and autoconf with
207 --with-automake and --with-autoconf
209 Check autogen.sh options by running autogen.sh --help
211 autogen.sh can pass on arguments to configure - you just need to separate them
212 from autogen.sh with -- between the two.
213 prefix has been added to autogen.sh but will be passed on to configure because
214 some build scripts like that.
216 When you have done this once, you can use autoregen.sh to re-autogen with
217 the last passed options as a handy shortcut.  Use it.
219 After the autogen.sh stage, you can follow the directions listed in
220 "COMPILING FROM SOURCE"
222 You can also run your whole cvs stack uninstalled.  The script in
223 the gstreamer module /docs/faq/gst-uninstalled) is helpful in setting
224 up your environment for this.
226 PLUG-IN DEPENDENCIES AND LICENSES
227 ---------------------------------
229 GStreamer is developed under the terms of the LGPL (see LICENSE file for
230 details). Some of our plug-ins however rely on libraries which are available
231 under other licenses. This means that if you are distributing an application
232 which has a non-GPL compatible license (for instance a closed-source
233 application) with GStreamer, you have to make sure not to distribute GPL-linked
234 plug-ins.
236 When using GPL-linked plug-ins, GStreamer is for all practical reasons
237 under the GPL itself.
239 HISTORY
240 -------
242 The fundamental design comes from the video pipeline at Oregon Graduate
243 Institute, as well as some ideas from DirectMedia.  It's based on plug-ins that
244 will provide the various codec and other functionality.  The interface
245 hopefully is generic enough for various companies (ahem, Apple) to release
246 binary codecs for Linux, until such time as they get a clue and release the
247 source.