2 Release notes for GStreamer Ugly Plug-ins 0.10.6 "The Sacrifice"
5 The GStreamer team is proud to announce a new release
6 in the 0.10.x stable series of the
7 GStreamer Ugly Plug-ins.
10 The 0.10.x series is a stable series targeted at end users.
11 It is not API or ABI compatible with the stable 0.8.x series.
12 It is, however, parallel installable with the 0.8.x series.
16 "When you have to shoot, shoot. Don't talk."
19 There are times when the world needs a color between black and white.
20 Quality code to match the good's, but two-timing, backstabbing and ready to
21 sell your freedom down the river. These plug-ins might have a patent noose
22 around their neck, or a lock-up license, or any other problem that makes you
23 think twice about shipping them.
26 We don't call them ugly because we like them less. Does a mother love her
27 son less because he's not as pretty as the other ones ? No - she commends
28 him on his great personality. These plug-ins are the life of the party.
29 And we'll still step in and set them straight if you report any unacceptable
30 behaviour - because there are two kinds of people in the world, my friend:
31 those with a rope around their neck and the people who do the cutting.
34 This module contains a set of plug-ins that have good quality and correct
35 functionality, but distributing them might pose problems. The license
36 on either the plug-ins or the supporting libraries might not be how we'd
37 like. The code might be widely known to present patent problems.
38 Distributors should check if they want/can ship these plug-ins.
41 Other modules containing plug-ins are:
44 gst-plugins-base
45 contains a basic set of well-supported plug-ins
46 gst-plugins-good
47 contains a set of well-supported plug-ins under our preferred license
48 gst-plugins-bad
49 contains a set of less supported plug-ins that haven't passed the
50 rigorous quality testing we expect
56 Features of this release
58 * fixes in handling of MPEG streams, Real streams and MP3
59 * AMR-NB fixes
60 * Other bug-fixes and improvements
61 * Parallel installability with 0.8.x series
62 * Threadsafe design and API
64 Bugs fixed in this release
66 * 336370 : [asfdemux] crashes on an assertion in gst_asf_demux_get_v...
67 * 332157 : [asfdemux] This WMV file is played very strangely
68 * 335760 : [asfdemux] dataflow error when seeking in zeldadslarge.wmv
69 * 349779 : [real] can't play ancient RealAudio 1.0/2.0 format files
70 * 353116 : [asfdemux] hangs playing some mms stations
71 * 365288 : [asfdemux] seeking not very smooth
72 * 370020 : [mpeg2dec] continue even after 5 consecutive decoding errors
73 * 385292 : [rmdemux] stream index leaked on shutdown
74 * 385311 : Memory leak initializing lame mp3 encoder plugin (gstlame.c)
75 * 385651 : [asfdemux] Jerky playback of " I love sky "
76 * 393890 : [win32] autogenerated win32/common/config.h needed
77 * 397219 : [rmdemux] captured realaudio stream with non-zero start p...
78 * 403188 : [asfdemux] bug parsing certain stream header object
79 * 421594 : [real] doesn't compile if zlib includes are missing
80 * 425374 : [asfdemux] seek in WMV rarely works
81 * 428698 : [rmdemux] crashes on files with many logical streams
82 * 429960 : [mpegdemux] playbin hangs with small external vobsub subt...
83 * 431707 : [amrnbparse] make pipeline hang
84 * 432533 : [mad, mp3parse] regression: CVS version doesn't parse dur...
85 * 438610 : [dvddemux] fails after flushing seek
86 * 440120 : [mpegdemux] crashes in gst_mpeg_demux_send_subbuffer() wi...
87 * 442706 : [dvdsubdec] crashes when flushing/on seek
88 * 444514 : [PATCH] dvdsubdec miscalculates (long) subtitle durations
89 * 386218 : [asfdemux] Division by zero when seeking live streams
91 Download
93 You can find source releases of gst-plugins-ugly in the download directory:
94 http://gstreamer.freedesktop.org/src/gst-plugins-ugly/
96 GStreamer Homepage
98 More details can be found on the project's website:
99 http://gstreamer.freedesktop.org/
101 Support and Bugs
103 We use GNOME's bugzilla for bug reports and feature requests:
104 http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
106 Developers
108 CVS is hosted on cvs.freedesktop.org.
109 All code is in CVS and can be checked out from there.
110 Interested developers of the core library, plug-ins, and applications should
111 subscribe to the gstreamer-devel list. If there is sufficient interest we
112 will create more lists as necessary.
115 Applications
117 Contributors to this release
119 * Jan Schmidt
120 * Julien MOUTTE
121 * Mark Nauwelaerts
122 * Michael Smith
123 * Mogens Jaeger
124 * René Stadler
125 * Roland Kay
126 * Sebastian Dröge
127 * Sebastien Moutte
128 * Stefan Kost
129 * Sébastien Moutte
130 * Thomas Vander Stichele
131 * Tim-Philipp Müller
132 * Wim Taymans
133 * Xavier B.
134 * Zaheer Abbas Merali