2 Release notes for GStreamer Ugly Plug-ins 0.10.13 "Appointed Point"
5 The GStreamer team is proud to announce a new release
6 in the 0.10.x stable series of the
7 GStreamer Ugly Plug-ins.
10 The 0.10.x series is a stable series targeted at end users.
11 It is not API or ABI compatible with the stable 0.8.x series.
12 It is, however, parallel installable with the 0.8.x series.
16 "When you have to shoot, shoot. Don't talk."
19 There are times when the world needs a color between black and white.
20 Quality code to match the good's, but two-timing, backstabbing and ready to
21 sell your freedom down the river. These plug-ins might have a patent noose
22 around their neck, or a lock-up license, or any other problem that makes you
23 think twice about shipping them.
26 We don't call them ugly because we like them less. Does a mother love her
27 son less because he's not as pretty as the other ones ? No - she commends
28 him on his great personality. These plug-ins are the life of the party.
29 And we'll still step in and set them straight if you report any unacceptable
30 behaviour - because there are two kinds of people in the world, my friend:
31 those with a rope around their neck and the people who do the cutting.
34 This module contains a set of plug-ins that have good quality and correct
35 functionality, but distributing them might pose problems. The license
36 on either the plug-ins or the supporting libraries might not be how we'd
37 like. The code might be widely known to present patent problems.
38 Distributors should check if they want/can ship these plug-ins.
41 Other modules containing plug-ins are:
44 gst-plugins-base
45 contains a basic set of well-supported plug-ins
46 gst-plugins-good
47 contains a set of well-supported plug-ins under our preferred license
48 gst-plugins-bad
49 contains a set of less supported plug-ins that haven't passed the
50 rigorous quality testing we expect
56 Features of this release
58 * Improve A52 decoder
59 * Add AMR-WB decoder and AMR-NB decoder/encoder based on OpenCore codecs
60 * ASF playback improvements
61 * Improve mp3 parser and seeking
63 Bugs fixed in this release
65 * 519721 : [asfdemux] wma tags are not copied when converting to another format
66 * 584890 : AMR plugins based on Opencore codecs
67 * 585956 : [mp3parse] indexing improvements
68 * 590432 : It's only possible to build the mad plugin when building id3tag as well
69 * 591348 : AMR plugins should check for opencore-amr .pc files
70 * 592787 : a52dec: Allow liba52 to use djbfft based IMDCT transform
71 * 596517 : x264 element no longer compiles against changed upstream API
72 * 598272 : a52dec leaks input buffers
73 * 598370 : Properly detect pre-releases
75 Download
77 You can find source releases of gst-plugins-ugly in the download directory:
78 http://gstreamer.freedesktop.org/src/gst-plugins-ugly/
80 GStreamer Homepage
82 More details can be found on the project's website:
83 http://gstreamer.freedesktop.org/
85 Support and Bugs
87 We use GNOME's bugzilla for bug reports and feature requests:
88 http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
90 Developers
92 GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
93 Interested developers of the core library, plug-ins, and applications should
94 subscribe to the gstreamer-devel list. If there is sufficient interest we
95 will create more lists as necessary.
98 Applications
100 Contributors to this release
102 * Christian Schaller
103 * David Schleef
104 * Edward Hervey
105 * Iago Toral
106 * Jan Schmidt
107 * Josep Torra
108 * Mark Nauwelaerts
109 * Mart Raudsepp
110 * Marvin Schmidt
111 * Michael Smith
112 * Olivier Crête
113 * René Stadler
114 * Sebastian Dröge
115 * Stefan Kost
116 * Thiago Santos
117 * Tim-Philipp Müller
118 * Wim Taymans