2 Release notes for GStreamer Ugly Plug-ins 0.10.11 "Their swords and their knives"
5 The GStreamer team is proud to announce a new release
6 in the 0.10.x stable series of the
7 GStreamer Ugly Plug-ins.
10 The 0.10.x series is a stable series targeted at end users.
11 It is not API or ABI compatible with the stable 0.8.x series.
12 It is, however, parallel installable with the 0.8.x series.
16 "When you have to shoot, shoot. Don't talk."
19 There are times when the world needs a color between black and white.
20 Quality code to match the good's, but two-timing, backstabbing and ready to
21 sell your freedom down the river. These plug-ins might have a patent noose
22 around their neck, or a lock-up license, or any other problem that makes you
23 think twice about shipping them.
26 We don't call them ugly because we like them less. Does a mother love her
27 son less because he's not as pretty as the other ones ? No - she commends
28 him on his great personality. These plug-ins are the life of the party.
29 And we'll still step in and set them straight if you report any unacceptable
30 behaviour - because there are two kinds of people in the world, my friend:
31 those with a rope around their neck and the people who do the cutting.
34 This module contains a set of plug-ins that have good quality and correct
35 functionality, but distributing them might pose problems. The license
36 on either the plug-ins or the supporting libraries might not be how we'd
37 like. The code might be widely known to present patent problems.
38 Distributors should check if they want/can ship these plug-ins.
41 Other modules containing plug-ins are:
44 gst-plugins-base
45 contains a basic set of well-supported plug-ins
46 gst-plugins-good
47 contains a set of well-supported plug-ins under our preferred license
48 gst-plugins-bad
49 contains a set of less supported plug-ins that haven't passed the
50 rigorous quality testing we expect
56 Features of this release
58 * Migrate twolame element from -bad
59 * mp3parse improvements
60 * Support scaling in the synaesthsia visualisation
61 * Improve realmedia streaming, supporting RDT and pnm://
62 * Improved ASF demuxing, including streaming-mode seeking
63 * Support for 4:4:4 MPEG-2 video
65 Bugs fixed in this release
67 * 571146 : [mpeg2dec] Probably uses wrong strides for 4:2:2 and 4:4:...
68 * 574461 : [mpeg2dec] Lower rank and make ffdec_mpeg2video PRIMARY
69 * 454228 : [mpegdemux] problem with mark shuttleworth clip
70 * 522699 : pnm:/something.ra streams can't be loaded in Totem from a...
71 * 527112 : [real] Can't play several real audio streams
72 * 556714 : Real Audio streams not working properly
73 * 560348 : plus7.arte.tv plays slooooowly
74 * 562065 : mpeg2dec does not handle STATE_SEQUENCE_MODIFIED from > =l...
75 * 562086 : mpeg2 stream crashes something in gstreamer
76 * 564885 : [mpegstream] memory leak
77 * 568836 : [asfdemux] add seeking support when operating in push mode
78 * 569317 : [PLUGIN-MOVE] Move twolame plugin from -bad to -ugly
79 * 575068 : [mp3parse] deadlock with accurate seeking
80 * 335067 : Need RTP ASF depayloader
81 * 571358 : [real] file playing stops immediately
83 Download
85 You can find source releases of gst-plugins-ugly in the download directory:
86 http://gstreamer.freedesktop.org/src/gst-plugins-ugly/
88 GStreamer Homepage
90 More details can be found on the project's website:
91 http://gstreamer.freedesktop.org/
93 Support and Bugs
95 We use GNOME's bugzilla for bug reports and feature requests:
96 http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
98 Developers
100 GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
101 Interested developers of the core library, plug-ins, and applications should
102 subscribe to the gstreamer-devel list. If there is sufficient interest we
103 will create more lists as necessary.
106 Applications
108 Contributors to this release
110 * Alessandro Decina
111 * Cygwin Ports maintainer
112 * David Schleef
113 * Edward Hervey
114 * Hans de Goede
115 * Jan Schmidt
116 * Mark Nauwelaerts
117 * Michael Smith
118 * René Stadler
119 * Roland Moser
120 * Sebastian Dröge
121 * Simon Holm Thøgersen
122 * Stefan Kost
123 * Tim-Philipp Müller
124 * Wim Taymans
125 * Yves Lefebvre
126 * Zaheer Merali