1 * check qcam plugin; it includes source of the qcam package that might
2 be librified
4 * check xvideo; the flags need better handling but first try to understand
5 it better ;)
7 * check SDL optimisation flags
9 * check GST_* in configure.ac, there is too much in it
11 * decide where to put the control lib
13 * work on spec file :
14 add plugins with AC stuff (maybe from bits ?)
15 write script that builds rpm's one from one
16 get postun script right; gstreamer-register should be installed for example
18 * check options in a52, it has some arch stuff and some opti stuff that
19 looks dodgy
21 * what to do with the perftest in mpeg2dec ?
23 * riff: do we need those cflags ?
25 * festival should have checks and stuff and added properly
27 * fix ffmpeg
29 * add ladspa header check stuff