asfdemux: don't leak payload bufs in gst_asf_demux_free_stream
[glsdk/gst-plugins-ugly0-10.git] / configure.ac
1 AC_PREREQ(2.60)
3 dnl please read gstreamer/docs/random/autotools before changing this file
5 dnl initialize autoconf
6 dnl releases only do -Wall, cvs and prerelease does -Werror too
7 dnl use a three digit version number for releases, and four for cvs/prerelease
8 AC_INIT(GStreamer Ugly Plug-ins, 0.10.18.3,
9     http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer,
10     gst-plugins-ugly)
12 AG_GST_INIT
14 dnl initialize automake
15 AM_INIT_AUTOMAKE([-Wno-portability 1.10])
17 dnl define PACKAGE_VERSION_* variables
18 AS_VERSION
20 dnl check if this is a release version
21 AS_NANO(GST_GIT="no", GST_GIT="yes")
23 dnl can autoconf find the source ?
24 AC_CONFIG_SRCDIR([ext/mad/gstmad.c])
26 dnl define the output header for config
27 AM_CONFIG_HEADER(config.h)
29 dnl AM_MAINTAINER_MODE only provides the option to configure to enable it
30 AM_MAINTAINER_MODE
32 dnl sets host_* variables
33 AC_CANONICAL_HOST
35 dnl use pretty build output with automake >= 1.11
36 m4_ifdef([AM_SILENT_RULES],[AM_SILENT_RULES([yes])],
37   [AM_DEFAULT_VERBOSITY=1
38    AC_SUBST(AM_DEFAULT_VERBOSITY)])
40 dnl our libraries and install dirs use major.minor as a version
41 GST_MAJORMINOR=$PACKAGE_VERSION_MAJOR.$PACKAGE_VERSION_MINOR
42 dnl we override it here if we need to for the release candidate of new series
43 GST_MAJORMINOR=0.10
44 AC_SUBST(GST_MAJORMINOR)
46 dnl FIXME: this macro doesn't actually work;
47 dnl the generated libtool script has no support for the listed tags.
48 dnl So this needs to be fixed first if we want to use this
49 dnl AS_LIBTOOL_TAGS([CXX])
51 AC_LIBTOOL_WIN32_DLL
52 AM_PROG_LIBTOOL
54 dnl *** required versions of GStreamer stuff ***
55 GST_REQ=0.10.35.2
56 GSTPB_REQ=0.10.35.2
58 dnl *** autotools stuff ****
60 dnl allow for different autotools
61 AS_AUTOTOOLS_ALTERNATE
63 dnl Add parameters for aclocal
64 AC_SUBST(ACLOCAL_AMFLAGS, "-I m4 -I common/m4")
66 dnl set up gettext
67 dnl the version check needs to stay here because autopoint greps for it
68 AM_GNU_GETTEXT_VERSION(0.17)
69 AM_GNU_GETTEXT([external])
70 AG_GST_GETTEXT([gst-plugins-ugly-$GST_MAJORMINOR])
72 dnl *** check for arguments to configure ***
74 AG_GST_ARG_DEBUG
75 AG_GST_ARG_PROFILING
76 AG_GST_ARG_VALGRIND
77 AG_GST_ARG_GCOV
79 AG_GST_ARG_EXAMPLES
81 AG_GST_ARG_WITH_PKG_CONFIG_PATH
82 AG_GST_ARG_WITH_PACKAGE_NAME
83 AG_GST_ARG_WITH_PACKAGE_ORIGIN
85 AG_GST_ARG_WITH_PLUGINS
87 AG_GST_ARG_ENABLE_EXTERNAL
89 AG_GST_ARG_ENABLE_EXPERIMENTAL
91 dnl *** checks for platform ***
93 dnl * hardware/architecture *
95 dnl common/m4/gst-arch.m4
96 dnl check CPU type
97 AG_GST_ARCH
99 dnl Determine endianness
100 AC_C_BIGENDIAN
102 dnl *** checks for programs ***
104 dnl find a compiler
105 AC_PROG_CC
106 AC_PROG_CC_STDC
108 dnl determine c++ compiler
109 AC_PROG_CXX
110 dnl determine if c++ is available on this system
111 AC_CHECK_PROG(HAVE_CXX, $CXX, yes, no)
113 dnl check if the compiler supports '-c' and '-o' options
114 AM_PROG_CC_C_O
116 AC_PATH_PROG(VALGRIND_PATH, valgrind, no)
117 AM_CONDITIONAL(HAVE_VALGRIND, test ! "x$VALGRIND_PATH" = "xno")
119 dnl check if the compiler supports do while(0) macros
120 AG_GST_CHECK_DOWHILE_MACROS
122 dnl check for documentation tools
123 GTK_DOC_CHECK([1.3])
124 AS_PATH_PYTHON([2.1])
125 AG_GST_PLUGIN_DOCS([1.3],[2.1])
127 dnl *** checks for libraries ***
129 dnl check for libm, for sin()
130 AC_CHECK_LIBM
131 AC_SUBST(LIBM)
133 dnl *** checks for header files ***
135 dnl used by ext/a52dec
136 AX_CREATE_STDINT_H
138 dnl Check for malloc.h
139 AC_CHECK_HEADERS([malloc.h])
141 dnl *** checks for types/defines ***
143 dnl *** checks for structures ***
145 dnl *** checks for compiler characteristics ***
147 dnl *** checks for library functions ***
149 dnl Check for a way to display the function name in debug output
150 AG_GST_CHECK_FUNCTION
152 dnl *** checks for dependency libraries ***
154 dnl GLib is required
155 AG_GST_GLIB_CHECK([2.24])
156 ORC_CHECK([0.4.11])
158 dnl checks for gstreamer
159 dnl uninstalled is selected preferentially -- see pkg-config(1)
160 AG_GST_CHECK_GST($GST_MAJORMINOR, [$GST_REQ], yes)
161 AG_GST_CHECK_GST_BASE($GST_MAJORMINOR, [$GST_REQ], yes)
162 AG_GST_CHECK_GST_CHECK($GST_MAJORMINOR, [$GST_REQ], no)
163 AG_GST_CHECK_GST_PLUGINS_BASE($GST_MAJORMINOR, [$GSTPB_REQ], yes)
164 AM_CONDITIONAL(HAVE_GST_CHECK, test "x$HAVE_GST_CHECK" = "xyes")
166 dnl Check for documentation xrefs
167 GLIB_PREFIX="`$PKG_CONFIG --variable=prefix glib-2.0`"
168 GST_PREFIX="`$PKG_CONFIG --variable=prefix gstreamer-$GST_MAJORMINOR`"
169 GSTPB_PREFIX="`$PKG_CONFIG --variable=prefix gstreamer-plugins-base-$GST_MAJORMINOR`"
170 AC_SUBST(GLIB_PREFIX)
171 AC_SUBST(GST_PREFIX)
172 AC_SUBST(GSTPB_PREFIX)
174 dnl *** set variables based on configure arguments ***
176 dnl set license and copyright notice
177 GST_LICENSE="LGPL"
178 AC_DEFINE_UNQUOTED(GST_LICENSE, "$GST_LICENSE", [GStreamer license])
179 AC_SUBST(GST_LICENSE)
181 dnl set location of plugin directory
182 AG_GST_SET_PLUGINDIR
184 dnl set release date/time
185 AG_GST_SET_PACKAGE_RELEASE_DATETIME_WITH_NANO([$PACKAGE_VERSION_NANO],
186   ["${srcdir}/gst-plugins-ugly.doap"],
187   [$PACKAGE_VERSION_MAJOR.$PACKAGE_VERSION_MINOR.$PACKAGE_VERSION_MICRO])
189 dnl define an ERROR_CFLAGS Makefile variable
190 AG_GST_SET_ERROR_CFLAGS($GST_GIT, [
191     -Wmissing-declarations -Wmissing-prototypes -Wredundant-decls
192     -Wwrite-strings -Wformat-nonliteral -Wformat-security -Wold-style-definition
193     -Winit-self -Wmissing-include-dirs -Waddress
194     -Waggregate-return -Wno-multichar -Wnested-externs ])
196 dnl define an ERROR_CXXFLAGS Makefile variable
197 AG_GST_SET_ERROR_CXXFLAGS($GST_GIT, [
198     -Wmissing-declarations -Wredundant-decls
199     -Wwrite-strings -Wformat-nonliteral -Wformat-security
200     -Winit-self -Wmissing-include-dirs -Waddress -Waggregate-return
201     -Wno-multichar])
203 dnl define correct level for debugging messages
204 AG_GST_SET_LEVEL_DEFAULT($GST_GIT)
206 dnl used in examples
207 AG_GST_DEFAULT_ELEMENTS
209 dnl *** plug-ins to include ***
211 dnl these are all the gst plug-ins, compilable without additional libs
212 AG_GST_CHECK_PLUGIN(asfdemux)
213 AG_GST_CHECK_PLUGIN(dvdlpcmdec)
214 AG_GST_CHECK_PLUGIN(dvdsub)
215 AG_GST_CHECK_PLUGIN(iec958)
216 AG_GST_CHECK_PLUGIN(mpegaudioparse)
217 AG_GST_CHECK_PLUGIN(mpegstream)
218 AG_GST_CHECK_PLUGIN(realmedia)
219 AG_GST_CHECK_PLUGIN(synaesthesia)
221 AC_CHECK_HEADERS([winsock2.h], HAVE_WINSOCK2_H=yes)
223 if test "x$HAVE_WINSOCK2_H" = "xyes"; then
224   WIN32_LIBS="-lws2_32"
225   AC_SUBST(WIN32_LIBS)
226 fi
228 dnl disable experimental plug-ins
229 if test "x$BUILD_EXPERIMENTAL" != "xyes"; then
230   AG_GST_DISABLE_PLUGIN(synaesthesia)
231 fi
233 dnl *** ext plug-ins ***
234 dnl keep this list sorted alphabetically !
236 if test "x$BUILD_EXTERNAL" = "xyes"; then
238 echo
239 AC_MSG_NOTICE([Checking libraries for plugins in ext/])
240 echo
242 dnl *** a52dec ***
243 translit(dnm, m, l) AM_CONDITIONAL(USE_A52DEC, true)
244 AG_GST_CHECK_FEATURE(A52DEC, [a52dec], a52dec, [
245   AC_CHECK_A52DEC(HAVE_A52DEC=yes, HAVE_A52DEC=no)
246 ])
248 dnl *** amr-nb ***
249 translit(dnm, m, l) AM_CONDITIONAL(USE_AMRNB, true)
250 AG_GST_CHECK_FEATURE(AMRNB, [amrnb library], amrnb, [
251   PKG_CHECK_MODULES(AMRNB, opencore-amrnb, HAVE_AMRNB="yes",
252       [ AG_GST_CHECK_LIBHEADER(AMRNB, opencore-amrnb,
253                            Decoder_Interface_init, $LIBM,
254                            opencore-amrnb/interf_dec.h,
255                            AMRNB_LIBS="-lopencore-amrnb")
256       ])
257   AC_SUBST(AMRNB_CFLAGS)
258   AC_SUBST(AMRNB_LIBS)
259 ])
261 dnl *** amr-wb dec ***
262 translit(dnm, m, l) AM_CONDITIONAL(USE_AMRWB, true)
263 AG_GST_CHECK_FEATURE(AMRWB, [amrwb library], amrwbdec, [
264   PKG_CHECK_MODULES(AMRWB, opencore-amrwb, HAVE_AMRWB="yes",
265       [ AG_GST_CHECK_LIBHEADER(AMRWB, opencore-amrwb,
266                            D_IF_decode, ,
267                            opencore-amrwb/dec_if.h,
268                            AMRWB_LIBS="-lopencore-amrwb")
269       ])
270   AC_SUBST(AMRWB_CFLAGS)
271   AC_SUBST(AMRWB_LIBS)
272 ])
274 dnl *** cdio ***
275 translit(dnm, m, l) AM_CONDITIONAL(USE_CDIO, true)
276 AG_GST_CHECK_FEATURE(CDIO, [cdio library], cdio, [
277   AG_GST_PKG_CHECK_MODULES(CDIO, libcdio >= 0.76)
278 ])
280 dnl *** dvdread ***
281 translit(dnm, m, l) AM_CONDITIONAL(USE_DVDREAD, true)
282 AG_GST_CHECK_FEATURE(DVDREAD, [dvdread library], dvdreadsrc, [
283   AG_GST_CHECK_LIBHEADER(DVDREAD, dvdread, DVDOpen, , dvdread/dvd_reader.h, DVDREAD_LIBS="-ldvdread")
284   AC_SUBST(DVDREAD_LIBS)
285 ])
287 dnl *** lame ***
288 translit(dnm, m, l) AM_CONDITIONAL(USE_LAME, true)
289 AG_GST_CHECK_FEATURE(LAME, [lame mp3 encoder library], lame, [
290   AG_GST_CHECK_LIBHEADER(LAME, mp3lame, lame_init, $LIBM, lame/lame.h,
291   [
292     HAVE_LAME="yes"
293     LAME_LIBS="-lmp3lame $LIBM"
294     dnl is lame presets available
295     LAME_CFLAGS=""
296     AC_TRY_COMPILE([#include <lame/lame.h>], [ int preset = MEDIUM ],
297       [LAME_CFLAGS="-DGSTLAME_PRESET"],
298       [LAME_CFLAGS=""]
299     )
300     AC_TRY_COMPILE([#include <lame/lame.h>], [
301         void *ptr = &lame_set_VBR_quality
302       ],
303       [LAME_CFLAGS="$LAME_CFLAGS -DHAVE_LAME_SET_VBR_QUALITY"],
304       [LAME_CFLAGS="$LAME_CFLAGS"]
305     )
306   AC_SUBST(LAME_CFLAGS)
307   AC_SUBST(LAME_LIBS)
308   ])
309 ])
311 dnl *** mad ***
312 translit(dnm, m, l) AM_CONDITIONAL(USE_MAD, true)
313 AG_GST_CHECK_FEATURE(MAD, [mad mp3 decoder], mad, [
315   dnl check with pkg-config first
316   AG_GST_PKG_CHECK_MODULES(MAD, mad >= 0.15)
317   MAD_LIBS="$MAD_LIBS"
318   if test "x$HAVE_MAD" = "xno"; then
319     dnl fall back to oldskool detection
320     AC_CHECK_HEADER(mad.h, [
321       AC_CHECK_LIB(mad, mad_decoder_finish,
322         HAVE_MAD="yes" MAD_LIBS="-lmad")
323     ])
324   fi
325 ])
326 AC_SUBST(MAD_LIBS)
328 dnl *** mpeg2dec ***
329 translit(dnm, m, l) AM_CONDITIONAL(USE_MPEG2DEC, true)
330 AG_GST_CHECK_FEATURE(MPEG2DEC, [mpeg2dec], mpeg2dec, [
331   AG_GST_PKG_CHECK_MODULES(MPEG2DEC, libmpeg2 >= 0.4.0)
332 ])
334 dnl *** sidplay : works with libsidplay 1.36.x (not 2.x.x) ***
335 translit(dnm, m, l) AM_CONDITIONAL(USE_SIDPLAY, true)
336 AG_GST_CHECK_FEATURE(SIDPLAY, [libsidplay], sid, [
337   GST_PATH_SIDPLAY()
338 ])
340 dnl *** twolame ***
341 translit(dnm, m, l) AM_CONDITIONAL(USE_TWOLAME, true)
342 AG_GST_CHECK_FEATURE(TWOLAME, [twolame], twolame, [
343   PKG_CHECK_MODULES(TWOLAME, twolame >= 0.3.10, [
344       HAVE_TWOLAME="yes"], [
345       HAVE_TWOLAME="no"
346   ])
347   AC_SUBST(TWOLAME_CFLAGS)
348   AC_SUBST(TWOLAME_LIBS)
349 ])
351 dnl *** x264 (MPEG-4 part 10/h.264/AVC encoder) ***
352 translit(dnm, m, l) AM_CONDITIONAL(USE_X264, true)
353 AG_GST_CHECK_FEATURE(X264, [x264 plug-in], x264, [
354   AG_GST_PKG_CHECK_MODULES(X264, x264 >= 0.55.0)
355 ])
357 else
359 dnl not building plugins with external dependencies,
360 dnl but we still need to set the conditionals
362 AM_CONDITIONAL(USE_A52DEC, false)
363 AM_CONDITIONAL(USE_AMRNB, false)
364 AM_CONDITIONAL(USE_AMRWB, false)
365 AM_CONDITIONAL(USE_CDIO, false)
366 AM_CONDITIONAL(USE_DVDREAD, false)
367 AM_CONDITIONAL(USE_LAME, false)
368 AM_CONDITIONAL(USE_MAD, false)
369 AM_CONDITIONAL(USE_MPEG2DEC, false)
370 AM_CONDITIONAL(USE_SIDPLAY, false)
371 AM_CONDITIONAL(USE_TWOLAME, false)
372 AM_CONDITIONAL(USE_X264, false)
374 fi dnl of EXT plugins
376 dnl *** finalize CFLAGS, LDFLAGS, LIBS
378 dnl Overview:
379 dnl GST_OPTION_CFLAGS:  common flags for profiling, debugging, errors, ...
380 dnl GST_*:              flags shared by built objects to link against GStreamer
381 dnl GST_ALL_LDFLAGS:    linker flags shared by all
382 dnl GST_LIB_LDFLAGS:    additional linker flags for all libaries
383 dnl GST_LT_LDFLAGS:     library versioning of our libraries
384 dnl GST_PLUGIN_LDFLAGS: flags to be used for all plugins
386 dnl GST_OPTION_CFLAGS
387 if test "x$USE_DEBUG" = xyes; then
388    PROFILE_CFLAGS="-g"
389 fi
390 AC_SUBST(PROFILE_CFLAGS)
392 if test "x$PACKAGE_VERSION_NANO" = "x1"; then
393   dnl Define _only_ during CVS (not pre-releases or releases)
394   DEPRECATED_CFLAGS="-DGST_DISABLE_DEPRECATED"
395 else
396   DEPRECATED_CFLAGS=""
397 fi
398 AC_SUBST(DEPRECATED_CFLAGS)
400 dnl every flag in GST_OPTION_CFLAGS and GST_OPTION_CXXFLAGS can be overridden
401 dnl at make time with e.g. make ERROR_CFLAGS=""
402 GST_OPTION_CFLAGS="\$(WARNING_CFLAGS) \$(ERROR_CFLAGS) \$(DEBUG_CFLAGS) \$(PROFILE_CFLAGS) \$(GCOV_CFLAGS) \$(OPT_CFLAGS) \$(DEPRECATED_CFLAGS)"
403 GST_OPTION_CXXFLAGS="\$(WARNING_CXXFLAGS) \$(ERROR_CXXFLAGS) \$(DEBUG_CFLAGS) \$(PROFILE_CFLAGS) \$(GCOV_CFLAGS) \$(OPT_CFLAGS) \$(DEPRECATED_CFLAGS)"
404 AC_SUBST(GST_OPTION_CFLAGS)
405 AC_SUBST(GST_OPTION_CXXFLAGS)
407 dnl FIXME: do we want to rename to GST_ALL_* ?
408 dnl prefer internal headers to already installed ones
409 dnl also add builddir include for enumtypes and marshal
410 dnl add GST_OPTION_CFLAGS, but overridable
411 GST_CXXFLAGS="-I\$(top_srcdir)/gst-libs -I\$(top_builddir)/gst-libs $GST_CFLAGS $GLIB_EXTRA_CFLAGS \$(GST_OPTION_CXXFLAGS)"
412 GST_CFLAGS="-I\$(top_srcdir)/gst-libs -I\$(top_builddir)/gst-libs $GST_CFLAGS $GLIB_EXTRA_CFLAGS \$(GST_OPTION_CFLAGS)"
413 AC_SUBST(GST_CFLAGS)
414 AC_SUBST(GST_CXXFLAGS)
415 AC_SUBST(GST_LIBS)
417 dnl LDFLAGS really should only contain flags, not libs - they get added before
418 dnl whatevertarget_LIBS and -L flags here affect the rest of the linking
419 GST_ALL_LDFLAGS="-no-undefined"
420 AC_SUBST(GST_ALL_LDFLAGS)
422 dnl this really should only contain flags, not libs - they get added before
423 dnl whatevertarget_LIBS and -L flags here affect the rest of the linking
424 GST_PLUGIN_LDFLAGS="-module -avoid-version -export-symbols-regex '^[_]*gst_plugin_desc.*' $GST_ALL_LDFLAGS"
425 AC_SUBST(GST_PLUGIN_LDFLAGS)
427 dnl *** output files ***
429 AC_CONFIG_FILES(
430 Makefile
431 common/Makefile
432 common/m4/Makefile
433 gst-libs/Makefile
434 gst-libs/gst/Makefile
435 gst/Makefile
436 gst/asfdemux/Makefile
437 gst/dvdlpcmdec/Makefile
438 gst/dvdsub/Makefile
439 gst/iec958/Makefile
440 gst/mpegaudioparse/Makefile
441 gst/mpegstream/Makefile
442 gst/realmedia/Makefile
443 gst/synaesthesia/Makefile
444 ext/Makefile
445 ext/a52dec/Makefile
446 ext/amrnb/Makefile
447 ext/amrwbdec/Makefile
448 ext/cdio/Makefile
449 ext/dvdread/Makefile
450 ext/lame/Makefile
451 ext/mad/Makefile
452 ext/mpeg2dec/Makefile
453 ext/sidplay/Makefile
454 ext/twolame/Makefile
455 ext/x264/Makefile
456 docs/Makefile
457 docs/plugins/Makefile
458 docs/version.entities
459 tests/Makefile
460 tests/check/Makefile
461 m4/Makefile
462 po/Makefile.in
463 pkgconfig/Makefile
464 pkgconfig/gstreamer-plugins-ugly-uninstalled.pc
465 gst-plugins-ugly.spec
468 dnl Create the config.h file for Visual Studio builds
469 dnl Beware of spaces and /'s in some of the shell variable contents.
470 sed \
471     -e 's/.*config.h.in.*autoheader.*/\/* Autogenerated config.h created for win32 Visual Studio builds *\/\n\n\/* PREFIX -- specifically added for Windows for easier moving *\/\n#define PREFIX "C:\\\\gstreamer"\n\n/' \
472     -e 's/.* GETTEXT_PACKAGE$/#define GETTEXT_PACKAGE "'$GETTEXT_PACKAGE'"/' \
473     -e 's/.* GST_DATADIR$/#define GST_DATADIR PREFIX "\\\\share"/' \
474     -e 's/.* GST_LEVEL_DEFAULT$/#define GST_LEVEL_DEFAULT GST_LEVEL_ERROR/' \
475     -e 's/.* GST_LICENSE$/#define GST_LICENSE "'$GST_LICENSE'"/' \
476     -e 's/.* GST_MAJORMINOR$/#define GST_MAJORMINOR "'$GST_MAJORMINOR'"/' \
477     -e "s,.* GST_PACKAGE_NAME$,#define GST_PACKAGE_NAME \"${GST_PACKAGE_NAME}\"," \
478     -e 's/.* GST_PACKAGE_ORIGIN$/#define GST_PACKAGE_ORIGIN "Unknown package origin"/' \
479     -e "s,.* GST_PACKAGE_RELEASE_DATETIME$,#define GST_PACKAGE_RELEASE_DATETIME \"${GST_PACKAGE_RELEASE_DATETIME}\"," \
480     -e 's/.* HAVE_CPU_I386$/#define HAVE_CPU_I386 1/' \
481     -e 's/.* HAVE_FGETPOS$/#define HAVE_FGETPOS 1/' \
482     -e 's/.* HAVE_FSETPOS$/#define HAVE_FSETPOS 1/' \
483     -e 's/.* HAVE_LIBXML2$/#define HAVE_LIBXML2 1/' \
484     -e 's/.* HAVE_PROCESS_H$/#define HAVE_PROCESS_H 1/' \
485     -e 's/.* HAVE_STDLIB_H$/#define HAVE_STDLIB_H 1/' \
486     -e 's/.* HAVE_STRING_H$/#define HAVE_STRING_H 1/' \
487     -e 's/.* HAVE_SYS_STAT_H$/#define HAVE_SYS_STAT_H 1/' \
488     -e 's/.* HAVE_SYS_TYPES_H$/#define HAVE_SYS_TYPES_H 1/' \
489     -e 's/.* HAVE_WIN32$/#define HAVE_WIN32 1/' \
490     -e 's/.* HAVE_WINSOCK2_H$/#define HAVE_WINSOCK2_H 1/' \
491     -e 's/.* HOST_CPU$/#define HOST_CPU "i686"/' \
492     -e 's/.* LIBDIR$/#ifdef _DEBUG\n#  define LIBDIR PREFIX "\\\\debug\\\\lib"\n#else\n#  define LIBDIR PREFIX "\\\\lib"\n#endif/' \
493     -e 's/.* LOCALEDIR$/#define LOCALEDIR PREFIX "\\\\share\\\\locale"/' \
494     -e "s/.* PACKAGE$/#define PACKAGE \"$PACKAGE\"/" \
495     -e 's/.* PACKAGE_BUGREPORT$/#define PACKAGE_BUGREPORT "http:\/\/bugzilla.gnome.org\/enter_bug.cgi?product=GStreamer"/' \
496     -e "s/.* PACKAGE_NAME$/#define PACKAGE_NAME \"$PACKAGE_NAME\"/" \
497     -e "s/.* PACKAGE_STRING$/#define PACKAGE_STRING \"$PACKAGE_STRING\"/" \
498     -e 's/.* PACKAGE_TARNAME$/#define PACKAGE_TARNAME "'$PACKAGE_TARNAME'"/' \
499     -e 's/.* PACKAGE_VERSION$/#define PACKAGE_VERSION "'$PACKAGE_VERSION'"/' \
500     -e 's/.* PLUGINDIR$/#ifdef _DEBUG\n#  define PLUGINDIR PREFIX "\\\\debug\\\\lib\\\\gstreamer-0.10"\n#else\n#  define PLUGINDIR PREFIX "\\\\lib\\\\gstreamer-0.10"\n#endif/' \
501     -e 's/.* USE_BINARY_REGISTRY$/#define USE_BINARY_REGISTRY/' \
502     -e 's/.* VERSION$/#define VERSION "'$VERSION'"/' \
503     -e "s/.* DEFAULT_AUDIOSINK$/#define DEFAULT_AUDIOSINK \"directsoundsink\"/" \
504     -e "s/.* DEFAULT_AUDIOSRC$/#define DEFAULT_AUDIOSRC \"audiotestsrc\"/" \
505     -e "s/.* DEFAULT_VIDEOSRC$/#define DEFAULT_VIDEOSRC \"videotestsrc\"/" \
506     -e "s/.* DEFAULT_VISUALIZER$/#define DEFAULT_VISUALIZER \"goom\"/" \
507     config.h.in >win32/common/config.h-new
509 AC_OUTPUT
511 AG_GST_OUTPUT_PLUGINS
513 ORC_OUTPUT