]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gst-plugins-ugly0-10.git/blob - gst-plugins-ugly.spec.in
rmdemux: delay announcing container tags until we have pads
[glsdk/gst-plugins-ugly0-10.git] / gst-plugins-ugly.spec.in
1 %define majorminor  @GST_MAJORMINOR@
2 %define gstreamer   gstreamer
4 %define gst_minver  0.10.0
6 Name:           %{gstreamer}-plugins-ugly
7 Version:        @VERSION@
8 Release:        @PACKAGE_VERSION_RELEASE@.gst
9 Summary:        GStreamer streaming media framework "ugly" plug-ins
11 Group:          Applications/Multimedia
12 License:        LGPL
13 URL:            http://gstreamer.freedesktop.org/
14 Vendor:         GStreamer Backpackers Team <package@gstreamer.freedesktop.org>
15 Source:         http://gstreamer.freedesktop.org/src/gst-plugins-ugly/gst-plugins-ugly-%{version}.tar.gz
16 BuildRoot:      %{_tmppath}/%{name}-%{version}-%{release}-root-%(%{__id_u} -n)
18 Requires:       %{gstreamer} >= %{gst_minver}
19 BuildRequires:  %{gstreamer}-devel >= %{gst_minver}
20 BuildRequires:  gcc-c++
22 @USE_SIDPLAY_TRUE@BuildRequires:  libsidplay-devel >= 1.36.0
23 @USE_A52DEC_TRUE@BuildRequires:  a52dec-devel >= 0.7.3
24 @USE_DVDREAD_TRUE@BuildRequires:  libdvdread-devel >= 0.9.0
25 @USE_LAME_TRUE@BuildRequires:  lame-devel >= 3.89
26 @USE_MAD_TRUE@BuildRequires:  libid3tag-devel >= 0.15.0
27 @USE_MAD_TRUE@BuildRequires:  libmad-devel >= 0.15.0
28 @USE_MPEG2DEC_TRUE@BuildRequires:  mpeg2dec-devel >= 0.4.0
30 @USE_SIDPLAY_TRUE@Provides:       gstreamer-sid = %{version}-%{release}
31 @USE_LAME_TRUE@Provides:      gstreamer-lame = %{version}-%{release}
32 @USE_MAD_TRUE@Provides:       gstreamer-mad = %{version}-%{release}
33 @USE_A52DEC_TRUE@Provides:       gstreamer-a52dec = %{version}-%{release}
34 @USE_DVDREAD_TRUE@Provides:       gstreamer-dvdread = %{version}-%{release}
35 @USE_MPEG2DEC_TRUE@Provides:       gstreamer-mpeg2dec = %{version}-%{release}
37 @USE_X264_TRUE@Requires: x264-libs
39 %description
40 GStreamer is a streaming media framework, based on graphs of elements which
41 operate on media data.
43 This package contains well-written plug-ins that can't be shipped in
44 gstreamer-plugins-good because:
45 - the license is not LGPL
46 - the license of the library is not LGPL
47 - there are possible licensing issues with the code.
49 # %package devel
50 # Summary:        Development files for GStreamer Ugly Plugins
51 # Group:          Development/Libraries
52 #
53 # Requires:       %{name} = %{version}-%{release}
54 #
55 # %description devel
56 # GStreamer is a streaming media framework, based on graphs of elements which
57 # operate on media data.
58 #
59 # This package contains well-written plug-ins that can't be shipped in
60 # gstreamer-plugins-good because:
61 # - the license is not LGPL
62 # - the license of the library is not LGPL
63 # - there are possible licensing issues with the code.
64
65 # This package contains development files and documentation.
67 %prep
68 %setup -q -n gst-plugins-ugly-%{version}
69 %build
70 %configure \
71   --enable-debug \
72   --enable-gtk-doc 
74 make %{?_smp_mflags}
75                                                                                 
76 %install
77 rm -rf $RPM_BUILD_ROOT
79 # Install doc temporarily in order to be included later by rpm
80 %makeinstall
82 # Clean out files that should not be part of the rpm.
83 rm -f $RPM_BUILD_ROOT%{_libdir}/gstreamer-%{majorminor}/*.la
84 rm -f $RPM_BUILD_ROOT%{_libdir}/gstreamer-%{majorminor}/*.a
85 rm -f $RPM_BUILD_ROOT%{_libdir}/*.a
86 rm -f $RPM_BUILD_ROOT%{_libdir}/*.la
88 %find_lang gst-plugins-ugly-%{majorminor}
90 %clean
91 rm -rf $RPM_BUILD_ROOT
93 %files -f gst-plugins-ugly-%{majorminor}.lang
94 %defattr(-, root, root, -)
95 %doc AUTHORS COPYING README REQUIREMENTS gst-plugins-ugly.doap
96 %{_libdir}/gstreamer-%{majorminor}/libgstasf.so
97 %{_libdir}/gstreamer-%{majorminor}/libgstdvdlpcmdec.so
98 %{_libdir}/gstreamer-%{majorminor}/libgstiec958.so
99 %{_libdir}/gstreamer-%{majorminor}/libgstmpegaudioparse.so
100 %{_libdir}/gstreamer-%{majorminor}/libgstmpegstream.so
101 %{_libdir}/gstreamer-%{majorminor}/libgstrmdemux.so
102 %{_libdir}/gstreamer-%{majorminor}/libgstdvdsub.so
104 # plugins with dependencies
105 @USE_SIDPLAY_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstsid.so
106 @USE_LAME_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstlame.so
107 @USE_MAD_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstmad.so
108 @USE_A52DEC_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgsta52dec.so
109 @USE_DVDREAD_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstdvdread.so
110 @USE_MPEG2DEC_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstmpeg2dec.so
111 @USE_TWOLAME_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgsttwolame.so
112 %doc %{_datadir}/gtk-doc/html/gst-plugins-ugly-plugins-%{majorminor}/*
113 @USE_X264_TRUE@%{_datadir}/gstreamer-%{majorminor}/presets/GstX264Enc.prs
114 @USE_X264_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstx264.so
115 @USE_AMRNB_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstamrnb.so
116 @USE_AMRWB_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstamrwbdec.so
117 @USE_AMRNB_TRUE@%{_datadir}/gstreamer-%{majorminor}/presets/GstAmrnbEnc.prs
118 @USE_CDIO_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstcdio.so
121 %changelog
122 * Fri Jun 5 2009 Jan Schmidt <thaytan at mad dot scientist dot com>
123 - Move x264enc plugin from -bad
125 * Fri Dec 15 2006 Thomas Vander Stichele <thomas at apestaart dot org>
126 - further cleanup
127 - add .doap file
129 * Fri Sep 02 2005 Thomas Vander Stichele <thomas at apestaart dot org>
130 - clean out for split into ugly