asfdemux: avoid unnecessary stream lookup
[glsdk/gst-plugins-ugly0-10.git] / gst / asfdemux / asfpacket.c
1 /* GStreamer ASF/WMV/WMA demuxer
2  * Copyright (C) 2007 Tim-Philipp Müller <tim centricular net>
3  *
4  * This library is free software; you can redistribute it and/or
5  * modify it under the terms of the GNU Library General Public
6  * License as published by the Free Software Foundation; either
7  * version 2 of the License, or (at your option) any later version.
8  *
9  * This library is distributed in the hope that it will be useful,
10  * but WITHOUT ANY WARRANTY; without even the implied warranty of
11  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
12  * Library General Public License for more details.
13  *
14  * You should have received a copy of the GNU Library General Public
15  * License along with this library; if not, write to the
16  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
17  * Boston, MA 02111-1307, USA.
18  */
20 /* FIXME:
21  *  file:///home/tpm/samples/video/asf//336370-regis-velo862.wmv
22  *  file:///home/tpm/samples/video/asf//336370-eichhoer.wmv
23  * throw errors (not always necessarily) in this code path
24  * (looks like they carry broken payloads/packets though) */
26 #include "asfpacket.h"
28 #include <gst/gstutils.h>
29 #include <gst/gstinfo.h>
30 #include <string.h>
32 /* we are unlikely to deal with lengths > 2GB here any time soon, so just
33  * return a signed int and use that for error reporting */
34 static inline gint
35 asf_packet_read_varlen_int (guint lentype_flags, guint lentype_bit_offset,
36     const guint8 ** p_data, guint * p_size)
37 {
38   static const guint lens[4] = { 0, 1, 2, 4 };
39   guint len, val;
41   len = lens[(lentype_flags >> lentype_bit_offset) & 0x03];
43   /* will make caller bail out with a short read if there's not enough data */
44   if (G_UNLIKELY (*p_size < len)) {
45     GST_WARNING ("need %u bytes, but only %u bytes available", len, *p_size);
46     return -1;
47   }
49   switch (len) {
50     case 0:
51       val = 0;
52       break;
53     case 1:
54       val = GST_READ_UINT8 (*p_data);
55       break;
56     case 2:
57       val = GST_READ_UINT16_LE (*p_data);
58       break;
59     case 4:
60       val = GST_READ_UINT32_LE (*p_data);
61       break;
62     default:
63       g_assert_not_reached ();
64   }
66   *p_data += len;
67   *p_size -= len;
69   return (gint) val;
70 }
72 static GstBuffer *
73 asf_packet_create_payload_buffer (AsfPacket * packet, const guint8 ** p_data,
74     guint * p_size, guint payload_len)
75 {
76   guint off;
78   g_assert (payload_len <= *p_size);
80   off = (guint) (*p_data - GST_BUFFER_DATA (packet->buf));
81   g_assert (off < GST_BUFFER_SIZE (packet->buf));
83   *p_data += payload_len;
84   *p_size -= payload_len;
86   return gst_buffer_create_sub (packet->buf, off, payload_len);
87 }
89 static AsfPayload *
90 asf_payload_find_previous_fragment (AsfPayload * payload, AsfStream * stream)
91 {
92   AsfPayload *ret;
94   if (G_UNLIKELY (stream->payloads->len == 0)) {
95     GST_DEBUG ("No previous fragments to merge with for stream %u", stream->id);
96     return NULL;
97   }
99   ret =
100       &g_array_index (stream->payloads, AsfPayload, stream->payloads->len - 1);
102   if (G_UNLIKELY (ret->mo_size != payload->mo_size ||
103           ret->mo_number != payload->mo_number || ret->mo_offset != 0)) {
104     if (payload->mo_size != 0) {
105       GST_WARNING ("Previous fragment does not match continued fragment");
106       return NULL;
107     } else {
108       /* Warn about this case, but accept it anyway: files in the wild sometimes
109        * have continued packets where the subsequent fragments say that they're
110        * zero-sized. */
111       GST_WARNING ("Previous fragment found, but current fragment has "
112           "zero size, accepting anyway");
113     }
114   }
115 #if 0
116   if (this_fragment->mo_offset + this_payload_len > first_fragment->mo_size) {
117     GST_WARNING ("Merged fragments would be bigger than the media object");
118     return FALSE;
119   }
120 #endif
122   return ret;
125 /* TODO: if we have another payload already queued for this stream and that
126  * payload doesn't have a duration, maybe we can calculate a duration for it
127  * (if the previous timestamp is smaller etc. etc.) */
128 static void
129 gst_asf_payload_queue_for_stream (GstASFDemux * demux, AsfPayload * payload,
130     AsfStream * stream)
132   GST_DEBUG_OBJECT (demux, "Got payload for stream %d ts:%" GST_TIME_FORMAT,
133       stream->id, GST_TIME_ARGS (payload->ts));
134   /* remember the first timestamp in the stream */
135   if (G_UNLIKELY (!GST_CLOCK_TIME_IS_VALID (demux->first_ts) &&
136           GST_CLOCK_TIME_IS_VALID (payload->ts))) {
137     GST_DEBUG_OBJECT (demux, "first ts: %" GST_TIME_FORMAT,
138         GST_TIME_ARGS (payload->ts));
139     demux->first_ts = payload->ts;
140   }
142   /* make timestamps start from 0 */
143   if (G_LIKELY (demux->first_ts < payload->ts))
144     payload->ts -= demux->first_ts;
145   else
146     payload->ts = 0;
148   /* remove any incomplete payloads that will never be completed */
149   while (stream->payloads->len > 0) {
150     AsfPayload *prev;
151     guint idx_last;
153     idx_last = stream->payloads->len - 1;
154     prev = &g_array_index (stream->payloads, AsfPayload, idx_last);
156     if (G_UNLIKELY (gst_asf_payload_is_complete (prev)))
157       break;
159     GST_DEBUG_OBJECT (demux, "Dropping incomplete fragmented media object "
160         "queued for stream %u", stream->id);
162     gst_buffer_replace (&prev->buf, NULL);
163     g_array_remove_index (stream->payloads, idx_last);
165     /* there's data missing, so there's a discontinuity now */
166     GST_BUFFER_FLAG_SET (payload->buf, GST_BUFFER_FLAG_DISCONT);
167   }
169   /* If we're about to queue a key frame that is before the segment start, we
170    * can ditch any previously queued payloads (which would also be before the
171    * segment start). This makes sure the decoder doesn't decode more than
172    * absolutely necessary after a seek (we don't push out payloads that are
173    * before the segment start until we have at least one that falls within the
174    * segment) */
175   if (G_UNLIKELY (GST_CLOCK_TIME_IS_VALID (payload->ts) &&
176           payload->ts < demux->segment.start && payload->keyframe)) {
177     GST_DEBUG_OBJECT (demux, "Queueing keyframe before segment start, removing"
178         " %u previously-queued payloads, which would be out of segment too and"
179         " hence don't have to be decoded", stream->payloads->len);
180     while (stream->payloads->len > 0) {
181       AsfPayload *last;
182       guint idx_last;
184       idx_last = stream->payloads->len - 1;
185       last = &g_array_index (stream->payloads, AsfPayload, idx_last);
186       gst_buffer_replace (&last->buf, NULL);
187       g_array_remove_index (stream->payloads, idx_last);
188     }
190     /* Mark discontinuity (should be done via stream->discont anyway though) */
191     GST_BUFFER_FLAG_SET (payload->buf, GST_BUFFER_FLAG_DISCONT);
192   }
194   /* remember the first queued timestamp for the segment */
195   if (G_UNLIKELY (!GST_CLOCK_TIME_IS_VALID (demux->segment_ts) &&
196           GST_CLOCK_TIME_IS_VALID (payload->ts))) {
197     GST_DEBUG_OBJECT (demux, "segment ts: %" GST_TIME_FORMAT,
198         GST_TIME_ARGS (payload->ts));
199     demux->segment_ts = payload->ts;
200     /* always note, but only determines segment when streaming */
201     if (demux->streaming)
202       gst_segment_set_seek (&demux->segment, demux->in_segment.rate,
203           GST_FORMAT_TIME, demux->segment.flags, GST_SEEK_TYPE_SET,
204           demux->segment_ts, GST_SEEK_TYPE_NONE, 0, NULL);
205   }
207   g_array_append_vals (stream->payloads, payload, 1);
210 static void
211 asf_payload_parse_replicated_data_extensions (AsfStream * stream,
212     AsfPayload * payload)
214   AsfPayloadExtension *ext;
215   guint off;
217   if (!stream->ext_props.valid || stream->ext_props.payload_extensions == NULL)
218     return;
220   off = 8;
221   for (ext = stream->ext_props.payload_extensions; ext->len > 0; ++ext) {
222     if (G_UNLIKELY (off + ext->len > payload->rep_data_len)) {
223       GST_WARNING ("not enough replicated data for defined extensions");
224       return;
225     }
226     switch (ext->id) {
227       case ASF_PAYLOAD_EXTENSION_DURATION:
228         if (G_LIKELY (ext->len == 2)) {
229           guint16 tdur = GST_READ_UINT16_LE (payload->rep_data + off);
230           /* packet durations of 1ms are mostly invalid */
231           if (tdur != 1)
232             payload->duration = tdur * GST_MSECOND;
233         } else {
234           GST_WARNING ("unexpected DURATION extensions len %u", ext->len);
235         }
236         break;
237       case ASF_PAYLOAD_EXTENSION_SYSTEM_CONTENT:
238         if (G_LIKELY (ext->len == 1)) {
239           guint8 data = payload->rep_data[off];
241           payload->interlaced = data & 0x1;
242           payload->rff = data & 0x8;
243           payload->tff = (data & 0x2) || !(data & 0x4);
244           GST_DEBUG ("SYSTEM_CONTENT: interlaced:%d, rff:%d, tff:%d",
245               payload->interlaced, payload->rff, payload->tff);
246         } else {
247           GST_WARNING ("unexpected SYSTEM_CONTE extensions len %u", ext->len);
248         }
249         break;
250       case ASF_PAYLOAD_EXTENSION_SYSTEM_PIXEL_ASPECT_RATIO:
251         if (G_LIKELY (ext->len == 2)) {
252           payload->par_x = payload->rep_data[off];
253           payload->par_y = payload->rep_data[off + 1];
254           GST_DEBUG ("PAR %d / %d", payload->par_x, payload->par_y);
255         } else {
256           GST_WARNING ("unexpected SYSTEM_PIXEL_ASPECT_RATIO extensions len %u",
257               ext->len);
258         }
259         break;
260       default:
261         GST_WARNING ("UNKNOWN PAYLOAD EXTENSION !");
262         break;
263     }
264     off += ext->len;
265   }
268 static gboolean
269 gst_asf_demux_parse_payload (GstASFDemux * demux, AsfPacket * packet,
270     gint lentype, const guint8 ** p_data, guint * p_size)
272   AsfPayload payload = { 0, };
273   AsfStream *stream;
274   gboolean is_compressed;
275   guint payload_len;
276   guint stream_num;
278   if (G_UNLIKELY (*p_size < 1)) {
279     GST_WARNING_OBJECT (demux, "Short packet!");
280     return FALSE;
281   }
283   stream_num = GST_READ_UINT8 (*p_data) & 0x7f;
284   payload.keyframe = ((GST_READ_UINT8 (*p_data) & 0x80) != 0);
286   *p_data += 1;
287   *p_size -= 1;
289   payload.ts = GST_CLOCK_TIME_NONE;
290   payload.duration = GST_CLOCK_TIME_NONE;
291   payload.par_x = 0;
292   payload.par_y = 0;
293   payload.interlaced = FALSE;
294   payload.tff = FALSE;
295   payload.rff = FALSE;
297   payload.mo_number =
298       asf_packet_read_varlen_int (packet->prop_flags, 4, p_data, p_size);
299   payload.mo_offset =
300       asf_packet_read_varlen_int (packet->prop_flags, 2, p_data, p_size);
301   payload.rep_data_len =
302       asf_packet_read_varlen_int (packet->prop_flags, 0, p_data, p_size);
304   is_compressed = (payload.rep_data_len == 1);
306   GST_LOG_OBJECT (demux, "payload for stream %u", stream_num);
307   GST_LOG_OBJECT (demux, "keyframe   : %s", (payload.keyframe) ? "yes" : "no");
308   GST_LOG_OBJECT (demux, "compressed : %s", (is_compressed) ? "yes" : "no");
310   if (G_UNLIKELY (*p_size < payload.rep_data_len)) {
311     GST_WARNING_OBJECT (demux, "Short packet! rep_data_len=%u, size=%u",
312         payload.rep_data_len, *p_size);
313     return FALSE;
314   }
316   memcpy (payload.rep_data, *p_data,
317       MIN (sizeof (payload.rep_data), payload.rep_data_len));
319   *p_data += payload.rep_data_len;
320   *p_size -= payload.rep_data_len;
322   if (G_UNLIKELY (*p_size == 0)) {
323     GST_WARNING_OBJECT (demux, "payload without data!?");
324     return FALSE;
325   }
327   /* we use -1 as lentype for a single payload that's the size of the packet */
328   if (G_UNLIKELY ((lentype >= 0 && lentype <= 3))) {
329     payload_len = asf_packet_read_varlen_int (lentype, 0, p_data, p_size);
330     if (*p_size < payload_len) {
331       GST_WARNING_OBJECT (demux, "Short packet! payload_len=%u, size=%u",
332           payload_len, *p_size);
333       return FALSE;
334     }
335   } else {
336     payload_len = *p_size;
337   }
339   GST_LOG_OBJECT (demux, "payload length: %u", payload_len);
341   stream = gst_asf_demux_get_stream (demux, stream_num);
343   if (G_UNLIKELY (stream == NULL)) {
344     GST_WARNING_OBJECT (demux, "Payload for unknown stream %u, skipping",
345         stream_num);
346     if (*p_size < payload_len) {
347       *p_data += *p_size;
348       *p_size = 0;
349     } else {
350       *p_data += payload_len;
351       *p_size -= payload_len;
352     }
353     return TRUE;
354   }
356   if (G_UNLIKELY (!is_compressed)) {
357     GST_LOG_OBJECT (demux, "replicated data length: %u", payload.rep_data_len);
359     if (payload.rep_data_len >= 8) {
360       payload.mo_size = GST_READ_UINT32_LE (payload.rep_data);
361       payload.ts = GST_READ_UINT32_LE (payload.rep_data + 4) * GST_MSECOND;
362       if (G_UNLIKELY (payload.ts < demux->preroll))
363         payload.ts = 0;
364       else
365         payload.ts -= demux->preroll;
366       asf_payload_parse_replicated_data_extensions (stream, &payload);
368       GST_LOG_OBJECT (demux, "media object size   : %u", payload.mo_size);
369       GST_LOG_OBJECT (demux, "media object ts     : %" GST_TIME_FORMAT,
370           GST_TIME_ARGS (payload.ts));
371       GST_LOG_OBJECT (demux, "media object dur    : %" GST_TIME_FORMAT,
372           GST_TIME_ARGS (payload.duration));
373     } else if (payload.rep_data_len != 0) {
374       GST_WARNING_OBJECT (demux, "invalid replicated data length, very bad");
375       *p_data += payload_len;
376       *p_size -= payload_len;
377       return FALSE;
378     }
380     GST_LOG_OBJECT (demux, "media object offset : %u", payload.mo_offset);
382     GST_LOG_OBJECT (demux, "payload length: %u", payload_len);
384     if (payload_len > 0) {
385       payload.buf = asf_packet_create_payload_buffer (packet, p_data, p_size,
386           payload_len);
388       /* n-th fragment of a fragmented media object? */
389       if (payload.mo_offset != 0) {
390         AsfPayload *prev;
392         if ((prev = asf_payload_find_previous_fragment (&payload, stream))) {
393           if (payload.mo_offset != GST_BUFFER_SIZE (prev->buf)) {
394             GST_WARNING_OBJECT (demux, "Offset doesn't match previous data?!");
395           }
396           /* note: buffer join/merge might not preserve buffer flags */
397           prev->buf = gst_buffer_join (prev->buf, payload.buf);
398           GST_LOG_OBJECT (demux, "Merged fragments, merged size: %u",
399               GST_BUFFER_SIZE (prev->buf));
400         } else {
401           gst_buffer_unref (payload.buf);
402         }
403         payload.buf = NULL;
404       } else {
405         gst_asf_payload_queue_for_stream (demux, &payload, stream);
406       }
407     }
408   } else {
409     const guint8 *payload_data;
410     GstClockTime ts, ts_delta;
411     guint num;
413     GST_LOG_OBJECT (demux, "Compressed payload, length=%u", payload_len);
415     payload_data = *p_data;
417     *p_data += payload_len;
418     *p_size -= payload_len;
420     ts = payload.mo_offset * GST_MSECOND;
421     if (G_UNLIKELY (ts < demux->preroll))
422       ts = 0;
423     else
424       ts -= demux->preroll;
425     ts_delta = payload.rep_data[0] * GST_MSECOND;
427     for (num = 0; payload_len > 0; ++num) {
428       guint sub_payload_len;
430       sub_payload_len = GST_READ_UINT8 (payload_data);
432       GST_LOG_OBJECT (demux, "subpayload #%u: len=%u, ts=%" GST_TIME_FORMAT,
433           num, sub_payload_len, GST_TIME_ARGS (ts));
435       ++payload_data;
436       --payload_len;
438       if (G_UNLIKELY (payload_len < sub_payload_len)) {
439         GST_WARNING_OBJECT (demux, "Short payload! %u bytes left", payload_len);
440         return FALSE;
441       }
443       if (G_LIKELY (sub_payload_len > 0)) {
444         payload.buf = asf_packet_create_payload_buffer (packet,
445             &payload_data, &payload_len, sub_payload_len);
447         payload.ts = ts;
448         if (G_LIKELY (ts_delta))
449           payload.duration = ts_delta;
450         else
451           payload.duration = GST_CLOCK_TIME_NONE;
453         gst_asf_payload_queue_for_stream (demux, &payload, stream);
454       }
456       ts += ts_delta;
457     }
458   }
460   return TRUE;
463 gboolean
464 gst_asf_demux_parse_packet (GstASFDemux * demux, GstBuffer * buf)
466   AsfPacket packet = { 0, };
467   const guint8 *data;
468   gboolean has_multiple_payloads;
469   gboolean ret = TRUE;
470   guint8 ec_flags, flags1;
471   guint size;
473   data = GST_BUFFER_DATA (buf);
474   size = GST_BUFFER_SIZE (buf);
475   GST_LOG_OBJECT (demux, "Buffer size: %u", size);
477   /* need at least two payload flag bytes, send time, and duration */
478   if (G_UNLIKELY (size < 2 + 4 + 2))
479     goto short_packet;
481   packet.buf = buf;
483   ec_flags = GST_READ_UINT8 (data);
485   /* skip optional error correction stuff */
486   if ((ec_flags & 0x80) != 0) {
487     guint ec_len_type, ec_len;
489     ec_len_type = (ec_flags & 0x60) >> 5;
490     if (ec_len_type == 0) {
491       ec_len = ec_flags & 0x0f;
492     } else {
493       GST_WARNING_OBJECT (demux, "unexpected error correction length type %u",
494           ec_len_type);
495       ec_len = 2;
496     }
497     GST_LOG_OBJECT (demux, "packet has error correction (%u bytes)", ec_len);
499     /* still need at least two payload flag bytes, send time, and duration */
500     if (size <= (1 + ec_len) + 2 + 4 + 2)
501       goto short_packet;
503     data += 1 + ec_len;
504     size -= 1 + ec_len;
505   }
507   /* parse payload info */
508   flags1 = GST_READ_UINT8 (data);
509   packet.prop_flags = GST_READ_UINT8 (data + 1);
511   data += 2;
512   size -= 2;
514   has_multiple_payloads = (flags1 & 0x01) != 0;
516   packet.length = asf_packet_read_varlen_int (flags1, 5, &data, &size);
518   packet.sequence = asf_packet_read_varlen_int (flags1, 1, &data, &size);
520   packet.padding = asf_packet_read_varlen_int (flags1, 3, &data, &size);
522   if (G_UNLIKELY (size < 6))
523     goto short_packet;
525   packet.send_time = GST_READ_UINT32_LE (data) * GST_MSECOND;
526   packet.duration = GST_READ_UINT16_LE (data + 4) * GST_MSECOND;
528   data += 4 + 2;
529   size -= 4 + 2;
531   GST_LOG_OBJECT (demux, "flags            : 0x%x", flags1);
532   GST_LOG_OBJECT (demux, "multiple payloads: %u", has_multiple_payloads);
533   GST_LOG_OBJECT (demux, "packet length    : %u", packet.length);
534   GST_LOG_OBJECT (demux, "sequence         : %u", packet.sequence);
535   GST_LOG_OBJECT (demux, "padding          : %u", packet.padding);
536   GST_LOG_OBJECT (demux, "send time        : %" GST_TIME_FORMAT,
537       GST_TIME_ARGS (packet.send_time));
538   GST_LOG_OBJECT (demux, "duration         : %" GST_TIME_FORMAT,
539       GST_TIME_ARGS (packet.duration));
541   if (G_UNLIKELY (packet.padding == (guint) - 1 || size < packet.padding))
542     goto short_packet;
544   size -= packet.padding;
546   /* adjust available size for parsing if there's less actual packet data for
547    * parsing than there is data in bytes (for sample see bug 431318) */
548   if (G_UNLIKELY (packet.length != 0 && packet.padding == 0
549           && packet.length < demux->packet_size)) {
550     GST_LOG_OBJECT (demux, "shortened packet with implicit padding, "
551         "adjusting available data size");
552     if (size < demux->packet_size - packet.length) {
553       /* the buffer is smaller than the implicit padding */
554       goto short_packet;
555     } else {
556       /* subtract the implicit padding */
557       size -= (demux->packet_size - packet.length);
558     }
559   }
561   if (has_multiple_payloads) {
562     guint i, num, lentype;
564     if (G_UNLIKELY (size < 1))
565       goto short_packet;
567     num = (GST_READ_UINT8 (data) & 0x3F) >> 0;
568     lentype = (GST_READ_UINT8 (data) & 0xC0) >> 6;
570     ++data;
571     --size;
573     GST_LOG_OBJECT (demux, "num payloads     : %u", num);
575     for (i = 0; i < num; ++i) {
576       GST_LOG_OBJECT (demux, "Parsing payload %u/%u, size left: %u", i + 1, num,
577           size);
579       ret = gst_asf_demux_parse_payload (demux, &packet, lentype, &data, &size);
581       if (G_UNLIKELY (!ret)) {
582         GST_WARNING_OBJECT (demux, "Failed to parse payload %u/%u", i + 1, num);
583         break;
584       }
585     }
586   } else {
587     GST_LOG_OBJECT (demux, "Parsing single payload");
588     ret = gst_asf_demux_parse_payload (demux, &packet, -1, &data, &size);
589   }
591   return ret;
593 /* ERRORS */
594 short_packet:
595   {
596     GST_WARNING_OBJECT (demux, "Short packet!");
597     return FALSE;
598   }