1 /* config.h.in. Generated from configure.ac by autoheader. */
2 /* This copy of config.h.in is specifically for win32 Visual Studio builds */
4 /* Define to 1 if translation of program messages to the user's native
5 language is requested. */
6 #undef ENABLE_NLS
8 /* gettext package name */
9 #define GETTEXT_PACKAGE "gst-plugins-ugly-0.10"
11 /* macro to use to show function name */
12 #define GST_FUNCTION "(function)"
14 /* Defined if gcov is enabled to force a rebuild due to config.h changing */
15 #undef GST_GCOV_ENABLED
17 /* Default errorlevel to use */
18 #undef GST_LEVEL_DEFAULT
20 /* GStreamer license */
21 #define GST_LICENSE "LGPL"
23 /* package name in plugins */
24 #define GST_PACKAGE_NAME "GStreamer Ugly Plug-ins source release"
26 /* package origin */
27 #define GST_PACKAGE_ORIGIN "Unknown package origin"
29 /* support for features: gstalsa */
30 #undef HAVE_ALSA
32 /* support for features: cdparanoia */
33 #undef HAVE_CDPARANOIA
35 /* Define if the host CPU is an Alpha */
36 #undef HAVE_CPU_ALPHA
38 /* Define if the host CPU is an ARM */
39 #undef HAVE_CPU_ARM
41 /* Define if the host CPU is a HPPA */
42 #undef HAVE_CPU_HPPA
44 /* Define if the host CPU is an x86 */
45 #define HAVE_CPU_I386 1
47 /* Define if the host CPU is a IA64 */
48 #undef HAVE_CPU_IA64
50 /* Define if the host CPU is a M68K */
51 #undef HAVE_CPU_M68K
53 /* Define if the host CPU is a MIPS */
54 #undef HAVE_CPU_MIPS
56 /* Define if the host CPU is a PowerPC */
57 #undef HAVE_CPU_PPC
59 /* Define if the host CPU is a 64 bit PowerPC */
60 #undef HAVE_CPU_PPC64
62 /* Define if the host CPU is a S390 */
63 #undef HAVE_CPU_S390
65 /* Define if the host CPU is a SPARC */
66 #undef HAVE_CPU_SPARC
68 /* Define if the host CPU is a x86_64 */
69 #undef HAVE_CPU_X86_64
71 /* Define if the GNU dcgettext() function is already present or preinstalled.
72 */
73 #undef HAVE_DCGETTEXT
75 /* Define to 1 if you have the <dlfcn.h> header file. */
76 #undef HAVE_DLFCN_H
78 /* support for features: */
79 #undef HAVE_EXTERNAL
81 /* FIONREAD ioctl found in sys/filio.h */
82 #undef HAVE_FIONREAD_IN_SYS_FILIO
84 /* FIONREAD ioctl found in sys/ioclt.h */
85 #undef HAVE_FIONREAD_IN_SYS_IOCTL
87 /* defined if the compiler implements __func__ */
88 #undef HAVE_FUNC
90 /* defined if the compiler implements __FUNCTION__ */
91 #undef HAVE_FUNCTION
93 /* Define if the GNU gettext() function is already present or preinstalled. */
94 #undef HAVE_GETTEXT
96 /* support for features: gnomevfssrc */
97 #undef HAVE_GNOME_VFS
99 /* support for features: v4lsrc v4lmjpegsrc v4lmjpegsink */
100 #undef HAVE_GST_V4L
102 /* Define if you have the iconv() function. */
103 #undef HAVE_ICONV
105 /* Define to 1 if you have the <inttypes.h> header file. */
106 #undef HAVE_INTTYPES_H
108 /* Define to 1 if you have the `asound' library (-lasound). */
109 #undef HAVE_LIBASOUND
111 /* support for features: libvisual */
112 #undef HAVE_LIBVISUAL
114 /* Define if you have C99's lrint function. */
115 #undef HAVE_LRINT
117 /* Define if you have C99's lrintf function. */
118 #undef HAVE_LRINTF
120 /* Define to 1 if you have the <malloc.h> header file. */
121 #undef HAVE_MALLOC_H
123 /* Define to 1 if you have the <memory.h> header file. */
124 #undef HAVE_MEMORY_H
126 /* support for features: oggdemux oggmux */
127 #undef HAVE_OGG
129 /* support for features: pango */
130 #undef HAVE_PANGO
132 /* defined if the compiler implements __PRETTY_FUNCTION__ */
133 #undef HAVE_PRETTY_FUNCTION
135 /* Define if RDTSC is available */
136 #undef HAVE_RDTSC
138 /* Define to 1 if you have the <regex.h> header file. */
139 #undef HAVE_REGEX_H
141 /* Define to 1 if you have the <stdint.h> header file. */
142 #undef HAVE_STDINT_H
144 /* Define to 1 if you have the <stdlib.h> header file. */
145 #define HAVE_STDLIB_H 1
147 /* Define to 1 if you have the <strings.h> header file. */
148 #undef HAVE_STRINGS_H
150 /* Define to 1 if you have the <string.h> header file. */
151 #define HAVE_STRING_H 1
153 /* Define to 1 if you have the <sys/socket.h> header file. */
154 #undef HAVE_SYS_SOCKET_H
156 /* Define to 1 if you have the <sys/stat.h> header file. */
157 #undef HAVE_SYS_STAT_H 1
159 /* Define to 1 if you have the <sys/types.h> header file. */
160 #undef HAVE_SYS_TYPES_H 1
162 /* support for features: theoradec theoraenc */
163 #undef HAVE_THEORA
165 /* Define to 1 if you have the <unistd.h> header file. */
166 #undef HAVE_UNISTD_H
168 /* Define if valgrind should be used */
169 #undef HAVE_VALGRIND
171 /* support for features: vorbisenc vorbisdec */
172 #undef HAVE_VORBIS
174 /* defined if vorbis_synthesis_restart is present */
175 #undef HAVE_VORBIS_SYNTHESIS_RESTART
177 /* support for features: ximagesink */
178 #undef HAVE_X
180 /* support for features: xshm */
181 #undef HAVE_XSHM
183 /* support for features: xvimagesink */
184 #undef HAVE_XVIDEO
186 /* gettext locale dir */
187 #define LOCALEDIR PREFIX "\\share\\locale"
189 /* Name of package */
190 #define PACKAGE "gst-plugins-ugly"
192 /* Define to the address where bug reports for this package should be sent. */
193 #define PACKAGE_BUGREPORT "http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer"
195 /* Define to the full name of this package. */
196 #undef PACKAGE_NAME "GStreamer Ugly Plug-ins"
198 /* Define to the full name and version of this package. */
199 #undef PACKAGE_STRING "GStreamer Ugly Plug-ins 0.10.12"
201 /* Define to the one symbol short name of this package. */
202 #undef PACKAGE_TARNAME "gst-plugins-ugly"
204 /* Define to the version of this package. */
205 #undef PACKAGE_VERSION "0.10.12"
207 /* directory where plugins are located */
208 #undef PLUGINDIR
210 /* The size of a `char', as computed by sizeof. */
211 #undef SIZEOF_CHAR
213 /* The size of a `int', as computed by sizeof. */
214 #undef SIZEOF_INT
216 /* The size of a `long', as computed by sizeof. */
217 #undef SIZEOF_LONG
219 /* The size of a `short', as computed by sizeof. */
220 #undef SIZEOF_SHORT
222 /* The size of a `void*', as computed by sizeof. */
223 #undef SIZEOF_VOIDP
225 /* Define to 1 if you have the ANSI C header files. */
226 #undef STDC_HEADERS
228 /* Version number of package */
229 #define VERSION "0.10.12"
231 /* Define to 1 if your processor stores words with the most significant byte
232 first (like Motorola and SPARC, unlike Intel and VAX). */
233 #undef WORDS_BIGENDIAN
235 /* Define to 1 if the X Window System is missing or not being used. */
236 #undef X_DISPLAY_MISSING