]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gst-plugins-ugly0-10.git/blob - win32/common/config.h
win32: change how win32/common/config.h is updated
[glsdk/gst-plugins-ugly0-10.git] / win32 / common / config.h
1 /* Autogenerated config.h created for win32 Visual Studio builds */
3 /* PREFIX -- specifically added for Windows for easier moving */
4 #define PREFIX "C:\\gstreamer"
8 /* Define if building universal (internal helper macro) */
9 #undef AC_APPLE_UNIVERSAL_BUILD
11 /* Default audio sink */
12 #define DEFAULT_AUDIOSINK "directaudiosink"
14 /* Default audio source */
15 #define DEFAULT_AUDIOSRC "audiotestsrc"
17 /* Default video sink */
18 #undef DEFAULT_VIDEOSINK
20 /* Default video source */
21 #define DEFAULT_VIDEOSRC "videotestsrc"
23 /* Default visualizer */
24 #define DEFAULT_VISUALIZER "goom"
26 /* Define to 1 if translation of program messages to the user's native
27    language is requested. */
28 #undef ENABLE_NLS
30 /* gettext package name */
31 #define GETTEXT_PACKAGE "gst-plugins-ugly-0.10"
33 /* macro to use to show function name */
34 #undef GST_FUNCTION
36 /* Defined if gcov is enabled to force a rebuild due to config.h changing */
37 #undef GST_GCOV_ENABLED
39 /* Default errorlevel to use */
40 #define GST_LEVEL_DEFAULT GST_LEVEL_ERROR
42 /* GStreamer license */
43 #define GST_LICENSE "LGPL"
45 /* package name in plugins */
46 #define GST_PACKAGE_NAME "GStreamer Ugly Plug-ins git"
48 /* package origin */
49 #define GST_PACKAGE_ORIGIN "Unknown package origin"
51 /* Define to enable a52dec (used by a52dec). */
52 #undef HAVE_A52DEC
54 /* Define to enable amrnb library (used by amrnb). */
55 #undef HAVE_AMRNB
57 /* Define to enable amrwb library (used by amrwbdec). */
58 #undef HAVE_AMRWB
60 /* Define to enable cdio library (used by cdio). */
61 #undef HAVE_CDIO
63 /* Define to 1 if you have the MacOS X function CFLocaleCopyCurrent in the
64    CoreFoundation framework. */
65 #undef HAVE_CFLOCALECOPYCURRENT
67 /* Define to 1 if you have the MacOS X function CFPreferencesCopyAppValue in
68    the CoreFoundation framework. */
69 #undef HAVE_CFPREFERENCESCOPYAPPVALUE
71 /* Define if the host CPU is an Alpha */
72 #undef HAVE_CPU_ALPHA
74 /* Define if the host CPU is an ARM */
75 #undef HAVE_CPU_ARM
77 /* Define if the host CPU is a CRIS */
78 #undef HAVE_CPU_CRIS
80 /* Define if the host CPU is a CRISv32 */
81 #undef HAVE_CPU_CRISV32
83 /* Define if the host CPU is a HPPA */
84 #undef HAVE_CPU_HPPA
86 /* Define if the host CPU is an x86 */
87 #define HAVE_CPU_I386 1
89 /* Define if the host CPU is a IA64 */
90 #undef HAVE_CPU_IA64
92 /* Define if the host CPU is a M68K */
93 #undef HAVE_CPU_M68K
95 /* Define if the host CPU is a MIPS */
96 #undef HAVE_CPU_MIPS
98 /* Define if the host CPU is a PowerPC */
99 #undef HAVE_CPU_PPC
101 /* Define if the host CPU is a 64 bit PowerPC */
102 #undef HAVE_CPU_PPC64
104 /* Define if the host CPU is a S390 */
105 #undef HAVE_CPU_S390
107 /* Define if the host CPU is a SPARC */
108 #undef HAVE_CPU_SPARC
110 /* Define if the host CPU is a x86_64 */
111 #undef HAVE_CPU_X86_64
113 /* Define if the GNU dcgettext() function is already present or preinstalled.
114    */
115 #undef HAVE_DCGETTEXT
117 /* Define to 1 if you have the <dlfcn.h> header file. */
118 #undef HAVE_DLFCN_H
120 /* define for working do while(0) macros */
121 #undef HAVE_DOWHILE_MACROS
123 /* Define to enable dvdread library (used by dvdreadsrc). */
124 #undef HAVE_DVDREAD
126 /* Define to enable building of experimental plug-ins. */
127 #undef HAVE_EXPERIMENTAL
129 /* Define to enable building of plug-ins with external deps. */
130 #undef HAVE_EXTERNAL
132 /* defined if the compiler implements __func__ */
133 #undef HAVE_FUNC
135 /* defined if the compiler implements __FUNCTION__ */
136 #undef HAVE_FUNCTION
138 /* Define if the GNU gettext() function is already present or preinstalled. */
139 #undef HAVE_GETTEXT
141 /* Define if you have the iconv() function and it works. */
142 #undef HAVE_ICONV
144 /* Define to 1 if you have the <inttypes.h> header file. */
145 #undef HAVE_INTTYPES_H
147 /* Define to enable lame mp3 encoder library (used by lame). */
148 #undef HAVE_LAME
150 /* Define to enable mad mp3 decoder (used by mad). */
151 #undef HAVE_MAD
153 /* Define to 1 if you have the <malloc.h> header file. */
154 #undef HAVE_MALLOC_H
156 /* Define to 1 if you have the <memory.h> header file. */
157 #undef HAVE_MEMORY_H
159 /* Define to enable mpeg2dec (used by mpeg2dec). */
160 #undef HAVE_MPEG2DEC
162 /* defined if the compiler implements __PRETTY_FUNCTION__ */
163 #undef HAVE_PRETTY_FUNCTION
165 /* Define if RDTSC is available */
166 #undef HAVE_RDTSC
168 /* Define to enable libsidplay (used by sid). */
169 #undef HAVE_SIDPLAY
171 /* Define to 1 if you have the <stdint.h> header file. */
172 #undef HAVE_STDINT_H
174 /* Define to 1 if you have the <stdlib.h> header file. */
175 #define HAVE_STDLIB_H 1
177 /* Define to 1 if you have the <strings.h> header file. */
178 #undef HAVE_STRINGS_H
180 /* Define to 1 if you have the <string.h> header file. */
181 #define HAVE_STRING_H 1
183 /* Define to 1 if you have the <sys/stat.h> header file. */
184 #define HAVE_SYS_STAT_H 1
186 /* Define to 1 if you have the <sys/types.h> header file. */
187 #define HAVE_SYS_TYPES_H 1
189 /* Define to enable twolame (used by twolame). */
190 #undef HAVE_TWOLAME
192 /* Define to 1 if you have the <unistd.h> header file. */
193 #undef HAVE_UNISTD_H
195 /* Define if valgrind should be used */
196 #undef HAVE_VALGRIND
198 /* Define to 1 if you have the <winsock2.h> header file. */
199 #define HAVE_WINSOCK2_H 1
201 /* Define to enable x264 plug-in (used by x264). */
202 #undef HAVE_X264
204 /* the host CPU */
205 #define HOST_CPU "i686"
207 /* gettext locale dir */
208 #define LOCALEDIR PREFIX "\\share\\locale"
210 /* Define to the sub-directory in which libtool stores uninstalled libraries.
211    */
212 #undef LT_OBJDIR
214 /* Define to 1 if your C compiler doesn't accept -c and -o together. */
215 #undef NO_MINUS_C_MINUS_O
217 /* Name of package */
218 #define PACKAGE "gst-plugins-ugly"
220 /* Define to the address where bug reports for this package should be sent. */
221 #define PACKAGE_BUGREPORT "http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer"
223 /* Define to the full name of this package. */
224 #define PACKAGE_NAME "GStreamer Ugly Plug-ins"
226 /* Define to the full name and version of this package. */
227 #define PACKAGE_STRING "GStreamer Ugly Plug-ins 0.10.13.1"
229 /* Define to the one symbol short name of this package. */
230 #define PACKAGE_TARNAME "gst-plugins-ugly"
232 /* Define to the home page for this package. */
233 #undef PACKAGE_URL
235 /* Define to the version of this package. */
236 #define PACKAGE_VERSION "0.10.13.1"
238 /* directory where plugins are located */
239 #ifdef _DEBUG
240 #  define PLUGINDIR PREFIX "\\debug\\lib\\gstreamer-0.10"
241 #else
242 #  define PLUGINDIR PREFIX "\\lib\\gstreamer-0.10"
243 #endif
245 /* The size of `char', as computed by sizeof. */
246 #undef SIZEOF_CHAR
248 /* The size of `int', as computed by sizeof. */
249 #undef SIZEOF_INT
251 /* The size of `long', as computed by sizeof. */
252 #undef SIZEOF_LONG
254 /* The size of `short', as computed by sizeof. */
255 #undef SIZEOF_SHORT
257 /* The size of `void*', as computed by sizeof. */
258 #undef SIZEOF_VOIDP
260 /* Define to 1 if you have the ANSI C header files. */
261 #undef STDC_HEADERS
263 /* Version number of package */
264 #define VERSION "0.10.13.1"
266 /* Define WORDS_BIGENDIAN to 1 if your processor stores words with the most
267    significant byte first (like Motorola and SPARC, unlike Intel). */
268 #if defined AC_APPLE_UNIVERSAL_BUILD
269 # if defined __BIG_ENDIAN__
270 #  define WORDS_BIGENDIAN 1
271 # endif
272 #else
273 # ifndef WORDS_BIGENDIAN
274 #  undef WORDS_BIGENDIAN
275 # endif
276 #endif