Release notes for GStreamer Ugly Plug-ins 0.10.13 "Appointed Point" The GStreamer team is proud to announce a new release in the 0.10.x stable series of the GStreamer Ugly Plug-ins. The 0.10.x series is a stable series targeted at end users. It is not API or ABI compatible with the stable 0.8.x series. It is, however, parallel installable with the 0.8.x series. "When you have to shoot, shoot. Don't talk." There are times when the world needs a color between black and white. Quality code to match the good's, but two-timing, backstabbing and ready to sell your freedom down the river. These plug-ins might have a patent noose around their neck, or a lock-up license, or any other problem that makes you think twice about shipping them. We don't call them ugly because we like them less. Does a mother love her son less because he's not as pretty as the other ones ? No - she commends him on his great personality. These plug-ins are the life of the party. And we'll still step in and set them straight if you report any unacceptable behaviour - because there are two kinds of people in the world, my friend: those with a rope around their neck and the people who do the cutting. This module contains a set of plug-ins that have good quality and correct functionality, but distributing them might pose problems. The license on either the plug-ins or the supporting libraries might not be how we'd like. The code might be widely known to present patent problems. Distributors should check if they want/can ship these plug-ins. Other modules containing plug-ins are: gst-plugins-base contains a basic set of well-supported plug-ins gst-plugins-good contains a set of well-supported plug-ins under our preferred license gst-plugins-bad contains a set of less supported plug-ins that haven't passed the rigorous quality testing we expect Features of this release * Improve A52 decoder * Add AMR-WB decoder and AMR-NB decoder/encoder based on OpenCore codecs * ASF playback improvements * Improve mp3 parser and seeking Bugs fixed in this release * 519721 : [asfdemux] wma tags are not copied when converting to another format * 584890 : AMR plugins based on Opencore codecs * 585956 : [mp3parse] indexing improvements * 590432 : It's only possible to build the mad plugin when building id3tag as well * 591348 : AMR plugins should check for opencore-amr .pc files * 592787 : a52dec: Allow liba52 to use djbfft based IMDCT transform * 596517 : x264 element no longer compiles against changed upstream API * 598272 : a52dec leaks input buffers * 598370 : Properly detect pre-releases Download You can find source releases of gst-plugins-ugly in the download directory: http://gstreamer.freedesktop.org/src/gst-plugins-ugly/ GStreamer Homepage More details can be found on the project's website: http://gstreamer.freedesktop.org/ Support and Bugs We use GNOME's bugzilla for bug reports and feature requests: http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer Developers GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there. Interested developers of the core library, plug-ins, and applications should subscribe to the gstreamer-devel list. If there is sufficient interest we will create more lists as necessary. Applications Contributors to this release * Christian Schaller * David Schleef * Edward Hervey * Iago Toral * Jan Schmidt * Josep Torra * Mark Nauwelaerts * Mart Raudsepp * Marvin Schmidt * Michael Smith * Olivier Crête * René Stadler * Sebastian Dröge * Stefan Kost * Thiago Santos * Tim-Philipp Müller * Wim Taymans