/* GStreamer Adaptive Multi-Rate Narrow-Band (AMR-NB) plugin * Copyright (C) 2004 Ronald Bultje * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ #ifdef HAVE_CONFIG_H #include "config.h" #endif #include #include "amrnbparse.h" GST_DEBUG_CATEGORY_STATIC (amrnbparse_debug); #define GST_CAT_DEFAULT amrnbparse_debug static GstStaticPadTemplate src_template = GST_STATIC_PAD_TEMPLATE ("src", GST_PAD_SRC, GST_PAD_ALWAYS, GST_STATIC_CAPS ("audio/AMR, " "rate = (int) 8000, " "channels = (int) 1") ); static GstStaticPadTemplate sink_template = GST_STATIC_PAD_TEMPLATE ("sink", GST_PAD_SINK, GST_PAD_ALWAYS, GST_STATIC_CAPS ("audio/x-amr-nb-sh") ); static const gint block_size[16] = { 12, 13, 15, 17, 19, 20, 26, 31, 5, 0, 0, 0, 0, 0, 0, 0 }; static void gst_amrnbparse_base_init (GstAmrnbParseClass * klass); static void gst_amrnbparse_class_init (GstAmrnbParseClass * klass); static void gst_amrnbparse_init (GstAmrnbParse * amrnbparse); //static const GstFormat *gst_amrnbparse_formats (GstPad * pad); static const GstQueryType *gst_amrnbparse_querytypes (GstPad * pad); static gboolean gst_amrnbparse_query (GstPad * pad, GstQuery * query); static gboolean gst_amrnbparse_event (GstPad * pad, GstEvent * event); static GstFlowReturn gst_amrnbparse_chain (GstPad * pad, GstBuffer * buffer); static void gst_amrnbparse_loop (GstPad * pad); static gboolean gst_amrnbparse_sink_activate (GstPad * sinkpad); static GstStateChangeReturn gst_amrnbparse_state_change (GstElement * element, GstStateChange transition); static GstElementClass *parent_class = NULL; GType gst_amrnbparse_get_type (void) { static GType amrnbparse_type = 0; if (!amrnbparse_type) { static const GTypeInfo amrnbparse_info = { sizeof (GstAmrnbParseClass), (GBaseInitFunc) gst_amrnbparse_base_init, NULL, (GClassInitFunc) gst_amrnbparse_class_init, NULL, NULL, sizeof (GstAmrnbParse), 0, (GInstanceInitFunc) gst_amrnbparse_init, }; amrnbparse_type = g_type_register_static (GST_TYPE_ELEMENT, "GstAmrnbParse", &amrnbparse_info, 0); } return amrnbparse_type; } static void gst_amrnbparse_base_init (GstAmrnbParseClass * klass) { GstElementClass *element_class = GST_ELEMENT_CLASS (klass); GstElementDetails gst_amrnbparse_details = { "AMR-NB parser", "Codec/Parser/Audio", "Adaptive Multi-Rate Narrow-Band audio parser", "Ronald Bultje " }; gst_element_class_add_pad_template (element_class, gst_static_pad_template_get (&sink_template)); gst_element_class_add_pad_template (element_class, gst_static_pad_template_get (&src_template)); gst_element_class_set_details (element_class, &gst_amrnbparse_details); } static void gst_amrnbparse_class_init (GstAmrnbParseClass * klass) { GstElementClass *element_class = GST_ELEMENT_CLASS (klass); parent_class = g_type_class_peek_parent (klass); element_class->change_state = gst_amrnbparse_state_change; GST_DEBUG_CATEGORY_INIT (amrnbparse_debug, "amrnbparse", 0, "AMR-NB stream parsing"); } static void gst_amrnbparse_init (GstAmrnbParse * amrnbparse) { /* create the sink pad */ amrnbparse->sinkpad = gst_pad_new_from_template (gst_static_pad_template_get (&sink_template), "sink"); gst_pad_set_chain_function (amrnbparse->sinkpad, GST_DEBUG_FUNCPTR (gst_amrnbparse_chain)); gst_pad_set_event_function (amrnbparse->sinkpad, GST_DEBUG_FUNCPTR (gst_amrnbparse_event)); gst_pad_set_activate_function (amrnbparse->sinkpad, gst_amrnbparse_sink_activate); gst_element_add_pad (GST_ELEMENT (amrnbparse), amrnbparse->sinkpad); /* create the src pad */ amrnbparse->srcpad = gst_pad_new_from_template (gst_static_pad_template_get (&src_template), "src"); gst_pad_set_query_function (amrnbparse->srcpad, GST_DEBUG_FUNCPTR (gst_amrnbparse_query)); gst_pad_set_query_type_function (amrnbparse->srcpad, GST_DEBUG_FUNCPTR (gst_amrnbparse_querytypes)); gst_element_add_pad (GST_ELEMENT (amrnbparse), amrnbparse->srcpad); amrnbparse->adapter = gst_adapter_new (); /* init rest */ amrnbparse->ts = 0; } /* * Position querying. */ #if 0 static const GstFormat * gst_amrnbparse_formats (GstPad * pad) { static const GstFormat list[] = { GST_FORMAT_TIME, 0 }; return list; } #endif static const GstQueryType * gst_amrnbparse_querytypes (GstPad * pad) { static const GstQueryType list[] = { GST_QUERY_POSITION, 0 }; return list; } static gboolean gst_amrnbparse_query (GstPad * pad, GstQuery * query) { GstAmrnbParse *amrnbparse; gboolean res = TRUE; amrnbparse = GST_AMRNBPARSE (GST_PAD_PARENT (pad)); switch (GST_QUERY_TYPE (query)) { case GST_QUERY_POSITION: { GstFormat format; gint64 cur; gst_query_parse_position (query, &format, NULL); if (format != GST_FORMAT_TIME) return FALSE; cur = amrnbparse->ts; gst_query_set_position (query, GST_FORMAT_TIME, cur); res = TRUE; break; } case GST_QUERY_DURATION: { GstFormat format; gint64 tot; GstPad *peer; gst_query_parse_duration (query, &format, NULL); if (format != GST_FORMAT_TIME) return FALSE; tot = -1; peer = gst_pad_get_peer (amrnbparse->sinkpad); if (peer) { GstFormat pformat; gint64 pcur, ptot; pformat = GST_FORMAT_BYTES; res = gst_pad_query_position (peer, &pformat, &pcur); res &= gst_pad_query_duration (peer, &pformat, &ptot); gst_object_unref (GST_OBJECT (peer)); if (res) { tot = amrnbparse->ts * ((gdouble) ptot / pcur); } } gst_query_set_duration (query, GST_FORMAT_TIME, tot); res = TRUE; break; } default: res = gst_pad_query_default (pad, query); break; } return res; } /* * Data reading. */ static gboolean gst_amrnbparse_event (GstPad * pad, GstEvent * event) { GstAmrnbParse *amrnbparse; gboolean res; amrnbparse = GST_AMRNBPARSE (GST_PAD_PARENT (pad)); GST_LOG ("handling event %d", GST_EVENT_TYPE (event)); switch (GST_EVENT_TYPE (event)) { case GST_EVENT_EOS: default: break; } res = gst_pad_event_default (amrnbparse->sinkpad, event); return res; } /* streaming mode */ static GstFlowReturn gst_amrnbparse_chain (GstPad * pad, GstBuffer * buffer) { GstAmrnbParse *amrnbparse; GstFlowReturn res; gint block, mode; const guint8 *data; GstBuffer *out; amrnbparse = GST_AMRNBPARSE (GST_PAD_PARENT (pad)); gst_adapter_push (amrnbparse->adapter, buffer); res = GST_FLOW_OK; /* init */ if (amrnbparse->need_header) { if (gst_adapter_available (amrnbparse->adapter) < 6) goto done; data = gst_adapter_peek (amrnbparse->adapter, 6); if (memcmp (data, "#!AMR\n", 6) != 0) goto done; gst_adapter_flush (amrnbparse->adapter, 6); amrnbparse->need_header = FALSE; } while (TRUE) { if (gst_adapter_available (amrnbparse->adapter) < 1) break; data = gst_adapter_peek (amrnbparse->adapter, 1); /* get size */ mode = (data[0] >> 3) & 0x0F; block = block_size[mode] + 1; /* add one for the mode */ if (gst_adapter_available (amrnbparse->adapter) < block) break; out = gst_buffer_new_and_alloc (block); data = gst_adapter_peek (amrnbparse->adapter, block); memcpy (GST_BUFFER_DATA (out), data, block); /* output */ GST_BUFFER_DURATION (out) = GST_SECOND * 160 / 8000; GST_BUFFER_TIMESTAMP (out) = amrnbparse->ts; amrnbparse->ts += GST_BUFFER_DURATION (out); gst_buffer_set_caps (out, (GstCaps *) gst_pad_get_pad_template_caps (amrnbparse->srcpad)); GST_DEBUG ("Pushing %d bytes of data", block); res = gst_pad_push (amrnbparse->srcpad, out); gst_adapter_flush (amrnbparse->adapter, block); } done: return res; } static gboolean gst_amrnbparse_read_header (GstAmrnbParse * amrnbparse) { GstBuffer *buffer; GstFlowReturn ret; guint8 *data; gint size; ret = gst_pad_pull_range (amrnbparse->sinkpad, amrnbparse->offset, 6, &buffer); if (ret != GST_FLOW_OK) return FALSE; data = GST_BUFFER_DATA (buffer); size = GST_BUFFER_SIZE (buffer); if (size < 6) goto not_enough; if (memcmp (data, "#!AMR\n", 6)) goto no_header; amrnbparse->offset += 6; return TRUE; not_enough: { gst_buffer_unref (buffer); return FALSE; } no_header: { gst_buffer_unref (buffer); return FALSE; } } /* random access mode, could just read a fixed size buffer and push it to * the chain function but we don't... */ static void gst_amrnbparse_loop (GstPad * pad) { GstAmrnbParse *amrnbparse; GstBuffer *buffer; guint8 *data; gint size; gint block, mode; GstFlowReturn ret; amrnbparse = GST_AMRNBPARSE (GST_PAD_PARENT (pad)); /* init */ if (amrnbparse->need_header) { gboolean got_header; got_header = gst_amrnbparse_read_header (amrnbparse); if (!got_header) { GST_LOG_OBJECT (amrnbparse, "could not read header"); goto need_pause; } amrnbparse->need_header = FALSE; } ret = gst_pad_pull_range (amrnbparse->sinkpad, amrnbparse->offset, 1, &buffer); if (ret != GST_FLOW_OK) goto need_pause; data = GST_BUFFER_DATA (buffer); size = GST_BUFFER_SIZE (buffer); /* EOS */ if (size < 1) goto eos; /* get size */ mode = (data[0] >> 3) & 0x0F; block = block_size[mode] + 1; /* add one for the mode */ gst_buffer_unref (buffer); ret = gst_pad_pull_range (amrnbparse->sinkpad, amrnbparse->offset, block, &buffer); if (ret != GST_FLOW_OK) goto need_pause; amrnbparse->offset += block; /* output */ GST_BUFFER_DURATION (buffer) = GST_SECOND * 160 / 8000; GST_BUFFER_TIMESTAMP (buffer) = amrnbparse->ts; amrnbparse->ts += GST_BUFFER_DURATION (buffer); gst_buffer_set_caps (buffer, (GstCaps *) gst_pad_get_pad_template_caps (amrnbparse->srcpad)); GST_DEBUG ("Pushing %d bytes of data", block); ret = gst_pad_push (amrnbparse->srcpad, buffer); if (ret != GST_FLOW_OK) goto need_pause; return; need_pause: { GST_LOG_OBJECT (amrnbparse, "pausing task"); gst_pad_pause_task (pad); return; } eos: { GST_LOG_OBJECT (amrnbparse, "pausing task"); gst_pad_push_event (amrnbparse->srcpad, gst_event_new_eos ()); gst_pad_pause_task (pad); return; } } static gboolean gst_amrnbparse_sink_activate (GstPad * sinkpad) { gboolean result = FALSE; GstAmrnbParse *amrnbparse; GstActivateMode mode; amrnbparse = GST_AMRNBPARSE (GST_OBJECT_PARENT (sinkpad)); GST_OBJECT_LOCK (sinkpad); mode = GST_PAD_ACTIVATE_MODE (sinkpad); GST_OBJECT_UNLOCK (sinkpad); switch (mode) { case GST_ACTIVATE_PUSH: amrnbparse->seekable = FALSE; result = TRUE; break; case GST_ACTIVATE_PULL: /*gst_pad_peer_set_active (sinkpad, mode); */ amrnbparse->need_header = TRUE; amrnbparse->seekable = TRUE; amrnbparse->ts = 0; result = gst_pad_start_task (sinkpad, (GstTaskFunction) gst_amrnbparse_loop, sinkpad); break; case GST_ACTIVATE_NONE: /* step 1, unblock clock sync (if any) */ /* step 2, make sure streaming finishes */ result = gst_pad_stop_task (sinkpad); break; } return result; } static GstStateChangeReturn gst_amrnbparse_state_change (GstElement * element, GstStateChange transition) { GstAmrnbParse *amrnbparse; GstStateChangeReturn ret; amrnbparse = GST_AMRNBPARSE (element); switch (transition) { case GST_STATE_CHANGE_NULL_TO_READY: break; case GST_STATE_CHANGE_READY_TO_PAUSED: break; default: break; } ret = GST_ELEMENT_CLASS (parent_class)->change_state (element, transition); switch (transition) { case GST_STATE_CHANGE_PAUSED_TO_READY: break; case GST_STATE_CHANGE_READY_TO_NULL: break; default: break; } return ret; }