%define majorminor @GST_MAJORMINOR@ %define gstreamer gstreamer09 %define gstregister %{_bindir}/gst-register-%{majorminor} %define register %{gstregister} > /dev/null 2>&1 || : %define gst_minver 0.9.1 Name: %{gstreamer}-plugins-ugly Version: @VERSION@ Release: @GST_PLUGINS_UGLY_VERSION_RELEASE@.gst Summary: GStreamer streaming media framework "ugly" plug-ins Group: Applications/Multimedia License: LGPL URL: http://gstreamer.freedesktop.org/ Vendor: GStreamer Backpackers Team Source: http://gstreamer.freedesktop.org/src/gst-plugins-ugly/gst-plugins-ugly-%{version}.tar.gz BuildRoot: %{_tmppath}/%{name}-%{version}-%{release}-root-%(%{__id_u} -n) Requires: %{gstreamer} >= %{gst_minver} BuildRequires: %{gstreamer}-devel >= %{gst_minver} BuildRequires: gcc-c++ @USE_SIDPLAY_TRUE@BuildRequires: libsidplay-devel >= 1.36.0 # @USE_A52DEC_TRUE@BuildRequires: a52dec-devel >= 0.7.3 # @USE_DVDNAV_TRUE@BuildRequires: libdvdnav-devel >= 0.1.3 # @USE_DVDREAD_TRUE@BuildRequires: libdvdread-devel >= 0.9.0 @USE_LAME_TRUE@BuildRequires: lame-devel >= 3.89 @USE_MAD_TRUE@BuildRequires: libid3tag-devel >= 0.15.0 @USE_MAD_TRUE@BuildRequires: libmad-devel >= 0.15.0 @USE_MPEG2DEC_TRUE@BuildRequires: mpeg2dec-devel >= 0.4.0 @USE_SIDPLAY_TRUE@Provides: gstreamer-sid = %{version}-%{release} @USE_LAME_TRUE@Provides: gstreamer-lame = %{version}-%{release} @USE_MAD_TRUE@Provides: gstreamer-mad = %{version}-%{release} # @USE_A52DEC_TRUE@Provides: gstreamer-a52dec = %{version}-%{release} # @USE_DVDNAV_TRUE@Provides: gstreamer-dvdnavsrc = %{version}-%{release} # @USE_DVDREAD_TRUE@Provides: gstreamer-dvdreadsrc = %{version}-%{release} @USE_MPEG2DEC_TRUE@Provides: gstreamer-mpeg2dec = %{version}-%{release} %description GStreamer is a streaming media framework, based on graphs of elements which operate on media data. This package contains well-written plug-ins that can't be shipped in gstreamer-plugins-good because: - the license is not LGPL - the license of the library is not LGPL - there are possible licensing issues with the code. # %package devel # Summary: Development files for GStreamer Ugly Plugins # Group: Development/Libraries # # Requires: %{name} = %{version}-%{release} # # %description devel # GStreamer is a streaming media framework, based on graphs of elements which # operate on media data. # # This package contains well-written plug-ins that can't be shipped in # gstreamer-plugins-good because: # - the license is not LGPL # - the license of the library is not LGPL # - there are possible licensing issues with the code. # # This package contains development files and documentation. %prep %setup -q -n gst-plugins-ugly-%{version} %build %configure \ --enable-debug \ --enable-gtk-doc make %{?_smp_mflags} %install rm -rf $RPM_BUILD_ROOT # Install doc temporarily in order to be included later by rpm %makeinstall # Clean out files that should not be part of the rpm. rm -f $RPM_BUILD_ROOT%{_libdir}/gstreamer-%{majorminor}/*.la rm -f $RPM_BUILD_ROOT%{_libdir}/gstreamer-%{majorminor}/*.a rm -f $RPM_BUILD_ROOT%{_libdir}/*.a rm -f $RPM_BUILD_ROOT%{_libdir}/*.la # %find_lang gst-plugins-ugly-%{majorminor} %clean rm -rf $RPM_BUILD_ROOT %post %{register} %postun %{register} %files #%files -f gst-plugins-ugly-%{majorminor}.lang %defattr(-, root, root, -) %doc AUTHORS COPYING README REQUIREMENTS # plugins without external dependencies #%{_libdir}/gstreamer-%{majorminor}/libgstac3parse.so #%{_libdir}/gstreamer-%{majorminor}/libgstasfdemux.so %{_libdir}/gstreamer-%{majorminor}/libgstdvdlpcmdec.so %{_libdir}/gstreamer-%{majorminor}/libgstiec958.so %{_libdir}/gstreamer-%{majorminor}/libgstmpegaudioparse.so #%{_libdir}/gstreamer-%{majorminor}/libgstmpegstream.so %{_libdir}/gstreamer-%{majorminor}/libgstrmdemux.so #%{_libdir}/gstreamer-%{majorminor}/libgstsynaesthesia.so # plugins with dependencies @USE_SIDPLAY_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstsid.so @USE_LAME_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstlame.so @USE_MAD_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstmad.so # @USE_A52DEC_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgsta52dec.so # @USE_DVDNAV_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstdvdnavsrc.so # @USE_DVDREAD_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstdvdreadsrc.so @USE_MPEG2DEC_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstmpeg2dec.so # %files devel # %defattr(-, root, root, -) # %doc %{_datadir}/gtk-doc/html/gstreamer-plugins-ugly-plugins-%{majorminor}/* %changelog * Fri Sep 02 2005 Thomas Vander Stichele - clean out for split into ugly * Mon Feb 14 2005 Christian Schaller - Add vnc plugin * Wed Jan 19 2005 Christian Schaller - add dv1394 plugin * Wed Dec 22 2004 Christian Schaller - Add -plugins- to plugin names * Thu Dec 9 2004 Christian Schaller - Add the mms plugin * Wed Oct 06 2004 Christian Schaller - Add Wim's new mng decoder plugin - add shout2 plugin for Zaheer, hope it is correctly done :) * Wed Sep 29 2004 Christian Schaller - Fix USE statement for V4L2 * Thu Sep 28 2004 Christian Schaller - Remove kio plugin (as it was broken) * Wed Sep 21 2004 Christian Schaller - Reorganize SPEC to fit better with fedora.us and freshrpms.net packages - Make sure gstinterfaces.so is in the package - Add all new plugins * Mon Mar 15 2004 Thomas Vander Stichele - put back media-info - add ffmpegcolorspace plugin * Sun Mar 07 2004 Christian Schaller - Remove rm commands for media-info stuff - Add libdir/* * Thu Mar 04 2004 Christian Schaller - Add missing gconf schema install in %post * Tue Mar 02 2004 Thomas Vander Stichele - Libraries/Multimedia doesn't exist, remove it * Tue Mar 02 2004 Thomas Vander Stichele - added speex plugin. * Mon Mar 01 2004 Thomas Vander Stichele - Cleaned up the mess. Could we PLEASE keep this sort of organized and - alphabetic for easy lookup ? * Fri Feb 13 2004 Christian Schaller - Added latest new headers * Wed Jan 21 2004 Christian Schaller - added NAS plugin - added i18n locale dir * Fri Jan 16 2004 Christian Schaller - added libcaca plugin - added libgstcolorspace - fixed name of libgsthermescolorspace * Wed Jan 14 2004 Christian Schaller - Add gamma plugin - Have the pixbuf plugin deleted for now * Wed Dec 18 2003 Christian Schaller - remove gsttagediting.h as it is gone - replace it with gst/tag/tag.h * Sun Nov 23 2003 Christian Schaller - Update spec file for latest changes - add faad plugin * Thu Oct 16 2003 Christian Schaller - Add new colorbalance and tuner and xoverlay stuff - Change name of kde-audio-devel to arts-devel * Sat Sep 27 2003 Christian Schaller - Add majorminor to man page names - add navigation lib to package * Tue Sep 11 2003 Christian Schaller - Add -%{majorminor} to each instance of gst-register * Tue Aug 19 2003 Christian Schaller - Add new plugins * Sat Jul 12 2003 Thomas Vander Stichele - move gst/ mpeg plugins to base package - remove hermes conditional from snapshot - remove one instance of resample plugin - fix up silly versioned plugins efence and rmdemux * Sat Jul 05 2003 Christian Schaller - Major overhaul of SPEC file to make it compatible with what Red Hat ships as default - Probably a little less sexy, but cross-distro SPEC files are a myth anyway so making it convenient for RH users wins out - Keeping conditionals even with new re-org so that developers building the RPMS don't need everything installed - Add bunch of obsoletes to ease migration from earlier official GStreamer RPMS - Remove plugins that doesn't exist anymore * Sun Mar 02 2003 Christian Schaller - Remove USE_RTP statement from RTP plugin - Move RTP plugin to no-deps section * Sat Mar 01 2003 Christian Schaller - Remove videosink from SPEC * Thu Jan 23 2003 Thomas Vander Stichele - various fixes - make video output packages provide gstreamer-videosink * Thu Jan 23 2003 Thomas Vander Stichele - split out ffmpeg stuff to separate plugin * Fri Dec 27 2002 Thomas Vander Stichele - add virtual provides for audio sources and sinks * Sun Dec 15 2002 Christian Schaller - Update mpeg2dec REQ to be 0.3.1 * Tue Dec 10 2002 Thomas Vander Stichele - only install schema once - move out devel lib stuff to -devel package * Sun Dec 08 2002 Thomas Vander Stichele - fix location of libgstpng - changes for parallel installability * Thu Nov 28 2002 Christian Schaller - Put in libgstpng plugin - rm the libgstmedia-info stuff until thomas think they are ready * Fri Nov 01 2002 Thomas Vander Stichele - don't use compprep until ABI issues can be fixed * Wed Oct 30 2002 Thomas Vander Stichele - added smpte plugin - split out dvdnavread package - fixed snapshot deps and added hermes conditionals * Tue Oct 29 2002 Thomas Vander Stichele - added -play package, libs, and .pc files * Thu Oct 24 2002 Christian Schaller - Added wavenc to audio formats package * Sat Oct 20 2002 Christian Scchaller - Removed all .la files - added separate non-openquicktime demuxer plugin - added snapshot plugin - added videotest plugin - Split avi plugin out to avi and windec plugins since aviplugin do not depend on avifile - Added cdplayer plugin * Fri Sep 20 2002 Thomas Vander Stichele - added gst-compprep calls * Wed Sep 18 2002 Thomas Vander Stichele - add gst-register-%{majorminor} calls everywhere again since auto-reregister doesn't work - added gstreamer-audio-formats to mad's requires since it needs the typefind to work properly * Mon Sep 9 2002 Christian Schaller - Added v4l2 plugin * Thu Aug 27 2002 Christian Schaller - Fixed USE_DV_TRUE to USE_LIBDV_TRUE - Added Gconf and floatcast headers to gstreamer-plugins-devel package - Added mixmatrix plugin to audio-effects package * Thu Jul 11 2002 Thomas Vander Stichele - fixed oss package to buildrequire instead of require glibc headers * Mon Jul 08 2002 Thomas Vander Stichele - fixed -devel package group * Fri Jul 05 2002 Thomas Vander Stichele - release 0.4.0 ! - added gstreamer-libs.pc - removed all gst-register-%{majorminor} calls since this should be done automatically now * Thu Jul 04 2002 Thomas Vander Stichele - fix issue with SDL package - make all packages STRICTLY require the right version to avoid ABI issues - make gst-plugins obsolete gst-plugin-libs - also send output of gst-register-%{majorminor} to /dev/null to lower the noise * Wed Jul 03 2002 Thomas Vander Stichele - require glibc-devel instead of glibc-kernheaders since the latter is only since 7.3 and glibc-devel pulls in the right package anyway * Sun Jun 23 2002 Thomas Vander Stichele - changed header location of plug-in libs * Mon Jun 17 2002 Thomas Vander Stichele - major cleanups - adding gst-register-%{majorminor} on postun everywhere - remove ldconfig since we don't actually install libs in system dirs - removed misc package - added video-effects - dot every Summary - uniformify all descriptions a little * Thu Jun 06 2002 Thomas Vander Stichele - various BuildRequires: additions * Tue Jun 04 2002 Thomas Vander Stichele - added USE_LIBADSPA_TRUE bits to ladspa package * Mon Jun 03 2002 Thomas Vander Stichele - Added libfame package * Mon May 12 2002 Christian Fredrik Kalager Schaller - Added jack, dxr3, http packages - Added visualisation plug-ins, effecttv and synaesthesia - Created devel package - Removed gstreamer-plugins-libs package (moved it into gstreamer-plugins) - Replaced prefix/dirname with _macros * Mon May 06 2002 Thomas Vander Stichele - added gstreamer-GConf package * Wed Mar 13 2002 Thomas Vander Stichele - added more BuildRequires and Requires - rearranged some plug-ins - added changelog ;)