%define majorminor @GST_MAJORMINOR@ %define gstreamer gstreamer %define gst_minver 0.10.0 Name: %{gstreamer}-plugins-ugly Version: @VERSION@ Release: @PACKAGE_VERSION_RELEASE@.gst Summary: GStreamer streaming media framework "ugly" plug-ins Group: Applications/Multimedia License: LGPL URL: http://gstreamer.freedesktop.org/ Vendor: GStreamer Backpackers Team Source: http://gstreamer.freedesktop.org/src/gst-plugins-ugly/gst-plugins-ugly-%{version}.tar.gz BuildRoot: %{_tmppath}/%{name}-%{version}-%{release}-root-%(%{__id_u} -n) Requires: %{gstreamer} >= %{gst_minver} BuildRequires: %{gstreamer}-devel >= %{gst_minver} BuildRequires: gcc-c++ @USE_SIDPLAY_TRUE@BuildRequires: libsidplay-devel >= 1.36.0 @USE_A52DEC_TRUE@BuildRequires: a52dec-devel >= 0.7.3 @USE_DVDREAD_TRUE@BuildRequires: libdvdread-devel >= 0.9.0 @USE_LAME_TRUE@BuildRequires: lame-devel >= 3.89 @USE_MAD_TRUE@BuildRequires: libmad-devel >= 0.15.0 @USE_MPEG2DEC_TRUE@BuildRequires: mpeg2dec-devel >= 0.4.0 @USE_SIDPLAY_TRUE@Provides: gstreamer-sid = %{version}-%{release} @USE_LAME_TRUE@Provides: gstreamer-lame = %{version}-%{release} @USE_MAD_TRUE@Provides: gstreamer-mad = %{version}-%{release} @USE_A52DEC_TRUE@Provides: gstreamer-a52dec = %{version}-%{release} @USE_DVDREAD_TRUE@Provides: gstreamer-dvdread = %{version}-%{release} @USE_MPEG2DEC_TRUE@Provides: gstreamer-mpeg2dec = %{version}-%{release} @USE_X264_TRUE@Requires: x264-libs %description GStreamer is a streaming media framework, based on graphs of elements which operate on media data. This package contains well-written plug-ins that can't be shipped in gstreamer-plugins-good because: - the license is not LGPL - the license of the library is not LGPL - there are possible licensing issues with the code. # %package devel # Summary: Development files for GStreamer Ugly Plugins # Group: Development/Libraries # # Requires: %{name} = %{version}-%{release} # # %description devel # GStreamer is a streaming media framework, based on graphs of elements which # operate on media data. # # This package contains well-written plug-ins that can't be shipped in # gstreamer-plugins-good because: # - the license is not LGPL # - the license of the library is not LGPL # - there are possible licensing issues with the code. # # This package contains development files and documentation. %prep %setup -q -n gst-plugins-ugly-%{version} %build %configure \ --enable-debug \ --enable-gtk-doc make %{?_smp_mflags} %install rm -rf $RPM_BUILD_ROOT # Install doc temporarily in order to be included later by rpm %makeinstall # Clean out files that should not be part of the rpm. rm -f $RPM_BUILD_ROOT%{_libdir}/gstreamer-%{majorminor}/*.la rm -f $RPM_BUILD_ROOT%{_libdir}/gstreamer-%{majorminor}/*.a rm -f $RPM_BUILD_ROOT%{_libdir}/*.a rm -f $RPM_BUILD_ROOT%{_libdir}/*.la %find_lang gst-plugins-ugly-%{majorminor} %clean rm -rf $RPM_BUILD_ROOT %files -f gst-plugins-ugly-%{majorminor}.lang %defattr(-, root, root, -) %doc AUTHORS COPYING README REQUIREMENTS gst-plugins-ugly.doap %{_libdir}/gstreamer-%{majorminor}/libgstasf.so %{_libdir}/gstreamer-%{majorminor}/libgstdvdlpcmdec.so %{_libdir}/gstreamer-%{majorminor}/libgstiec958.so %{_libdir}/gstreamer-%{majorminor}/libgstmpegaudioparse.so %{_libdir}/gstreamer-%{majorminor}/libgstmpegstream.so %{_libdir}/gstreamer-%{majorminor}/libgstrmdemux.so %{_libdir}/gstreamer-%{majorminor}/libgstdvdsub.so # plugins with dependencies @USE_SIDPLAY_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstsid.so @USE_LAME_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstlame.so @USE_MAD_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstmad.so @USE_A52DEC_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgsta52dec.so @USE_DVDREAD_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstdvdread.so @USE_MPEG2DEC_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstmpeg2dec.so @USE_TWOLAME_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgsttwolame.so %doc %{_datadir}/gtk-doc/html/gst-plugins-ugly-plugins-%{majorminor}/* @USE_X264_TRUE@%{_datadir}/gstreamer-%{majorminor}/presets/GstX264Enc.prs @USE_X264_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstx264.so @USE_AMRNB_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstamrnb.so @USE_AMRWB_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstamrwbdec.so @USE_AMRNB_TRUE@%{_datadir}/gstreamer-%{majorminor}/presets/GstAmrnbEnc.prs @USE_CDIO_TRUE@%{_libdir}/gstreamer-%{majorminor}/libgstcdio.so %changelog * Fri Jun 5 2009 Jan Schmidt - Move x264enc plugin from -bad * Fri Dec 15 2006 Thomas Vander Stichele - further cleanup - add .doap file * Fri Sep 02 2005 Thomas Vander Stichele - clean out for split into ugly