/* GStreamer ASF/WMV/WMA demuxer * Copyright (C) 2007 Tim-Philipp Müller * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Library General Public * License as published by the Free Software Foundation; either * version 2 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Library General Public License for more details. * * You should have received a copy of the GNU Library General Public * License along with this library; if not, write to the * Free Software Foundation, Inc., 59 Temple Place - Suite 330, * Boston, MA 02111-1307, USA. */ /* FIXME: * file:///home/tpm/samples/video/asf//336370-regis-velo862.wmv * file:///home/tpm/samples/video/asf//336370-eichhoer.wmv * throw errors (not always necessarily) in this code path * (looks like they carry broken payloads/packets though) */ #include "asfpacket.h" #include #include #include /* we are unlikely to deal with lengths > 2GB here any time soon, so just * return a signed int and use that for error reporting */ static gint asf_packet_read_varlen_int (guint lentype_flags, guint lentype_bit_offset, const guint8 ** p_data, guint * p_size) { const guint lens[4] = { 0, 1, 2, 4 }; guint len, val; len = lens[(lentype_flags >> lentype_bit_offset) & 0x03]; /* will make caller bail out with a short read if there's not enough data */ if (*p_size < len) { GST_WARNING ("need %u bytes, but only %u bytes available", len, *p_size); return -1; } switch (len) { case 0: val = 0; break; case 1: val = GST_READ_UINT8 (*p_data); break; case 2: val = GST_READ_UINT16_LE (*p_data); break; case 4: val = GST_READ_UINT32_LE (*p_data); break; default: g_assert_not_reached (); } *p_data += len; *p_size -= len; return (gint) val; } static GstBuffer * asf_packet_create_payload_buffer (AsfPacket * packet, const guint8 ** p_data, guint * p_size, guint payload_len) { guint off; g_assert (payload_len <= *p_size); off = (guint) (*p_data - GST_BUFFER_DATA (packet->buf)); g_assert (off < GST_BUFFER_SIZE (packet->buf)); *p_data += payload_len; *p_size -= payload_len; return gst_buffer_create_sub (packet->buf, off, payload_len); } static AsfPayload * asf_payload_find_previous_fragment (AsfPayload * payload, AsfStream * stream) { AsfPayload *ret; if (stream->payloads->len == 0) { GST_DEBUG ("No previous fragments to merge with for stream %u", stream->id); return NULL; } ret = &g_array_index (stream->payloads, AsfPayload, stream->payloads->len - 1); if (ret->mo_size != payload->mo_size || ret->mo_number != payload->mo_number || ret->mo_offset != 0) { GST_WARNING ("Previous fragment does not match continued fragment"); return NULL; } #if 0 if (this_fragment->mo_offset + this_payload_len > first_fragment->mo_size) { GST_WARNING ("Merged fragments would be bigger than the media object"); return FALSE; } #endif return ret; } /* TODO: if we have another payload already queued for this stream and that * payload doesn't have a duration, maybe we can calculate a duration for it * (if the previous timestamp is smaller etc. etc.) */ static void gst_asf_payload_queue_for_stream (GstASFDemux * demux, AsfPayload * payload, AsfStream * stream) { /* remember the first timestamp in the stream */ if (!GST_CLOCK_TIME_IS_VALID (demux->first_ts) && GST_CLOCK_TIME_IS_VALID (payload->ts)) { GST_DEBUG_OBJECT (demux, "first ts: %" GST_TIME_FORMAT, GST_TIME_ARGS (payload->ts)); demux->first_ts = payload->ts; if (demux->push_mode) { gst_segment_set_seek (&demux->segment, demux->segment.rate, GST_FORMAT_TIME, demux->segment.flags, GST_SEEK_TYPE_SET, demux->first_ts, GST_SEEK_TYPE_NONE, 0, NULL); } } /* better drop a few frames at the beginning than send bogus timestamps */ if (G_UNLIKELY (payload->ts < demux->first_ts)) { GST_LOG_OBJECT (stream->pad, "Dropping payload with timestamp %" GST_TIME_FORMAT " which is before the first timestamp %" GST_TIME_FORMAT, GST_TIME_ARGS (payload->ts), GST_TIME_ARGS (demux->first_ts)); gst_buffer_replace (&payload->buf, NULL); return; } /* make timestamps start from 0 */ if (!demux->push_mode) payload->ts -= demux->first_ts; /* remove any incomplete payloads that will never be completed */ while (stream->payloads->len > 0) { AsfPayload *prev; guint idx_last; idx_last = stream->payloads->len - 1; prev = &g_array_index (stream->payloads, AsfPayload, idx_last); if (gst_asf_payload_is_complete (prev)) break; GST_DEBUG_OBJECT (demux, "Dropping incomplete fragmented media object " "queued for stream %u", stream->id); gst_buffer_replace (&prev->buf, NULL); g_array_remove_index (stream->payloads, idx_last); /* there's data missing, so there's a discontinuity now */ GST_BUFFER_FLAG_SET (payload->buf, GST_BUFFER_FLAG_DISCONT); } /* If we're about to queue a key frame that is before the segment start, we * can ditch any previously queued payloads (which would also be before the * segment start). This makes sure the decoder doesn't decode more than * absolutely necessary after a seek (we don't push out payloads that are * before the segment start until we have at least one that falls within the * segment) */ if (GST_CLOCK_TIME_IS_VALID (payload->ts) && payload->ts < demux->segment.start && payload->keyframe) { GST_DEBUG_OBJECT (demux, "Queueing keyframe before segment start, removing" " %u previously-queued payloads, which would be out of segment too and" " hence don't have to be decoded", stream->payloads->len); while (stream->payloads->len > 0) { AsfPayload *last; guint idx_last; idx_last = stream->payloads->len - 1; last = &g_array_index (stream->payloads, AsfPayload, idx_last); gst_buffer_replace (&last->buf, NULL); g_array_remove_index (stream->payloads, idx_last); } /* Mark discontinuity (should be done via stream->discont anyway though) */ GST_BUFFER_FLAG_SET (payload->buf, GST_BUFFER_FLAG_DISCONT); } g_array_append_vals (stream->payloads, payload, 1); } static void asf_payload_parse_replicated_data_extensions (AsfStream * stream, AsfPayload * payload) { AsfPayloadExtension *ext; guint off; if (!stream->ext_props.valid || stream->ext_props.payload_extensions == NULL) return; off = 8; for (ext = stream->ext_props.payload_extensions; ext->len > 0; ++ext) { if (off + ext->len > payload->rep_data_len) { GST_WARNING ("not enough replicated data for defined extensions"); return; } switch (ext->id) { case ASF_PAYLOAD_EXTENSION_DURATION: if (ext->len == 2) { payload->duration = GST_READ_UINT16_LE (payload->rep_data + off) * GST_MSECOND; } else { GST_WARNING ("unexpected DURATION extensions len %u", ext->len); } break; default: break; } off += ext->len; } } static gboolean gst_asf_demux_parse_payload (GstASFDemux * demux, AsfPacket * packet, gint lentype, const guint8 ** p_data, guint * p_size) { AsfPayload payload = { 0, }; AsfStream *stream; gboolean is_compressed; guint payload_len; guint stream_num; if (*p_size < 1) { GST_WARNING_OBJECT (demux, "Short packet!"); return FALSE; } stream_num = GST_READ_UINT8 (*p_data) & 0x7f; payload.keyframe = ((GST_READ_UINT8 (*p_data) & 0x80) != 0); *p_data += 1; *p_size -= 1; payload.ts = GST_CLOCK_TIME_NONE; payload.duration = GST_CLOCK_TIME_NONE; payload.mo_number = asf_packet_read_varlen_int (packet->prop_flags, 4, p_data, p_size); payload.mo_offset = asf_packet_read_varlen_int (packet->prop_flags, 2, p_data, p_size); payload.rep_data_len = asf_packet_read_varlen_int (packet->prop_flags, 0, p_data, p_size); is_compressed = (payload.rep_data_len == 1); GST_LOG_OBJECT (demux, "payload for stream %u", stream_num); GST_LOG_OBJECT (demux, "keyframe : %s", (payload.keyframe) ? "yes" : "no"); GST_LOG_OBJECT (demux, "compressed : %s", (is_compressed) ? "yes" : "no"); if (*p_size < payload.rep_data_len) { GST_WARNING_OBJECT (demux, "Short packet! rep_data_len=%u, size=%u", payload.rep_data_len, *p_size); return FALSE; } memcpy (payload.rep_data, *p_data, MIN (sizeof (payload.rep_data), payload.rep_data_len)); *p_data += payload.rep_data_len; *p_size -= payload.rep_data_len; if (*p_size == 0) { GST_WARNING_OBJECT (demux, "payload without data!?"); return FALSE; } /* we use -1 as lentype for a single payload that's the size of the packet */ if (lentype >= 0 && lentype <= 3) { payload_len = asf_packet_read_varlen_int (lentype, 0, p_data, p_size); if (*p_size < payload_len) { GST_WARNING_OBJECT (demux, "Short packet! payload_len=%u, size=%u", payload_len, *p_size); return FALSE; } } else { payload_len = *p_size; } GST_LOG_OBJECT (demux, "payload length: %u", payload_len); stream = gst_asf_demux_get_stream (demux, stream_num); if (stream == NULL) { GST_WARNING_OBJECT (demux, "Payload for unknown stream %u, skipping", stream_num); *p_data += payload_len; *p_size -= payload_len; return TRUE; } if (!is_compressed) { GST_LOG_OBJECT (demux, "replicated data length: %u", payload.rep_data_len); if (payload.rep_data_len >= 8) { payload.mo_size = GST_READ_UINT32_LE (payload.rep_data); payload.ts = GST_READ_UINT32_LE (payload.rep_data + 4) * GST_MSECOND; payload.ts -= demux->preroll * GST_MSECOND; asf_payload_parse_replicated_data_extensions (stream, &payload); GST_LOG_OBJECT (demux, "media object size : %u", payload.mo_size); GST_LOG_OBJECT (demux, "media object ts : %" GST_TIME_FORMAT, GST_TIME_ARGS (payload.ts)); GST_LOG_OBJECT (demux, "media object dur : %" GST_TIME_FORMAT, GST_TIME_ARGS (payload.duration)); } else if (payload.rep_data_len != 0) { GST_WARNING_OBJECT (demux, "invalid replicated data length, very bad"); *p_data += payload_len; *p_size -= payload_len; return FALSE; } GST_LOG_OBJECT (demux, "media object offset : %u", payload.mo_offset); GST_LOG_OBJECT (demux, "payload length: %u", payload_len); if ((stream = gst_asf_demux_get_stream (demux, stream_num))) { payload.buf = asf_packet_create_payload_buffer (packet, p_data, p_size, payload_len); /* n-th fragment of a fragmented media object? */ if (payload.mo_offset != 0) { AsfPayload *prev; if ((prev = asf_payload_find_previous_fragment (&payload, stream))) { if (payload.mo_offset != GST_BUFFER_SIZE (prev->buf)) { GST_WARNING_OBJECT (demux, "Offset doesn't match previous data?!"); } /* note: buffer join/merge might not preserve buffer flags */ prev->buf = gst_buffer_join (prev->buf, payload.buf); GST_LOG_OBJECT (demux, "Merged fragments, merged size: %u", GST_BUFFER_SIZE (prev->buf)); } else { gst_buffer_unref (payload.buf); } payload.buf = NULL; } else { gst_asf_payload_queue_for_stream (demux, &payload, stream); } } } else { const guint8 *payload_data; GstClockTime ts, ts_delta; guint num; GST_LOG_OBJECT (demux, "Compressed payload, length=%u", payload_len); payload_data = *p_data; *p_data += payload_len; *p_size -= payload_len; ts = (payload.mo_offset - demux->preroll) * GST_MSECOND; ts_delta = payload.rep_data[0] * GST_MSECOND; for (num = 0; payload_len > 0; ++num) { guint sub_payload_len; sub_payload_len = GST_READ_UINT8 (payload_data); GST_LOG_OBJECT (demux, "subpayload #%u: len=%u, ts=%" GST_TIME_FORMAT, num, sub_payload_len, GST_TIME_ARGS (ts)); ++payload_data; --payload_len; if (payload_len < sub_payload_len) { GST_WARNING_OBJECT (demux, "Short payload! %u bytes left", payload_len); return FALSE; } if (sub_payload_len > 0) { payload.buf = asf_packet_create_payload_buffer (packet, &payload_data, &payload_len, sub_payload_len); payload.ts = ts; payload.duration = ts_delta; gst_asf_payload_queue_for_stream (demux, &payload, stream); } ts += ts_delta; } } return TRUE; } gboolean gst_asf_demux_parse_packet (GstASFDemux * demux, GstBuffer * buf) { AsfPacket packet = { 0, }; const guint8 *data; gboolean has_multiple_payloads; gboolean ret = TRUE; guint8 ec_flags, flags1; guint size; data = GST_BUFFER_DATA (buf); size = GST_BUFFER_SIZE (buf); /* need at least two payload flag bytes, send time, and duration */ if (size < 2 + 4 + 2) goto short_packet; packet.buf = buf; ec_flags = GST_READ_UINT8 (data); /* skip optional error correction stuff */ if ((ec_flags & 0x80) != 0) { guint ec_len_type, ec_len; ec_len_type = (ec_flags & 0x60) >> 5; if (ec_len_type == 0) { ec_len = ec_flags & 0x0f; } else { GST_WARNING_OBJECT (demux, "unexpected error correction length type %u", ec_len_type); ec_len = 2; } GST_LOG ("packet has error correction (%u bytes)", ec_len); /* still need at least two payload flag bytes, send time, and duration */ if (size <= (1 + ec_len) + 2 + 4 + 2) goto short_packet; data += 1 + ec_len; size -= 1 + ec_len; } /* parse payload info */ flags1 = GST_READ_UINT8 (data); packet.prop_flags = GST_READ_UINT8 (data + 1); data += 2; size -= 2; has_multiple_payloads = (flags1 & 0x01) != 0; packet.length = asf_packet_read_varlen_int (flags1, 5, &data, &size); packet.sequence = asf_packet_read_varlen_int (flags1, 1, &data, &size); packet.padding = asf_packet_read_varlen_int (flags1, 3, &data, &size); if (size < 6) goto short_packet; packet.send_time = GST_READ_UINT32_LE (data) * GST_MSECOND; packet.duration = GST_READ_UINT16_LE (data + 4) * GST_MSECOND; data += 4 + 2; size -= 4 + 2; GST_LOG_OBJECT (demux, "multiple payloads: %u", has_multiple_payloads); GST_LOG_OBJECT (demux, "packet length : %u", packet.length); GST_LOG_OBJECT (demux, "sequence : %u", packet.sequence); GST_LOG_OBJECT (demux, "padding : %u", packet.padding); GST_LOG_OBJECT (demux, "send time : %" GST_TIME_FORMAT, GST_TIME_ARGS (packet.send_time)); GST_LOG_OBJECT (demux, "duration : %" GST_TIME_FORMAT, GST_TIME_ARGS (packet.duration)); if (packet.padding == (guint) - 1 || size < packet.padding) goto short_packet; size -= packet.padding; /* adjust available size for parsing if there's less actual packet data for * parsing than there is data in bytes (for sample see bug 431318) */ if (packet.length != 0 && packet.length < demux->packet_size) { GST_LOG_OBJECT (demux, "shortened packet, adjusting available data size"); size -= (demux->packet_size - packet.length); } if (has_multiple_payloads) { guint i, num, lentype; if (size < 1) goto short_packet; num = (GST_READ_UINT8 (data) & 0x3F) >> 0; lentype = (GST_READ_UINT8 (data) & 0xC0) >> 6; ++data; --size; GST_LOG_OBJECT (demux, "num payloads : %u", num); for (i = 0; i < num; ++i) { GST_LOG_OBJECT (demux, "Parsing payload %u/%u", i + 1, num); ret = gst_asf_demux_parse_payload (demux, &packet, lentype, &data, &size); if (!ret) { GST_WARNING_OBJECT (demux, "Failed to parse payload %u/%u", i + 1, num); break; } } } else { GST_LOG_OBJECT (demux, "Parsing single payload"); ret = gst_asf_demux_parse_payload (demux, &packet, -1, &data, &size); } return ret; /* ERRORS */ short_packet: { GST_WARNING_OBJECT (demux, "Short packet!"); return FALSE; } }