/* Autogenerated config.h created for win32 Visual Studio builds */ /* PREFIX -- specifically added for Windows for easier moving */ #define PREFIX "C:\\gstreamer" /* Define if building universal (internal helper macro) */ #undef AC_APPLE_UNIVERSAL_BUILD /* Default audio sink */ #define DEFAULT_AUDIOSINK "directsoundsink" /* Default audio source */ #define DEFAULT_AUDIOSRC "audiotestsrc" /* Default video sink */ #undef DEFAULT_VIDEOSINK /* Default video source */ #define DEFAULT_VIDEOSRC "videotestsrc" /* Default visualizer */ #define DEFAULT_VISUALIZER "goom" /* Disable Orc */ #undef DISABLE_ORC /* Define to 1 if translation of program messages to the user's native language is requested. */ #undef ENABLE_NLS /* gettext package name */ #define GETTEXT_PACKAGE "gst-plugins-ugly-0.10" /* macro to use to show function name */ #undef GST_FUNCTION /* Defined if gcov is enabled to force a rebuild due to config.h changing */ #undef GST_GCOV_ENABLED /* Default errorlevel to use */ #define GST_LEVEL_DEFAULT GST_LEVEL_ERROR /* GStreamer license */ #define GST_LICENSE "LGPL" /* package name in plugins */ #define GST_PACKAGE_NAME "GStreamer Ugly Plug-ins prerelease" /* package origin */ #define GST_PACKAGE_ORIGIN "Unknown package origin" /* GStreamer package release date/time for plugins as YYYY-MM-DD */ #define GST_PACKAGE_RELEASE_DATETIME "2012-02-05T11:36Z" /* Define to enable a52dec (used by a52dec). */ #undef HAVE_A52DEC /* Define to enable amrnb library (used by amrnb). */ #undef HAVE_AMRNB /* Define to enable amrwb library (used by amrwbdec). */ #undef HAVE_AMRWB /* Define to enable cdio library (used by cdio). */ #undef HAVE_CDIO /* Define to 1 if you have the MacOS X function CFLocaleCopyCurrent in the CoreFoundation framework. */ #undef HAVE_CFLOCALECOPYCURRENT /* Define to 1 if you have the MacOS X function CFPreferencesCopyAppValue in the CoreFoundation framework. */ #undef HAVE_CFPREFERENCESCOPYAPPVALUE /* Define if the host CPU is an Alpha */ #undef HAVE_CPU_ALPHA /* Define if the host CPU is an ARM */ #undef HAVE_CPU_ARM /* Define if the host CPU is a CRIS */ #undef HAVE_CPU_CRIS /* Define if the host CPU is a CRISv32 */ #undef HAVE_CPU_CRISV32 /* Define if the host CPU is a HPPA */ #undef HAVE_CPU_HPPA /* Define if the host CPU is an x86 */ #define HAVE_CPU_I386 1 /* Define if the host CPU is a IA64 */ #undef HAVE_CPU_IA64 /* Define if the host CPU is a M68K */ #undef HAVE_CPU_M68K /* Define if the host CPU is a MIPS */ #undef HAVE_CPU_MIPS /* Define if the host CPU is a PowerPC */ #undef HAVE_CPU_PPC /* Define if the host CPU is a 64 bit PowerPC */ #undef HAVE_CPU_PPC64 /* Define if the host CPU is a S390 */ #undef HAVE_CPU_S390 /* Define if the host CPU is a SPARC */ #undef HAVE_CPU_SPARC /* Define if the host CPU is a x86_64 */ #undef HAVE_CPU_X86_64 /* Define if the GNU dcgettext() function is already present or preinstalled. */ #undef HAVE_DCGETTEXT /* Define to 1 if you have the header file. */ #undef HAVE_DLFCN_H /* define for working do while(0) macros */ #undef HAVE_DOWHILE_MACROS /* Define to enable dvdread library (used by dvdreadsrc). */ #undef HAVE_DVDREAD /* Define to enable building of experimental plug-ins. */ #undef HAVE_EXPERIMENTAL /* Define to enable building of plug-ins with external deps. */ #undef HAVE_EXTERNAL /* defined if the compiler implements __func__ */ #undef HAVE_FUNC /* defined if the compiler implements __FUNCTION__ */ #undef HAVE_FUNCTION /* Define if the GNU gettext() function is already present or preinstalled. */ #undef HAVE_GETTEXT /* Define if you have the iconv() function and it works. */ #undef HAVE_ICONV /* Define to 1 if you have the header file. */ #undef HAVE_INTTYPES_H /* Define to enable lame mp3 encoder library (used by lame). */ #undef HAVE_LAME /* Define to enable mad mp3 decoder (used by mad). */ #undef HAVE_MAD /* Define to 1 if you have the header file. */ #undef HAVE_MALLOC_H /* Define to 1 if you have the header file. */ #undef HAVE_MEMORY_H /* Define to enable mpeg2dec (used by mpeg2dec). */ #undef HAVE_MPEG2DEC /* Use Orc */ #undef HAVE_ORC /* defined if the compiler implements __PRETTY_FUNCTION__ */ #undef HAVE_PRETTY_FUNCTION /* Define if RDTSC is available */ #undef HAVE_RDTSC /* Define to enable libsidplay (used by sid). */ #undef HAVE_SIDPLAY /* Define to 1 if you have the header file. */ #undef HAVE_STDINT_H /* Define to 1 if you have the header file. */ #define HAVE_STDLIB_H 1 /* Define to 1 if you have the header file. */ #undef HAVE_STRINGS_H /* Define to 1 if you have the header file. */ #define HAVE_STRING_H 1 /* Define to 1 if you have the header file. */ #define HAVE_SYS_STAT_H 1 /* Define to 1 if you have the header file. */ #define HAVE_SYS_TYPES_H 1 /* Define to enable twolame (used by twolame). */ #undef HAVE_TWOLAME /* Define to 1 if you have the header file. */ #undef HAVE_UNISTD_H /* Define if valgrind should be used */ #undef HAVE_VALGRIND /* Define to 1 if you have the header file. */ #define HAVE_WINSOCK2_H 1 /* Define to enable x264 plug-in (used by x264). */ #undef HAVE_X264 /* the host CPU */ #define HOST_CPU "i686" /* gettext locale dir */ #define LOCALEDIR PREFIX "\\share\\locale" /* Define to the sub-directory in which libtool stores uninstalled libraries. */ #undef LT_OBJDIR /* Define to 1 if your C compiler doesn't accept -c and -o together. */ #undef NO_MINUS_C_MINUS_O /* Name of package */ #define PACKAGE "gst-plugins-ugly" /* Define to the address where bug reports for this package should be sent. */ #define PACKAGE_BUGREPORT "http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer" /* Define to the full name of this package. */ #define PACKAGE_NAME "GStreamer Ugly Plug-ins" /* Define to the full name and version of this package. */ #define PACKAGE_STRING "GStreamer Ugly Plug-ins 0.10.18.3" /* Define to the one symbol short name of this package. */ #define PACKAGE_TARNAME "gst-plugins-ugly" /* Define to the home page for this package. */ #undef PACKAGE_URL /* Define to the version of this package. */ #define PACKAGE_VERSION "0.10.18.3" /* directory where plugins are located */ #ifdef _DEBUG # define PLUGINDIR PREFIX "\\debug\\lib\\gstreamer-0.10" #else # define PLUGINDIR PREFIX "\\lib\\gstreamer-0.10" #endif /* The size of `char', as computed by sizeof. */ #undef SIZEOF_CHAR /* The size of `int', as computed by sizeof. */ #undef SIZEOF_INT /* The size of `long', as computed by sizeof. */ #undef SIZEOF_LONG /* The size of `short', as computed by sizeof. */ #undef SIZEOF_SHORT /* The size of `void*', as computed by sizeof. */ #undef SIZEOF_VOIDP /* Define to 1 if you have the ANSI C header files. */ #undef STDC_HEADERS /* Version number of package */ #define VERSION "0.10.18.3" /* Define WORDS_BIGENDIAN to 1 if your processor stores words with the most significant byte first (like Motorola and SPARC, unlike Intel). */ #if defined AC_APPLE_UNIVERSAL_BUILD # if defined __BIG_ENDIAN__ # define WORDS_BIGENDIAN 1 # endif #else # ifndef WORDS_BIGENDIAN # undef WORDS_BIGENDIAN # endif #endif