/* config.h.in. Generated from configure.ac by autoheader. */ /* This copy of config.h.in is specifically for win32 Visual Studio builds */ /* Define to 1 if translation of program messages to the user's native language is requested. */ #undef ENABLE_NLS /* gettext package name */ #define GETTEXT_PACKAGE "gst-plugins-ugly-0.10" /* macro to use to show function name */ #define GST_FUNCTION "(function)" /* Defined if gcov is enabled to force a rebuild due to config.h changing */ #undef GST_GCOV_ENABLED /* Default errorlevel to use */ #undef GST_LEVEL_DEFAULT /* GStreamer license */ #define GST_LICENSE "LGPL" /* package name in plugins */ #define GST_PACKAGE_NAME "GStreamer Ugly Plug-ins CVS/prerelease" /* package origin */ #define GST_PACKAGE_ORIGIN "Unknown package origin" /* support for features: gstalsa */ #undef HAVE_ALSA /* support for features: cdparanoia */ #undef HAVE_CDPARANOIA /* Define if the host CPU is an Alpha */ #undef HAVE_CPU_ALPHA /* Define if the host CPU is an ARM */ #undef HAVE_CPU_ARM /* Define if the host CPU is a HPPA */ #undef HAVE_CPU_HPPA /* Define if the host CPU is an x86 */ #define HAVE_CPU_I386 1 /* Define if the host CPU is a IA64 */ #undef HAVE_CPU_IA64 /* Define if the host CPU is a M68K */ #undef HAVE_CPU_M68K /* Define if the host CPU is a MIPS */ #undef HAVE_CPU_MIPS /* Define if the host CPU is a PowerPC */ #undef HAVE_CPU_PPC /* Define if the host CPU is a 64 bit PowerPC */ #undef HAVE_CPU_PPC64 /* Define if the host CPU is a S390 */ #undef HAVE_CPU_S390 /* Define if the host CPU is a SPARC */ #undef HAVE_CPU_SPARC /* Define if the host CPU is a x86_64 */ #undef HAVE_CPU_X86_64 /* Define if the GNU dcgettext() function is already present or preinstalled. */ #undef HAVE_DCGETTEXT /* Define to 1 if you have the header file. */ #undef HAVE_DLFCN_H /* support for features: */ #undef HAVE_EXTERNAL /* FIONREAD ioctl found in sys/filio.h */ #undef HAVE_FIONREAD_IN_SYS_FILIO /* FIONREAD ioctl found in sys/ioclt.h */ #undef HAVE_FIONREAD_IN_SYS_IOCTL /* defined if the compiler implements __func__ */ #undef HAVE_FUNC /* defined if the compiler implements __FUNCTION__ */ #undef HAVE_FUNCTION /* Define if the GNU gettext() function is already present or preinstalled. */ #undef HAVE_GETTEXT /* support for features: gnomevfssrc */ #undef HAVE_GNOME_VFS /* support for features: v4lsrc v4lmjpegsrc v4lmjpegsink */ #undef HAVE_GST_V4L /* Define if you have the iconv() function. */ #undef HAVE_ICONV /* Define to 1 if you have the header file. */ #undef HAVE_INTTYPES_H /* Define to 1 if you have the `asound' library (-lasound). */ #undef HAVE_LIBASOUND /* support for features: libvisual */ #undef HAVE_LIBVISUAL /* Define if you have C99's lrint function. */ #undef HAVE_LRINT /* Define if you have C99's lrintf function. */ #undef HAVE_LRINTF /* Define to 1 if you have the header file. */ #undef HAVE_MALLOC_H /* Define to 1 if you have the header file. */ #undef HAVE_MEMORY_H /* support for features: oggdemux oggmux */ #undef HAVE_OGG /* support for features: pango */ #undef HAVE_PANGO /* defined if the compiler implements __PRETTY_FUNCTION__ */ #undef HAVE_PRETTY_FUNCTION /* Define if RDTSC is available */ #undef HAVE_RDTSC /* Define to 1 if you have the header file. */ #undef HAVE_REGEX_H /* Define to 1 if you have the header file. */ #undef HAVE_STDINT_H /* Define to 1 if you have the header file. */ #define HAVE_STDLIB_H 1 /* Define to 1 if you have the header file. */ #undef HAVE_STRINGS_H /* Define to 1 if you have the header file. */ #define HAVE_STRING_H 1 /* Define to 1 if you have the header file. */ #undef HAVE_SYS_SOCKET_H /* Define to 1 if you have the header file. */ #undef HAVE_SYS_STAT_H 1 /* Define to 1 if you have the header file. */ #undef HAVE_SYS_TYPES_H 1 /* support for features: theoradec theoraenc */ #undef HAVE_THEORA /* Define to 1 if you have the header file. */ #undef HAVE_UNISTD_H /* Define if valgrind should be used */ #undef HAVE_VALGRIND /* support for features: vorbisenc vorbisdec */ #undef HAVE_VORBIS /* defined if vorbis_synthesis_restart is present */ #undef HAVE_VORBIS_SYNTHESIS_RESTART /* support for features: ximagesink */ #undef HAVE_X /* support for features: xshm */ #undef HAVE_XSHM /* support for features: xvimagesink */ #undef HAVE_XVIDEO /* gettext locale dir */ #define LOCALEDIR PREFIX "\\share\\locale" /* Name of package */ #define PACKAGE "gst-plugins-ugly" /* Define to the address where bug reports for this package should be sent. */ #define PACKAGE_BUGREPORT "http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer" /* Define to the full name of this package. */ #undef PACKAGE_NAME "GStreamer Ugly Plug-ins" /* Define to the full name and version of this package. */ #undef PACKAGE_STRING "GStreamer Ugly Plug-ins 0.10.10.1" /* Define to the one symbol short name of this package. */ #undef PACKAGE_TARNAME "gst-plugins-ugly" /* Define to the version of this package. */ #undef PACKAGE_VERSION "0.10.10.1" /* directory where plugins are located */ #undef PLUGINDIR /* The size of a `char', as computed by sizeof. */ #undef SIZEOF_CHAR /* The size of a `int', as computed by sizeof. */ #undef SIZEOF_INT /* The size of a `long', as computed by sizeof. */ #undef SIZEOF_LONG /* The size of a `short', as computed by sizeof. */ #undef SIZEOF_SHORT /* The size of a `void*', as computed by sizeof. */ #undef SIZEOF_VOIDP /* Define to 1 if you have the ANSI C header files. */ #undef STDC_HEADERS /* Version number of package */ #define VERSION "0.10.10.1" /* Define to 1 if your processor stores words with the most significant byte first (like Motorola and SPARC, unlike Intel and VAX). */ #undef WORDS_BIGENDIAN /* Define to 1 if the X Window System is missing or not being used. */ #undef X_DISPLAY_MISSING /* Define to `__inline__' or `__inline' if that's what the C compiler calls it, or to nothing if 'inline' is not supported under any name. */ #ifndef __cplusplus #undef inline #endif