diff --git a/ChangeLog b/ChangeLog
index 4454a6de707ce7bd6b829c618c1cb17d13d8a14b..3823344459e48e4b5ee7c5b2f9d7396c4ed414fb 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
+2006-06-12 Wim Taymans <wim@fluendo.com>
+
+ * tests/check/elements/amrnbenc.c: (push_data):
+ Init memory before feeding it to the encoder to make
+ the valgrind test succeed.
+
+2006-06-12 Edward Hervey <edward@fluendo.com>
+
+ * gst/asfdemux/.cvsignore:
+ More ignore
+
+2006-06-11 Tim-Philipp Müller <tim at centricular dot net>
+
+ * .cvsignore:
+ Ignore files generated by 'make dist'.
+
+2006-06-11 Thomas Vander Stichele <thomas at apestaart dot org>
+
+ * autogen.sh:
+ * configure.ac:
+ * ext/a52dec/Makefile.am:
+ * ext/dvdnav/Makefile.am:
+ * ext/dvdread/Makefile.am:
+ * ext/lame/Makefile.am:
+ * ext/mad/Makefile.am:
+ * ext/mpeg2dec/Makefile.am:
+ * ext/sidplay/Makefile.am:
+ update build files
+
+2006-06-07 Wim Taymans <wim@fluendo.com>
+
+ * ext/mpeg2dec/gstmpeg2dec.c: (gst_mpeg2dec_finalize),
+ (gst_mpeg2dec_reset), (clear_buffers), (handle_picture),
+ (gst_mpeg2dec_sink_convert), (gst_mpeg2dec_src_convert),
+ (gst_mpeg2dec_change_state):
+ * ext/mpeg2dec/gstmpeg2dec.h:
+ Simplify and don't leak our buffer pool.
+ Use _scale_int.
+ Remove unfixed bug number from previous ChangeLog entry.
+
+2006-06-07 Wim Taymans <wim@fluendo.com>
+
+ * ext/mpeg2dec/gstmpeg2dec.c: (gst_mpeg2dec_base_init),
+ (gst_mpeg2dec_class_init), (gst_mpeg2dec_init),
+ (gst_mpeg2dec_finalize), (gst_mpeg2dec_reset),
+ (gst_mpeg2dec_qos_reset), (gst_mpeg2dec_alloc_buffer),
+ (gst_mpeg2dec_negotiate_format), (init_dummybuf),
+ (handle_sequence), (handle_picture), (handle_slice),
+ (gst_mpeg2dec_chain), (gst_mpeg2dec_sink_event),
+ (gst_mpeg2dec_src_event), (gst_mpeg2dec_change_state):
+ * ext/mpeg2dec/gstmpeg2dec.h:
+ Fix padtemplate as we can now do fractional framerates.
+ Small cleanups.
+ Use GstSegment.
+ Add simple frame dropping QoS.
+ Precalc buffer output sizes and UV offsets.
+ Always give libmpeg2 a valid fbuf when it wants one.
+ don't trust libmpeg to discard our buffers but manage it
+ ourselves.
+ Fixes #343627, #335288
+
+2006-06-05 Sebastien Moutte <sebastien@moutte.net>
+
+ * win32/MANIFEST:
+ Add a manifest for futures ugly win32 releases.
+ * gst/iec958/ac3iec.c: (ac3iec_chain_raw):
+ Move bufcaps declaration at the begining of the instructions
+ block.
+
+2006-06-02 Stefan Kost <ensonic@users.sf.net>
+
+ * ext/a52dec/gsta52dec.h:
+ * ext/amrnb/amrnbdec.h:
+ * ext/amrnb/amrnbenc.h:
+ * ext/amrnb/amrnbparse.h:
+ * ext/mpeg2dec/gstmpeg2dec.h:
+ * ext/sidplay/gstsiddec.h:
+ * gst/ac3parse/gstac3parse.h:
+ * gst/asfdemux/gstasfdemux.h:
+ * gst/asfdemux/gstasfmux.h:
+ * gst/dvdlpcmdec/gstdvdlpcmdec.h:
+ * gst/iec958/ac3iec.h:
+ * gst/mpegaudioparse/gstmpegaudioparse.h:
+ * gst/mpegstream/gstdvddemux.h:
+ * gst/mpegstream/gstmpegclock.h:
+ * gst/mpegstream/gstmpegdemux.h:
+ * gst/mpegstream/gstmpegparse.h:
+ Fix more gobject macros: obj<->klass, GstXXX<->GstXXXClass
+
+2006-05-27 Tim-Philipp Müller <tim at centricular dot net>
+
+ * README:
+ Replace current README (containing the release notes from
+ some 0.9.x version) with a proper README taken from the core.
+
+2006-05-24 Wim Taymans <wim@fluendo.com>
+
+ * ext/amrnb/amrnbdec.c: (gst_amrnbdec_event), (gst_amrnbdec_chain):
+ * ext/amrnb/amrnbparse.c: (gst_amrnbparse_init),
+ (gst_amrnbparse_sink_event), (gst_amrnbparse_chain),
+ (gst_amrnbparse_sink_activate), (gst_amrnbparse_state_change):
+ * ext/amrnb/amrnbparse.h:
+ Sortof first quick cleanup of all this mess...
+ Don't crap out on empty and invalid FTs but treat them as
+ empty packets, the decoder handles them fine.
+ Fixes #342222.
+
+2006-05-22 Tim-Philipp Müller <tim at centricular dot net>
+
+ * gst/asfdemux/gstasf.c: (plugin_init):
+ Call gst_riff_init() so the riff debug category gets set up
+ before it is being used.
+
+2006-05-19 Michael Smith <msmith@fluendo.com>
+
+ * gst/iec958/ac3_padder.c: (ac3p_parse):
+ * gst/iec958/ac3_padder.h:
+ * gst/iec958/ac3iec.c: (ac3iec_init), (ac3iec_set_property),
+ (ac3iec_chain_raw), (ac3iec_change_state):
+ * gst/iec958/ac3iec.h:
+ Write rate into the caps, for the allowed ac3 rates. Some minor
+ cleanups.
+
+2006-05-18 Tim-Philipp Müller <tim at centricular dot net>
+
+ Patch by: James "Doc" Livingston <doclivingston gmail com>
+
+ * ext/mad/gstid3tag.c: (gst_id3_tag_get_tag_to_render):
+ Do tag merging correctly (#339918). Output taglists
+ properly in debug statements too while we're at it.
+
2006-05-11 Jan Schmidt <thaytan@mad.scientist.com>
* ext/a52dec/gsta52dec.c: (gst_a52dec_chain):