]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gst-plugins-ugly0-10.git/blobdiff - ChangeLog
MAINTAINERS: Updating all the maintainers files
[glsdk/gst-plugins-ugly0-10.git] / ChangeLog
index cb99f28b12872b961e9447bd3ee76fe0cc07815f..3bb3c3e54eb49ff87ef61705eeff4f68ebb0cafb 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
@@ -1,3 +1,165 @@
+2007-06-22  Jan Schmidt  <thaytan@mad.scientist.com>
+
+       * MAINTAINERS:
+       Updating all the maintainers files
+
+2007-06-22  Edward Hervey  <edward@fluendo.com>
+
+       * ext/amrnb/amrnbdec.c: (gst_amrnbdec_init):
+       * gst/ac3parse/gstac3parse.c: (gst_ac3parse_init):
+       * gst/asfdemux/gstasfmux.c: (gst_asfmux_init):
+       * gst/dvdlpcmdec/gstdvdlpcmdec.c: (gst_dvdlpcmdec_init):
+       * gst/dvdsub/gstdvdsubdec.c: (gst_dvd_sub_dec_init):
+       * gst/iec958/ac3iec.c: (ac3iec_init):
+       * gst/mpegstream/gstrfc2250enc.c: (gst_rfc2250_enc_init):
+       Fix leaks some more.
+
+2007-06-21  Edward Hervey  <edward@fluendo.com>
+
+       * gst/mpegaudioparse/gstmpegaudioparse.c: (gst_mp3parse_init):
+       "She's leaking me", said valgrind.
+
+2007-06-19  Jan Schmidt  <thaytan@mad.scientist.com>
+
+       * gst/mpegaudioparse/gstmpegaudioparse.c: (mp3_caps_create):
+       Fix "pad caps are not a real subset of its template caps" warning.
+
+2007-06-19  Wim Taymans  <wim@fluendo.com>
+
+       Patch by: Laurent Glayal <spglegle at yahoo dot fr>
+
+       * ext/amrnb/amrnbdec.c: (gst_amrnbdec_class_init),
+       (gst_amrnbdec_finalize):
+       Don't leak the adapter, unref it in a new finalize method instead.
+       Fixes #448782.
+
+2007-06-19  Jan Schmidt  <thaytan@mad.scientist.com>
+
+       * configure.ac:
+       Back to CVS
+
+       * gst-plugins-ugly.doap:
+       Add 0.10.6 to the list of releases.
+
+=== release 0.10.6 ===
+
+2007-06-19  Jan Schmidt <thaytan@mad.scientist.com>
+
+       * configure.ac:
+         releasing 0.10.6, "The Sacrifice"
+
+2007-06-15  Jan Schmidt  <thaytan@mad.scientist.com>
+
+       * win32/vs6/gst_plugins_ugly.dsw:
+       * win32/vs6/libgstac3parse.dsp:
+       * win32/vs6/libgstasfdemux.dsp:
+       * win32/vs6/libgstdvdlpcmdec.dsp:
+       * win32/vs6/libgstdvdsub.dsp:
+       * win32/vs6/libgstiec958.dsp:
+       * win32/vs6/libgstlame.dsp:
+       * win32/vs6/libgstmad.dsp:
+       * win32/vs6/libgstmpegaudioparse.dsp:
+       * win32/vs6/libgstmpegstream.dsp:
+       * win32/vs6/libgstrealmedia.dsp:
+       * win32/vs6/libgstsynaesthesia.dsp:
+         Convert line endings to CRLF and mark as binary files.
+
+2007-06-13  Tim-Philipp Müller  <tim at centricular dot net>
+
+       * ext/dvdnav/dvdnavsrc.c: (gst_dvd_nav_src_set_property):
+         Don't forget to unlock when setting the device property, or
+         we'll sooner or later deadlock.
+
+2007-06-12  Sebastien Moutte  <sebastien@moutte.net>
+
+       * gst/dvdsub/gstdvdsubdec.c:(gst_dvd_sub_dec_parse_subpic):
+       Use gst_util_guint64_to_gdouble for conversion.
+       * win32/vs6/libgstasfdemux.dsp:
+       Add asfpacket.c to the build.
+       
+2007-06-08  Jan Schmidt  <thaytan@mad.scientist.com>
+
+       * gst/mpegaudioparse/gstmpegaudioparse.c: (gst_mp3parse_reset),
+       (gst_mp3parse_emit_frame), (gst_mp3parse_handle_first_frame):
+       * gst/mpegaudioparse/gstmpegaudioparse.h:
+       If the Xing header provides a total time, use it to calculate the
+       correct average bitrate immediately, instead of sending updates as 
+       we parse the stream.
+
+2007-06-05  Sebastian Dröge  <slomo@circular-chaos.org>
+
+       Patch by by: Mark Nauwelaerts <manauw at skynet dot be>
+
+       * gst/dvdsub/gstdvdsubdec.c: (gst_dvd_sub_dec_parse_subpic):
+       Use GstClockTime instead of guint for a time variable to prevent
+       overflows on too large subtitle durations. Fixes #444514.
+
+2007-05-31  Tim-Philipp Müller  <tim at centricular dot net>
+
+       Patch by: Mark Nauwelaerts <manauw at skynet be>
+
+       * gst/dvdsub/gstdvdsubdec.c: (gst_dvd_sub_dec_sink_event):
+         Clear state when handling the serialized FLUSH_STOP event instead of
+         the FLUSH_START event, thereby making sure we don't free buffers the
+         chain function is still using. Fixes dvdsubdec crashing when flusing
+         or seeking (#442706).
+
+2007-05-23  Tim-Philipp Müller  <tim at centricular dot net>
+
+       * gst/mpegaudioparse/gstmpegaudioparse.c: (gst_mp3parse_chain):
+         Initialise variable to make fc4 build bot happy.
+
+2007-05-21  Tim-Philipp Müller  <tim at centricular dot net>
+
+       * gst/mpegstream/gstmpegdemux.c: (gst_mpeg_demux_send_subbuffer):
+         Add sanity check so we don't abort for broken or non-MPEG streams,
+         but instead error out. Fixes crashes/aborts for when our typefinder
+         wrongly identifies quicktime files as mpeg (which should be fixed in
+         -base now too). (#440120).
+
+2007-05-18  Stefan Kost  <ensonic@users.sf.net>
+
+       * ext/amrnb/amrnbdec.c (gst_amrnbdec_debug, GST_CAT_DEFAULT,
+         block_size, _do_init, gst_amrnbdec_base_init,
+         gst_amrnbdec_class_init, gst_amrnbdec_init):
+       * ext/amrnb/amrnbenc.c (gst_amrnbenc_debug, GST_CAT_DEFAULT, _do_init,
+         gst_amrnbenc_base_init, gst_amrnbenc_class_init, gst_amrnbenc_init):
+       * ext/amrnb/amrnbparse.c (gst_amrnbparse_debug, GST_CAT_DEFAULT,
+         block_size, _do_init, gst_amrnbparse_base_init,
+         gst_amrnbparse_class_init, gst_amrnbparse_init):
+         First round of cleanups, that use GST_BOILERPLATE, GST_ELEMENT_DETAILS,
+         GST_DEBUG_FUNCPTR and add log-category.
+
+2007-05-18  Jan Schmidt  <thaytan@mad.scientist.com>
+
+       * gst/mpegaudioparse/gstmpegaudioparse.c:
+       (mp3_type_frame_length_from_header), (gst_mp3parse_reset),
+       (gst_mp3parse_emit_frame), (gst_mp3parse_handle_first_frame),
+       (gst_mp3parse_chain), (mp3parse_total_bytes),
+       (mp3parse_total_time):
+       * gst/mpegaudioparse/gstmpegaudioparse.h:
+       Implement parsing of Xing headers from the first frame of the stream,
+       and use it to report duration correctly where possible.
+
+2007-05-16  Tim-Philipp Müller  <tim at centricular dot net>
+
+       * gst/realmedia/rmdemux.c: (gst_rmdemux_descramble_cook_audio):
+         After descrambling, push the packets out as individual packets
+         instead of one big descrambled buffer. Makes cook audio decoding
+         work with the 'realaudiodec' decoder from gst-plugins-bad.
+
+2007-05-16  Tim-Philipp Müller  <tim at centricular dot net>
+
+       * gst/realmedia/rmdemux.c: (gst_rmdemux_init),
+       (gst_rmdemux_sink_event), (gst_rmdemux_perform_seek),
+       (gst_rmdemux_reset), (gst_rmdemux_chain), (gst_rmdemux_add_stream),
+       (gst_rmdemux_parse_packet):
+       * gst/realmedia/rmdemux.h:
+         Remember first timestamp encountered in stream and re-timestamp
+         stream to start from zero (fixes #397219); only send one newsegment
+         event, not two; when seeking, send newsegment events from the
+         streaming thread and not from the seeking thread.
+
 2007-05-16  Tim-Philipp Müller  <tim at centricular dot net>
 
        Based on patch by: Mark Nauwelaerts  <manauw skynet be>
 
 === release 0.10.0 ===
 
-2005-12-05   <thomas (at) apestaart (dot) org>
+2005-12-05  Thomas Vander Stichele  <thomas (at) apestaart (dot) org>
 
        * configure.ac:
          releasing 0.10.0, "Brie"
 
 === release 0.9.7 ===
 
-2005-12-01   <thomas (at) apestaart (dot) org>
+2005-12-01  Thomas Vander Stichele  <thomas (at) apestaart (dot) org>
 
        * configure.ac:
          releasing 0.9.7, "Canis Meus Naso Non Habet"