diff --git a/ChangeLog b/ChangeLog
index 09f041bdf503ef9293605af08cd84d34cc0059be..754fc27614f9577b7ceabcf4a52d74d2196b68c8 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
+2004-10-01 Christian Schaller <christian@fluendo.com>
+
+ * Patch fra Phil Blundell
+ * Bug 152341
+ * ext/ivorbis/vorbis.c
+
+2004-10-01 Wim Taymans <wim@fluendo.com>
+
+ * ext/speex/gstspeexdec.c: (gst_speex_dec_class_init),
+ (speex_dec_get_formats), (speex_dec_convert),
+ (speex_dec_src_query), (speex_dec_src_event), (speex_dec_event),
+ (speex_dec_chain), (gst_speexdec_get_property),
+ (gst_speexdec_set_property):
+ Small cleanups.
+
+2004-10-01 Wim Taymans <wim@fluendo.com>
+
+ * gst/wavparse/gstwavparse.c: (gst_wavparse_class_init),
+ (gst_wavparse_stream_init), (gst_wavparse_fmt),
+ (gst_wavparse_other), (gst_wavparse_loop),
+ (gst_wavparse_pad_convert), (gst_wavparse_pad_query),
+ (gst_wavparse_srcpad_event):
+ * gst/wavparse/gstwavparse.h:
+ Added some more debugging info.
+ Fix the case where the length of the file is 0.
+ Make sure we seek to sample borders.
+
+2004-10-01 Wim Taymans <wim@fluendo.com>
+
+ * gst/playback/README:
+ * gst/playback/gstdecodebin.c: (gst_decode_bin_factory_filter),
+ (gst_decode_bin_init), (find_compatibles), (close_pad_link),
+ (try_to_link_1), (no_more_pads), (close_link), (type_found):
+ Add some debug info to decodebin, update README
+
+2004-10-01 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * ext/dvdnav/dvdnavsrc.c: (dvdnav_handle_navigation_event):
+ Don't use g_print(); use GST_DEBUG().
+
+2004-10-01 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * ext/ogg/gstoggmux.c: (gst_ogg_mux_next_buffer),
+ (gst_ogg_mux_queue_pads):
+ Handle EOS properly.
+
+2004-10-01 Sebastien Cote <sc5@hermes.usherb.ca>
+
+ Reviewed by: Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * ext/faad/gstfaad.c: (gst_faad_init), (gst_faad_sinkconnect),
+ (gst_faad_chain), (gst_faad_change_state):
+ * ext/faad/gstfaad.h:
+ Allow playback of raw (unframed) MPEG AAC files (#148993).
+
+2004-10-01 Sebastien Cote <sc5@hermes.usherb.ca>
+
+ Reviewed by: Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * gst/wavparse/gstwavparse.c: (gst_wavparse_fmt):
+ Throw error if we didn't recognize the stream. Fixes #152289.
+
+2004-10-01 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * gst/videoscale/gstvideoscale.c: (gst_videoscale_link):
+ Fix negotiation.
+
+2004-10-01 Francis Labonte <francis_labonte@hotmail.com>
+
+ Reviewed by: Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * gst/wavparse/gstwavparse.c: (gst_wavparse_fmt):
+ Fix memleak.
+
+2004-10-01 Balamurali Viswanathan <balamurali.viswanathan@wipro.com>
+
+ Reviewed by: Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * sys/sunaudio/gstsunaudio.c: (gst_sunaudiosink_setparams):
+ Solve #152805.
+ * sys/sunaudio/gstsunmixer.c: (gst_sunaudiomixer_set_mute):
+ Solve 152806.
+
+2004-10-01 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * gst-libs/gst/riff/riff-media.c:
+ (gst_riff_create_video_caps_with_data),
+ (gst_riff_create_audio_caps_with_data):
+ Add codec_data handling (like asfdemux used to do).
+ * gst/asfdemux/gstasf.c: (plugin_init):
+ * gst/asfdemux/gstasfdemux.c: (gst_asf_demux_base_init),
+ (gst_asf_demux_add_audio_stream), (gst_asf_demux_add_video_stream):
+ Use riff-media for caps creation instead of our own (mostly
+ broken) copy of its functions.
+
+2004-10-01 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * sys/v4l/v4lsrc_calls.c: (gst_v4lsrc_try_capture):
+ Don't actually error out if we get another return value than
+ -EINVAL. Opposite to what I first thought, drivers have random
+ return values for this, although -EINVAL is the expected return
+ value. Since this is not fatal, we shouldn't use
+ GST_ELEMENT_ERROR() but just GST_ERROR_OBJECT().
+
+2004-10-01 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * ext/dvdread/dvdreadsrc.c: (dvdreadsrc_class_init),
+ (dvdreadsrc_init), (dvdreadsrc_dispose), (dvdreadsrc_set_property),
+ (dvdreadsrc_get_property), (_open), (_seek), (_read),
+ (dvdreadsrc_get), (dvdreadsrc_open_file),
+ (dvdreadsrc_change_state):
+ Fix. Don't do one big huge loop around the whole DVD, that will
+ cache all data and thus eat sizeof(dvd) (several GB) before we
+ see something.
+ * gst-libs/gst/riff/riff-read.c: (gst_riff_read_seek):
+ Actually NULL'ify event after using it.
+ * gst/matroska/ebml-read.c: (gst_ebml_read_use_event),
+ (gst_ebml_read_handle_event), (gst_ebml_read_element_id),
+ (gst_ebml_read_element_length), (gst_ebml_read_element_data),
+ (gst_ebml_read_seek), (gst_ebml_read_skip):
+ Handle events.
+ * gst/mpegstream/gstdvddemux.c: (gst_dvd_demux_base_init),
+ (gst_dvd_demux_init), (gst_dvd_demux_get_audio_stream),
+ (gst_dvd_demux_get_subpicture_stream), (gst_dvd_demux_plugin_init):
+ Fix timing (this will probably break if I seek using menus, but
+ I didn't get there yet). VOBs and normal DVDs should now work.
+ Add a mpeg2-only pad with high rank so this get autoplugged for
+ MPEG-2 movies.
+ * gst/mpegstream/gstmpegdemux.c: (gst_mpeg_demux_base_init),
+ (gst_mpeg_demux_class_init), (gst_mpeg_demux_init),
+ (gst_mpeg_demux_new_output_pad), (gst_mpeg_demux_get_video_stream),
+ (gst_mpeg_demux_get_audio_stream),
+ (gst_mpeg_demux_get_private_stream), (gst_mpeg_demux_parse_packet),
+ (gst_mpeg_demux_parse_pes), (gst_mpeg_demux_plugin_init):
+ Use this as second rank for MPEG-1 and MPEG-2. Still use this for
+ MPEG-1 but use dvddemux for MPEG-2.
+ * gst/mpegstream/gstmpegparse.c: (gst_mpeg_parse_class_init),
+ (gst_mpeg_parse_init), (gst_mpeg_parse_new_pad),
+ (gst_mpeg_parse_parse_packhead):
+ Timing. Only add pad template if it exists. Add sink template from
+ class and not from ourselves. This means we will always use the
+ correct sink template even if it is not the one defined in this
+ file.
+
+2004-09-29 Wim Taymans <wim@fluendo.com>
+
+ * gst/mpegstream/gstmpegdemux.c: (gst_mpeg_demux_parse_packet),
+ (gst_mpeg_demux_parse_pes):
+ * gst/mpegstream/gstmpegparse.c: (gst_mpeg_parse_parse_packhead):
+ Fix playback of mpeg again, timestamps where screwed up by
+ patch 1.61.
+
+2004-09-29 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * ext/flac/gstflacdec.c: (gst_flacdec_src_query):
+ Only return true if we actually filled something in. Prevents
+ player applications from showing a random length for flac files.
+ * gst-libs/gst/riff/riff-read.c: (gst_riff_read_class_init),
+ (gst_riff_read_use_event), (gst_riff_read_handle_event),
+ (gst_riff_read_seek), (gst_riff_read_skip), (gst_riff_read_strh),
+ (gst_riff_read_strf_vids_with_data),
+ (gst_riff_read_strf_auds_with_data), (gst_riff_read_strf_iavs):
+ OK, ok, so I implemented event handling. Apparently it's normal
+ that we receive random events at random points without asking
+ for it.
+ * gst/avi/gstavidemux.c: (gst_avi_demux_reset),
+ (gst_avi_demux_src_convert), (gst_avi_demux_handle_src_query),
+ (gst_avi_demux_handle_src_event), (gst_avi_demux_stream_index),
+ (gst_avi_demux_sync), (gst_avi_demux_stream_scan),
+ (gst_avi_demux_massage_index), (gst_avi_demux_stream_header),
+ (gst_avi_demux_handle_seek), (gst_avi_demux_process_next_entry),
+ (gst_avi_demux_stream_data), (gst_avi_demux_loop):
+ * gst/avi/gstavidemux.h:
+ Implement non-lineair chunk handling and subchunk processing.
+ The first solves playback of AVI files where the audio and video
+ data of individual buffers that we read are not synchronized.
+ This should not happen according to the wonderful AVI specs, but
+ of course it does happen in reality. It is also a prerequisite for
+ the second. Subchunk processing allows us to cut chunks in small
+ pieces and process each of these pieces separately. This is
+ required because I've seen several AVI files with incredibly large
+ audio chunks, even some files with only one audio chunk for the
+ whole file. This allows for proper playback including seeking.
+ This patch is supposed to fix all AVI A/V sync issues.
+ * gst/flx/gstflxdec.c: (gst_flxdec_class_init),
+ (flx_decode_chunks), (flx_decode_color), (gst_flxdec_loop):
+ Work.
+ * gst/modplug/gstmodplug.cc:
+ Proper return value setting for the query() function.
+ * gst/playback/gstplaybasebin.c: (setup_source):
+ Being in non-playing state (after, e.g., EOS) is not necessarily
+ a bad thing. Allow for that. This fixes playback of short files.
+ They don't actually playback fully now, because the clock already
+ runs. This means that small files (<500kB) with a small length
+ (<2sec) will still not or barely play. Other files, such as mod
+ or flx, will work correctly, however.
+
+2004-09-28 Wim Taymans <wim@fluendo.com>
+
+ * ext/speex/gstspeex.c: (plugin_init):
+ * ext/speex/gstspeexdec.c: (gst_speex_dec_base_init),
+ (gst_speex_dec_class_init), (speex_dec_get_formats),
+ (speex_get_event_masks), (speex_get_query_types),
+ (gst_speex_dec_init), (speex_dec_convert), (speex_dec_src_query),
+ (speex_dec_src_event), (speex_dec_event), (speex_dec_chain),
+ (gst_speexdec_get_property), (gst_speexdec_set_property),
+ (speex_dec_change_state):
+ * ext/speex/gstspeexdec.h:
+ * ext/speex/gstspeexenc.c: (gst_speexenc_get_formats),
+ (gst_speexenc_get_type), (speex_caps_factory), (raw_caps_factory),
+ (gst_speexenc_base_init), (gst_speexenc_class_init),
+ (gst_speexenc_sinkconnect), (gst_speexenc_convert_src),
+ (gst_speexenc_convert_sink), (gst_speexenc_get_query_types),
+ (gst_speexenc_src_query), (gst_speexenc_init),
+ (gst_speexenc_get_tag_value), (comment_init), (comment_add),
+ (gst_speexenc_metadata_set1), (gst_speexenc_set_metadata),
+ (gst_speexenc_setup), (gst_speexenc_buffer_from_data),
+ (gst_speexenc_push_buffer), (gst_speexenc_set_header_on_caps),
+ (gst_speexenc_chain), (gst_speexenc_get_property),
+ (gst_speexenc_set_property), (gst_speexenc_change_state):
+ * ext/speex/gstspeexenc.h:
+ Rewrote speex encoder, make sure it can be embedded in ogg.
+ Implemented speex decoder.
+
+2004-09-28 Christian Schaller <christian@fluendo.com>
+
+ * configure.ac:
+ Remove kioslave plugin. Markey is brewing a new working one
+ * ext/Makefile.am: Remove kioslave plugin
+ * ext/kio: remove
+ * gst-plugins.spec.in: remove kio plugin from spec
+
+2004-09-27 Wim Taymans <wim@fluendo.com>
+
+ * gst/tcp/gstmultifdsink.c: (gst_multifdsink_add),
+ (gst_multifdsink_remove), (gst_multifdsink_remove_client_link),
+ (is_sync_frame), (gst_multifdsink_client_queue_buffer),
+ (gst_multifdsink_new_client),
+ (gst_multifdsink_handle_client_write),
+ (gst_multifdsink_recover_client), (gst_multifdsink_queue_buffer),
+ (gst_multifdsink_handle_clients):
+ * gst/tcp/gstmultifdsink.h:
+ Make syncing to keyframes actually work for new clients and lagging
+ clients.
+
+2004-09-26 Benjamin Otte <in7y118@public.uni-hamburg.de>
+
+ * gst/debug/gstnavigationtest.c: (gst_navigationtest_class_init),
+ (gst_navigationtest_handle_src_event), (draw_box_planar411),
+ (gst_navigationtest_planar411), (gst_navigationtest_change_state):
+ * gst/debug/gstnavigationtest.h:
+ make navigationtest display button-press and button-release events
+
+2004-09-26 Iain <iaingnome@gmail.com>
+
+ * gst/interleave/interleave.c (all_channels_new_media): Checks if all
+ the channels have received a new media event.
+ (interleave_buffered_loop): Compresses a new media event on all
+ channels into one.
+
+2004-09-26 Iain <iaingnome@gmail.com>
+
+ * gst/wavenc/gstwavenc.c (gst_wavenc_chain): Company says we need to
+ call the sinkpad's default event handler and not the srcpads. He also
+ says this is confusing :)
+ (gst_wavenc_stop_file): Company says that seek events only go upstream
+ we should send a discontinuous downstream instead.
+
+2004-09-25 Christian Schaller <christian@fluendo.com>
+
+ * Update SPEC file to be usable in conjunction with Fedora Core,
+ Fedora.us and freshrpms packages
+ * Fix typo in multifilesrc test Makefile
+
+2004-09-24 Wim Taymans <wim@fluendo.com>
+
+ * gst/playback/gstplaybasebin.c: (new_decoded_pad):
+ Only signal the no_more_pads signal when we have
+ added the stream to our list.
+
+2004-09-24 Wim Taymans <wim@fluendo.com>
+
+ * gst/playback/gstplaybasebin.c: (remove_prerolls),
+ (new_decoded_pad):
+ * gst/playback/gstplaybasebin.h:
+ * gst/playback/gstplaybin.c: (setup_sinks):
+ Don't try to preroll or decode more than one audio/video
+ track.
+
+2004-09-24 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * gst/playback/gstplaybasebin.c: (gst_play_base_bin_change_state):
+ Throw error if we failed to find a suitable output. This should
+ throw an error if we successfully set up a pipeline (e.g. because
+ we recognized a media file) but found no decodable streams in it
+ (e.g. because it contains only media stream types for which we
+ have no decoders, or because it's not a media type).
+
+2004-09-23 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * ext/dirac/Makefile.am:
+ * ext/dirac/gstdirac.cc:
+ * ext/dirac/gstdiracdec.cc:
+ * ext/dirac/gstdiracdec.h:
+ Do something. Don't actually know if this works because I don't
+ have a demuxer yet.
+ * ext/gsm/gstgsmdec.c: (gst_gsmdec_getcaps):
+ Add channels=1 to caps returned from _getcaps().
+ * ext/ogg/gstogmparse.c: (gst_ogm_audio_parse_get_type),
+ (gst_ogm_video_parse_get_type), (gst_ogm_audio_parse_base_init),
+ (gst_ogm_video_parse_base_init), (gst_ogm_parse_init),
+ (gst_ogm_audio_parse_init), (gst_ogm_video_parse_init),
+ (gst_ogm_parse_sink_convert), (gst_ogm_parse_chain),
+ (gst_ogm_parse_change_state):
+ Separate between audio/video so ogmaudioparse actually uses the
+ audio pad templates. Both audio and video work now, including
+ autoplugging. Also use sometimes-srcpad hack.
+ * gst-libs/gst/riff/riff-read.c: (gst_riff_read_seek):
+ Handle events better. Don't hang on infinite loops.
+ * gst/avi/gstavidemux.c: (gst_avi_demux_class_init),
+ (gst_avi_demux_init), (gst_avi_demux_reset),
+ (gst_avi_demux_src_convert), (gst_avi_demux_handle_src_query),
+ (gst_avi_demux_stream_header), (gst_avi_demux_stream_data),
+ (gst_avi_demux_change_state):
+ * gst/avi/gstavidemux.h:
+ Improve A/V sync. Still not perfect.
+ * gst/matroska/ebml-read.c: (gst_ebml_read_seek),
+ (gst_ebml_read_skip):
+ Handle events better.
+ * gst/qtdemux/qtdemux.c: (gst_qtdemux_handle_sink_event),
+ (gst_qtdemux_loop_header), (qtdemux_parse_trak),
+ (qtdemux_audio_caps):
+ Add IMA4. Improve event handling. Save offset after a seek when
+ the headers are at the end of the file so that we don't end up in
+ an infinite loop.
+ * gst/typefind/gsttypefindfunctions.c: (qt_type_find):
+ Add low-priority typefind support for files with no length.
+
+2004-09-23 Zaheer Abbas Merali <zaheerabbas at merali dot org>
+
+ * testsuite/multifilesink/Makefile.am:
+ fix typo
+
+2004-09-22 Julien MOUTTE <julien@moutte.net>
+
+ * sys/ximage/ximagesink.c: (gst_ximagesink_ximage_destroy):
+ * sys/xvimage/xvimagesink.c: (gst_xvimagesink_check_xshm_calls): Fix
+ mistakes from thaytan's patches.
+
+2004-09-23 Jan Schmidt <thaytan@mad.scientist.com>
+
+ * sys/ximage/ximagesink.c: (gst_ximagesink_ximage_destroy):
+ For completeness, XSync in the destroy function as xvimage does.
+
+2004-09-23 Jan Schmidt <thaytan@mad.scientist.com>
+
+ * ext/gdk_pixbuf/pixbufscale.c: (gst_pixbufscale_getcaps):
+ Correct caps negotiation
+ * gst/volume/gstvolume.c: (volume_chain_float),
+ (volume_chain_int16):
+ Modify debug output to be little more informative
+ * sys/ximage/ximagesink.c: (gst_ximagesink_check_xshm_calls):
+ * sys/xvimage/xvimagesink.c: (gst_xvimagesink_check_xshm_calls),
+ (gst_xvimagesink_xvimage_destroy):
+ Add XSync calls after detaching from the shared memory segment to
+ avoid a crash.
+
+2004-09-22 Zaheer Abbas Merali <zaheerabbas at merali dot org>
+
+ * ext/ogg/gstoggmux.c: (gst_ogg_mux_init),
+ (gst_ogg_mux_next_buffer), (gst_ogg_mux_loop):
+ * ext/vorbis/vorbis.c: (plugin_init):
+ * ext/vorbis/vorbisenc.c: (gst_vorbisenc_init),
+ (gst_vorbisenc_chain):
+ * ext/vorbis/vorbisenc.h:
+ remove explicit newmedia support from oggmux and vorbisenc
+ add debug category to vorbisenc
+ * gst/multifilesink/gstmultifilesink.c:
+ (gst_multifilesink_class_init), (gst_multifilesink_init),
+ (gst_multifilesink_dispose), (gst_multifilesink_set_location),
+ (gst_multifilesink_set_property), (gst_multifilesink_next_file),
+ (gst_multifilesink_handle_event), (gst_multifilesink_chain),
+ (plugin_init):
+ * gst/multifilesink/gstmultifilesink.h:
+ add support for streamheader in multifilesink
+
+2004-09-22 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * gst/asfdemux/gstasfdemux.c: (_read_var_length), (_read_guid),
+ (gst_asf_demux_process_segment), (gst_asf_demux_handle_data),
+ (gst_asf_demux_process_chunk), (gst_asf_demux_handle_sink_event):
+ Prevent infinite loops. More correct error reporting.
+ * gst/auparse/gstauparse.c: (gst_auparse_chain):
+ Error out if negotiation fails.
+ * gst/playback/gstplaybasebin.c: (setup_source),
+ (gst_play_base_bin_change_state), (gst_play_base_bin_error),
+ (gst_play_base_bin_found_tag):
+ Error/tag forwarding. Pre-roll fixes for source errors on state
+ changes (e.g. "file does not exist") to prevent hangs.
+
+2004-09-21 Zaheer Abbas Merali <zaheerabbas at merali dot org>
+
+ * testsuite/multifilesink/Makefile.am:
+ * testsuite/multifilesink/lame_test.c: (gst_newmedia_base_init),
+ (gst_newmedia_class_init), (gst_newmedia_init),
+ (gst_newmedia_chain), (gst_newmedia_trigger), (test_format),
+ (newfile_signal), (test_signal), (main):
+ * testsuite/multifilesink/multifilesrc_test.c: (main):
+ * testsuite/multifilesink/oggtheora_test.c:
+ (gst_newmedia_base_init), (gst_newmedia_class_init),
+ (gst_newmedia_init), (gst_newmedia_chain), (gst_newmedia_trigger),
+ (test_format), (newfile_signal), (test_signal), (main):
+ * testsuite/multifilesink/oggvorbis_test.c:
+ (gst_newmedia_base_init), (gst_newmedia_class_init),
+ (gst_newmedia_init), (gst_newmedia_chain), (gst_newmedia_trigger),
+ (test_format), (newfile_signal), (test_signal), (main):
+ * testsuite/multifilesink/wavenc_test.c: (gst_newmedia_base_init),
+ (gst_newmedia_class_init), (gst_newmedia_init),
+ (gst_newmedia_chain), (gst_newmedia_trigger), (test_format),
+ (newfile_signal), (test_signal), (main):
+ New media tests
+
+2004-09-20 Christian Schaller <christian@fluendo.com>
+
+ * Fix mixmod license to LGPL as they have relicensed
+ * Move Dirac and Effectv into LGPL section of README_license
+
+2004-09-20 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+
+ * ext/mad/gstmad.c: (gst_mad_check_caps_reset),
+ (gst_mad_change_state):
+ Allow for mp3 rate/channels changes. However, only very
+ conservatively. Reason that we *have* to enable this is smiply
+ because the mad find_sync() function is not good enough, it will
+ regularly sync on random data as valid frames and therefore make
+ us provide random caps as *final* caps of the stream. The best fix
+ I could think of is to simply require several of the same stream
+ changes in a row before we change caps.
+ The actual testcase that works now is #
+ * ext/ogg/Makefile.am:
+ * ext/ogg/gstogg.c: (plugin_init):
+ * ext/ogg/gstogmparse.c:
+ OGM support (video only for now; I need an audio sample file).
+ * gst/asfdemux/gstasfdemux.c: (gst_asf_demux_base_init),
+ (gst_asf_demux_process_stream), (gst_asf_demux_video_caps),
+ (gst_asf_demux_add_video_stream):
+ WMV extradata.
+ * gst/playback/gstplaybasebin.c: (unknown_type):
+ Don't error out on single unknown-types after all. It's wrong.
+ If we found type of video and audio but not of a subtitle stream,
+ it will still error out (which is unwanted). Will find a better fix
+ later on.
+ * gst/typefind/gsttypefindfunctions.c: (ogmvideo_type_find),
+ (ogmaudio_type_find), (plugin_init):
+ OGM support.
+
+2004-09-20 Johan Dahlin <johan@gnome.org>
+
+ * ext/jpeg/gstjpegdec.c (gst_jpegdec_chain): Allocate the buffer
+ after setting caps.
+
+2004-09-19 Zaheer Abbas Merali <zaheerabbas at merali dot org>
+
+ * gst/wavenc/gstwavenc.c: (gst_wavenc_init), (gst_wavenc_chain):
+ * gst/wavenc/gstwavenc.h:
+ Added newmedia support to wavenc
+
+2004-09-17 Wim Taymans <wim@fluendo.com>
+
+ * gst/tcp/gstfdset.c: (gst_fdset_fd_has_closed),
+ (gst_fdset_fd_has_error), (gst_fdset_fd_can_read),
+ (gst_fdset_fd_can_write), (gst_fdset_wait):
+ * gst/tcp/gstmultifdsink.c: (gst_client_status_get_type),
+ (gst_multifdsink_init), (gst_multifdsink_add),
+ (gst_multifdsink_remove), (gst_multifdsink_get_stats),
+ (gst_multifdsink_remove_client_link),
+ (gst_multifdsink_client_queue_buffer),
+ (gst_multifdsink_handle_client_write),
+ (gst_multifdsink_recover_client), (gst_multifdsink_handle_clients),
+ (gst_multifdsink_close), (gst_multifdsink_change_state):
+ * gst/tcp/gstmultifdsink.h:
+ * gst/tcp/gsttcpserversink.c: (gst_tcpserversink_class_init),
+ (gst_tcpserversink_removed):
+ Small cleanups in fdset.c
+ Use a hastable to map fd to the client structure for faster
+ lookup in _remove and get_stats.
+ Added virtual function to close the fds.
+ Handle clients even when the select/poll call was unblocked because
+ of a command.
+ Implement syncing to keyframe in the recovery procedure.
+
2004-09-16 Iain <iaingnome@gmail.com>
* gst/audioconvert/gstaudioconvert.c (_fixate_caps_to_int): Free the
Create cues for audio only files.
2004-08-31 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
+>>>>>>> 1.1090
* ext/alsa/gstalsamixer.c: (gst_alsa_mixer_build_list):
* ext/alsa/gstalsamixertrack.c: (gst_alsa_mixer_track_new):
* testsuite/alsa/srcstate.c:
add test for alsasrc changing state
->>>>>>> 1.958
2004-07-27 Zaheer Abbas Merali <zaheerabbas at merali dot org>
* gst/silence/gstsilence.c: (gst_silence_init), (gst_silence_link),