index 13c94f8ad5800d5406f1a3e495f4574bba755343..d7f935e6c4e743dd8900616a9ccfa7bb430dc45d 100644 (file)
--- a/NEWS
+++ b/NEWS
-This is GStreamer Ugly Plug-insĀ 0.10.15 "Englishman in a Baseball Cap"
+This is GStreamer Ugly Plug-insĀ 0.10.16 "Because He Knows the Time is Short"
+
+Changes since 0.10.15:
+
+ * refactor x264enc to use current x264 API correctly, add new properties and new defaults
+ * liboil is no longer required, but orc is now required
+ * build: require orc >= 0.4.5, GLib >= 2.20, automake >= 1.10, autoconf >= 2.60; liboil is no longer required
+ * asfdemux: fix playback of files or streams that are shorter than the advertised preroll value
+ * asfdemux: fix sending eos event for chained asfs in pull mode (exotic)
+ * asfdemux: fix playback of files or streams that advertise miniscule preroll values
+ * lamemp3enc: implement latency query
+ * rmdemux: fix playback of sipro audio streams
+ * x264enc: refactor code in preparation for presets/tunings
+ * x264enc: add "profile" property (and default to MAIN profile)
+ * x264enc: improve defaults: medium speed/quality preset; auto mode for threads
+ * x264enc: add "speed-preset", "tune" and "psy-tune" properties
+ * x264enc: add "option-string" property to specify advanced parameters
+ * x264enc: set time base if needed, fixes visual artifacts
+ * x264enc: add "sliced-threads", "sync-lookahead", "intra-refresh", "mb-tree", and "rc-lookahead" properties
+ * x264enc: fix compilation against ancient x264 versions (X264_BUILD <= 75)
+ * x264enc: speed up first pass of multi-pass encoding (has no impact on quality)
+ * x264enc: fix flushing of delayed frames with new default settings
+
+Bugs fixed since 0.10.15:
+
+ * 599718 : [asf] support chained asfs
+ * 600412 : [asfdemux] Wrong handling of downstream GstFlowReturn
+ * 607798 : x264enc needs updating to support new features and use x264 correctly
+ * 618896 : lamemp3enc doesn't implement latency query
+ * 620007 : Gibberish sound when playing a certain RealMedia file of Sipro/ACELP.net audio codec
+ * 620344 : Update gst-plugins-ugly docs on website
+ * 622407 : [asfdemux] doesn't detect some streams if preroll value is very small
+ * 624786 : x264enc time base is wrong
+ * 625557 : x264enc doesn't flush delayed frames properly
+ * 626577 : [x264enc] regression: doesn't work with older versions of x264
+ * 627946 : mp3parse misuses GST_FLOW_IS_FATAL, doesn't forward GST_FLOW_UNEXPECTED upstream
Changes since 0.10.14: