index ca4540fb640ca5aac17688c22782245cdf5dd7c7..795efaabb07ee71f623aa07ee57c9b9180dbde47 100644 (file)
--- a/NEWS
+++ b/NEWS
-This is GStreamer Ugly Plug-insĀ 0.10.5 "She said"
+This is GStreamer Ugly Plug-insĀ 0.10.18 "Extra Life"
+
+Changes since 0.10.17:
+
+ * amrwbdec: avoid stalling on invalid frame
+ * asfpacket: don't rely on data from duration extension
+ * dvdsubdec: Implement clipping if the video size is smaller than the subpicture size
+ * dvdsubdec: Output only a single buffer per subpicture and set the correct duration
+ * lamemp3enc: implement sinkpad get_caps() function to proxy rate and channels restrictions from downstream
+ * mad: build the mad plugin even if libid3tag is not available
+ * mpeg2dec: do not fail fatally when downstream is unlinked (let upstream handle that)
+ * mpeg2dec: don't deadlock when setting an index
+ * mpegstream: increase allowable gap between streams
+ * x264enc: allow changing the bitrate and quantitizers dynamically
+ * x264enc: don't register flags with a value of 0
+ * x264enc: implement getcaps function to proxy downstream caps restrictions upstream
+ * x264enc: make tag event writable before modifying tag list in place
+ * x264enc: set max bitrate in quality mode
+
+Bugs fixed since 0.10.17:
+
+ * 539708 : [mpegstream] Increase allowable gap between streams
+ * 607698 : asfdemux: fix parsing of packets with padding
+ * 619136 : [dvdsubdec] spits out buffers at video framerate
+ * 621663 : x264enc: support changing bitrate property on the fly
+ * 639291 : [xingmux] Return NULL instead of 0 for a function returning gboolean
+ * 639715 : amrparse: seek error with EOS
+ * 640272 : x264enc: make tag event writable before modifying tag list in place
+ * 641151 : lame: doesn't negotiate sample rate properly
+ * 642360 : x264enc: Don't register flags which have 0 as a value
+ * 644704 : [dvdsubedc] no SPU clipping implemented
+ * 647709 : mpeg2dec: errors out on not-linked flow return
+
+Changes since 0.10.16:
+
+ * asfdemux: Handle new type of DRM'd asf files
+ * dvdreadsrc: fix handling of multi-angle streams
+ * dvdreadsrc: improve error messages on read errors
+ * mad: if gst_pad_alloc_buffer() returns a buffer with the wrong size allocate a new one
+ * mad: support reverse playback
+ * mpeg2dec: convert the position to stream time before answering to a position query
+ * mpeg2dec: fix position query by trusting upstream
+ * mpeg2dec: refactor cropping code to use libgstvideo functions
+ * mpeg2dec: use gst_pad_alloc_buffer() when cropping buffers
+ * mpegparse: re-fix flow return handling
+ * rmdemux: set GST_BUFFER_FLAG_DELTA_UNIT properly
+ * x264enc: add a note to the docs about encoder latency and queues
+ * x264enc: also accept YV12 input
+ * x264enc: Handle codec/encoder tags
+ * x264enc: Work around a rate control issue in libx264
+ * x264: use pkg-config to locate libx264
+ * x264: vbv-buf-capacity should have a minimum of 0
+ * xingmux: Don't ignore WRONG_STATE and NOT_LINKED when pushing data downstream
+
+Bugs fixed since 0.10.16:
+
+ * 539254 : [dvdreadsrc] DVDs with multiple angles switch angles during read
+ * 571146 : mpeg2dec: possibly uses wrong strides for 4:2:2 and 4:4:4 YUV with unusual display width or height
+ * 599515 : Fix dvb for DVB API 3.3
+ * 621465 : [x264enc] Video codec information copied incorrectly to output
+ * 632549 : [mpeg2dec] answers to position queries are wrong for DVDs
+ * 632861 : [x264enc] really bad quality with tune=zerolatency
+ * 634840 : x264: use pkg-config to locate dependencies for plugin
+ * 635291 : x264enc: " vbv-buf-capacity " property should have minimum value of 0
+ * 635461 : Crash in mad decoder when changing number of audio output channels in Totem while media is running
+ * 636107 : x264enc: docs should indicate specifics of using with queues
+ * 637093 : rmdemux: set GST_BUFFER_FLAG_DELTA_UNIT properly
+ * 637932 : realmedia: do not use the pad buffer allocation functions in demuxers
+ * 639226 : [asfdemux] Doesn't handle new PlayReady DRM files
+
+Changes since 0.10.15:
+
+ * refactor x264enc to use current x264 API correctly, add new properties and new defaults
+ * liboil is no longer required, but orc is now required
+ * build: require orc >= 0.4.5, GLib >= 2.20, automake >= 1.10, autoconf >= 2.60; liboil is no longer required
+ * asfdemux: fix playback of files or streams that are shorter than the advertised preroll value
+ * asfdemux: fix sending eos event for chained asfs in pull mode (exotic)
+ * asfdemux: fix playback of files or streams that advertise miniscule preroll values
+ * lamemp3enc: implement latency query
+ * rmdemux: fix playback of sipro audio streams
+ * x264enc: refactor code in preparation for presets/tunings
+ * x264enc: add "profile" property (and default to MAIN profile)
+ * x264enc: improve defaults: medium speed/quality preset; auto mode for threads
+ * x264enc: add "speed-preset", "tune" and "psy-tune" properties
+ * x264enc: add "option-string" property to specify advanced parameters
+ * x264enc: set time base if needed, fixes visual artifacts
+ * x264enc: add "sliced-threads", "sync-lookahead", "intra-refresh", "mb-tree", and "rc-lookahead" properties
+ * x264enc: fix compilation against ancient x264 versions (X264_BUILD <= 75)
+ * x264enc: speed up first pass of multi-pass encoding (has no impact on quality)
+ * x264enc: fix flushing of delayed frames with new default settings
+
+Bugs fixed since 0.10.15:
+
+ * 599718 : [asf] support chained asfs
+ * 600412 : [asfdemux] Wrong handling of downstream GstFlowReturn
+ * 607798 : x264enc needs updating to support new features and use x264 correctly
+ * 618896 : lamemp3enc doesn't implement latency query
+ * 620007 : Gibberish sound when playing a certain RealMedia file of Sipro/ACELP.net audio codec
+ * 620344 : Update gst-plugins-ugly docs on website
+ * 622407 : [asfdemux] doesn't detect some streams if preroll value is very small
+ * 624786 : x264enc time base is wrong
+ * 625557 : x264enc doesn't flush delayed frames properly
+ * 626577 : [x264enc] regression: doesn't work with older versions of x264
+ * 627946 : mp3parse misuses GST_FLOW_IS_FATAL, doesn't forward GST_FLOW_UNEXPECTED upstream
+
+Changes since 0.10.14:
+
+ * amrnbenc: give element a rank (SECONDARY) so it's autoplugged
+ * rmdemux: descramble sipro audio before pushing out
+ * x264enc: fix up codec_data / avcC header construction some more
+ * x264enc: Put pixel-aspect-ratio from input into the src pad caps
+
+Bugs fixed since 0.10.14:
+
+ * 612995 : x264enc: pixel-aspect-ratio does not appear in src pad caps
+ * 613815 : A call in gst/realmedia/rmutils.c discards qualifiers from pointer target type
+ * 615410 : x264 orders NALs differently than x264enc expects
+ * 617078 : Wrong include paths in amr elements
+ * 619776 : [x264enc] is unable to do Baseline with recent x264
+ * 618098 : [rmdemux] Add descrambling for Sipro codec
+
+Changes since 0.10.13:
+
+ * amrwbdec: give decoder a rank so decodebin/playbin will use it
+ * asfdemux: fix flow aggregation
+ * asfdemux: try harder to put sane timestamps and durations on buffers
+ * asfdemux: accept fragments in a continued packet where the subsequent fragments declare a size of 0
+ * asfdemux: improve seek behaviour for audio-only files without an index
+ * asfdemux: careful to avoid crash on bogus data; avoid strlen() on NULL pointers
+ * asfdemux: add support for chained asfs (push mode)
+ * asfdemux: map WM/TrackNumber to GST_TAG_TRACK_NUMBER and prefer over WM/Track
+ * asfdemux: post bitrate tags
+ * mp3parse: seeking fixes: fix non-flushing seek, conserve stop time for non-accurate seek
+ * rtspreal: memory leak fixes; make config header construction valgrind clean
+ * rmdemux: fix AC-3 in RealAudio playback; post bitrate tags
+ * x264enc: fix up avcC header construction and playback by flash players
+ * x264enc: Make upstream GstForceKeyUnit thread-safe
+ * x264enc: make use of Access Unit delimiters configurable
+ * x264enc: adapt to slightly modified x264 API
+ * xingmux: fix unaligned memory access, makes things work better on ARM/SPARC
+
+Bugs fixes since 0.10.13:
+
+ * 606662 : h264: add stream-format to output caps
+ * 563276 : Internal GStreamer error: negotiation problem - after opening avi file
+ * 586464 : [xingmux] Unit test failures on sparc and arm/eabi
+ * 598761 : [mpegaudioparse] Reduce processing time by 2
+ * 599095 : x264enc: Adapt to slightly modified x264 API
+ * 599297 : [asfdemux] Doesn't populate video bitrate field
+ * 599299 : [rmdemux] Doesn't populate video bitrate field
+ * 599333 : Segfault with asfdemuxer
+ * 599676 : RealAudio file with AC-3 audio no longer plays
+ * 600037 : [asfdemux] ASF MPEG4 Part 2 file captured from Linksys WVC200 Camera corrupted/fails
+ * 601419 : x264enc crashes
+ * 602280 : [asfdemux] fix segmentation fault when utf8 tag name is null
+ * 602556 : x264enc and ffenc upstream GstForceKeyUnit handling are not thread-safe
+ * 603695 : Innaccurate seeking in MP3 files results in cut off playback
+ * 608564 : [ffdec_cook] memory leak
+ * 610432 : [asfdemux] handle negative payload timestamps
+ * 611473 : [regression] outgoing buffers with a duration of zero
+ * 608533 : [real] memory leak in real audio stream via rtsp
+ * 610089 : Flash players are unable to show x264 encoded streams
+
+Changes since 0.10.12:
+
+ * Improve A52 decoder
+ * Add AMR-WB decoder and AMR-NB decoder/encoder based on OpenCore codecs
+ * ASF playback improvements
+ * Improve mp3 parser and seeking
+
+Bugs fixed since 0.10.12:
+
+ * 519721 : [asfdemux] wma tags are not copied when converting to another format
+ * 584890 : AMR plugins based on Opencore codecs
+ * 585956 : [mp3parse] indexing improvements
+ * 590432 : It's only possible to build the mad plugin when building id3tag as well
+ * 591348 : AMR plugins should check for opencore-amr .pc files
+ * 592787 : a52dec: Allow liba52 to use djbfft based IMDCT transform
+ * 596517 : x264 element no longer compiles against changed upstream API
+ * 598272 : a52dec leaks input buffers
+ * 598370 : Properly detect pre-releases
+
+Changes since 0.10.11:
+
+ * Real and WMS RTSP improvements
+ * Other cleanups and bug fixes
+ * Improve ASF file handling
+ * Large MPEG video file support
+ * Interlacing support for MPEG video
+ * New 'lamemp3dec' mp3 encoder element
+ * x264enc moved from -bad
+ * Remove id3mux in favour of the new id3tag element in -bad
+
+Bugs fixed since 0.10.11:
+
+ * 401173 : [asfdemux] Stream doesn't play, stuck on first frame
+ * 494528 : Simplifications of the LAME plugin
+ * 574461 : [mpeg2dec] Lower rank and make ffdec_mpeg2video PRIMARY
+ * 576305 : twolame plugin does not detet proper version
+ * 579058 : [asfdemux] proper handling of RTSP input
+ * 580803 : [PLUGIN-MOVE] Move x264enc to -ugly
+ * 580869 : dvdsubdec ARGB support
+ * 581341 : [lamemp3enc] doesn't build with LAME 3.97: implicit decla...
+ * 581756 : [id3mux] replace with something more reliable
+ * 582056 : [asfdemux] forcing an EOS on the pipeline doesn't work wi...
+ * 582375 : mpeg2dec not building in gst-plugins-ugly
+ * 583112 : [asfdemux] extract coverart (WM/Picture tag)
+ * 573720 : [mp3parse] Memory leak when playing shoutcast streams
+ * 581464 : xing data is being ignored
+ * 578524 : synaesthesia MSVC compatibility
+
+Changes since 0.10.10:
+
+ * Migrate twolame element from -bad
+ * mp3parse improvements
+ * Support scaling in the synaesthsia visualisation
+ * Improve realmedia streaming, supporting RDT and pnm://
+ * Improved ASF demuxing, including streaming-mode seeking
+ * Support for 4:4:4 MPEG-2 video
+
+Bugs fixed since 0.10.10:
+
+ * 571146 : [mpeg2dec] Probably uses wrong strides for 4:2:2 and 4:4:...
+ * 574461 : [mpeg2dec] Lower rank and make ffdec_mpeg2video PRIMARY
+ * 454228 : [mpegdemux] problem with mark shuttleworth clip
+ * 522699 : pnm:/something.ra streams can't be loaded in Totem from a...
+ * 527112 : [real] Can't play several real audio streams
+ * 556714 : Real Audio streams not working properly
+ * 560348 : plus7.arte.tv plays slooooowly
+ * 562065 : mpeg2dec does not handle STATE_SEQUENCE_MODIFIED from > =l...
+ * 562086 : mpeg2 stream crashes something in gstreamer
+ * 564885 : [mpegstream] memory leak
+ * 568836 : [asfdemux] add seeking support when operating in push mode
+ * 569317 : [PLUGIN-MOVE] Move twolame plugin from -bad to -ugly
+ * 575068 : [mp3parse] deadlock with accurate seeking
+ * 335067 : Need RTP ASF depayloader
+ * 571358 : [real] file playing stops immediately
+
+Changes since 0.10.9:
+
+ * asfdemux and rmdemux fixes
+ * RDT support
+ * AMR-NB parser improvements
+ * Fix a52dec channel output negotiation
+ * Compilation fixes for mad, mpeg2dec
+
+Bugs fixed since 0.10.9:
+
+ * 546859 : Asfdemux doesn't properly error out on not-linked
+ * 536274 : handle flush seeking in amrnbparse
+ * 554142 : mad plugin with disable index seeking issue
+ * 554150 : mpeg2dec plugin with disable index seeking issue
+ * 556184 : [PATCH] mpeg2dec: prefer container's pixel aspect ratio o...
+ * 556277 : mp3parse generate discontinuities.
+ * 558277 : generic states test fails
+ * 559569 : GStreamer mp3 consistent and regular stuttering
+ * 559682 : negotiation problem
+ * 561161 : [sidplay] Uses GST_CFLAGS for C++
+ * 424070 : [amrnbdec] add IF2 handling
+ * 536226 : fix query duration
+ * 558896 : DVD playing on Vista using dvddemux element seg-faults on...
+
+Changes since 0.10.8:
+
+ * Improvements in a52 and mp3 decoding
+ * Bug fixes in Xing header muxer
+ * MPEG demuxer improvements and dvdreadsrc bug-fixes
+ * Fix build with LAME 3.97 and above
+ * Fix LAME parameter settings to allow setting the bitrate properly
+
+Bugs fixed since 0.10.8:
+
+ * 476149 : Fix and add needed features to dvdnavsrc
+ * 490372 : Variable bit rates are limited to 160 kbps in higher qual...
+ * 498004 : preset is ignored by lame plugin
+ * 540194 : [mpegdemux] Doesn't handle files with a non-zero start ti...
+ * 542646 : gstreamer endless loop by zzuf sample
+ * 544039 : [lame] Doesn't build with 3.97
+ * 545370 : playing some mp3s segfaults
+ * 546859 : Asfdemux doesn't properly error out on not-linked
+ * 548194 : a52dec doesn't set up segment for raw files correctly.
+ * 537235 : [mp3parse] some mp3 files do not play with gstreamer
+
+Changes since 0.10.7:
+
+ * ASF demuxer fixes
+ * MP3 parsing and Xing header output bug-fixes
+ * Real streaming and demuxing improvements
+
+Bugs fixed since 0.10.7:
+
+ * 527572 : Crash in volume_process_int32
+ * 321857 : [mp3parse] needs to post DURATION message for VBR mp3s
+ * 428021 : [mad, mp3parse] better duration estimates for VBR
+ * 517985 : [lame] compile error on Solaris, broken GST_ELEMENT_ERROR...
+ * 518676 : xingmux doesn't work anymore
+ * 518933 : mp3 tags are not copied when converting to another format
+ * 521459 : RTSP extension for Real Audio doesn't extract Author, Co...
+ * 524346 : Framerate not being displayed correctly on running gst-di...
+ * 529488 : [sidplay] Missing sentinel in function call
+ * 532807 : [rmdemux] Doesn't properly aggregate flow returns
+ * 533581 : [mad] inconsistent use of rate and channels
+ * 533832 : [rmdemux] reset variables on flush
+
+Changes since 0.10.6:
+
+ * Many bug fixes and improvements
+ * Accurate seeking support in mp3
+ * xingmux moved from -bad
+ * RealMedia and WMS RTSP support
+ * LAME mp3 encoder fixes
+ * Support non-square pixels in ASF
+ * rmdemux fixes
+ * amrnb fixes
+ * dvdreadsrc seeking fix
+ * Initial MPEG-2 reverse playback support
+ * New element: dvdsubdec
+
+Bugs fixed since 0.10.6:
+
+ * 358891 : [dvdreadsrc] aborts due to src- > cur_pack == dsi_pack.dsi_...
+ * 337681 : Seeking problem with MP3s in banshee and rhythmbox
+ * 414988 : Stream encoded by lame has gap after decoding
+ * 427309 : [rmdemux] trouble playing RV10 video
+ * 439390 : [lame] fix up so we can control sample rate conversion
+ * 450879 : Missing files in po/POTFILES.in
+ * 452025 : ./configure breaks when cross-compiling LAME
+ * 454311 : missing xml/{element-synaesthesia-details.xml,plugin-syna...
+ * 466442 : amrnbenc has not properties to add header and select band...
+ * 495885 : [mpegdemux] unknown stream id 0xbe
+ * 500467 : [rmdemux] totem crashed with SIGSEGV
+ * 500808 : gstmpeg2dec compile problem in MSVC 6.0
+ * 507821 : Skip over broken seektable in Xing headers
+ * 511497 : [PLUGIN-MOVE] Move xingheader to gst-plugins-ugly
+ * 514297 : mpeg2dec with corrupted packets causes fps denominator so...
+ * 515575 : [lame] unit test shows memory leak
+ * 515708 : [dvdsubparse] Leaks a pad template
+ * 515725 : [xingmux] Fails on big endian systems
+ * 516278 : [dvdreadsrc] FORMAT_BYTES based seek stopped working sinc...
+ * 516811 : [mp3parse] immediate EOS when playing back AVIs
+ * 516989 : [dvdreadsrc] wrong (negative) stream position returned du...
+ * 308312 : Make mp3parse plugin implement GST_SEEK_FLAG_ACCURATE
+ * 508595 : [lame] wrong output caps in mono encoding mode
+ * 140136 : [mpeg] plays choppy in gst-player/totem
+ * 448782 : add finalize() to amrnbdec element
+ * 491305 : [playbin?] intro-leopard.mov sometimes EOSes immediately,...
+ * 504671 : [rtspsrc] spews warnings on setup and shutdown
+
+Changes since 0.10.5:
+
+ * fixes in handling of MPEG streams, Real streams and MP3
+ * AMR-NB fixes
+ * Other bug-fixes and improvements
+
+Bugs fixed since 0.10.5:
+
+ * 336370 : [asfdemux] crashes on an assertion in gst_asf_demux_get_v...
+ * 332157 : [asfdemux] This WMV file is played very strangely
+ * 335760 : [asfdemux] dataflow error when seeking in zeldadslarge.wmv
+ * 349779 : [real] can't play ancient RealAudio 1.0/2.0 format files
+ * 353116 : [asfdemux] hangs playing some mms stations
+ * 365288 : [asfdemux] seeking not very smooth
+ * 370020 : [mpeg2dec] continue even after 5 consecutive decoding errors
+ * 385292 : [rmdemux] stream index leaked on shutdown
+ * 385311 : Memory leak initializing lame mp3 encoder plugin (gstlame.c)
+ * 385651 : [asfdemux] Jerky playback of " I love sky "
+ * 393890 : [win32] autogenerated win32/common/config.h needed
+ * 397219 : [rmdemux] captured realaudio stream with non-zero start p...
+ * 403188 : [asfdemux] bug parsing certain stream header object
+ * 421594 : [real] doesn't compile if zlib includes are missing
+ * 425374 : [asfdemux] seek in WMV rarely works
+ * 428698 : [rmdemux] crashes on files with many logical streams
+ * 429960 : [mpegdemux] playbin hangs with small external vobsub subt...
+ * 431707 : [amrnbparse] make pipeline hang
+ * 432533 : [mad, mp3parse] regression: CVS version doesn't parse dur...
+ * 438610 : [dvddemux] fails after flushing seek
+ * 440120 : [mpegdemux] crashes in gst_mpeg_demux_send_subbuffer() wi...
+ * 442706 : [dvdsubdec] crashes when flushing/on seek
+ * 444514 : [PATCH] dvdsubdec miscalculates (long) subtitle durations
+ * 386218 : [asfdemux] Division by zero when seeking live streams
Changes since 0.10.4: