index 1bd0d623fc81d3121724d27092437fd1f41f52be..322a56abef07fdeb573da19a4dbce658deab809f 100644 (file)
--- a/README
+++ b/README
WHAT IT IS
----------
WHAT IT IS
----------
-This is gst-plugins, a set of plug-ins for GStreamer.
+This is GStreamer Ugly Plug-ins.
+
+This package is in the 0.9.x series. This means that this is a
+development series leading up to a stable 0.10.x series.
+You have been warned.
+
+GStreamer 0.9 development series - Hung by a Thread
+---------------------------------------------------
+
+Starring
+
+ GSTREAMER
+
+The core around which all other modules revolve. Base functionality and
+libraries, some essential elements, documentation, and testing.
+
+ BASE
+
+A well-groomed and well-maintained collection of GStreamer plug-ins and
+elements, spanning the range of possible types of elements one would want
+to write for GStreamer.
+
+And introducing, for the first time ever, on the development screen ...
+
+ THE GOOD
+
+ --- "Such ingratitude. After all the times I've saved your life."
+
+A collection of plug-ins you'd want to have right next to you on the
+battlefield. Shooting sharp and making no mistakes, these plug-ins have it
+all: good looks, good code, and good licensing. Documented and dressed up
+in tests. If you're looking for a role model to base your own plug-in on,
+here it is.
+
+If you find a plot hole or a badly lip-synced line of code in them,
+let us know - it is a matter of honour for us to ensure Blondie doesn't look
+like he's been walking 100 miles through the desert without water.
+
+ THE UGLY
+
+ --- "When you have to shoot, shoot. Don't talk."
+
+There are times when the world needs a color between black and white.
+Quality code to match the good's, but two-timing, backstabbing and ready to
+sell your freedom down the river. These plug-ins might have a patent noose
+around their neck, or a lock-up license, or any other problem that makes you
+think twice about shipping them.
+
+We don't call them ugly because we like them less. Does a mother love her
+son less because he's not as pretty as the other ones ? No - she commends
+him on his great personality. These plug-ins are the life of the party.
+And we'll still step in and set them straight if you report any unacceptable
+behaviour - because there are two kinds of people in the world, my friend:
+those with a rope around their neck and the people who do the cutting.
+
+ THE BAD
+
+ --- "That an accusation?"
+
+No perfectly groomed moustache or any amount of fine clothing is going to
+cover up the truth - these plug-ins are Bad with a capital B.
+They look fine on the outside, and might even appear to get the job done, but
+at the end of the day they're a black sheep. Without a golden-haired angel
+to watch over them, they'll probably land in an unmarked grave at the final
+showdown.
+
+Don't bug us about their quality - exercise your Free Software rights,
+patch up the offender and send us the patch on the fastest steed you can
+steal from the Confederates. Because you see, in this world, there's two
+kinds of people, my friend: those with loaded guns and those who dig.
+You dig.
+
+The Lowdown
+-----------
+
+ --- "I've never seen so many plug-ins wasted so badly."
+
+GStreamer Plug-ins has grown so big that it's hard to separate the wheat from
+the chaff. Also, distributors have brought up issues about the legal status
+of some of the plug-ins we ship. To remedy this, we've divided the previous
+set of available plug-ins into four modules:
+
+- gst-plugins-base: a small and fixed set of plug-ins, covering a wide range
+ of possible types of elements; these are continuously kept up-to-date
+ with any core changes during the development series.
+
+ - We believe distributors can safely ship these plug-ins.
+ - People writing elements should base their code on these elements.
+ - These elements come with examples, documentation, and regression tests.
+
+- gst-plugins-good: a set of plug-ins that we consider to have good quality
+ code, correct functionality, our preferred license (LGPL for the plug-in
+ code, LGPL or LGPL-compatible for the supporting library).
+
+ - We believe distributors can safely ship these plug-ins.
+ - People writing elements should base their code on these elements.
+
+- gst-plugins-ugly: a set of plug-ins that have good quality and correct
+ functionality, but distributing them might pose problems. The license
+ on either the plug-ins or the supporting libraries might not be how we'd
+ like. The code might be widely known to present patent problems.
+
+ - Distributors should check if they want/can ship these plug-ins.
+ - People writing elements should base their code on these elements.
+
+- gst-plugins-bad: a set of plug-ins that aren't up to par compared to the
+ rest. They might be close to being good quality, but they're missing
+ something - be it a good code review, some documentation, a set of tests,
+ a real live maintainer, or some actual wide use.
+ If the blanks are filled in they might be upgraded to become part of
+ either gst-plugins-good or gst-plugins-ugly, depending on the other factors.
+
+ - If the plug-ins break, you can't complain - instead, you can fix the
+ problem and send us a patch, or bribe someone into fixing them for you.
+ - New contributors can start here for things to work on.
+
+INSTALLING FROM PACKAGES
+------------------------
+You should always prefer installing from packages first. GStreamer is
+well-maintained for a number of distributions, including Fedora, Debian,
+Ubuntu, Mandrake, Gentoo, ...
+
+Only in cases where you:
+- want to hack on GStreamer
+- want to verify that a bug has been fixed
+- do not have a sane distribution
+should you choose to build from source tarballs or CVS.
+
+Find more information about the various packages at
+http://gstreamer.freedesktop.org/download/
+
+COMPILING FROM SOURCE TARBALLS
+------------------------------
+- again, make sure that you really need to install from source !
+ If GStreamer is one of your first projects ever that you build from source,
+ consider taking on an easier project.
-COMPILING FROM SOURCE
----------------------
-- make sure you compiled and at least did a test-run of GStreamer (core)
- check output of ./configure --help to see if any options apply to you
- check output of ./configure --help to see if any options apply to you
-- configure the source tree:
- - if you installed GStreamer, then do:
- ./configure
- If configure complains about missing GStreamer, you should try the
- following command:
- $export PKG_CONFIG_PATH=prefix/lib/pkgconfig
- where prefix should be replaced by the prefix you used to configure
- GStreamer. (Be mindful NOT to ADD a trailing / to that option !).
- After that, rerun ./configure. If this doesn't fix it, you have other
- issues ;)
-
- - if you didn't install GStreamer, you can still compile the plug-ins.
- Add the path to gstreamer-uninstalled.pc (which lives in the gstreamer
- source tree) to PKG_CONFIG_PATH
- or run configure --with-pkg-config-path=(path to gstreamer uninstalled)
-
- - the output of configure will give you a list of plug-ins with external
- dependencies (ie, depending on other libs, see below). By no means
- should you try to get them all built on your first run. This is hard
- enough as it is ;) Resist the urge to get the most features for now.
- It doesn't list all of the non-depending plug-ins, which get built
- regardless (unless you explicitly asked it not to).
-
-- build the tree:
+- run
+ ./configure
make
make
- If any plug-in causes a problem at this stage, you should re-configure
- with --disable-(dependency)
- and doublecheck if configure reports this plug-in as being disabled.
- Then re-run make.
-
-- install:
- - if you installed GStreamer, and want to install the plug-ins as well, run
- make install
- and, as root, run
- gst-register
- - if you installed GStreamer, but don't want to install the plug-ins, run
- gst-register --gst-plugin-path=.
- - if you didn't install GStreamer, then do
- path/to/gstreamer/tools/gst-register --gst-plugin-path=.
- (Replace path/to/gstreamer obviously)
-
-- test:
- - run
- gst-launch sinesrc ! fakesink
- and prefix gst-launch with the path to gstreamer/tools if you didn't install
- GStreamer.
- If this doesn't give any errors, you can abort it.
-
- - try replacing fakesink with your choice of
- osssink/esdsink/artsdsink/alsasink/jacksink (depending on what output
- method you have available) and see if you hear a C tone.
-
-- After this, you should look into installing an application, like
- gst-player, gst-editor or monkey-media with rhythmbox.
+
+ to build GStreamer.
+- if you want to install it (not required), run
+ make install
+- You should create a registry for things to work.
+ If you ran make install in the previous step, run
+ gst-register
+ as root.
+
+ If you didn't install, run
+ tools/gst-register
+ as a normal user.
+
+- try out a simple test:
+ gst-launch fakesrc num_buffers=5 ! fakesink
+ (If you didn't install GStreamer, again prefix gst-launch with tools/)
+
+ If it outputs a bunch of messages from fakesrc and fakesink, everything is
+ ok.
+
+- After this, you're ready to install gst-plugins, which will provide the
+ functionality you're probably looking for by now, so go on and read
+ that README.
COMPILING FROM CVS
------------------
COMPILING FROM CVS
------------------
-When building from CVS sources, you will need to run autogen.sh to generate
+When building from CVS sources, you will need to run autogen.sh to generate
the build system files.
the build system files.
-GStreamer is cutting-edge stuff. To be a CVS developer, you need
-what used to be considered cutting-edge tools.
-
-ATM, most of us have at least these versions :
-
-* autoconf 2.52 (NOT 2.52d)
-* automake 1.5
-* gettext 0.11.5
-* libtool 1.4 (NOT Gentoo's genetic failure 1.4.2)
-* pkg-config 0.8.0
+You will need a set of additional tools typical for building from CVS,
+including:
+- autoconf
+- automake
+- libtool
-autogen.sh will check for these versions and complain if you don't have
+autogen.sh will check for recent enough versions and complain if you don't have
them. You can also specify specific versions of automake and autoconf with
--with-automake and --with-autoconf
them. You can also specify specific versions of automake and autoconf with
--with-automake and --with-autoconf
from autogen.sh with -- between the two.
prefix has been added to autogen.sh but will be passed on to configure because
some build scripts like that.
from autogen.sh with -- between the two.
prefix has been added to autogen.sh but will be passed on to configure because
some build scripts like that.
-You will probably have to pass at least --with-pkg-config-path to autogen.sh
-to point to the CVS version of GStreamer.
When you have done this once, you can use autoregen.sh to re-autogen with
the last passed options as a handy shortcut. Use it.
When you have done this once, you can use autoregen.sh to re-autogen with
the last passed options as a handy shortcut. Use it.
After the autogen.sh stage, you can follow the directions listed in
"COMPILING FROM SOURCE"
After the autogen.sh stage, you can follow the directions listed in
"COMPILING FROM SOURCE"
+You can also run your whole cvs stack uninstalled. The script in
+the gstreamer module /docs/faq/gst-uninstalled) is helpful in setting
+up your environment for this.
+
PLUG-IN DEPENDENCIES AND LICENSES
---------------------------------
PLUG-IN DEPENDENCIES AND LICENSES
---------------------------------
-GStreamer is developed under the terms of the LGPL (see LICENSE file for
-details). Some of our plug-ins however rely on libraries which are available
-under other licenses. This means that if you are using an application which
-has a non-GPL compatible license (for instance a closed-source application)
+GStreamer is developed under the terms of the LGPL (see LICENSE file for
+details). Some of our plug-ins however rely on libraries which are available
+under other licenses. This means that if you are using an application which
+has a non-GPL compatible license (for instance a closed-source application)
with GStreamer, you have to make sure not to use GPL-linked plug-ins.
with GStreamer, you have to make sure not to use GPL-linked plug-ins.
-When using GPL-linked plug-ins, GStreamer is for all practical reasons
-under the GPL itself.
-
-There is a LICESENSE_readme file containing licensing information on the plugins
+When using GPL-linked plug-ins, GStreamer is for all practical reasons
+under the GPL itself.
+
+HISTORY
+-------
+The fundamental design comes from the video pipeline at Oregon Graduate
+Institute, as well as some ideas from DirectMedia. It's based on plug-ins that
+will provide the various codec and other functionality. The interface
+hopefully is generic enough for various companies (ahem, Apple) to release
+binary codecs for Linux, until such time as they get a clue and release the
+source.