releasing 0.9.2
[glsdk/gst-plugins-ugly0-10.git] / RELEASE
diff --git a/RELEASE b/RELEASE
index e69de29bb2d1d6434b8b29ae775ad8c2e48c5391..7a2a7a12a284b9316c3b54055af3b491d0712de5 100644 (file)
--- a/RELEASE
+++ b/RELEASE
@@ -0,0 +1,103 @@
+
+GStreamer: Release notes for GStreamer Ugly Plug-ins 0.9.1 "The Rat"
+        
+
+The GStreamer team is petrified to announce a new release
+in the 0.9.x development series of the
+GStreamer Ugly Plug-ins.
+
+
+The 0.9.x series is a development series and not recommended for end users.
+It is not API or ABI compatible with the stable 0.8.x series.
+It is, however, parallel installable with the 0.8.x series.
+
+
+"When you have to shoot, shoot.  Don't talk."
+
+
+There are times when the world needs a color between black and white.
+Quality code to match the good's, but two-timing, backstabbing and ready to
+sell your freedom down the river.  These plug-ins might have a patent noose
+around their neck, or a lock-up license, or any other problem that makes you
+think twice about shipping them.
+
+
+We don't call them ugly because we like them less.  Does a mother love her
+son less because he's not as pretty as the other ones ? No  - she commends
+him on his great personality.  These plug-ins are the life of the party.
+And we'll still step in and set them straight if you report any unacceptable
+behaviour - because there are two kinds of people in the world, my friend:
+those with a rope around their neck and the people who do the cutting.
+
+
+This module contains a set of plug-ins that have good quality and correct
+functionality, but distributing them might pose problems.  The license
+on either the plug-ins or the supporting libraries might not be how we'd
+like. The code might be widely known to present patent problems.
+Distributors should check if they want/can ship these plug-ins.
+
+
+Other modules containing plug-ins are:
+
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+    rigorous quality testing we expect
+
+
+
+  
+Features of this release
+    
+      * Parallel installability with 0.8.x series
+      * Threadsafe design and API
+
+Bugs fixed in this release
+    
+
+Download
+
+You can find source releases of gst-plugins-ugly in the download directory:
+http://gstreamer.freedesktop.org/src/gst-plugins-ugly/
+
+GStreamer Homepage
+
+More details can be found on the project's website:
+http://gstreamer.freedesktop.org/
+
+Support and Bugs
+
+We use GNOME's bugzilla for bug reports and feature requests:
+http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
+
+Developers
+
+CVS is hosted on cvs.freedesktop.org.
+All code is in CVS and can be checked out from there.
+Interested developers of the core library, plug-ins, and applications should
+subscribe to the gstreamer-devel list. If there is sufficient interest we
+will create more lists as necessary.
+
+        
+Applications
+  
+Contributors to this release
+    
+      * Andy Wingo
+      * Christian Schaller
+      * David Schleef
+      * Edward Hervey
+      * Jan Schmidt
+      * Michael Smith
+      * Philippe Khalaf
+      * Ronald Bultje
+      * Stefan Kost
+      * Thomas Vander Stichele
+      * Tim-Philipp Müller
+      * Wim Taymans
+      * Zaheer Abbas Merali
\ No newline at end of file