index 092874ccc939400611d4fe37b57341e0b10fb830..a89531cb580ae0c560835285e0119d4a52f2d12e 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-Release notes for GStreamer Ugly Plug-ins 0.10.12 "Moving Along The Highway"
+Release notes for GStreamer Ugly Plug-ins 0.10.18 "Extra Life"
The GStreamer team is proud to announce a new release
Features of this release
- * Real and WMS RTSP improvements
- * Other cleanups and bug fixes
- * Improve ASF file handling
- * Large MPEG video file support
- * Interlacing support for MPEG video
- * New 'lamemp3dec' mp3 encoder element
- * x264enc moved from -bad
- * Remove id3mux in favour of the new id3tag element in -bad
+ * amrwbdec: avoid stalling on invalid frame
+ * asfpacket: don't rely on data from duration extension
+ * dvdsubdec: Implement clipping if the video size is smaller than the subpicture size
+ * dvdsubdec: Output only a single buffer per subpicture and set the correct duration
+ * lamemp3enc: implement sinkpad get_caps() function to proxy rate and channels restrictions from downstream
+ * mad: build the mad plugin even if libid3tag is not available
+ * mpeg2dec: do not fail fatally when downstream is unlinked (let upstream handle that)
+ * mpeg2dec: don't deadlock when setting an index
+ * mpegstream: increase allowable gap between streams
+ * x264enc: allow changing the bitrate and quantitizers dynamically
+ * x264enc: don't register flags with a value of 0
+ * x264enc: implement getcaps function to proxy downstream caps restrictions upstream
+ * x264enc: make tag event writable before modifying tag list in place
+ * x264enc: set max bitrate in quality mode
Bugs fixed in this release
- * 401173 : [asfdemux] Stream doesn't play, stuck on first frame
- * 494528 : Simplifications of the LAME plugin
- * 574461 : [mpeg2dec] Lower rank and make ffdec_mpeg2video PRIMARY
- * 576305 : twolame plugin does not detet proper version
- * 579058 : [asfdemux] proper handling of RTSP input
- * 580803 : [PLUGIN-MOVE] Move x264enc to -ugly
- * 580869 : dvdsubdec ARGB support
- * 581341 : [lamemp3enc] doesn't build with LAME 3.97: implicit decla...
- * 581756 : [id3mux] replace with something more reliable
- * 582056 : [asfdemux] forcing an EOS on the pipeline doesn't work wi...
- * 582375 : mpeg2dec not building in gst-plugins-ugly
- * 583112 : [asfdemux] extract coverart (WM/Picture tag)
- * 573720 : [mp3parse] Memory leak when playing shoutcast streams
- * 581464 : xing data is being ignored
- * 578524 : synaesthesia MSVC compatibility
+ * 539708 : [mpegstream] Increase allowable gap between streams
+ * 607698 : asfdemux: fix parsing of packets with padding
+ * 619136 : [dvdsubdec] spits out buffers at video framerate
+ * 621663 : x264enc: support changing bitrate property on the fly
+ * 639291 : [xingmux] Return NULL instead of 0 for a function returning gboolean
+ * 639715 : amrparse: seek error with EOS
+ * 640272 : x264enc: make tag event writable before modifying tag list in place
+ * 641151 : lame: doesn't negotiate sample rate properly
+ * 642360 : x264enc: Don't register flags which have 0 as a value
+ * 644704 : [dvdsubedc] no SPU clipping implemented
+ * 647709 : mpeg2dec: errors out on not-linked flow return
Download
Contributors to this release
- * Alessandro Decina
- * Christian Schaller
- * David Hoyt
- * David Schleef
+ * Brendan Le Foll
* Edward Hervey
- * Felipe Contreras
- * Jan Schmidt
- * Janin Kolenc
- * Josef Zlomek
- * Josep Torra
- * Kapil Agrawal
- * Marc-Andre Lureau
+ * Luis de Bethencourt
* Mark Nauwelaerts
- * Michael Smith
- * Michal Benes
+ * Miguel Angel Cabrera Moya
+ * Olivier Crête
* Sebastian Dröge
+ * Sjoerd Simons
* Stefan Kost
+ * Thibault Saunier
* Tim-Philipp Müller
- * Wim Taymans
+ * Vincent Penquerc'h
+ * Yang Xichuan
\ No newline at end of file