index 7a2a7a12a284b9316c3b54055af3b491d0712de5..a89531cb580ae0c560835285e0119d4a52f2d12e 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-GStreamer: Release notes for GStreamer Ugly Plug-ins 0.9.1 "The Rat"
+Release notes for GStreamer Ugly Plug-ins 0.10.18 "Extra Life"
-The GStreamer team is petrified to announce a new release
-in the 0.9.x development series of the
+The GStreamer team is proud to announce a new release
+in the 0.10.x stable series of the
GStreamer Ugly Plug-ins.
-The 0.9.x series is a development series and not recommended for end users.
+The 0.10.x series is a stable series targeted at end users.
It is not API or ABI compatible with the stable 0.8.x series.
It is, however, parallel installable with the 0.8.x series.
+
"When you have to shoot, shoot. Don't talk."
+
Features of this release
- * Parallel installability with 0.8.x series
- * Threadsafe design and API
+ * amrwbdec: avoid stalling on invalid frame
+ * asfpacket: don't rely on data from duration extension
+ * dvdsubdec: Implement clipping if the video size is smaller than the subpicture size
+ * dvdsubdec: Output only a single buffer per subpicture and set the correct duration
+ * lamemp3enc: implement sinkpad get_caps() function to proxy rate and channels restrictions from downstream
+ * mad: build the mad plugin even if libid3tag is not available
+ * mpeg2dec: do not fail fatally when downstream is unlinked (let upstream handle that)
+ * mpeg2dec: don't deadlock when setting an index
+ * mpegstream: increase allowable gap between streams
+ * x264enc: allow changing the bitrate and quantitizers dynamically
+ * x264enc: don't register flags with a value of 0
+ * x264enc: implement getcaps function to proxy downstream caps restrictions upstream
+ * x264enc: make tag event writable before modifying tag list in place
+ * x264enc: set max bitrate in quality mode
Bugs fixed in this release
-
+
+ * 539708 : [mpegstream] Increase allowable gap between streams
+ * 607698 : asfdemux: fix parsing of packets with padding
+ * 619136 : [dvdsubdec] spits out buffers at video framerate
+ * 621663 : x264enc: support changing bitrate property on the fly
+ * 639291 : [xingmux] Return NULL instead of 0 for a function returning gboolean
+ * 639715 : amrparse: seek error with EOS
+ * 640272 : x264enc: make tag event writable before modifying tag list in place
+ * 641151 : lame: doesn't negotiate sample rate properly
+ * 642360 : x264enc: Don't register flags which have 0 as a value
+ * 644704 : [dvdsubedc] no SPU clipping implemented
+ * 647709 : mpeg2dec: errors out on not-linked flow return
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Contributors to this release
- * Andy Wingo
- * Christian Schaller
- * David Schleef
+ * Brendan Le Foll
* Edward Hervey
- * Jan Schmidt
- * Michael Smith
- * Philippe Khalaf
- * Ronald Bultje
+ * Luis de Bethencourt
+ * Mark Nauwelaerts
+ * Miguel Angel Cabrera Moya
+ * Olivier Crête
+ * Sebastian Dröge
+ * Sjoerd Simons
* Stefan Kost
- * Thomas Vander Stichele
+ * Thibault Saunier
* Tim-Philipp Müller
- * Wim Taymans
- * Zaheer Abbas Merali
+ * Vincent Penquerc'h
+ * Yang Xichuan
\ No newline at end of file