index 8af4105c3e8b6172f1017e3fd421d0c36d2e1cfa..a89531cb580ae0c560835285e0119d4a52f2d12e 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-Release notes for GStreamer Ugly Plug-ins 0.10.7 "I Cheated Time"
+Release notes for GStreamer Ugly Plug-ins 0.10.18 "Extra Life"
The GStreamer team is proud to announce a new release
Features of this release
- * Many bug fixes and improvements
- * Accurate seeking support in mp3
- * xingmux moved from -bad
- * RealMedia and WMS RTSP support
- * LAME mp3 encoder fixes
- * Support non-square pixels in ASF
- * rmdemux fixes
- * amrnb fixes
- * dvdreadsrc seeking fix
- * Initial MPEG-2 reverse playback support
- * New element: dvdsubdec
+ * amrwbdec: avoid stalling on invalid frame
+ * asfpacket: don't rely on data from duration extension
+ * dvdsubdec: Implement clipping if the video size is smaller than the subpicture size
+ * dvdsubdec: Output only a single buffer per subpicture and set the correct duration
+ * lamemp3enc: implement sinkpad get_caps() function to proxy rate and channels restrictions from downstream
+ * mad: build the mad plugin even if libid3tag is not available
+ * mpeg2dec: do not fail fatally when downstream is unlinked (let upstream handle that)
+ * mpeg2dec: don't deadlock when setting an index
+ * mpegstream: increase allowable gap between streams
+ * x264enc: allow changing the bitrate and quantitizers dynamically
+ * x264enc: don't register flags with a value of 0
+ * x264enc: implement getcaps function to proxy downstream caps restrictions upstream
+ * x264enc: make tag event writable before modifying tag list in place
+ * x264enc: set max bitrate in quality mode
Bugs fixed in this release
- * 358891 : [dvdreadsrc] aborts due to src- > cur_pack == dsi_pack.dsi_...
- * 337681 : Seeking problem with MP3s in banshee and rhythmbox
- * 414988 : Stream encoded by lame has gap after decoding
- * 427309 : [rmdemux] trouble playing RV10 video
- * 439390 : [lame] fix up so we can control sample rate conversion
- * 450879 : Missing files in po/POTFILES.in
- * 452025 : ./configure breaks when cross-compiling LAME
- * 454311 : missing xml/{element-synaesthesia-details.xml,plugin-syna...
- * 466442 : amrnbenc has not properties to add header and select band...
- * 495885 : [mpegdemux] unknown stream id 0xbe
- * 500467 : [rmdemux] totem crashed with SIGSEGV
- * 500808 : gstmpeg2dec compile problem in MSVC 6.0
- * 507821 : Skip over broken seektable in Xing headers
- * 511497 : [PLUGIN-MOVE] Move xingheader to gst-plugins-ugly
- * 514297 : mpeg2dec with corrupted packets causes fps denominator so...
- * 515575 : [lame] unit test shows memory leak
- * 515708 : [dvdsubparse] Leaks a pad template
- * 515725 : [xingmux] Fails on big endian systems
- * 516278 : [dvdreadsrc] FORMAT_BYTES based seek stopped working sinc...
- * 516811 : [mp3parse] immediate EOS when playing back AVIs
- * 516989 : [dvdreadsrc] wrong (negative) stream position returned du...
- * 308312 : Make mp3parse plugin implement GST_SEEK_FLAG_ACCURATE
- * 508595 : [lame] wrong output caps in mono encoding mode
- * 140136 : [mpeg] plays choppy in gst-player/totem
- * 448782 : add finalize() to amrnbdec element
- * 491305 : [playbin?] intro-leopard.mov sometimes EOSes immediately,...
- * 504671 : [rtspsrc] spews warnings on setup and shutdown
+ * 539708 : [mpegstream] Increase allowable gap between streams
+ * 607698 : asfdemux: fix parsing of packets with padding
+ * 619136 : [dvdsubdec] spits out buffers at video framerate
+ * 621663 : x264enc: support changing bitrate property on the fly
+ * 639291 : [xingmux] Return NULL instead of 0 for a function returning gboolean
+ * 639715 : amrparse: seek error with EOS
+ * 640272 : x264enc: make tag event writable before modifying tag list in place
+ * 641151 : lame: doesn't negotiate sample rate properly
+ * 642360 : x264enc: Don't register flags which have 0 as a value
+ * 644704 : [dvdsubedc] no SPU clipping implemented
+ * 647709 : mpeg2dec: errors out on not-linked flow return
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Contributors to this release
- * Alexander Shopov
- * Daniel Charles
- * David Schleef
+ * Brendan Le Foll
* Edward Hervey
- * Ilkka Tuohela
- * Jakub Bogusz
- * Jan Schmidt
- * Jorge González González
- * Julien MOUTTE
- * Laurent Glayal
+ * Luis de Bethencourt
* Mark Nauwelaerts
- * Raphael Higino
+ * Miguel Angel Cabrera Moya
+ * Olivier Crête
* Sebastian Dröge
- * Sebastien Moutte
+ * Sjoerd Simons
* Stefan Kost
- * Tal Shalif
- * Thijs Vermeir
- * Thomas Vander Stichele
+ * Thibault Saunier
* Tim-Philipp Müller
- * Wenzheng Hu
- * Wim Taymans
- * Zaheer Abbas Merali
+ * Vincent Penquerc'h
+ * Yang Xichuan
\ No newline at end of file