diff --git a/REQUIREMENTS b/REQUIREMENTS
index 6cc1e9fb722fbb78334c7f964d5844528223bcc7..911231f198400b480a36a83048c7aaea89c81dae 100644 (file)
--- a/REQUIREMENTS
+++ b/REQUIREMENTS
+GStreamer uses a *large* array of tools and libraries, most of which are
+optional. We have attempted to make sure that any code that depends on
+optional libraries doesn't get built unless you have those libraries. If
+you find this not to be the case, please, let us know by filing a bug
+report at http://bugzilla.gnome.org/.
+
+
+Required tools:
+===============
+
+An extra set of tools is required if you wish to build GStreamer out of
+CVS (using autogen.sh):
+
+autoconf 2.52 or better
+automake 1.5
+gettext 0.11.5
+libtool v1.4 or better
+pkgconfig 0.9.0 or better (http://www.freedesktop.org/software/pkgconfig/)
+
+Required libraries:
+===================
+
+The core GStreamer libraries. See the gstreamer/ module in GStreamer cvs, or
+the version that corresponds to this plugin release.
+
+Optional libraries:
+===================
+
This file lists supporting libraries for which gst-plugins contains plugins,
as well as their minimum version. You can find the corresponding plugins in
ext/(library)
-a52dec 0.7.3
-avifile >= 0.6.0 (cvs)
+libHermes (for colorspace conversions; you need this for any video work)
+ http://www.clanlib.org/hermes/
+libghttp (for httpsrc)
+ http://ftp.gnome.org/pub/GNOME/stable/sources/libghttp/
+libaudiofile (for afsrc/afsink
+ http://oss.sgi.com/projects/audiofile/
+libmad (for the mad mp3 decoder plugin)
+ http://www.mars.org/home/rob/proj/mpeg/
+libjpeg (for jpegenc/jpegdec)
+ http://www.ijg.org/
+libopenquicktime (for the QT plugin)
+ http://sourceforge.net/projects/openquicktime/
+libXv (for videosink)
+libxaudio (for xa mp3 decoder)
+ http://www.xaudio.com/
+libvorbis (for vorbisenc, vorbisdec)
+ http://www.xiph.org/ogg/vorbis/index.html
+libcdparanoia (for cdparanoia ripper)
+ http://www.xiph.org/paranoia/index.html
+liblame (for lame mp3 encoder)
+ http://www.mp3dev.org/mp3/
+libshout (for the shoutcast plugin)
+ http://www.icecast.org
+libasound (for the alsa src/sink plugin)
+ http://alsa-project.org/
+librtp (for the rtp sink plugin)
+ http://www.linphone.org/ortp/
+aalib (for the aa sink plugin)
+ http://aa-project.sourceforge.net/aalib/
+aRts (for the arts plugin wrapper, and the artsd sink)
+ http://www.arts-project.org
+raw1394/linux1394 (for the dv plugin)
+ http://linux1394.sourceforge.net
+libdvdread (for the dvdsrc)
+ http://www.dtek.chalmers.se/groups/dvd/
+ (optional: libcss for encrypted DVDs)
+libdvdnav (for the dvdnavsrc)
+ http://dvd.sourceforge.net/
+ (optional: libcss for encrypted DVDs)
+ >= 0.1.9
+libesound (for the esd sink
+ ftp.gnome.org/pub/GNOME/stable/sources/esound)
+gnome-vfs (for the gnome-vfs src)
+ >= 2.4.0
+libgsm (for the gsm plugin)
+ http://kbs.cs.tu-berlin.de/~jutta/toast.html
+sdl (for the sdl sink)
+ http://www.libsdl.org
+xmms (for the xmms plugins wrapper)
+ http://www.xmms.org
+mpeg2dec/a52dec (for mpeg2 related plugins and dvd playback)
+ http://libmpeg2.sourceforge.net/
+ and http://liba52.sourceforge.net/
+ >= v0.3.1/v0.7.2
+swfdec (for the swfdec plugin)
+ http://swfdec.sourceforge.net
+ >= 0.2.0
+flac (for the FLAC lossless audio format)
+ http://flac.sourceforge.net
+ >= 1.0.3 preferred, 1.0.2 should work
+gtk (for the gdk_pixbuf plugin)
+ http://www.gtk.org/
+ >= 2.2.1 preferred, 2.0 ok
+pango (for the textoverlay plugins)
+ http://www.pango.org/
+
+Optional debian packages:
+=========================
+gtk-doc-tools 0.4-0.2 -- needed to build documentation