diff --git a/configure.ac b/configure.ac
index 48d252eccc9f37bb013b05cc58c83f1b53c59a5c..3ebe17d39e0d5c149b171126645881c934ceecc8 100644 (file)
--- a/configure.ac
+++ b/configure.ac
-dnl autoconf configuration file for plugins
+dnl autoconf configuration file for gst-plugins
AC_INIT
-dnl FIXME take something else ?
-AC_CONFIG_SRCDIR([COPYING])
-
AC_CANONICAL_TARGET([])
-AM_CONFIG_HEADER(config.h)
-
-GST_VERSION_MAJOR=0
-GST_VERSION_MINOR=3
-GST_VERSION_MICRO=11
-
-dnl we use a datestamped release tag during CVS development
-GST_VERSION_RELEASE=`date +%Y%m%d`
-dnl we use a normal release tag increased manually when releasing
-dnl GST_VERSION_RELEASE=1
-
-GST_VERSION=$GST_VERSION_MAJOR.$GST_VERSION_MINOR.$GST_VERSION_MICRO
+dnl We disable static building for development, for time savings
+dnl this goes before AS_LIBTOOL to appease autoconf
+dnl *NOTE*: dnl this line before release, so release does static too
+AM_DISABLE_STATIC
-PACKAGE=gst-plugins
-VERSION=$GST_VERSION
+dnl when going to/from release please set the nano (fourth number) right !
+dnl We disable static building for development, for time savings
+AM_DISABLE_STATIC
+AS_VERSION(gst-plugins, GST_PLUGINS, 0, 3, 4, 0)
+AM_INIT_AUTOMAKE($PACKAGE,$VERSION)
+AS_LIBTOOL(GST_PLUGINS, 0, 0, 0, yes)
-AC_DEFINE_UNQUOTED(PACKAGE, "$PACKAGE")
-AC_DEFINE_UNQUOTED(VERSION, "$VERSION")
-AC_SUBST(PACKAGE)
-AC_SUBST(VERSION)
-AC_DEFINE_UNQUOTED(GST_VERSION_RELEASE, "$GST_VERSION_RELEASE")
-AC_SUBST(GST_VERSION_RELEASE)
+dnl we'll move this to a configure option later on which will be turned on
+dnl by autogen
+dnl GST_ERROR="-Wall -Werror"
+GST_ERROR="-Werror"
-dnl libtool
-GST_CURRENT=2
-GST_REVISION=0
-GST_AGE=0
-GST_LIBVERSION=$GST_CURRENT:$GST_REVISION:$GST_AGE
+dnl FIXME take something else ?
+AC_CONFIG_SRCDIR([gst/law/alaw.c])
+AM_CONFIG_HEADER(config.h)
-AM_INIT_AUTOMAKE($PACKAGE, $VERSION)
dnl Add parameters for aclocal
dnl (This must come after AM_INIT_AUTOMAKE, since it modifies ACLOCAL)
-ACLOCAL="$ACLOCAL $ACLOCAL_FLAGS"
-
-AC_SUBST(GST_VERSION_MAJOR)
-AC_SUBST(GST_VERSION_MINOR)
-AC_SUBST(GST_VERSION_MICRO)
-AC_SUBST(GST_VERSION)
-
-AC_SUBST(GST_CURRENT)
-AC_SUBST(GST_REVISION)
-AC_SUBST(GST_AGE)
-AC_SUBST(GST_LIBVERSION)
+ACLOCAL="$ACLOCAL -I m4 -I common/m4 $ACLOCAL_FLAGS"
AM_MAINTAINER_MODE
AC_PROG_CXXCPP
AC_ISC_POSIX
-dnl We disable static building for development, for time savings
-dnl *NOTE*: dnl this line before release, so release does static too
-AM_DISABLE_STATIC
-AC_LIBTOOL_DLOPEN
-AM_PROG_LIBTOOL
-
AC_HEADER_STDC([])
dnl ###########################################
[HAVE_EXPERIMENTAL=yes],disabled,
[
AC_MSG_WARN(building experimental plugins)
- USE_SMOOTHWAVE="yes"
+ USE_RTP="yes"
+ USE_TARKIN="yes"
],[
AC_MSG_NOTICE(not building experimental plugins)
- USE_SMOOTHWAVE="no"
+ USE_RTP="no"
+ USE_TARKIN="no"
])
dnl broken plugins; stuff that doesn't seem to build at the moment
GST_CHECK_FEATURE(BROKEN, [enable building of broken plugins],,
HAVE_BROKEN=yes,disabled,
[
- AC_MSG_WARN(building broken plugins)
+ AC_MSG_WARN([building broken plugins -- no bug reports on these, only patches :)])
+ USE_SMOOTHWAVE="yes"
USE_VGA="yes"
USE_XMMS="yes"
- dnl AC_MSG_NOTICE(actually there are no broken plugins at the moment)
],[
+ USE_SMOOTHWAVE="no"
USE_VGA="no"
USE_XMMS="no"
AC_MSG_NOTICE(not building broken plugins)
fi
dnl check for gstreamer; uninstalled is selected preferentially -- see pkg-config(1)
-PKG_CHECK_MODULES(GST, gstreamer >= 0.3.1, HAVE_GST="yes", HAVE_GST="no")
+PKG_CHECK_MODULES(GST, gstreamer >= $GST_PLUGINS_MAJOR.$GST_PLUGINS_MINOR.$GST_PLUGINS_MICRO,
+ HAVE_GST="yes", HAVE_GST="no")
if test "x$HAVE_GST" = "xno"; then
AC_MSG_ERROR(no GStreamer found)
fi
+GST_TOOLS_DIR=`pkg-config --variable=toolsdir gstreamer`
+if test -z $GST_TOOLS_DIR; then
+ AC_MSG_ERROR([no tools dir defined in GStreamer pkg-config file; core upgrade needed.])
+fi
+AC_SUBST(GST_TOOLS_DIR)
+
dnl Set up conditionals for (target) architecture:
dnl ==============================================
dnl (ie CPUID)
case "x${target_cpu}" in
xi386 | xi486) ;;
- *) AC_DEFINE(HAVE_RDTSC) ;;
+ *) AC_DEFINE(HAVE_RDTSC, 1, [Define if RDTSC is available]) ;;
esac ;;
xpowerpc) HAVE_CPU_PPC=yes
AC_DEFINE(HAVE_CPU_PPC, 1, [Define if the target CPU is a PPC]) ;;
dnl Determine endianness
AC_C_BIGENDIAN
-dnl Check for MMX-capable compiler
-AC_MSG_CHECKING(for MMX-capable compiler)
-AC_TRY_RUN([
-#include "include/mmx.h"
-
-main()
-{ movq_r2r(mm0, mm1); return 0; }
-],
-[
-HAVE_LIBMMX="yes"
-AC_MSG_RESULT(yes)
-],
-HAVE_LIBMMX="no"
-AC_MSG_RESULT(no)
-,
-HAVE_LIBMMX="no"
-AC_MSG_RESULT(no)
-)
-
-dnl
-dnl We should really use AC_SYS_LARGEFILE, but the problem is
-dnl many of the plugins don't include "config.h". To assure
-dnl binary compatibility, it is necessary that all gstreamer
-dnl code be compiled with the same sizeof(off_t), so we use
-dnl the following crude hack.
-dnl
-
-AC_MSG_CHECKING(for large file support)
-AC_TRY_RUN([
-#define _LARGEFILE_SOURCE
-#define _FILE_OFFSET_BITS 64
-#include <sys/types.h>
-int main () { return !(sizeof(off_t) == 8); }
-],
-[
-AC_MSG_RESULT(yes)
-GST_CFLAGS="$GST_CFLAGS -D_LARGEFILE_SOURCE -D_FILE_OFFSET_BITS=64"
-],
-[
-AC_MSG_RESULT(no)
-],
-[
-AC_MSG_RESULT(no)
-])
-
dnl Check for essential libraries first:
dnl ====================================
-if test -n "`echo $GST_CFLAGS | grep USE_GLIB2`"; then
- USE_GLIB2=yes
-else
- USE_GLIB2=no
-fi
-
-dnl needed for some plugins and demos, now's a nice time to check for gtk
-if test x$USE_GLIB2 = xno; then
- AM_PATH_GTK(1.2.0,,
- AC_MSG_ERROR(Cannot find gtk: Is gtk-config in path?))
- HAVE_GTK=yes
- # we have to have it
-else
- PKG_CHECK_MODULES(GTK2, gtk+-2.0, HAVE_GTK=yes, HAVE_GTK=no)
-
- GTK_CFLAGS=$GTK2_CFLAGS
- GTK_LIBS=$GTK2_LIBS
-fi
+GST_GLIB2_CHECK()
+PKG_CHECK_MODULES(GTK2, gtk+-2.0, HAVE_GTK=yes, HAVE_GTK=no)
+GTK_CFLAGS=$GTK2_CFLAGS
+GTK_LIBS=$GTK2_LIBS
AC_SUBST(GTK_LIBS)
AC_SUBST(GTK_CFLAGS)
dnl Check for X11 extensions
AC_PATH_XTRA
if test "-DX_DISPLAY_MISSING" = "$X_CFLAGS"; then
- AC_MSG_ERROR(can not find X11)
+ AC_MSG_NOTICE([cannot find X11, the build system needs fixage])
fi
AC_SUBST(X_CFLAGS)
AC_SUBST(X_PRE_LIBS)
dnl ==========================================================================
dnl ============================= gst plugins ================================
dnl ==========================================================================
+GST_PLUGIN_LDFLAGS='-module -avoid-version'
+AC_SUBST(GST_PLUGIN_LDFLAGS)
GST_PLUGINS_ALL="\
ac3parse adder audioscale auparse avi chart\
- cutter deinterlace flx intfloat law level\
+ cutter deinterlace flx goom intfloat law level\
median mpeg1enc mpeg1sys mpeg1videoparse mpeg2enc mpeg2sub\
- mpegaudio mpegaudioparse mpegstream mpegtypes\
- passthrough playondemand rtjpeg silence sine\
+ mpegaudio mpegaudioparse mpegstream mpegtypes modplug\
+ monoscope passthrough playondemand rtjpeg silence sine\
smooth spectrum speed stereo stereomono\
synaesthesia udp videoscale volenv volume vumeter wavparse y4m"
dnl ==========================================================================
+dnl *** DXR3 card ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_DXR3, true)
+GST_CHECK_FEATURE(DXR3, [DXR3 hardware mpeg video decoder], dxr3videosink, [
+ AC_CHECK_HEADER(linux/em8300.h, HAVE_DXR3="yes", HAVE_DXR3="no")
+])
+
dnl *** OSS audio ***
translit(dnm, m, l) AM_CONDITIONAL(USE_OSS, true)
GST_CHECK_FEATURE(OSS, [OSS audio], osssrc osssink, [
dnl *** QuickCam ***
translit(dnm, m, l) AM_CONDITIONAL(USE_QCAM, true)
-GST_CHECK_FEATURE(QCAM, [QuickCam], qcamsrc, HAVE_QCAM="yes")
+GST_CHECK_FEATURE(QCAM, [QuickCam], qcamsrc, [
+dnl this one is for hadess, no qcam when no nasm found
+ if test "x$HAVE_NASM" = "xno";
+ then
+ HAVE_QCAM="no"
+ AC_MSG_WARN([QuickCam needs nasm])
+ else
+ HAVE_QCAM="yes"
+ fi
+])
dnl *** Video 4 Linux ***
translit(dnm, m, l) AM_CONDITIONAL(USE_V4L, true)
-GST_CHECK_FEATURE(V4L, [Video 4 Linux], v4lsrc, [
+GST_CHECK_FEATURE(V4L, [Video 4 Linux], v4lsrc v4lmjpegsrc v4lmjpegsink, [
AC_CHECK_DECL(VID_TYPE_MPEG_ENCODER, HAVE_V4L="yes", HAVE_V4L="no", [#include <linux/videodev.h>])
])
dnl FIXME: perhaps warn user if they have a shared libXv since
dnl this is an error until XFree86 starts shipping one
translit(dnm, m, l) AM_CONDITIONAL(USE_XVIDEO, true)
-GST_CHECK_FEATURE(XVIDEO, [X11 XVideo extensions], xvideosink, [
+GST_CHECK_FEATURE(XVIDEO, [X11 XVideo extensions], xvideosink videosink, [
dnl check for PIC static lib
GST_CHECK_LIBHEADER(XVIDEO, Xv_pic, XvQueryExtension, $X_LIBS $X_PRE_LIBS -lXext -lX11 $X_EXTRA_LIBS, X11/extensions/Xvlib.h, XVIDEO_LIBS="-lXv_pic -lXext")
if test x$HAVE_XVIDEO = xno; then
dnl *** a52dec ***
translit(dnm, m, l) AM_CONDITIONAL(USE_A52DEC, true)
GST_CHECK_FEATURE(A52DEC, [a52dec], a52dec, [
- GST_CHECK_LIBHEADER(A52DEC, a52, a52_init, -lm, a52dec/a52.h, A52DEC_LIBS="-la52")
+ AC_CHECK_A52DEC(HAVE_A52DEC=yes, HAVE_A52DEC=no)
])
dnl *** aalib ***
dnl **** ESound ****
translit(dnm, m, l) AM_CONDITIONAL(USE_ESD, true)
-GST_CHECK_FEATURE(ESD, [esound plugins], esdsrc esdsink, [
+GST_CHECK_FEATURE(ESD, [esound plugins], esdsink esdmon, [
AM_PATH_ESD(0.2.12, HAVE_ESD=yes, HAVE_ESD=no)
])
])
dnl *** Gnome VFS ***
-dnl this check uses the GST_CHECK_CONFIGPROG macro with gnome-config vfs
translit(dnm, m, l) AM_CONDITIONAL(USE_GNOME_VFS, true)
GST_CHECK_FEATURE(GNOME_VFS, [Gnome VFS], gnomevfssrc, [
-translit(dnm, m, l) AC_SUBST(GNOME_VFS_LIBS)
-translit(dnm, m, l) AC_SUBST(GNOME_VFS_CFLAGS)
-GST_CHECK_CONFIGPROG(GNOME_VFS, gnome-config vfs)
+ PKG_CHECK_MODULES(GNOME_VFS, gnome-vfs-2.0, HAVE_GNOME_VFS="yes", HAVE_GNOME_VFS="no")
+ AC_SUBST(GNOME_VFS_CFLAGS)
+ AC_SUBST(GNOME_VFS_LIBS)
])
dnl *** gsm ***
if test $HAVE_GSM != "yes"; then
GST_CHECK_LIBHEADER(GSM, gsm, gsm_create, , gsm/gsm.h, GSM_LIBS="-lgsm")
if test $HAVE_GSM = "yes"; then
- AC_DEFINE(GSM_HEADER_IN_SUBDIR)
+ AC_DEFINE(GSM_HEADER_IN_SUBDIR, 1, [Define if GSM header in gsm/ subdir])
fi
fi
AC_SUBST(GSM_LIBS)
AC_SUBST(GST_HTTPSRC_GET_TYPE)
])
-dnl *** lame ***
-translit(dnm, m, l) AM_CONDITIONAL(USE_LAME, true)
-GST_CHECK_FEATURE(LAME, [lame mp3 encoder library], lame, [
-GST_CHECK_LIBHEADER(LAME, mp3lame, lame_init, -lm, lame/lame.h, LAME_LIBS="-lmp3lame")
+dnl *** Jack ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_JACK, true)
+GST_CHECK_FEATURE(JACK, Jack, jack, [
+ PKG_CHECK_MODULES(JACK, jack, HAVE_JACK="yes", HAVE_JACK="no")
+ AC_SUBST(JACK_CFLAGS)
+ AC_SUBST(JACK_LIBS)
])
-AC_SUBST(LAME_LIBS)
-
-
-dnl FIXME : check if these CPP flags can be dealt with otherwise
-dnl libdvcheck_save_CPPFLAGS="$CPPFLAGS"
-dnl CPPFLAGS="$CPPFLAGS $GST_CFLAGS"
-dnl AC_CHECK_HEADER(libdv/dv.h, :, HAVE_LIBDV=no)
-dnl CPPFLAGS="$libdvcheck_save_CPPFLAGS"
dnl *** jpeg ***
dnl FIXME: we could use header checks here as well IMO
AC_SUBST(JPEG_LIBS)
])
-dnl *** jpeg-mmx ***
-AC_ARG_WITH(jpeg-mmx-path, [ --with-jpeg-mmx-path, path to mmx accelerated jpeg lib])
-translit(dnm, m, l) AM_CONDITIONAL(USE_JPEG_MMX, true)
-GST_CHECK_FEATURE(JPEG_MMX, [jpeg-mmx], jpegmmxenc jpegmmxdec, [
- AC_CHECK_LIB(jpeg-mmx, jpeg_start_compress, HAVE_JPEG_MMX="yes", HAVE_JPEG_MMX="no", "-L$with_jpeg_mmx_path")
- JPEG_MMX_LIBS="-L$with_jpeg_mmx_path -ljpeg-mmx"
- JPEG_MMX_CFLAGS="-I$with_jpeg_mmx_path"
- AC_SUBST(JPEG_MMX_LIBS)
- AC_SUBST(JPEG_MMX_CFLAGS)
+dnl *** lame ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LAME, true)
+GST_CHECK_FEATURE(LAME, [lame mp3 encoder library], lame, [
+GST_CHECK_LIBHEADER(LAME, mp3lame, lame_init, -lm, lame/lame.h, HAVE_LAME="yes" LAME_LIBS="-lmp3lame")
+])
+AC_SUBST(LAME_LIBS)
+
+dnl *** libcolorspace ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LCS, true)
+GST_CHECK_FEATURE(LCS, Lcs, lcs, [
+ PKG_CHECK_MODULES(LCS, lcs, HAVE_LCS="yes", HAVE_LCS="no")
+ AC_SUBST(LCS_CFLAGS)
+ AC_SUBST(LCS_LIBS)
])
+dnl FIXME : check if these CPP flags can be dealt with otherwise
+dnl libdvcheck_save_CPPFLAGS="$CPPFLAGS"
+dnl CPPFLAGS="$CPPFLAGS $GST_CFLAGS"
+dnl AC_CHECK_HEADER(libdv/dv.h, :, HAVE_LIBDV=no)
+dnl CPPFLAGS="$libdvcheck_save_CPPFLAGS"
+
dnl *** mad ***
dnl FIXME: we could use header checks here as well IMO
translit(dnm, m, l) AM_CONDITIONAL(USE_MAD, true)
GST_CHECK_FEATURE(MAD, [mad mp3 decoder], mad, [
AC_CHECK_LIB(mad, mad_decoder_finish, HAVE_MAD="yes" MAD_LIBS="-lmad")
+ if test "x$HAVE_MAD" = "xyes"; then
+ # installed with mad >= 0.14
+ HAVE_MAD="no"
+ save_libs=$LIBS
+ LIBS="-lz"
+ AC_CHECK_LIB(id3tag, id3_tag_query, HAVE_MAD="yes" MAD_LIBS="$MAD_LIBS -lid3tag")
+ LIBS=$save_LIBS
+ fi
])
AC_SUBST(MAD_LIBS)
AC_SUBST(MIKMOD_CFLAGS, "$LIBMIKMODCFLAGS")
])
+dnl *** mjpegtools ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_MJPEGTOOLS, true)
+GST_CHECK_FEATURE(MJPEGTOOLS, [mjpegtools], jpegmmxenc jpegmmxdec, [
+ PKG_CHECK_MODULES(MJPEGTOOLS, mjpegtools, HAVE_MJPEGTOOLS="yes", HAVE_MJPEGTOOLS="no")
+ AC_SUBST(MJPEGTOOLS_LIBS)
+ AC_SUBST(MJPEGTOOLS_CFLAGS)
+])
+
dnl *** mpeg2dec ***
translit(dnm, m, l) AM_CONDITIONAL(USE_MPEG2DEC, true)
GST_CHECK_FEATURE(MPEG2DEC, [mpeg2dec], mpeg2dec, [
- GST_CHECK_LIBHEADER(MPEG2DEC, mpeg2, mpeg2_init,, mpeg2dec/mpeg2.h, MPEG2DEC_LIBS="-lmpeg2 -lmpeg2dec")
- AC_SUBST(MPEG2DEC_LIBS)
+ AC_CHECK_MPEG2DEC(HAVE_MPEG2DEC=yes, HAVE_MPEG2DEC=no)
])
dnl *** openquicktime ***
AC_SUBST(RTP_LIBS)
])
-
dnl FIXME header check needs to use GLIB_CFLAGS in order to succeed for rtp
dnl can use GST_* which should have GLIB_* info
dnl AC_CHECK_HEADERS(rtp/rtp.h, HAVE_LIBRTP=yes, HAVE_LIBRTP=no)
if test $HAVE_GTK = "yes"; then HAVE_SMOOTHWAVE=yes; fi;
])
+dnl *** tarkin ***
+dnl for now the sources are included in the plugin
+dnl and should be moved to ext-libs/ perhaps
+translit(dnm, m, l) AM_CONDITIONAL(USE_TARKIN, true)
+GST_CHECK_FEATURE(TARKIN, [tarkinenc tarkindec], tarkin, [
+ HAVE_TARKIN="yes"
+])
+
dnl *** vorbis ***
dnl AM_PATH_VORBIS only takes two options
translit(dnm, m, l) AM_CONDITIONAL(USE_VORBIS, true)
dnl # Check command line parameters, and set shell variables accordingly #
dnl ######################################################################
+GST_DEBUGINFO
+
AC_ARG_ENABLE(libmmx,
[ --enable-libmmx use libmmx, if available],
[case "${enableval}" in
esac],
[USE_ATOMIC_H=$HAVE_ATOMIC_H]) dnl Default value
-AC_ARG_ENABLE(plugin-builddir,
-[ --enable-plugin-builddir allow tests/demos to use non-installed plugins ],
-[case "${enableval}" in
- yes) PLUGINS_USE_BUILDDIR=yes ;;
- no) PLUGINS_USE_BUILDDIR=no ;;
- *) AC_MSG_ERROR(bad value ${enableval} for --enable-plugin-builddir) ;;
-esac],
-[PLUGINS_USE_BUILDDIR=no]) dnl Default value
-
-AC_ARG_ENABLE(debug,
-[ --enable-debug compile with -g debugging info],
-[case "${enableval}" in
- yes) USE_DEBUG=yes ;;
- no) USE_DEBUG=no ;;
- *) AC_MSG_ERROR(bad value ${enableval} for --enable-debug) ;;
-esac],
-[USE_DEBUG=yes]) dnl Default value
-
-AC_ARG_ENABLE(DEBUG,
-[ --enable-DEBUG compiles in a large number of debugging messages],
-[case "${enableval}" in
- yes) ENABLE_DEBUG=yes ;;
- no) ENABLE_DEBUG=no ;;
- *) AC_MSG_ERROR(bad value ${enableval} for --enable-DEBUG) ;;
-esac],
-[ENABLE_DEBUG=yes]) dnl Default value
-if test x$ENABLE_DEBUG = xyes; then
- AC_DEFINE(GST_DEBUG_ENABLED, 1, [Define if DEBUG statements should be compiled in])
-fi
-
-AC_ARG_ENABLE(INFO,
-[ --disable-INFO disables compilation of informational messages],
-[case "${enableval}" in
- yes) ENABLE_INFO=yes ;;
- no) ENABLE_INFO=no ;;
- *) AC_MSG_ERROR(bad value ${enableval} for --enable-INFO) ;;
-esac],
-[ENABLE_INFO=yes]) dnl Default value
-if test x$ENABLE_INFO = xyes; then
- AC_DEFINE(GST_INFO_ENABLED, 1, [Define if INFO statements should be compiled in])
-fi
-
-AC_ARG_ENABLE(debug-color,
-[ --disable-debug-color disables color output of DEBUG and INFO output],
-[case "${enableval}" in
- yes) ENABLE_DEBUG_COLOR=yes ;;
- no) ENABLE_DEBUG_COLOR=no ;;
- *) AC_MSG_ERROR(bad value ${enableval} for --enable-debug-color) ;;
-esac],
-[ENABLE_DEBUG_COLOR=yes]) dnl Default value
-if test "x$ENABLE_DEBUG_COLOR" = xyes; then
- AC_DEFINE(GST_DEBUG_COLOR, 1, [Define if debugging messages should be colorized])
-fi
-
AC_ARG_ENABLE(profiling,
[ --enable-profiling adds -pg to compiler commandline, for profiling],
[case "${enableval}" in
esac],
[USE_PROFILING=no]) dnl Default value
-dnl default to building registry in the source tree if we are enabling plugin build dir
-if test "x$PLUGINS_USE_BUILDDIR"="xyes"; then
- GST_CONFIG_DIR=`pwd`
-else
- GST_CONFIG_DIR=/etc/gstreamer
-fi
-AC_ARG_WITH(configdir,
-[ --with-configdir specify path to use for configdir],
-[case "${withval}" in
- yes) AC_MSG_ERROR(bad value ${withval} for --with-configdir) ;;
- no) AC_MSG_ERROR(bad value ${withval} for --with-configdir) ;;
- *) GST_CONFIG_DIR="${withval}" ;;
-esac],
-[:]) dnl Default value
-
-AC_ARG_ENABLE(docs-build,
-[ --enable-docs-build enable building of documentation],
-[case "${enableval}" in
- yes) if $HAVE_GTK_DOC; then BUILD_DOCS=yes; else AC_MSG_ERROR([you don't have gtk-doc, so don't use --docs-build]); fi; ;;
- no) BUILD_DOCS=no ;;
- *) AC_MSG_ERROR(bad value ${enableval} for --enable-docs-build) ;;
-esac],
-[BUILD_DOCS=no]) dnl Default value
-
-AC_ARG_ENABLE(plugin-docs,
-[ --enable-plugin-docs enable the building of plugin documentation
- (this is currently broken, so off by default)],
-[case "${enableval}" in
- yes) BUILD_PLUGIN_DOCS=yes ;;
- no) BUILD_PLUGIN_DOCS=no ;;
- *) AC_MSG_ERROR(bad value ${enableval} for --enable-plugin-docs) ;;
-esac],
-[BUILD_PLUGIN_DOCS=no]) dnl Default value
-
AC_ARG_ENABLE(tests,
[ --disable-tests disable building test apps],
[case "${enableval}" in
esac],
[BUILD_EXAMPLES=yes]) dnl Default value
-dnl Next, check for the optional components:
-dnl ========================================
-
-
-AC_DEFUN(GST_SUBSYSTEM_DISABLE,
-[dnl
-dnl Add a subsystem --disable flag and all the necessary symbols and substitions
-dnl
-AC_ARG_ENABLE(translit([$1], A-Z, a-z),
-[ ]builtin(format, --disable-%-17s disable %s, translit([$1], A-Z, a-z), $2),
-[ case "${enableval}" in
- yes) GST_DISABLE_[$1]=no ;;
- no) GST_DISABLE_[$1]=yes ;;
- *) AC_MSG_ERROR(bad value ${enableval} for --enable-translit([$1], A-Z, a-z)) ;;
- esac],
-[GST_DISABLE_[$1]=no]) dnl Default value
-if test x$GST_DISABLE_[$1] = xyes; then
- AC_DEFINE(GST_DISABLE_[$1], 1, [Disable $2])
- GST_DISABLE_[$1]_DEFINE=-DGST_DISABLE_[$1]
-fi
-AM_CONDITIONAL(GST_DISABLE_[$1], test x$GST_DISABLE_[$1] = xyes)
-AC_SUBST(GST_DISABLE_[$1]_DEFINE)
-GST_SUBSYSTEM_DISABLE_DEFINES="$GST_SUBSYTEM_DISABLE_DEFINES $GST_DISABLE_[$1]_DEFINE"
-])
-
-translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_LOADSAVE, true)
-GST_SUBSYSTEM_DISABLE(LOADSAVE,[pipeline XML load/save])
-translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_TYPEFIND, true)
-GST_SUBSYSTEM_DISABLE(TYPEFIND,[typefind plugin],)
-translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_AUTOPLUG, true)
-GST_SUBSYSTEM_DISABLE(AUTOPLUG,[autoplugger subsystem])
-translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_PARSE, true)
-GST_SUBSYSTEM_DISABLE(PARSE,[command-line parser])
-translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_TRACE, true)
-GST_SUBSYSTEM_DISABLE(TRACE,[tracing subsystem])
-translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_REGISTRY, true)
-GST_SUBSYSTEM_DISABLE(REGISTRY,[plugin registry])
-
-GST_CFLAGS="$GST_CFLAGS $GST_SUBSYSTEM_DISABLE_DEFINES"
-
-
dnl ################################################
dnl # Set defines according to variables set above #
dnl ################################################
AC_DEFINE(HAVE_ATOMIC_H, 1, [Define if atomic.h header file is available])
fi
-if test "x$PLUGINS_USE_BUILDDIR" = xyes; then
- AC_DEFINE(PLUGINS_USE_BUILDDIR, 1, [Define if plugins should be loaded from the build tree - only developers should use this])
-fi
-
dnl if test "x$USE_DEBUG" = xyes; then
dnl CFLAGS="$CFLAGS -g"
dnl fi
dnl AC_SUBST(FOMIT_FRAME_POINTER)
dnl
-if test "x$HAVE_LIBMIKMOD" = xyes; then
- AC_DEFINE(HAVE_LIBMIKMOD)
-fi
-
-if test "x$HAVE_LIBGSM" = xyes; then
- AC_DEFINE(HAVE_LIBGSM)
-fi
-
dnl #############################
dnl # Set automake conditionals #
dnl #############################
AM_CONDITIONAL(EXPERIMENTAL, test "$EXPERIMENTAL" = "$xyes")
AM_CONDITIONAL(BROKEN, test "$BROKEN" = "$xyes")
-AM_CONDITIONAL(HAVE_LIBMIKMOD, test "x$HAVE_LIBMIKMOD" = "xyes")
-AM_CONDITIONAL(HAVE_LIBSDL, test "x$HAVE_LIBSDL" = "xyes")
AM_CONDITIONAL(HAVE_NASM, test "x$HAVE_NASM" = "xyes")
AM_CONDITIONAL(HAVE_LIBGLADE_GNOME, test "x$HAVE_LIBGLADE_GNOME" = "xyes")
AM_CONDITIONAL(HAVE_GNOME, test "x$HAVE_GNOME" = "xyes")
AM_CONDITIONAL(BUILD_TESTS, test "x$BUILD_TESTS" = "xyes")
AM_CONDITIONAL(BUILD_EXAMPLES, test "x$BUILD_EXAMPLES" = "xyes")
AM_CONDITIONAL(BUILD_PLUGIN_DOCS, test "x$BUILD_PLUGIN_DOCS" = "xyes")
-AM_CONDITIONAL(HAVE_PDFXMLTEX, $HAVE_PDFXMLTEX)
-AM_CONDITIONAL(HAVE_PDFTOPS, $HAVE_PDFTOPS)
-AM_CONDITIONAL(HAVE_XSLTPROC, $HAVE_XSLTPROC)
AM_CONDITIONAL(HAVE_FIG2DEV_PNG, $HAVE_FIG2DEV_PNG)
AM_CONDITIONAL(HAVE_FIG2DEV_PDF, $HAVE_FIG2DEV_PDF)
-AM_CONDITIONAL(HAVE_LIBRTP, test "x$HAVE_LIBRTP" = "xyes")
-AM_CONDITIONAL(HAVE_ARTS, test "x$HAVE_ARTS" = "xyes")
AM_CONDITIONAL(HAVE_RAW1394, test "x$HAVE_RAW1394" = "xyes")
-AM_CONDITIONAL(HAVE_LIBDV, test "x$HAVE_LIBDV" = "xyes")
-AM_CONDITIONAL(HAVE_GNOME_VFS, test "x$HAVE_GNOME_VFS" = "xyes")
-AM_CONDITIONAL(HAVE_LIBGSM, test "x$HAVE_LIBGSM" = "xyes")
-AM_CONDITIONAL(PLUGINS_USE_BUILDDIR, test "x$PLUGINS_USE_BUILDDIR" = "xyes")
-
-dnl ############################
-dnl # Set up some more defines #
-dnl ############################
-
-dnl Set location of configuration dir.
-AC_DEFINE_UNQUOTED(GST_CONFIG_DIR,"$GST_CONFIG_DIR")
-AC_SUBST(GST_CONFIG_DIR)
-
-dnl Set location of plugin directory
-if test "x${prefix}" = "xNONE"; then
- PLUGINS_DIR=${ac_default_prefix}/lib/gst
-else
- PLUGINS_DIR=${prefix}/lib/gst
-fi
-AC_DEFINE_UNQUOTED(PLUGINS_DIR,"$PLUGINS_DIR")
-AC_SUBST(PLUGINS_DIR)
-
-dnl Set location of uninstalled plugin directory
-PLUGINS_BUILDDIR=`pwd`
-AC_DEFINE_UNQUOTED(PLUGINS_BUILDDIR,"$PLUGINS_BUILDDIR")
-AC_SUBST(PLUGINS_BUILDDIR)
-
-GST_CFLAGS="$GST_CFLAGS -I\$(top_srcdir)/gst-libs"
+GST_CFLAGS="$GST_CFLAGS -I\$(top_srcdir)/gst-libs -Wall -Werror"
AC_SUBST(GST_LIBS)
AC_SUBST(GST_CFLAGS)
-dnl #############################
-dnl # Configure the subpackages #
-dnl #############################
-
-dnl AC_CONFIG_SUBDIRS(gist)
-dnl AC_CONFIG_SUBDIRS(plugins/mp3decode/xing/libxing)
-
-dnl ##################################################
-dnl # Prepare informative messages to display at end #
-dnl ##################################################
-
-infomessages=
-
-if test "x$PLUGINS_USE_BUILDDIR" = xyes; then
- infomessages="$infomessages
-*** Warning: You have configured using the --enable-plugin-builddir option.
-
-This option is for development purposes only: binaries built with
-it should be used with code in the build tree only. To build an
-installable version, use ./configure without the --enable-plugin-builddir
-option. Note that the autogen.sh script supplies the plugin builddir
-option automatically - it cannot be used to configure installable builds.
-
-"
-fi
-
dnl #########################
dnl # Make the output files #
dnl #########################
-AC_OUTPUT(
+dnl testsuite/autoplug/Makefile
+dnl testsuite/Makefile
+AC_CONFIG_FILES(
Makefile
gstreamer-libs.pc
gstreamer-libs-uninstalled.pc
gst/cutter/Makefile
gst/deinterlace/Makefile
gst/flx/Makefile
+gst/goom/Makefile
gst/intfloat/Makefile
gst/law/Makefile
gst/level/Makefile
gst/mpegaudioparse/Makefile
gst/mpegstream/Makefile
gst/mpegtypes/Makefile
+gst/modplug/Makefile
+gst/modplug/libmodplug/Makefile
+gst/monoscope/Makefile
gst/passthrough/Makefile
gst/playondemand/Makefile
gst/rtjpeg/Makefile
gst/wavparse/Makefile
gst/y4m/Makefile
sys/Makefile
+sys/dxr3/Makefile
sys/oss/Makefile
sys/qcam/Makefile
sys/v4l/Makefile
sys/vcd/Makefile
sys/vga/Makefile
sys/xvideo/Makefile
+sys/videosink/Makefile
ext/Makefile
ext/a52dec/Makefile
ext/aalib/Makefile
ext/gsm/Makefile
ext/hermes/Makefile
ext/http/Makefile
+ext/jack/Makefile
ext/jpeg/Makefile
+ext/lcs/Makefile
ext/ladspa/Makefile
ext/lame/Makefile
ext/mad/Makefile
ext/mikmod/Makefile
+ext/mjpegtools/Makefile
ext/mpeg2dec/Makefile
ext/openquicktime/Makefile
ext/raw1394/Makefile
ext/sidplay/Makefile
ext/smoothwave/Makefile
ext/vorbis/Makefile
+ext/tarkin/Makefile
ext/xmms/Makefile
gst-libs/Makefile
gst-libs/gst/Makefile
gst-libs/gst/riff/Makefile
examples/capsfilter/Makefile
examples/Makefile
+tools/Makefile
)
+AC_OUTPUT
+
echo -e "configure: *** Plugins that will be built : $GST_PLUGINS_YES"
echo
echo -e "configure: *** Plugins that will not be built : $GST_PLUGINS_NO"