diff --git a/configure.ac b/configure.ac
index 2a549229bcf52ee4dc25b74d42334e51bcca5ef8..553f8f99769a3ebce18142201fa132e710c68083 100644 (file)
--- a/configure.ac
+++ b/configure.ac
dnl when going to/from release please set the nano (fourth number) right !
dnl releases only do Wall, cvs and prerelease does Werror too
-AS_VERSION(gst-plugins, GST_PLUGINS_VERSION, 0, 7, 0, 1, GST_CVS="no", GST_CVS="yes")
+AS_VERSION(gst-plugins, GST_PLUGINS_VERSION, 0, 7, 5, 1, GST_CVS="no", GST_CVS="yes")
+
+dnl add a suffix to apps
+if test x$program_suffix = xNONE ; then
+ program_suffix=-$GST_PLUGINS_VERSION_MAJOR.$GST_PLUGINS_VERSION_MINOR
+fi
+
AM_INIT_AUTOMAKE($PACKAGE,$VERSION)
dnl our libraries and install dirs use major.minor as a version
dnl - interfaces added/removed/changed -> increment CURRENT, REVISION = 0
dnl - interfaces added -> increment AGE
dnl - interfaces removed -> AGE = 0
-AS_LIBTOOL(GST_PLUGINS, 1, 0, 0)
+AS_LIBTOOL(GST_PLUGINS, 2, 0, 0)
+AM_PROG_LIBTOOL
dnl FIXME take something else ?
AC_CONFIG_SRCDIR([gst/law/alaw.c])
AM_PROG_AS
AS="${CC}"
+dnl the gettext stuff needed
+AM_GNU_GETTEXT_VERSION(0.11.5)
+AM_GNU_GETTEXT([external])
+
+GETTEXT_PACKAGE=gst-plugins-$GST_MAJORMINOR
+AC_SUBST(GETTEXT_PACKAGE)
+AC_DEFINE_UNQUOTED([GETTEXT_PACKAGE], "$GETTEXT_PACKAGE",
+ [gettext package name])
+
+dnl define LOCALEDIR in config.h
+AS_AC_EXPAND(LOCALEDIR, $datadir/locale)
+AC_DEFINE_UNQUOTED([LOCALEDIR], "$LOCALEDIR",
+ [gettext locale dir])
+
dnl decide on error flags
AS_COMPILER_FLAG(-Wall, GST_WALL="yes", GST_WALL="no")
if test "x$GST_WALL" = "xyes"; then
- GST_ERROR="$GST_ERROR -Wall"
+ GST_ERROR="$GST_ERROR -Wall -Wno-sign-compare"
if test "x$GST_CVS" = "xyes"; then
AS_COMPILER_FLAG(-Werror,GST_ERROR="$GST_ERROR -Werror",GST_ERROR="$GST_ERROR")
+ GST_ERROR="$GST_ERROR -DG_DISABLE_DEPRECATED"
fi
-
- dnl set gcc-style optimization flags if using the gnu compiler.
- GST_FUNROLL_CFLAGS="$GST_FUNROLL_CFLAGS -funroll-all-loops"
- GST_FINLINE_CFLAGS="$GST_FINLINE_CFLAGS -finline-functions"
- GST_FFASTMATH_CFLAGS="$GST_FFASTMATH_CFLAGS -ffast-math"
- GST_FSCHEDULE_CFLAGS="$GST_FSCHEDULE_CFLAGS -fschedule-insns2"
- GST_FNOEXCEPTIONS_CFLAGS="$GST_FNOEXCEPTIONS_CFLAGS -fno-exceptions"
fi
dnl determine c++ compiler
AC_ISC_POSIX
AC_HEADER_STDC([])
+AC_C_INLINE
+AX_CREATE_STDINT_H
+
+dnl Check for a way to display the function name in debug output
+GST_CHECK_FUNCTION()
+
+dnl define correct errorlevel for debugging messages. We want to have GST_ERROR
+dnl messages printed when running cvs builds
+if test "x$GST_CVS" = "xyes"; then
+ AC_DEFINE(GST_LEVEL_DEFAULT, GST_LEVEL_ERROR, [Default errorlevel to use])
+fi
dnl ############################################
dnl # Super Duper options for plug-in building #
AC_HELP_STRING([--with-pkg-config-path],[colon-separated list of pkg-config(1) dirs]),
[export PKG_CONFIG_PATH=${withval}])
+dnl check architecture
+GST_ARCH()
+
dnl Check for nasm
AC_PATH_PROG(NASM_PATH, nasm, no)
AC_SUBST(NASM_PATH)
AC_SUBST(GST_CONTROL_LIBS)
-
-dnl Set up conditionals for (target) architecture:
-dnl ==============================================
-
-dnl Determine CPU
-case "x${target_cpu}" in
- xi?86 | k?) HAVE_CPU_I386=yes
- AC_DEFINE(HAVE_CPU_I386, 1, [Define if the target CPU is an x86])
- dnl FIXME could use some better detection
- dnl (ie CPUID)
- case "x${target_cpu}" in
- xi386 | xi486) ;;
- *) AC_DEFINE(HAVE_RDTSC, 1, [Define if RDTSC is available]) ;;
- esac ;;
- xpowerpc) HAVE_CPU_PPC=yes
- AC_DEFINE(HAVE_CPU_PPC, 1, [Define if the target CPU is a PPC]) ;;
- xalpha) HAVE_CPU_ALPHA=yes
- AC_DEFINE(HAVE_CPU_ALPHA, 1, [Define if the target CPU is an Alpha]) ;;
- xarm*) HAVE_CPU_ARM=yes
- AC_DEFINE(HAVE_CPU_ARM, 1, [Define if the target CPU is an ARM]) ;;
- xsparc*) HAVE_CPU_SPARC=yes
- AC_DEFINE(HAVE_CPU_SPARC, 1, [Define if the target CPU is a PPC]) ;;
- xmips*) HAVE_CPU_MIPS=yes
- AC_DEFINE(HAVE_CPU_MIPS, 1, [Define if the target CPU is a MIPS]) ;;
- xhppa*) HAVE_CPU_HPPA=yes
- AC_DEFINE(HAVE_CPU_HPPA, 1, [Define if the target CPU is a HPPA]) ;;
-esac
-
dnl Determine endianness
AC_C_BIGENDIAN
dnl ====================================
GST_GLIB2_CHECK()
-PKG_CHECK_MODULES(GTK2, gtk+-2.0, HAVE_GTK=yes, HAVE_GTK=no)
+
+dnl Check for additional libraries that we might use:
+dnl =================================================
+dnl GTK
+HAVE_GTK=NO
+PKG_CHECK_MODULES(GTK2, gtk+-2.0 >= 2.2.0, HAVE_GTK_22=yes, HAVE_GTK_22=no)
+if test "x$HAVE_GTK_22" = "xyes"; then
+ HAVE_GTK=yes
+ GTK_VERSION=`$PKG_CONFIG --variable=gtk_binary_version gtk+-2.0`
+ AC_SUBST(GTK_VERSION)
+ GTK_PREFIX=`$PKG_CONFIG --variable=prefix gdk-pixbuf-2.0`
+ GDK_PIXBUF_LIBDIR=`$PKG_CONFIG --variable=libdir gdk-pixbuf-2.0`
+ GDK_PIXBUF_PREFIXDIR=`$PKG_CONFIG --variable=prefix gdk-pixbuf-2.0`
+ AC_SUBST(GTK_BASE_DIR)
+else
+ PKG_CHECK_MODULES(GTK2, gtk+-2.0, HAVE_GTK_20=yes, HAVE_GTK_20=no)
+fi
+if test "x$HAVE_GTK_20" = "xyes"; then
+ HAVE_GTK=yes
+fi
GTK_CFLAGS=$GTK2_CFLAGS
GTK_LIBS=$GTK2_LIBS
AC_SUBST(GTK_LIBS)
AC_SUBST(GTK_CFLAGS)
+AC_SUBST(HAVE_GTK)
+# gdk_pixbuf gstreamer loader is considered experimental, so disable
+# by default
+if test "x$HAVE_GTK_22" = "xyes"; then
+ HAVE_GDK_LOADERS=yes
+else
+ HAVE_GDK_LOADERS=no
+fi
-dnl Check for X11 extensions
-AC_PATH_XTRA
-if test "-DX_DISPLAY_MISSING" = "$X_CFLAGS"; then
- AC_MSG_NOTICE([cannot find X11, the build system needs fixage])
+# we set the defaults always to make sure we have non-empty variables
+# for the Makefile
+
+# by default, stick to prefix
+GDK_PIXBUF_LOADER_DIR=${libdir}/gtk-2.0/\${GTK_VERSION}/loaders
+GDK_PIXBUF_CONF_DIR=${sysconfdir}/gtk-2.0
+
+
+AC_ARG_ENABLE(gdk-pixbuf-loader,
+ AC_HELP_STRING([--enable-gdk-pixbuf-loader],
+ [whether to enable building of gdk_pixbuf loader]),
+ :, HAVE_GDK_LOADERS="no")
+
+if test "x$HAVE_GDK_LOADERS" = "xyes"; then
+ AC_PATH_PROG(QUERYLOADERS, gdk-pixbuf-query-loaders, no)
+ # allow customization of pixbuf loader install location
+ # when nothing specified, adhere to prefix settings
+ # when called without any option with this argument, autodetect
+ # when called with a path, set to the given path
+
+ AC_ARG_WITH(gdk-pixbuf-loader-dir,
+ AC_HELP_STRING([--with-gdk-pixbuf-loader-dir],
+ [directory to install the gdk_pixbuf loader (none for pkg-config default)]),
+ [
+ if test "x${withval}" != xyes ; then
+ GDK_PIXBUF_LOADER_DIR="${withval}"
+ else
+ GDK_PIXBUF_LOADER_DIR="$GDK_PIXBUF_LIBDIR/gtk-2.0/\$GTK_VERSION/loaders"
+ fi
+ ]
+ )
+ AS_AC_EXPAND(GDK_PIXBUF_LOADER_DIR, $GDK_PIXBUF_LOADER_DIR)
+ AC_SUBST(GDK_PIXBUF_LOADER_DIR)
+ AC_MSG_NOTICE([Putting GTK+-2 pixbuf loaders in $GDK_PIXBUF_LOADER_DIR])
+
+ # allow customization of pixbuf loader configuration file
+ # when nothing specified, adhere to prefix settings
+ # when called without any option with this argument, autodetect
+ # when called with a path, set to the given path
+
+ AC_ARG_WITH(gdk-pixbuf-conf-dir,
+ AC_HELP_STRING([--with-gdk-pixbuf-conf-dir],
+ [directory to install the gdk_pixbuf config (none for pkg-config default)]),
+ [
+ if test "x${withval}" != xyes ; then
+ GDK_PIXBUF_CONF_DIR="${withval}"
+ else
+ GDK_PIXBUF_CONF_DIR="$GDK_PIXBUF_PREFIXDIR/etc/gtk-2.0/"
+ fi
+ ]
+ )
+ AS_AC_EXPAND(GDK_PIXBUF_CONF_DIR, $GDK_PIXBUF_CONF_DIR)
+ AC_SUBST(GDK_PIXBUF_CONF_DIR)
+ AC_MSG_NOTICE([Putting GTK+-2 pixbuf loader config in $GDK_PIXBUF_CONF_DIR])
+fi
+AM_CONDITIONAL(HAVE_GDK_LOADERS, test "x$HAVE_GDK_LOADERS" = "xyes")
+
+PKG_CHECK_MODULES(LIBOIL, liboil-0.1, HAVE_LIBOIL=yes, HAVE_LIBOIL=no)
+AC_SUBST(LIBOIL_CFLAGS)
+AC_SUBST(LIBOIL_LIBS)
+if test "x${HAVE_LIBOIL}" = xyes ; then
+ #AC_DEFINE_UNQUOTED(HAVE_LIBOIL, 1, [Define if liboil is being used])
+ true
fi
-AC_SUBST(X_CFLAGS)
-AC_SUBST(X_PRE_LIBS)
-AC_SUBST(X_EXTRA_LIBS)
-AC_SUBST(X_LIBS)
dnl ===========================================================================
dnl ============================= gst plug-ins ================================
dnl ===========================================================================
-GST_PLUGIN_LDFLAGS='-module -avoid-version'
+plugindir="\$(libdir)/gstreamer-$GST_MAJORMINOR"
+AC_SUBST(plugindir)
+
+GST_PLUGIN_LDFLAGS='-module -avoid-version -export-symbols-regex [_]*{gst_,Gst,GST_}.*'
AC_SUBST(GST_PLUGIN_LDFLAGS)
dnl these are all the gst plug-ins, compilable without additional libs
GST_PLUGINS_ALL="\
- ac3parse adder audioscale auparse avi \
- asfdemux audioconvert cdxaparse chart \
- cutter debug deinterlace effectv festival \
- filter flx goom intfloat law level median mixmatrix \
- mpeg1enc mpeg1sys mpeg1videoparse mpeg2enc mpeg2sub \
- mpegaudio mpegaudioparse mpegstream mpegtypes \
- monoscope oneton overlay passthrough playondemand qtdemux \
- realmedia rtp rtjpeg silence sine smooth smpte \
- spectrum speed stereo synaesthesia tcp udp vbidec \
- videocrop videofilter videoflip videoscale videotestsrc \
- volenv volume wavenc wavparse y4m"
+ ac3parse \
+ adder \
+ asfdemux \
+ audioconvert \
+ audioscale \
+ auparse \
+ avi \
+ cdxaparse \
+ chart \
+ colorspace \
+ cutter \
+ debug \
+ deinterlace \
+ effectv \
+ festival \
+ filter \
+ flx \
+ goom \
+ id3 \
+ interleave \
+ law \
+ level \
+ matroska \
+ median \
+ mixmatrix \
+ mpeg1sys \
+ mpeg1videoparse \
+ mpeg2sub \
+ mpegaudio \
+ mpegaudioparse \
+ mpegstream \
+ monoscope \
+ overlay \
+ passthrough \
+ playondemand \
+ qtdemux \
+ realmedia \
+ rtjpeg \
+ rtp \
+ silence \
+ sine \
+ smooth \
+ smpte \
+ spectrum \
+ speed \
+ stereo \
+ switch \
+ synaesthesia \
+ tags \
+ tcp \
+ typefind \
+ udp \
+ vbidec \
+ videocrop \
+ videodrop \
+ videoflip \
+ videofilter \
+ videoscale \
+ videotestsrc \
+ volenv \
+ volume \
+ wavenc \
+ wavparse \
+ y4m"
dnl see if we can build C++ plug-ins
if test "x$HAVE_CXX" = "xyes"; then
fi
])
-dnl *** Video 4 Linux ***
-dnl for information about the header/define, see sys/v4l/gstv4lelement.h
-translit(dnm, m, l) AM_CONDITIONAL(USE_V4L, true)
-GST_CHECK_FEATURE(V4L, [Video 4 Linux], v4lsrc v4lmjpegsrc v4lmjpegsink, [
- AC_CHECK_DECL(VID_TYPE_MPEG_ENCODER, HAVE_V4L="yes", HAVE_V4L="no", [
-#include <sys/types.h>
-#define _LINUX_TIME_H
-#include <linux/videodev.h>
- ])
-])
-
-dnl *** Video 4 Linux 2***
-dnl for information about the header/define, see sys/v4l2/gstv4l2element.h
-translit(dnm, m, l) AM_CONDITIONAL(USE_V4L2, true)
-GST_CHECK_FEATURE(V4L2, [Video 4 Linux 2], v4l2src, [
- AC_MSG_CHECKING([Checking for uptodate v4l2 installation])
- AC_TRY_COMPILE([
-#include <sys/types.h>
-#include <linux/types.h>
-#define _LINUX_TIME_H
-#include <linux/videodev2.h>
-#if defined(V4L2_MAJOR_VERSION) || defined(V4L2_MINOR_VERSION)
-#error too early v4l2 version or no v4l2 at all
-#endif
- ], [
-return 0;
- ], [ HAVE_V4L2="yes" && AC_MSG_RESULT(yes)],
- [ HAVE_V4L2="no" && AC_MSG_RESULT(no) &&
- AC_CHECK_HEADER(linux/videodev2.h,
- [ AC_MSG_WARN([video4linux2 headers were found, but they're old. Please update v4l2 to compile the v4l2 plugins])],
- [ AC_MSG_WARN([video4linux2 was not found])])])
-])
-
dnl *** Video CD ***
translit(dnm, m, l) AM_CONDITIONAL(USE_VCD, true)
GST_CHECK_FEATURE(VCD, [Video CD], vcdsrc, [
fi
])
+dnl Check for X11
+translit(dnm, m, l) AM_CONDITIONAL(USE_X, true)
+GST_CHECK_FEATURE(X, [X libraries and plugins],
+ [ximagesink], [
+ AC_PATH_XTRA
+dnl if test "x$X_CFLAGS" == "x" -o "$X_CFLAGS" == "-DX_DISPLAY_MISSING"
+ if test "x$X_DISPLAY_MISSING" = "x1"
+ then
+ AC_MSG_NOTICE([cannot find X11 development files])
+ HAVE_X="no"
+ else
+ dnl this is much more than we want
+ X_LIBS="$X_LIBS $X_PRE_LIBS $X_EXTRA_LIBS"
+ dnl AC_PATH_XTRA only defines the path needed to find the X libs, not the libs
+ dnl therefore we add them here
+ X_LIBS="$X_LIBS -lX11"
+ AC_SUBST(X_CFLAGS)
+ AC_SUBST(X_LIBS)
+ HAVE_X="yes"
+ fi
+ AC_SUBST(HAVE_X)
+])
+
dnl *** XVideo ***
dnl Look for the PIC library first, Debian requires it.
dnl Check debian-devel archives for gory details.
dnl non-PIC libXv, if not then don not use Xv.
dnl FIXME: perhaps warn user if they have a shared libXv since
dnl this is an error until XFree86 starts shipping one
-translit(dnm, m, l) AM_CONDITIONAL(USE_XFREE, true)
-GST_CHECK_FEATURE(XFREE, [X11 XFree86], xvideosink-X, [
- if test "-DX_DISPLAY_MISSING" = "$X_CFLAGS"; then
- HAVE_XFREE=no
- else
- HAVE_XFREE=yes
- fi
-])
dnl Check for Xv extension
translit(dnm, m, l) AM_CONDITIONAL(USE_XVIDEO, true)
-GST_CHECK_FEATURE(XVIDEO, [X11 XVideo extensions], xvideosink-Xv, [
- if test x$HAVE_XFREE = xyes; then
+GST_CHECK_FEATURE(XVIDEO, [X11 XVideo extensions],
+ [xvimagesink xvideosink], [
+ if test x$HAVE_X = xyes; then
AC_CHECK_LIB(Xv_pic, XvQueryExtension,
HAVE_XVIDEO="yes", HAVE_XVIDEO="no",
- $X_LIBS $X_PRE_LIBS -lXext -lX11 $X_EXTRA_LIBS)
+ $X_LIBS -lXext)
if test x$HAVE_XVIDEO = xyes; then
XVIDEO_LIBS="-lXv_pic -lXext"
if test x$HAVE_XVIDEO = xno; then
AC_CHECK_LIB(Xv, XvQueryExtension,
HAVE_XVIDEO="yes", HAVE_XVIDEO="no",
- $X_LIBS $X_PRE_LIBS -lXext -lX11 $X_EXTRA_LIBS)
+ $X_LIBS -lXext)
if test x$HAVE_XVIDEO = xyes; then
XVIDEO_LIBS="-lXv -lXext"
fi
])
+dnl check for X Shm
+translit(dnm, m, l) AM_CONDITIONAL(USE_XSHM, true)
+GST_CHECK_FEATURE(XSHM, [X Shared Memory extension], xshm, [
+ if test x$HAVE_X = xyes; then
+ AC_CHECK_LIB(Xext, XShmAttach,
+ HAVE_XSHM="yes", HAVE_XSHM="no",
+ $X_LIBS)
+ if test "x$HAVE_XSHM" = "xyes"; then
+ XSHM_LIBS="-lXext"
+ else
+ dnl On AIX, it is in XextSam instead, but we still need -lXext
+ AC_CHECK_LIB(XextSam, XShmAttach,
+ HAVE_XSHM="yes", HAVE_XSHM="no",
+ $X_LIBS)
+ if test "x$HAVE_XSHM" = "xyes"; then
+ XSHM_LIBS="-lXext -lXextSam"
+ fi
+ fi
+ fi
+], , [
+ AC_SUBST(HAVE_XSHM)
+ AC_SUBST(XSHM_LIBS)
+] )
+
+dnl v4l/v4l2 checks have been moved down because they require X
+
+dnl *** Video 4 Linux ***
+dnl for information about the header/define, see sys/v4l/gstv4lelement.h
+translit(dnm, m, l) AM_CONDITIONAL(USE_V4L, true)
+GST_CHECK_FEATURE(V4L, [Video 4 Linux], v4lsrc v4lmjpegsrc v4lmjpegsink, [
+ # first check X
+ HAVE_V4L="no"
+ if test "$HAVE_X" == "yes"
+ then
+ AC_CHECK_DECL(VID_TYPE_MPEG_ENCODER, HAVE_V4L="yes", HAVE_V4L="no", [
+#include <sys/types.h>
+#define _LINUX_TIME_H
+#include <linux/videodev.h>
+ ])
+ fi
+])
+
+dnl *** Video 4 Linux 2 ***
+dnl for information about the header/define, see sys/v4l2/gstv4l2element.h
+translit(dnm, m, l) AM_CONDITIONAL(USE_V4L2, true)
+GST_CHECK_FEATURE(V4L2, [Video 4 Linux 2], v4l2src, [
+ HAVE_V4L2="no"
+ if test "$HAVE_X" == "yes"
+ then
+ AC_MSG_CHECKING([Checking for uptodate v4l2 installation])
+ AC_TRY_COMPILE([
+#include <sys/types.h>
+#include <linux/types.h>
+#define _LINUX_TIME_H
+#include <linux/videodev2.h>
+#if defined(V4L2_MAJOR_VERSION) || defined(V4L2_MINOR_VERSION)
+#error too early v4l2 version or no v4l2 at all
+#endif
+ ], [
+return 0;
+ ], [ HAVE_V4L2="yes" && AC_MSG_RESULT(yes)],
+ [ HAVE_V4L2="no" && AC_MSG_RESULT(no) &&
+ AC_CHECK_HEADER(linux/videodev2.h,
+ [ AC_MSG_WARN([video4linux2 headers were found, but they're old. Please update v4l2 to compile the v4l2 plugins])],
+ [ AC_MSG_WARN([video4linux2 was not found])])
+ ])
+ fi
+])
+
dnl Next, check for the optional libraries:
dnl These are all libraries used in building plug-ins
dnl ================================================
dnl *** alsa ***
translit(dnm, m, l) AM_CONDITIONAL(USE_ALSA, true)
GST_CHECK_FEATURE(ALSA, [alsa plug-ins], gstalsa, [
- AM_PATH_ALSA(0.9.0, HAVE_ALSA=yes, HAVE_ALSA=no)
+ AM_PATH_ALSA(0.9.1, HAVE_ALSA=yes, HAVE_ALSA=no)
])
dnl *** arts ***
AS_SCRUB_INCLUDE(DVDNAV_CFLAGS)
])
-dnl *** MAS ***
-translit(dnm, m, l) AM_CONDITIONAL(USE_MAS, true)
-GST_CHECK_FEATURE(MAS, [mas library], massink, [
- translit(dnm, m, l) AC_SUBST(MAS_LIBS)
- translit(dnm, m, l) AC_SUBST(MAS_CFLAGS)
- GST_CHECK_CONFIGPROG(MAS, mas-config)
- AS_SCRUB_INCLUDE(MAS_CFLAGS)
-])
-
dnl **** ESound ****
translit(dnm, m, l) AM_CONDITIONAL(USE_ESD, true)
GST_CHECK_FEATURE(ESD, [esound plug-ins], esdsink esdmon, [
AS_SCRUB_INCLUDE(ESD_CFLAGS)
])
+dnl **** Free AAC Encoder (FAAC) ****
+translit(dnm, m, l) AM_CONDITIONAL(USE_FAAC, true)
+GST_CHECK_FEATURE(FAAC, [AAC encoder plug-in], faac, [
+ GST_CHECK_LIBHEADER(FAAC, faac, faacEncOpen, -lm, faac.h, FAAC_LIBS="-lfaac -lm")
+ AS_SCRUB_INCLUDE(FAAC_CFLAGS)
+ AC_SUBST(FAAC_LIBS)
+])
+
+dnl **** Free AAC Decoder (FAAD) ****
+translit(dnm, m, l) AM_CONDITIONAL(USE_FAAD, true)
+GST_CHECK_FEATURE(FAAD, [AAC decoder plug-in], faad, [
+ GST_CHECK_LIBHEADER(FAAD, faad, faacDecOpen, -lm, faad.h, FAAD_LIBS="-lfaad -lm")
+ AC_MSG_CHECKING([Checking for FAAD >= 2])
+ AC_TRY_COMPILE([
+#include <faad.h>
+#if !defined(FAAD2_VERSION) || !defined(FAAD_FMT_DOUBLE)
+#error Not faad2
+#endif
+ ], [ return 0; ],
+ [ HAVE_FAAD="yes" && AC_MSG_RESULT(yes)],
+ [ HAVE_FAAD="no" && AC_MSG_RESULT(no)])
+ AS_SCRUB_INCLUDE(FAAD_CFLAGS)
+ AC_SUBST(FAAD_LIBS)
+])
+
dnl **** festival ****
dnl translit(dnm, m, l) AM_CONDITIONAL(USE_FESTIVAL, true)
dnl GST_CHECK_FEATURE(FESTIVAL, [festival plug-ins], festivalsrc, [
AC_SUBST(FLAC_LIBS)
])
-dnl *** FFMPEG ***
-translit(dnm, m, l) AM_CONDITIONAL(USE_FFMPEG, true)
-GST_CHECK_FEATURE(FFMPEG, [ffmpeg plug-ins], ffmpeg, [
- # only slurp in the case where we are in CVS mode;
- # prerelease and release should get it disted
- if test "x$GST_PLUGINS_VERSION_NANO" = x1; then
- AC_MSG_NOTICE(slurping FFmpeg CVS source)
- AS_SLURP_FFMPEG(gst-libs/ext/ffmpeg, 2003-07-05 22:00 GMT,
- HAVE_FFMPEG=yes, HAVE_FFMPEG=no)
- else
- AC_MSG_NOTICE(FFmpeg CVS code should be included already)
- HAVE_FFMPEG=yes
- fi
- # we only bother with uninstalled (included) ffmpeg for now
- AC_DEFINE_UNQUOTED(HAVE_FFMPEG_UNINSTALLED, 1,
- [defined if we use uninstalled ffmpeg])
-])
-
dnl *** GDK pixbuf ***
translit(dnm, m, l) AM_CONDITIONAL(USE_GDK_PIXBUF, true)
GST_CHECK_FEATURE(GDK_PIXBUF, [GDK pixbuf], gdkpixbufsrc, [
- if test $HAVE_GTK = "yes"; then HAVE_GDK_PIXBUF=yes; fi;
+ if test $HAVE_GTK_22 = "yes"; then HAVE_GDK_PIXBUF=yes; fi;
])
dnl *** Gnome VFS ***
AC_SUBST(LIBDV_LIBS)
])
+dnl *** libcaca ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBCACA, true)
+GST_CHECK_FEATURE(LIBCACA, [libcaca], libcaca, [
+ GST_CHECK_CONFIGPROG(LIBCACA, caca-config)
+ AC_SUBST(LIBCACA_CFLAGS)
+ AC_SUBST(LIBCACA_LIBS)
+])
+
dnl *** libfame ***
translit(dnm, m, l) AM_CONDITIONAL(USE_LIBFAME, true)
GST_CHECK_FEATURE(LIBFAME, [libfame MPEG1/4 encoder], libfame, [
AC_SUBST(LIBPNG_LIBS)
])
+dnl *** librfb ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBRFB, true)
+GST_CHECK_FEATURE(LIBRFB, [librfb Remote Framebuffer], rfbsrc, [
+ PKG_CHECK_MODULES(LIBRFB, librfb-0.1, HAVE_LIBRFB="yes", HAVE_LIBRFB="no")
+ AC_SUBST(LIBRFB_CFLAGS)
+ AC_SUBST(LIBRFB_LIBS)
+])
dnl *** mad ***
dnl FIXME: we could use header checks here as well IMO
translit(dnm, m, l) AM_CONDITIONAL(USE_MAD, true)
GST_CHECK_FEATURE(MAD, [mad mp3 decoder], mad, [
dnl check with pkg-config first
- PKG_CHECK_MODULES(MAD, mad id3tag, HAVE_MAD="yes", HAVE_MAD="no")
+ PKG_CHECK_MODULES(MAD, mad >= 0.15 id3tag >= 0.15, HAVE_MAD="yes", HAVE_MAD="no")
if test "x$HAVE_MAD" = "xno"; then
dnl fall back to oldskool detection
AC_CHECK_LIB(mad, mad_decoder_finish, HAVE_MAD="yes" MAD_LIBS="-lmad")
if test "x$HAVE_MAD" = "xyes"; then
- # installed with mad >= 0.14
HAVE_MAD="no"
save_libs=$LIBS
LIBS="-lz"
- AC_CHECK_LIB(id3tag, id3_tag_query, HAVE_MAD="yes" MAD_LIBS="$MAD_LIBS -lid3tag")
+ AC_CHECK_LIB(id3tag, id3_tag_options, HAVE_MAD="yes" MAD_LIBS="-lmad -lid3tag -lz")
LIBS=$save_LIBS
fi
fi
])
AC_SUBST(MAD_LIBS)
-dnl *** matroska ***
-translit(dnm, m, l) AM_CONDITIONAL(USE_MATROSKA, true)
-GST_CHECK_FEATURE(MATROSKA, [matroska muxer/demuxer], matroska muxer/demuxer, [
- PATH_EBML([HAVE_MATROSKA=yes], [HAVE_MATROSKA=no])
- if test x$HAVE_MATROSKA = xyes; then
- PATH_MATROSKA(0.4.4, [HAVE_MATROSKA=yes], [HAVE_MATROSKA=no])
- fi
-])
-
dnl *** mikmod ***
translit(dnm, m, l) AM_CONDITIONAL(USE_MIKMOD, true)
GST_CHECK_FEATURE(MIKMOD, [mikmod plug-in], mikmod, [
AC_SUBST(MPEG2DEC_LIBS)
])
+dnl *** mpeg2enc ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_MPEG2ENC, true)
+GST_CHECK_FEATURE(MPEG2ENC, [mpeg2enc], mpeg2enc, [
+ HAVE_MPEG2ENC="no"
+ dnl we require a c++ compiler for this one
+ if [ test x$HAVE_CXX = xyes ]; then
+ dnl libmpeg2enc was first included in mjpegtools-1.6.2-rc3 (1.6.1.92)
+ dnl since many distros include mjpegtools specifically without mplex
+ dnl and mpeg2enc, we check for mpeg2enc on its own, too.
+ PKG_CHECK_MODULES(MPEG2ENC, mjpegtools >= 1.6.1.93, [
+ dnl switch over to c++ to test things
+ AC_LANG_CPLUSPLUS
+ OLD_CPPFLAGS="$CPPFLAGS"
+ CPPFLAGS="$CPPFLAGS $MPEG2ENC_CFLAGS"
+ AC_CHECK_HEADER(mpeg2encoder.hh, [
+ MPEG2ENC_LIBS="$MPEG2ENC_LIBS -lmpeg2encpp -lm -lpthread"
+ OLD_LIBS="$LIBS"
+ LIBS="$LIBS $MPEG2ENC_LIBS"
+ AC_MSG_CHECKING([for valid mpeg2enc objects])
+ AC_TRY_RUN([
+#include <mpeg2encoder.hh>
+#include <mpeg2encoptions.hh>
+
+int
+main (int argc,
+ char *argv[])
+{
+ MPEG2EncOptions *options = new MPEG2EncOptions ();
+ MPEG2Encoder encoder (*options);
+ return 0;
+}
+ ],[
+ HAVE_MPEG2ENC="yes"
+ AC_SUBST(MPEG2ENC_CFLAGS)
+ AC_SUBST(MPEG2ENC_LIBS)
+ AC_MSG_RESULT(yes)
+ ], AC_MSG_RESULT(no))
+ LIBS="$OLD_LIBS"
+ ])
+ CPPFLAGS="$OLD_CPPFLAGS"
+ AC_LANG_C
+ ],
+ HAVE_MPEG2ENC="no")
+ fi
+])
+
dnl *** mplex ***
translit(dnm, m, l) AM_CONDITIONAL(USE_MPLEX, true)
-GST_CHECK_FEATURE(MPLEX, [mplex], mplex, [HAVE_MPLEX=$HAVE_CXX])
+GST_CHECK_FEATURE(MPLEX, [mplex], mplex, [
+ HAVE_MPLEX="no"
+ dnl we require a c++ compiler for this one
+ if [ test x$HAVE_CXX = xyes ]; then
+ dnl libmplex was first included in mjpegtools-1.6.2-rc4 (1.6.1.93)
+ dnl since many distros include mjpegtools specifically without mplex
+ dnl and mpeg2enc, we check for mplex on its own, too.
+ PKG_CHECK_MODULES(MPLEX, mjpegtools >= 1.6.1.93, [
+ dnl switch over to c++ to test things
+ AC_LANG_CPLUSPLUS
+ OLD_CPPFLAGS="$CPPFLAGS"
+ CPPFLAGS="$CPPFLAGS $MPLEX_CFLAGS"
+ AC_CHECK_HEADER(interact.hpp, [
+ MPLEX_LIBS="$MPLEX_LIBS -lmplex2 -lm"
+ OLD_LIBS="$LIBS"
+ LIBS="$LIBS $MPLEX_LIBS"
+ AC_MSG_CHECKING([for valid mplex objects])
+ AC_TRY_RUN([
+#include <interact.hpp>
+#include <outputstrm.hpp>
+#include <multiplexor.hpp>
+
+int
+main (int argc,
+ char *argv[])
+{
+ class TestOutputStream : public OutputStream {
+ public:
+ TestOutputStream () : OutputStream () { }
+ void Write (uint8_t *a, unsigned int b) { }
+ void NextSegment () { }
+ off_t SegmentSize () { }
+ void Close () { }
+ int Open () { }
+ };
+ MultiplexJob *job = new MultiplexJob ();
+ vector<IBitStream *> inputs;
+ job->SetupInputStreams (inputs);
+ TestOutputStream *out = new TestOutputStream ();
+ Multiplexor mux (*job, *out);
+ return 0;
+}
+ ],[
+ HAVE_MPLEX="yes"
+ AC_SUBST(MPLEX_CFLAGS)
+ AC_SUBST(MPLEX_LIBS)
+ AC_MSG_RESULT(yes)
+ ], AC_MSG_RESULT(no))
+ LIBS="$OLD_LIBS"
+ ])
+ CPPFLAGS="$OLD_CPPFLAGS"
+ AC_LANG_C
+ ], HAVE_MPLEX="no")
+ fi
+])
+
+dnl *** musicbrainz ***
+dnl libmusicbrainz <= 2.0.2 has symbol clashes with ffmpeg
+translit(dnm, m, l) AM_CONDITIONAL(USE_MUSICBRAINZ, true)
+GST_CHECK_FEATURE(MUSICBRAINZ, [musicbrainz], musicbrainz, [
+ PKG_CHECK_MODULES(MUSICBRAINZ, libmusicbrainz > 2.0.2,
+ HAVE_MUSICBRAINZ="yes", HAVE_MUSICBRAINZ="no")
+ AC_SUBST(MUSICBRAINZ_CFLAGS)
+ AC_SUBST(MUSICBRAINZ_LIBS)
+])
+
+dnl *** nas ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_NAS, true)
+GST_CHECK_FEATURE(NAS, [nas plug-in], nassink, [
+ HAVE_NAS="no"
+ if test "x$HAVE_X" = "xyes"; then
+ save_cppflags=$CFLAGS
+ CPPFLAGS="$CPPFLAGS $X_CFLAGS"
+ GST_CHECK_LIBHEADER(NAS, audio, AuOpenServer, $X_LIBS, audio/audiolib.h,
+ NAS_LIBS="$X_LIBS -laudio" NAS_CFLAGS="$X_CFLAGS")
+ CPPFLAGS="$save_cppflags"
+ fi
+ AC_SUBST(NAS_CFLAGS)
+ AC_SUBST(NAS_LIBS)
+])
dnl *** pango ***
translit(dnm, m, l) AM_CONDITIONAL(USE_PANGO, true)
dnl *** SDL ***
translit(dnm, m, l) AM_CONDITIONAL(USE_SDL, true)
GST_CHECK_FEATURE(SDL, [SDL plug-in], sdlvideosink, [
- AM_PATH_SDL(, HAVE_SDL=yes, HAVE_SDL=no)
+ dnl sdlvideosink depends on the xoverlay interface, which depends on X
+ if test x$HAVE_X = xyes; then
+ AM_PATH_SDL(, HAVE_SDL=yes, HAVE_SDL=no)
+ fi
])
dnl *** shout ***
HAVE_TARKIN="yes"
])
+dnl *** ogg ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_OGG, true)
+GST_CHECK_FEATURE(OGG, [ogg de/encoder], oggdemux oggmux, [
+ XIPH_PATH_OGG(HAVE_OGG=yes, HAVE_OGG=no)
+ AS_SCRUB_INCLUDE(OGG_CFLAGS)
+])
+
+dnl *** theora ***
+dnl FIXME: theora doesn't have proper pc/m4 files yet, change this when this happens
+translit(dnm, m, l) AM_CONDITIONAL(USE_THEORA, true)
+GST_CHECK_FEATURE(THEORA, [ogg theora codec], theoradec, [
+ GST_CHECK_LIBHEADER(THEORA, theora, theora_version_string, , theora/theora.h, THEORA_LIBS="-ltheora")
+ AC_SUBST(THEORA_LIBS)
+])
+
dnl *** vorbis ***
dnl AM_PATH_VORBIS only takes two options
translit(dnm, m, l) AM_CONDITIONAL(USE_VORBIS, true)
XIPH_PATH_VORBIS(HAVE_VORBIS=yes, HAVE_VORBIS=no)
AS_SCRUB_INCLUDE(VORBIS_CFLAGS)
])
+if test "x$HAVE_VORBIS" = "xyes"; then
+ ac_cflags_save="$CFLAGS"
+ CFLAGS="-Wall -Werror"
+ AC_COMPILE_IFELSE(
+ AC_LANG_PROGRAM([
+#include <vorbis/codec.h>
+ ],[
+vorbis_dsp_state *v;
+
+vorbis_synthesis_restart (v);
+ ]), HAVE_VSR=yes, HAVE_VSR=no)
+ if test "x$HAVE_VSR" = "xyes"; then
+ AC_DEFINE_UNQUOTED(HAVE_VORBIS_SYNTHESIS_RESTART, 1,
+ [defined if vorbis_synthesis_restart is present])
+ fi
+ CFLAGS="$ac_cflags_save"
+fi
+
+dnl *** xine ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_XINE, true)
+GST_CHECK_FEATURE(XINE, [xine wrapper], xine, [
+ PKG_CHECK_MODULES(XINE, libxine >= 1.0.0, HAVE_XINE=yes, HAVE_XINE=no)
+ AC_SUBST(XINE_CFLAGS)
+ AC_SUBST(XINE_LIBS)
+],disabled)
dnl *** XVID ***
translit(dnm, m, l) AM_CONDITIONAL(USE_XVID, true)
GST_CHECK_FEATURE(XVID, [xvid plugins], xvid, [
- HAVE_XVID=yes
- AC_CHECK_HEADER(xvid.h, ,
- [ AC_MSG_WARN([Xvid headers not found]) &&
- HAVE_XVID=no ] )
- LIBS="-lm"
- AC_CHECK_LIB(xvidcore, xvid_encore, ,
- [ AC_MSG_WARN([Xvid encore libs not found]) &&
- HAVE_XVID=no ] )
- AC_CHECK_LIB(xvidcore, xvid_decore, ,
- [ AC_MSG_WARN([Xvid decore libs not found]) &&
- HAVE_XVID=no ] )
- if test x$HAVE_XVID = xyes; then
- XVID_LIBS="-lxvidcore -lm"
- AC_SUBST(XVID_LIBS)
- fi
+ HAVE_XVID=no
+ AC_CHECK_HEADER(xvid.h, [
+ OLD_LIBS="$LIBS"
+ LIBS="-lm"
+ AC_CHECK_LIB(xvidcore, xvid_encore, [
+ AC_CHECK_LIB(xvidcore, xvid_decore, [
+ AC_CHECK_LIB(xvidcore, xvid_global, [
+ AC_MSG_CHECKING([for uptodate XviD API version])
+ AC_TRY_RUN([
+#include <xvid.h>
+#if XVID_API != XVID_MAKE_API(4,0)
+#error "Incompatible XviD API version"
+#endif
+int main () { return 0; }
+ ],[ AC_MSG_RESULT(yes)
+ XVID_LIBS="-lxvidcore -lm"
+ AC_SUBST(XVID_LIBS)
+ HAVE_XVID=yes
+ ], AC_MSG_RESULT(no) )
+ ], )
+ ], )
+ ], )
+ LIBS="$OLD_LIBS"
+ ], )
])
GST_CFLAGS="$GST_CFLAGS -g"
fi
-if test "x$USE_PROFILING" = xyes; then
-dnl CFLAGS="$CFLAGS -pg -fprofile-arcs"
- FOMIT_FRAME_POINTER=""
-else
- FOMIT_FRAME_POINTER="-fomit-frame-pointer"
-fi
-
-dnl
-dnl AC_SUBST(FOMIT_FRAME_POINTER)
-dnl
-
dnl #############################
dnl # Set automake conditionals #
dnl #############################
dnl These should be "USE_*" instead of "HAVE_*", but some packages expect
dnl HAVE_ and it is likely to be easier to stick with the old name
-AM_CONDITIONAL(HAVE_CPU_I386, test "x$HAVE_CPU_I386" = "xyes")
-AM_CONDITIONAL(HAVE_CPU_PPC, test "x$HAVE_CPU_PPC" = "xyes")
-AM_CONDITIONAL(HAVE_CPU_ALPHA, test "x$HAVE_CPU_ALPHA" = "xyes")
-AM_CONDITIONAL(HAVE_CPU_ARM, test "x$HAVE_CPU_ARM" = "xyes")
-AM_CONDITIONAL(HAVE_CPU_SPARC, test "x$HAVE_CPU_SPARC" = "xyes")
AM_CONDITIONAL(HAVE_LIBMMX, test "x$USE_LIBMMX" = "xyes")
AM_CONDITIONAL(HAVE_ATOMIC_H, test "x$USE_ATOMIC_H" = "xyes")
dnl prefer internal headers to already installed ones
GST_CFLAGS="-I\$(top_srcdir)/gst-libs $GST_CFLAGS $GST_ERROR"
-GST_OPT_CFLAGS="$GST_FINLINE_CFLAGS $GST_FFASTMATH_CFLAGS"
AC_SUBST(GST_LIBS)
AC_SUBST(GST_CFLAGS)
-AC_SUBST(GST_FUNROLL_CFLAGS)
-AC_SUBST(GST_FINLINE_CFLAGS)
-AC_SUBST(GST_FFASTMATH_CFLAGS)
-AC_SUBST(GST_FSCHEDULE_CFLAGS)
-AC_SUBST(GST_FNOEXCEPTIONS_CFLAGS)
-AC_SUBST(GST_OPT_CFLAGS)
dnl ###########################
dnl # Configure external libs #
dnl ###########################
-if test "x$HAVE_FFMPEG" = xyes; then
- AC_CONFIG_SUBDIRS(gst-libs/ext/ffmpeg/ffmpeg)
-fi
+
+dnl ############################
+dnl # Set up some more defines #
+dnl ############################
+
+dnl set license and copyright notice
+AC_DEFINE(GST_LICENSE, "LGPL", [GStreamer license])
+dnl package name in plugins
+AC_ARG_WITH(package-name,
+AC_HELP_STRING([--with-package-name],[specify package name to use in plugins]),
+[case "${withval}" in
+ yes) AC_MSG_ERROR(bad value ${withval} for --with-package-name) ;;
+ no) AC_MSG_ERROR(bad value ${withval} for --with-package-name) ;;
+ *) GST_PACKAGE="${withval}" ;;
+esac],
+[GST_PACKAGE="GStreamer"]) dnl Default value
+AC_MSG_NOTICE(Using $GST_PACKAGE as package name)
+AC_DEFINE_UNQUOTED(GST_PACKAGE, "$GST_PACKAGE", [package name in plugins])
+dnl package origin URL
+AC_ARG_WITH(package-origin,
+AC_HELP_STRING([--with-package-origin],[specify package origin URL to use in plugins]),
+[case "${withval}" in
+ yes) AC_MSG_ERROR(bad value ${withval} for --with-package-origin) ;;
+ no) AC_MSG_ERROR(bad value ${withval} for --with-package-origin) ;;
+ *) GST_ORIGIN="${withval}" ;;
+esac],
+[GST_ORIGIN="http://gstreamer.net"]) dnl Default value
+AC_MSG_NOTICE(Using $GST_ORIGIN as package origin)
+AC_DEFINE_UNQUOTED(GST_ORIGIN, "$GST_ORIGIN", [package origin])
dnl #########################
dnl # Make the output files #
pkgconfig/gstreamer-libs-uninstalled.pc
pkgconfig/gstreamer-play.pc
pkgconfig/gstreamer-play-uninstalled.pc
+pkgconfig/gstreamer-interfaces.pc
+pkgconfig/gstreamer-interfaces-uninstalled.pc
gst-libs/gst/gconf/gstreamer-gconf.pc
gst-libs/gst/gconf/gstreamer-gconf-uninstalled.pc
gst-plugins.spec
gst/asfdemux/Makefile
gst/cdxaparse/Makefile
gst/chart/Makefile
+gst/colorspace/Makefile
gst/cutter/Makefile
gst/debug/Makefile
gst/deinterlace/Makefile
gst/filter/Makefile
gst/flx/Makefile
gst/goom/Makefile
-gst/intfloat/Makefile
+gst/id3/Makefile
+gst/interleave/Makefile
gst/law/Makefile
gst/level/Makefile
+gst/matroska/Makefile
gst/median/Makefile
gst/mixmatrix/Makefile
-gst/mpeg1enc/Makefile
gst/mpeg1sys/Makefile
gst/mpeg1videoparse/Makefile
-gst/mpeg2enc/Makefile
gst/mpeg2sub/Makefile
gst/mpegaudio/Makefile
gst/mpegaudioparse/Makefile
gst/mpegstream/Makefile
-gst/mpegtypes/Makefile
gst/modplug/Makefile
gst/modplug/libmodplug/Makefile
gst/monoscope/Makefile
-gst/oneton/Makefile
gst/overlay/Makefile
gst/passthrough/Makefile
gst/playondemand/Makefile
gst/spectrum/Makefile
gst/speed/Makefile
gst/stereo/Makefile
+gst/switch/Makefile
gst/synaesthesia/Makefile
+gst/tags/Makefile
gst/tcp/Makefile
+gst/typefind/Makefile
gst/udp/Makefile
gst/vbidec/Makefile
gst/videocrop/Makefile
+gst/videodrop/Makefile
gst/videofilter/Makefile
gst/videoflip/Makefile
gst/videoscale/Makefile
sys/Makefile
sys/cdrom/Makefile
sys/dxr3/Makefile
+sys/glsink/Makefile
sys/oss/Makefile
sys/qcam/Makefile
sys/v4l/Makefile
sys/v4l2/Makefile
sys/vcd/Makefile
+sys/ximage/Makefile
+sys/xvimage/Makefile
sys/xvideo/Makefile
ext/Makefile
ext/a52dec/Makefile
ext/dvdread/Makefile
ext/dvdnav/Makefile
ext/esd/Makefile
-ext/ffmpeg/Makefile
+ext/faac/Makefile
+ext/faad/Makefile
ext/flac/Makefile
ext/gdk_pixbuf/Makefile
ext/gnomevfs/Makefile
ext/lame/Makefile
ext/ivorbis/Makefile
ext/lcs/Makefile
+ext/libcaca/Makefile
ext/libfame/Makefile
ext/libpng/Makefile
+ext/librfb/Makefile
ext/mad/Makefile
-ext/mas/Makefile
-ext/matroska/Makefile
ext/mikmod/Makefile
ext/mpeg2dec/Makefile
+ext/mpeg2enc/Makefile
ext/mplex/Makefile
+ext/musicbrainz/Makefile
+ext/nas/Makefile
+ext/ogg/Makefile
ext/pango/Makefile
ext/raw1394/Makefile
ext/sdl/Makefile
ext/speex/Makefile
ext/sndfile/Makefile
ext/swfdec/Makefile
-ext/vorbis/Makefile
ext/tarkin/Makefile
+ext/theora/Makefile
+ext/vorbis/Makefile
+ext/xine/Makefile
ext/xvid/Makefile
gst-libs/Makefile
gst-libs/gst/Makefile
gst-libs/gst/audio/Makefile
+gst-libs/gst/colorbalance/Makefile
gst-libs/gst/floatcast/Makefile
gst-libs/gst/gconf/Makefile
gst-libs/gst/idct/Makefile
gst-libs/gst/media-info/Makefile
+gst-libs/gst/mixer/Makefile
+gst-libs/gst/navigation/Makefile
gst-libs/gst/play/Makefile
+gst-libs/gst/propertyprobe/Makefile
gst-libs/gst/resample/Makefile
gst-libs/gst/riff/Makefile
+gst-libs/gst/tag/Makefile
+gst-libs/gst/tuner/Makefile
gst-libs/gst/video/Makefile
+gst-libs/gst/xoverlay/Makefile
+gst-libs/gst/xwindowlistener/Makefile
gst-libs/ext/Makefile
-gst-libs/ext/ffmpeg/Makefile
-gst-libs/ext/mplex/Makefile
examples/dynparams/Makefile
examples/capsfilter/Makefile
examples/seeking/Makefile
examples/indexing/Makefile
+examples/gstplay/Makefile
+examples/switch/Makefile
examples/Makefile
-testsuite/autoplug/Makefile
testsuite/spider/Makefile
testsuite/alsa/Makefile
testsuite/Makefile
tools/Makefile
+tools/gst-launch-ext
gconf/Makefile
+gconf/gstreamer.schemas
pkgconfig/Makefile
+po/Makefile.in
)
AC_OUTPUT
-echo -e "configure: *** Plug-ins that will be built : $GST_PLUGINS_YES"
+echo -n "configure: *** Plug-ins that will be built :"
+echo -e "$GST_PLUGINS_YES" | sort
echo
-echo -e "configure: *** Plug-ins that will not be built : $GST_PLUGINS_NO"
+echo -n "configure: *** Plug-ins that will not be built :"
+echo -e "$GST_PLUGINS_NO" | sort
echo
if test "x$BUILD_EXTERNAL" = "xno"; then
echo "configure: *** No external plug-ins will be built"