diff --git a/ext/amrnb/amrnbenc.c b/ext/amrnb/amrnbenc.c
index 40632557f1a0aa3dde295381a3e2879d150f6cb4..3145f79f4c19524ee3b67a00104e89191d062eb6 100644 (file)
--- a/ext/amrnb/amrnbenc.c
+++ b/ext/amrnb/amrnbenc.c
static GstFlowReturn gst_amrnbenc_chain (GstPad * pad, GstBuffer * buffer);
static gboolean gst_amrnbenc_setcaps (GstPad * pad, GstCaps * caps);
-static GstElementStateReturn gst_amrnbenc_state_change (GstElement * element);
+static GstStateChangeReturn gst_amrnbenc_state_change (GstElement * element,
+ GstStateChange transition);
static GstElementClass *parent_class = NULL;
{
GstElementClass *element_class = GST_ELEMENT_CLASS (klass);
GstElementDetails gst_amrnbenc_details = {
- "AMR-NB decoder",
- "Codec/Decoder/Audio",
+ "AMR-NB encoder",
+ "Codec/Encoder/Audio",
"Adaptive Multi-Rate Narrow-Band audio encoder",
"Ronald Bultje <rbultje@ronald.bitfreak.net>, "
"Wim Taymans <wim@fluendo.com>"
GObjectClass *object_class = G_OBJECT_CLASS (klass);
GstElementClass *element_class = GST_ELEMENT_CLASS (klass);
- parent_class = g_type_class_ref (GST_TYPE_ELEMENT);
+ parent_class = g_type_class_peek_parent (klass);
object_class->finalize = gst_amrnbenc_finalize;
gst_amrnbenc_init (GstAmrnbEnc * amrnbenc)
{
/* create the sink pad */
- amrnbenc->sinkpad =
- gst_pad_new_from_template (gst_static_pad_template_get (&sink_template),
- "sink");
+ amrnbenc->sinkpad = gst_pad_new_from_static_template (&sink_template, "sink");
gst_pad_set_setcaps_function (amrnbenc->sinkpad, gst_amrnbenc_setcaps);
gst_pad_set_chain_function (amrnbenc->sinkpad, gst_amrnbenc_chain);
gst_element_add_pad (GST_ELEMENT (amrnbenc), amrnbenc->sinkpad);
/* create the src pad */
- amrnbenc->srcpad =
- gst_pad_new_from_template (gst_static_pad_template_get (&src_template),
- "src");
+ amrnbenc->srcpad = gst_pad_new_from_static_template (&src_template, "src");
gst_pad_use_fixed_caps (amrnbenc->srcpad);
gst_element_add_pad (GST_ELEMENT (amrnbenc), amrnbenc->srcpad);
/* init rest */
amrnbenc->handle = NULL;
- amrnbenc->channels = 0;
- amrnbenc->rate = 0;
- amrnbenc->ts = 0;
}
static void
"channels", G_TYPE_INT, amrnbenc->channels,
"rate", G_TYPE_INT, amrnbenc->rate, NULL);
+ /* precalc duration as it's constant now */
+ amrnbenc->duration = gst_util_uint64_scale_int (160, GST_SECOND,
+ amrnbenc->rate * amrnbenc->channels);
+
gst_pad_set_caps (amrnbenc->srcpad, copy);
gst_caps_unref (copy);
amrnbenc = GST_AMRNBENC (GST_PAD_PARENT (pad));
+ g_return_val_if_fail (amrnbenc->handle, GST_FLOW_WRONG_STATE);
+
if (amrnbenc->rate == 0 || amrnbenc->channels == 0)
goto not_negotiated;
+ /* discontinuity clears adapter, FIXME, maybe we can set some
+ * encoder flag to mask the discont. */
+ if (GST_BUFFER_FLAG_IS_SET (buffer, GST_BUFFER_FLAG_DISCONT)) {
+ gst_adapter_clear (amrnbenc->adapter);
+ amrnbenc->ts = 0;
+ }
+
+ /* take latest timestamp, FIXME timestamp is the one of the
+ * first buffer in the adapter. */
if (GST_BUFFER_TIMESTAMP_IS_VALID (buffer))
amrnbenc->ts = GST_BUFFER_TIMESTAMP (buffer);
guint8 *data;
gint outsize;
- /* get output, max size is 32 */
+ /* get output, max size is 32 */
out = gst_buffer_new_and_alloc (32);
- GST_BUFFER_DURATION (out) = GST_SECOND * 160 /
- (amrnbenc->rate * amrnbenc->channels);
+ GST_BUFFER_DURATION (out) = amrnbenc->duration;
GST_BUFFER_TIMESTAMP (out) = amrnbenc->ts;
- amrnbenc->ts += GST_BUFFER_DURATION (out);
- gst_buffer_set_caps (out, gst_pad_get_caps (amrnbenc->srcpad));
+ if (amrnbenc->ts != -1)
+ amrnbenc->ts += amrnbenc->duration;
+ gst_buffer_set_caps (out, GST_PAD_CAPS (amrnbenc->srcpad));
- data = (guint8 *) gst_adapter_peek (amrnbenc->adapter, 320);
+ /* The AMR encoder actually writes into the source data buffers it gets */
+ data = gst_adapter_take (amrnbenc->adapter, 320);
- /* decode */
+ /* encode */
outsize = Encoder_Interface_Encode (amrnbenc->handle, MR122, (short *) data,
(guint8 *) GST_BUFFER_DATA (out), 0);
- gst_adapter_flush (amrnbenc->adapter, 320);
+ g_free (data);
GST_BUFFER_SIZE (out) = outsize;
/* play */
- ret = gst_pad_push (amrnbenc->srcpad, out);
+ if ((ret = gst_pad_push (amrnbenc->srcpad, out)) != GST_FLOW_OK)
+ break;
}
-
return ret;
+ /* ERRORS */
not_negotiated:
{
+ GST_ELEMENT_ERROR (amrnbenc, STREAM, TYPE_NOT_FOUND,
+ (NULL), ("unknown type"));
return GST_FLOW_NOT_NEGOTIATED;
}
}
-static GstElementStateReturn
-gst_amrnbenc_state_change (GstElement * element)
+static GstStateChangeReturn
+gst_amrnbenc_state_change (GstElement * element, GstStateChange transition)
{
GstAmrnbEnc *amrnbenc;
- GstElementStateReturn ret;
- gint transition;
+ GstStateChangeReturn ret;
amrnbenc = GST_AMRNBENC (element);
- transition = GST_STATE_TRANSITION (element);
switch (transition) {
- case GST_STATE_NULL_TO_READY:
+ case GST_STATE_CHANGE_NULL_TO_READY:
if (!(amrnbenc->handle = Encoder_Interface_init (0)))
- return GST_STATE_FAILURE;
+ return GST_STATE_CHANGE_FAILURE;
break;
- case GST_STATE_READY_TO_PAUSED:
+ case GST_STATE_CHANGE_READY_TO_PAUSED:
+ amrnbenc->rate = 0;
+ amrnbenc->channels = 0;
amrnbenc->ts = 0;
gst_adapter_clear (amrnbenc->adapter);
break;
break;
}
- ret = GST_ELEMENT_CLASS (parent_class)->change_state (element);
+ ret = GST_ELEMENT_CLASS (parent_class)->change_state (element, transition);
switch (transition) {
- case GST_STATE_READY_TO_NULL:
+ case GST_STATE_CHANGE_READY_TO_NULL:
Encoder_Interface_exit (amrnbenc->handle);
break;
default: